Common Name: HEAT CONDUCTIVE COMPOUND
Manufacturer: HONEYWELL
MSDS Revision Date: 4/15/2004
   
Grainger Item Number(s): 1RZY3, 5TB81
Manufacturer Model Number(s): L4008A1015



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1. PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2. COMPOSITION, INFORMATION ON INGREDIENTS 
SECTION 3. HAZARD IDENTIFICATION 
SECTION 4. FIRST AID MEASURES 
SECTION 5. FIRE FIGHTING MEASURES 
SECTION 6. ACCIDENTAL RELEASE MEASURES 
SECTION 7. HANDLING AND STORAGE 
SECTION 8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 
SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10. STABILITY AND REACTIVITY 
SECTION 11. TOXICOLOGY INFORMATION 
SECTION 12. ECOLOGICAL INFORMATION 
SECTION 13. DISPOSAL CONSIDERATION 
SECTION 14. TRANSPORTATION INFORMATION 
SECTION 15. REGULATORY INFORMATION 
SECTION 16. OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET


SECTION 1. PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT NAME: HEAT CONDUCTIVE COMPOUND

MSDS ID: DS9021

SYNONYMS: MS1699

PRODUCT USE:
HEAT CONDUCTIVE MATERIAL USED TO ENHANCE CONTACT AND HEAT TRANSFER IN
TEMPERATURE SENSOR APPLICATIONS.

MANUFACTURER:
HONEYWELL INTERNATIONAL INC.
1985 DOUGLAS DRIVE NORTH
MINNEAPOLIS, MN 55422

CUSTOMER RESPONSE CENTER: 800-328-5111

EMERGENCY TELEPHONE INFORMATION: 800-707-4555 OR 602-365-3099

DATE REVISION: APRIL 15, 2004

NFPA RATINGS:
HEALTH       0
FLAMMABILITY 1
REACTIVITY   0


SECTION 2. COMPOSITION, INFORMATION ON INGREDIENTS 


INGREDIENTS                  CAS#        PERCENT   PEL           TLV

#2 LITHIUM COMPLEX GREASE (70%):

MINERAL OIL                  64742-65-0  35-56     5 MG/M3       0.2 MG/M3

MINERAL OIL                  64742-62-7  14-28     5 MG/M3       0.2 MG/M3

LITHIUM HYDROSTEARATE/       68815-49-6   2-11     NOT           NOT
SEBACATE COMPLEX                                   ESTABLISHED   ESTABLISHED

ZINC ALKYLDITHIOPHOSPHATE    68649-42-3   0-2      NOT           NOT
                                                   ESTABLISHED   ESTABLISHED

ALUMINUM PASTE (30%):

ALUMINUM, AS Al               7429-90-5  15-21     15 MG/M3      10 MG/M3

ALIPHATIC PETROLEUM           8052-41-3   1-8      400 PPM       100 PPM
DISTILLATES

STEARIC ACID                    57-11-4   1-2

AROMATIC PETROLEUM           64742-95-6   1-3      NOT           NOT
DISTILLATES                                        ESTABLISHED   ESTABLISHED

NIOSH RECOMMENDED EXPOSURE LIMIT: 350 MG/M3

ADDITIONAL INFORMATION:
PART NO. 120650 (0.5 OZ TUBE); PART NO. 107408 (4 OZ CAN); PART NO. 197007
(5 GAL CONTAINER). MAY ALSO CONTAIN MINUTE AMOUNTS OF LITHIUM AND MOLYBDENUM
LUBRICANT COMPOUNDS.


SECTION 3. HAZARD IDENTIFICATION 


ACUTE HEALTH HAZARD:
SKIN: EXCESSIVE CONTACT MAY CAUSE SKIN IRRITATION AND DERMATITIS.
EYE: DIRECT CONTACT WITH EYE WILL CAUSE IRRITATION.
INHALATION: UNDER INTENDED USE, INHALATION IS UNLIKELY.
INGESTION: INGESTION OF PRODUCT MAY CAUSE NAUSEA, VOMITING AND DIARRHEA.

CHRONIC HEALTH HAZARD:
EXISTING SKIN RASH OR DERMATITIS MAY BE AGGRAVATED BY REPEATED CONTACT.

OSHA HAZARD CLASSIFICATIONS: NONE

CARCINOGENICITY:
SOME JURISDICTIONS CONSIDER MINERAL OIL TO BE A HUMAN CARCINOGEN. EVIDENCE
FOR CARCINOGENICITY IS BASED ON INHALED OIL MIST, AN UNLIKELY EXPOSURE ROUTE
FOR THIS PRODUCT.

TARGET ORGANS: SKIN


SECTION 4. FIRST AID MEASURES 


EYE CONTACT:
FLUSH EYES WITH WATER FOR 15 MINUTES. REMOVE ANY CONTACT LENSES AND CONTINUE
TO FLUSH. OBTAIN MEDICAL ATTENTION IF IRRITATION DEVELOPS AND PERSISTS.

SKIN CONTACT:
REMOVE EXCESS WITH CLOTH OR PAPER. WASH THOROUGHLY WITH MILD SOAP AND WATER.
OBTAIN MEDICAL ATTENTION IF IRRITATION DEVELOPS AND PERSISTS.

INGESTION: CONTACT PHYSICIAN OR LOCAL POISON CONTROL CENTER IMMEDIATELY.

INHALATION:
REMOVE PATIENT TO FRESH AIR AND OBTAIN MEDICAL ATTENTION IF SYMPTOMS
DEVELOP.


SECTION 5. FIRE FIGHTING MEASURES 


FLASH POINT: >383 F (COC) WILL BURN IF EXPOSED TO FLAME.

EXTINGUISHING MEDIA: CARBON DIOXIDE, DRY CHEMICAL OR FOAM.

SPECIAL FIRE FIGHTING PROCEDURES: NONE

EXPLOSION HAZARDS: NONE.


SECTION 6. ACCIDENTAL RELEASE MEASURES 


SCRAPE UP AND DISPOSE AS SOLID WASTE IN ACCORDANCE WITH GOVERNMENT
REGULATIONS.


SECTION 7. HANDLING AND STORAGE 


STORE IN COOL, DRY PLACE. KEEP CONTAINER CLOSED WHEN NOT IN USE.


SECTION 8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 


VENTILATION:
NO SPECIAL VENTILATION IS REQUIRED WHEN WORKING WITH THIS PRODUCT.

RESPIRATORY PROTECTION: NONE

EYE PROTECTION:
NOT NORMALLY REQUIRED. HOWEVER, USE CHEMICAL SAFETY GOGGLES OR FACESHIELD IF
POTENTIAL FOR EYE CONTACT EXISTS, ESPECIALLY IF MATERIAL IS HEATED.

HAND/CLOTHING PROTECTION:
NOT NORMALLY REQUIRED. PROTECTIVE GLOVES AND CLOTHING ARE RECOMMENDED, AS
MATERIAL IS DIFFICULT TO REMOVE FROM SKIN AND CLOTHING.

OTHER PROTECTIVE EQUIPMENT: NONE


SECTION 9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE/ODOR:
ALUMINUM COLOR, SEMI-SOLID MATERIAL, MILD SOLVENT/GREASE ODOR

SOLUBLE IN WATER: NEGLIGIBLE

SPECIFIC GRAVITY: 1.03


SECTION 10. STABILITY AND REACTIVITY 


STABILITY: STABLE

REACTIVITY: HAZARDOUS POLYMERIZATION WILL NOT OCCUR

INCOMPATIBILITIES: STRONG OXIDIZING AGENTS AND HALOGENS

HAZARDOUS DECOMPOSITION PRODUCTS:
CARBON DIOXIDE, CARBON MONOXIDE, ALUMINUM OXIDE FUME


SECTION 11. TOXICOLOGY INFORMATION 


AROMATIC PETROLEUM DISTILLATE HAS AN ORAL DOSE LD50 (RAT) OF 840 MG/KG
STEARIC ACID HAS AN ORAL DOSE LD50 (RAT) OF 4640 MG/KG
ALIPHATIC PETROLEUM DISTILLATE INHALATION LC50 (RAT) IS 8200 MG/M3/8H


SECTION 12. ECOLOGICAL INFORMATION 


CHEMICAL FATE INFORMATION:
HYDROCARBON COMPONENTS WILL BIODEGRADE IN SOIL; RELATIVELY PERSISTENT IN
WATER.


SECTION 13. DISPOSAL CONSIDERATION 


DISPOSE OF AS SOLID WASTE IN ACCORDANCE WITH LOCAL, STATE OR PROVINCIAL, AND
FEDERAL REGULATIONS.


SECTION 14. TRANSPORTATION INFORMATION 


DOT CLASSIFICATION: NOT CLASSIFIED AS HAZARDOUS


SECTION 15. REGULATORY INFORMATION 


SECTION 313 SUPPLIER NOTIFICATION (UNITED STATES):

THIS PRODUCT CONTAINS THE FOLLOWING EPCRA SECTION 313 CHEMICALS SUBJECT TO
THE REPORTING REQUIREMENTS OF SECTION 313 OF THE EMERGENCY PLANNING AND
COMMUNITY RIGHT-TO-KNOW ACT OF 1986 (40 CFR 372):

CAS NUMBER           CHEMICAL NAME            PERCENT BY WEIGHT

7429-90-5            ALUMINUM                 UP TO 21%

68649-42-3           ZINC COMPOUNDS           UP TO 2%

INGREDIENTS ARE LISTED IN THE U.S. TSCA INVENTORY.

CANADA:
THIS PRODUCT HAS BEEN CLASSIFIED IN ACCORDANCE WITH THE HAZARD CRITERION OF
THE CPR AND THE MSDS CONTAINS ALL THE INFORMATION REQUIRED BY THE CPR.


SECTION 16. OTHER INFORMATION 


THIS INFORMATION IS FURNISHED WITHOUT WARRANTY, EXPRESSED OR IMPLIED, EXCEPT
THAT IT IS ACCURATE TO THE BEST OF OUR KNOWLEDGE.

PREPARED BY:
VICKI CHOUINARD, CIH, CSP, HONEYWELL INTERNATIONAL INC.
612-951-7168