Common Name: DURACELL LITHIUM MANGANESE DIOXIDE BATTERIES, DL1/3N (3V); PX28L (6V) AND BATTER
Manufacturer: GILLETTE
SDS Revision Date: 4/4/2005
SDS Format: No Format Specified
   
Item Number(s): 1ANB8, 2HYK8, 9NVL7
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
A. - IDENTIFICATION 
B. - PHYSICAL DATA 
C. - REACTIVITY 
D. - HEALTH HAZARD DATA 
E. - ENVIRONMENTAL IMPACT 
F. - EXPOSURE CONTROL METHODS 
G. - WORK PRACTICES 
H. - EMERGENCY PROCEDURES 
I. - FIRST AID AND MEDICAL EMERGENCY PROCEDURES 



G
GILLETTE ENVIRONMENT HEALTH AND SAFETY
37 A STREET
NEEDHAM, MA 02492

TEL: 781.292.8151

MATERIAL SAFETY DATA SHEET

NAME: DURACELL LITHIUM MANGANESE DIOXIDE BATTERIES

CAS NO: NOT APPLICABLE

EFFECTIVE DATE: 4/4/05

REV: 5


A. - IDENTIFICATION 


IDENTIFICATION                                                    %

MANGANESE DIOXIDE (1313-13-9)                                   15-30

1,2-DIMETHOXYETHANE (110-71-4)                                   5-10

PROPYLENE CARBONATE (108-32-7)                                   1-5

LITHIUM (7439-93-2)                                              1-5

ETHYLENE CARBONATE (96-49-1)                                     1-5

LITHIUM TRIFLUOROMETHANE SULFONATE (33454-82-9)                  0-5

CARBON BLACK (1333-86-4)                                         0-5

GRAPHITE (7782-42-5)                                             0-5

FORMULA: MIXTURE

MOLECULAR WEIGHT: NA

SYNONYMS:
LITHIUM MANGANESE DIOXIDE CELLS:
DL1/3N (3V); PX28L (6V) AND BATTERIES COMPRISED OF D1/3N CELLS.


B. - PHYSICAL DATA 


BOILING POINT:
NA DEG. F
NA DEG. C

MELTING POINT:
NA DEG. F
NA DEG. C

FREEZING POINT:
NA DEG. F
NA DEG. C

SPECIFIC GRAVITY (H2O=1): NA

VAPOR DENSITY (AIR=1): NA

VAPOR PRESSURE @ DEG. F: NA MMHg

EVAPORATION (ETHER = 1): NA

SATURATION IN AIR (BY VOLUME @ DEG. F): NA

AUTOIGNITION TEMPERATURE DEG. F DEG. C: NA

% VOLATILES: NA

SOLUBILITY IN WATER: NA

pH: NA

APPEARANCE/COLOR: SMALL CYLINDRICAL BATTERIES. CONTENTS DARK IN COLOR.

FLASH POINT AND TEST METHOD(S):
1,2-DIMETHOXYETHANE: 42.8 DEG. F, 6 DEG. C (CLOSED CUP)

FLAMMABLE LIMITS IN AIR (% BY VOLUME):
LOWER: NA %
UPPER: NA %


C. - REACTIVITY 


STABILITY:
(X) STABLE
( ) UNSTABLE

CONDITIONS TO AVOID:
DO NOT HEAT, CRUSH, DISASSEMBLE, SHORT CIRCUIT OR RECHARGE.

POLYMERIZATION:
( ) MAY OCCUR
(X) WILL NOT OCCUR

CONDITIONS TO AVOID: NOT APPLICABLE

INCOMPATIBLE MATERIALS: CONTENTS INCOMPATIBLE WITH STRONG OXIDIZING AGENTS.

HAZARDOUS DECOMPOSITION PRODUCTS:
THERMAL DEGRADATION MAY PRODUCE HAZARDOUS FUMES OF MANGANESE AND LITHIUM;
HYDROFLUORIC ACID; OXIDES OF CARBON AND SULFUR AND OTHER TOXIC BY-PRODUCTS.


D. - HEALTH HAZARD DATA 


OCCUPATIONAL EXPOSURE LIMITS PEL'S, TLV'S ETC.:

8-HOUR TWAS:
MANGANESE DIOXIDE (AS Mn):
5 MG/M3 (CEILING) (OSHA)
0.2 MG/M3 (ACGIH/GILLETTE)

1,2-DIMETHOXYETHANE: 0.15 PPM (GILLETTE)

CARBON BLACK:
3.5 MG/M3 (OSHA/ACGIH/U.K)
7 MG/M3 (STEL) (U.K.)

LITHIUM TRIFLUOROMETHANE SULFONATE: 0.1 MG/M3 (3M RECOMMENDATION)

GRAPHITE:
15 MG/M3 (DUST)
5 MG/M3 (RESPIRABLE) (OSHA)
2 MG/M3 (ACGIH)

THESE LEVELS ARE NOT ANTICIPATED UNDER NORMAL CONSUMER USE CONDITIONS.

WARNING SIGNALS: NOT APPLICABLE

ROUTES/EFFECTS OF EXPOSURE:
THESE CHEMICALS AND METALS ARE CONTAINED IN A SEALED CAN. FOR CONSUMER USE,
ADEQUATE HAZARD WARNINGS ARE INCLUDED ON BOTH THE PACKAGE AND ON THE
BATTERY. POTENTIAL FOR EXPOSURE SHOULD NOT EXIST UNLESS THE BATTERY LEAKS,
IS EXPOSED TO HIGH TEMPERATURE, IS ACCIDENTALLY SWALLOWED OR IS
MECHANICALLY, PHYSICALLY, OR ELECTRICALLY ABUSED.

1. INHALATION:
NOT ANTICIPATED. RESPIRATORY (AND EYE) IRRITATION MAY OCCUR IF FUMES ARE
RELEASED DUE TO HEAT OR AN ABUNDANCE OF LEAKING BATTERIES.

2. INGESTION:
AN INITIAL X-RAY SHOULD BE OBTAINED PROMPTLY TO DETERMINE BATTERY
LOCATION. BATTERIES LODGED IN THE ESOPHAGUS SHOULD BE REMOVED IMMEDIATELY
SINCE LEAKAGE, BURNS AND PERFORATION CAN OCCUR AS SOON AS 4-6 HOURS AFTER
INGESTION. IRRITATION TO THE INTERNAL/EXTERNAL MOUTH AREAS MAY OCCUR
FOLLOWING EXPOSURE TO A LEAKING BATTERY.

3. SKIN:
A. CONTACT: IRRITATION MAY OCCUR FOLLOWING EXPOSURE TO A LEAKING BATTERY.
B. ABSORPTION: NOT ANTICIPATED.

4. EYE CONTACT:
IRRITATION MAY OCCUR FOLLOWING EXPOSURE TO A LEAKING BATTERY.

5. OTHER: NOT APPLICABLE


E. - ENVIRONMENTAL IMPACT 


1. APPLICABLE REGULATIONS: ALL INGREDIENTS LISTED IN TSCA INVENTORY.

2. DOT HAZARD CLASS: NOT APPLICABLE

3. DOT SHIPPING NAME: NOT APPLICABLE

"DURACELL CERTIFIES THAT ALL OF ITS LITHIUM BATTERIES MEET THE REQUIREMENTS
OF THE UN MANUAL OF TESTS AND CRITERIA, PART III SUBSECTION 38.3. IF YOU
ASSEMBLE THESE BATTERIES INTO LARGER BATTERY PACKS, IT IS RECOMMENDED THAT
YOU PERFORM THE UN TESTS TO ENSURE THE REQUIREMENTS ARE MET PRIOR TO
SHIPMENT. CELLS AND BATTERIES ARE TO BE SEPARATED SO AS TO PREVENT SHORT
CIRCUITS AND PACKED IN STRONG PACKAGING, EXCEPT WHEN INSTALLED IN
EQUIPMENT. EXCEPT WHEN INSTALLED IN EQUIPMENT, EACH PACKAGE CONTAINING MORE
THAN 24 CELLS OR 12 BATTERIES MUST BE MARKED INDICATING THAT IT CONTAINS
LITHIUM BATTERIES AND THAT SPECIAL PROCEDURES SHOULD BE FOLLOWED IN THE
EVENT THAT THE PACKAGING IS DAMAGED. IN ADDITION, EACH SHIPMENT MUST BE
ACCOMPANIED BY APPROPRIATE DOCUMENTATION AND THE PACKAGE OF A TYPE CAPABLE
OF MEETING THE DROP TEST REQUIREMENTS. EXCEPT FOR PERSONAL USE, THE
SHIPMENT OF LITHIUM BATTERIES ABOARD PASSENGER AIRCRAFT IS NO LONGER
ALLOWED. THE FOLLOWING NEW MARKING REQUIREMENT APPLIES TO ALL LITHIUM
BATTERY SHIPMENTS THAT ARE EXEMPTED FROM CLASS 9 ACCORDING TO CFR 49:
PRIMARY LITHIUM BATTERIES - FORBIDDEN FROM TRANSPORT ABOARD PASSENGER
AIRCRAFT". THIS WORDING SHOULD APPEAR ON ALL PACKAGES OFFERED FOR
SHIPMENT."

ENVIRONMENTAL EFFECTS:
THESE BATTERIES PASS THE U. S. EPA'S TOXICITY CHARACTERISTIC LEACHING.
PROCEDURE AND THEREFORE, MAY BE DISPOSED OF WITH NORMAL WASTE.


F. - EXPOSURE CONTROL METHODS 


ENGINEERING CONTROLS: GENERAL VENTILATION UNDER NORMAL USE CONDITIONS.

EYE PROTECTION:
NONE UNDER NORMAL USE CONDITIONS. WEAR SAFETY GLASSES WHEN HANDLING LEAKING
BATTERIES.

SKIN PROTECTION:
NONE UNDER NORMAL USE CONDITIONS. USE BUTYL GLOVES WHEN HANDLING LEAKING
BATTERIES.

RESPIRATORY PROTECTION: NONE UNDER NORMAL USE CONDITIONS.

OTHER: KEEP BATTERIES AWAY FROM SMALL CHILDREN.


G. - WORK PRACTICES 


HANDLING AND STORAGE:
STORE AT ROOM TEMPERATURE. AVOID MECHANICAL OR ELECTRICAL ABUSE. DO NOT
SHORT OR INSTALL INCORRECTLY. BATTERIES MAY EXPLODE, PYROLIZE OR VENT IF
DISASSEMBLED, CRUSHED, RECHARGED OR EXPOSED TO HIGH TEMPERATURES. INSTALL
BATTERIES IN ACCORDANCE WITH EQUIPMENT INSTRUCTIONS. REPLACE ALL BATTERIES
IN EQUIPMENT AT THE SAME TIME. DO NOT CARRY BATTERIES LOOSE IN POCKET OR
BAG.

NORMAL CLEAN UP: NOT APPLICABLE

WASTE DISPOSAL METHODS:
NO SPECIAL PRECAUTIONS ARE REQUIRED FOR SMALL QUANTITIES. LARGE QUANTITIES
OF OPEN BATTERIES SHOULD BE TREATED AS HAZARDOUS WASTE. DISPOSE OF IN
ACCORDANCE WITH FEDERAL, STATE AND LOCAL REGULATIONS. DO NOT INCINERATE,
SINCE BATTERIES MAY EXPLODE AT EXCESSIVE TEMPERATURES.


H. - EMERGENCY PROCEDURES 


STEPS TO BE TAKEN IF MATERIAL IS RELEASED TO THE ENVIRONMENT OR SPILLED
IN THE WORK AREA:
NOTIFY SAFETY PERSONNEL OF LARGE SPILLS. EVACUATE THE AREA AND ALLOW VAPORS
TO DISSIPATE. INCREASE VENTILATION. AVOID EYE OR SKIN CONTACT. DO NOT
INHALE VAPORS. CLEAN-UP PERSONNEL SHOULD WEAR APPROPRIATE PROTECTIVE GEAR.
REMOVE SPILLED LIQUID WITH ABSORBENT AND CONTAIN FOR DISPOSAL.

FIRE AND EXPLOSION HAZARD:
BATTERIES MAY BURST AND RELEASE HAZARDOUS DECOMPOSITION PRODUCTS WHEN
EXPOSED TO A FIRE SITUATION. SEE SEC. C.

EXTINGUISHING MEDIA:
AS PER SURROUNDING AREA. DRY CHEMICAL, ALCOHOL FOAM, WATER OR CARBON
DIOXIDE. FOR INCIPIENT FIRES, CARBON DIOXIDE EXTINGUISHERS ARE MORE
EFFECTIVE THAN WATER.

FIREFIGHTING PROCEDURES:
COOL FIRE-EXPOSED BATTERIES AND ADJACENT STRUCTURES WITH WATER SPRAY FROM
A DISTANCE. USE SELF-CONTAINED BREATHING APPARATUS AND FULL PROTECTIVE
GEAR.


I. - FIRST AID AND MEDICAL EMERGENCY PROCEDURES 


EYES:
NOT ANTICIPATED. IF BATTERY IS LEAKING AND MATERIAL CONTACTS EYES, FLUSH
WITH COPIOUS AMOUNTS OF CLEAR, TEPID WATER FOR 30 MINUTES. CONSULT
PHYSICIAN AT ONCE.

SKIN:
NOT ANTICIPATED. IF BATTERY IS LEAKING, IRRIGATE EXPOSED SKIN WITH COPIOUS
AMOUNTS OF CLEAR, TEPID WATER FOR AT LEAST 15 MINUTES. IF IRRITATION,
INJURY OR PAIN PERSISTS, CONSULT A PHYSICIAN.

INHALATION:
NOT ANTICIPATED. IF BATTERY IS LEAKING, CONTENTS MAY BE IRRITATING TO
RESPIRATORY PASSAGES. REMOVE TO FRESH AIR. CONTACT PHYSICIAN IS IRRITATION
PERSISTS.

INGESTION:
CONSULT A PHYSICIAN. PUBLISHED REPORTS RECOMMEND REMOVAL FROM THE
ESOPHAGUS BE DONE ENDOSCOPICALLY (UNDER DIRECT VISUALIZATION). BATTERIES
BEYOND THE ESOPHAGUS NEED NOT BE RETRIEVED UNLESS THERE ARE SIGNS OF INJURY
TO THE GI TRACT OR A LARGE DIAMETER BATTERY FAILS TO PASS THE PYLORUS. IF
SYMPTOMATIC, FOLLOW-UP X-RAYS ARE NECESSARY ONLY TO CONFIRM PASSAGE OF
LARGER BATTERIES. CONFIRMATION BY STOOL INSPECTION IS PREFERABLE UNDER MOST
CIRCUMSTANCES. IF MOUTH AREA IRRITATION/BURNING HAS OCCURRED, RINSE THE
MOUTH AND SURROUNDING AREA WITH CLEAR, TEPID WATER FOR AT LEAST 15 MINUTES.

NOTES TO PHYSICIAN:
1) POTENTIAL LEAKAGE OF DIMETHOXYETHANE, PROPYLENE CARBONATE AND LITHIUM
TRIFLUOROMETHANE SULFONATE.

2) DIMETHYOXYETHANE RAPIDLY EVAPORATES.

3) UNDER CERTAIN MISUSE CONDITIONS AND BY ABUSIVELY OPENING THE BATTERY,
EXPOSED LITHIUM CAN REACT WITH WATER OR MOISTURE IN THE AIR CAUSING
POTENTIAL THERMAL BURNS OR FIRE.

REPLACES #: 2031.4

THE INFORMATION CONTAINED IN THE MATERIAL SAFETY DATA SHEET IS BASED ON
DATA CONSIDERED TO BE ACCURATE, HOWEVER, NO WARRANTY IS EXPRESSED OR
IMPLIED REGARDING THE ACCURACY OF THE DATA OR THE RESULTS TO BE OBTAINED
FROM THE USE THEREOF.

* IF MULTIPLE INGREDIENTS, INCLUDE CAS NUMBERS FOR EACH

NA=NOT AVAILABLE

FOOTNOTES: NOT APPLICABLE

MSDS: 5 (2/00)

GMEL#: 2031.5