Common Name: COLD CATHODE LAMPS (FOR GENERAL LIGHTING APPLICATION) (CONSISTS OF BALLAST/ADAPT
Manufacturer: TECHNICAL CONSUMER PRODUCTS
SDS Revision Date: 1/26/2005
SDS Format: No Format Specified
   
Item Number(s): 1LEH7, 1LEH8, 1LEH9, 1LEJ1, 1LEJ2, 1LEJ3, 1LEJ4, 1LEJ5, 1LEJ6, 1LEJ7, 1LEJ8, 1LEJ9, 1LEK1
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
INFORMATION AND APPLICABILITY 
PRODUCT AND COMPANY IDENTIFICATION 
COMPOSITION/INFORMATION ON INGREDIENTS 
PHYSICAL PROPERTIES 
EXPLOSION HAZARDS 
HEALTH CONCERNS 
PROCEDURES FOR DISPOSAL OF LAMPS 



TCP

COLD CATHODE LAMP SPECIFICATIONS

MATERIAL SAFETY DATA SHEET (MSDS)

COLD CATHODE LAMPS

MSDS: 001

ISSUE DATE: 1-26-05


INFORMATION AND APPLICABILITY 


TECHNICAL CONSUMER PRODUCTS BELIEVES THAT UNDER THE OCCUPATIONAL SAFETY
AND HEALTH ADMINISTRATION (OSHA) HAZARDS COMMUNICATIONS STANDARD, A LAMP
(LIGHT BULB) IS EXEMPTED AS AN "ARTICLE", AND THAT AS SUCH, DOES NOT
REQUIRE AN MSDS.
THE ORIGINAL OSHA STANDARD DEFINED AN ARTICLE AS SOMETHING THAT:

1) IS FORMED TO A SPECIFIC SHAPE AND DESIGN

2) HAS END USE FUNCTIONS DEPENDENT UPON ITS SHAPE AND DESIGN, AND

3) DOES NOT RELEASE OR OTHERWISE RESULT IN AN EXPOSURE TO A HAZARDOUS
CHEMICAL UNDER NORMAL CONDITIONS OF USE. IN FEBRUARY 1994, OSHA AMENDED
THE HAZARD COMMUNICATION STANDARD AND MODIFIED PART 3 OF THE ABOVE TO READ:
3) DOES NOT RELEASE MORE THAN VERY SMALL QUANTITIES OF A HAZARDOUS CHEMICAL
UNDER NORMAL CONDITIONS OF USE. STATE AND LOCAL REGULATIONS ALSO CONTAIN
SIMILAR EXEMPTIONS FOR SUCH ARTICLES. MATERIALS CONTAINED IN THE LAMP ARE
NOT RELEASED DURING NORMAL USE AND OPERATION. THE FOLLOWING INFORMATION IS
PROVIDED AS A COURTESY TO OUR CUSTOMERS.


PRODUCT AND COMPANY IDENTIFICATION 


DESCRIPTION:
TRADE NAME (AS LABELED):
COLD CATHODE LAMPS (FOR GENERAL LIGHTING APPLICATION) (CONSISTS OF
BALLAST/ADAPTER AS A UNIT)

MANUFACTURER:
TECHNICAL CONSUMER PRODUCTS INC.
SHANGHAI, JENSEN LTD.
300 LENA DRIVE
AURORA, OHIO 44202
1-800-324-1496


COMPOSITION/INFORMATION ON INGREDIENTS 


THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE INTACT.

LAMP ASSEMBLY - GLASS AND METAL:
THE GLASS IS MADE FROM SODA LIME SIMILAR TO THAT USED THROUGHOUT THE GLASS
INDUSTRY FOR OTHER COMMON CONSUMER ITEMS. THE METALS FOR THE ADAPTERS AND
FILAMENTS ARE GENERALLY MADE FROM VARIOUS AMOUNTS OF ALUMINUM, TIN, LEAD,
COPPER, ZINC, AND NICKEL. NONE OF THESE MATERIALS WOULD PRESENT A POTENTIAL
HAZARD IN THE EVENT OF BREAKAGE OF THE LAMP, ASIDE FROM THE HAZARD DUE TO
BROKEN GLASS.

MERCURY:
SMALL AMOUNTS OF MERCURY IS USED IN ALL FLUORESCENT LAMPS. GENERALLY AROUND
0.025% BY WEIGHT. THE AMOUNT OF MERCURY PRESENT IN ANY GIVEN LAMP WILL VARY
DEPENDING ON BOTH THE SIZE OF THE LAMP AND ON THE EQUIPMENT THAT WAS USED
IN ITS MANUFACTURE. TCP CONTINUES TO REDUCE THE AMOUNTS OF MERCURY USED IN
FLUORESCENT PRODUCTS.

PHOSPHOR:
(NUISANCE DUST) PHOSPHATE MIX USING MANGANESE, RARE EARTH ELEMENTS SUCH AS
LANTHANUM, AND YTTRIUM AS EITHER AN OXIDE OR AS A PHOSPHATE, ALONG WITH A
BARIUM/ALUMINUM OXIDE ALL ARE TIGHTLY BOUND IN THE PHOSPHOR MATRIX. THESE
PHOSPHORS PRODUCE BETTER LAMP EFFICIENCY AND COLOR RENDITION. THE PHOSPHOR
COMPONENTS MAY VARY SLIGHTLY DEPENDING ON THE COLOR OF THE LAMP. SOME LAMPS
MAY CONTAIN A THIN COATING OF TIN OXIDE INSIDE THE GLASS.


PHYSICAL PROPERTIES 


NOT APPLICABLE TO INTACT LAMP.


EXPLOSION HAZARDS 


WHEN EXPOSED TO HIGH TEMPERATURE, TOXIC FUMES MAY BE RELEASED FROM BROKEN
LAMPS.


HEALTH CONCERNS 


THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE INTACT.
NO ADVERSE EFFECTS ARE EXPECTED FROM OCCASIONAL EXPOSURE TO BROKEN LAMPS.
AS A MATTER OF GOOD PRACTICE, AVOID PROLONGED OR FREQUENT EXPOSURE TO
BROKEN LAMPS UNLESS THERE IS ADEQUATE VENTILATION. THE MAJOR HAZARD FROM
BROKEN LAMPS IS THE POSSIBILITY OF SUSTAINING GLASS CUTS.

MERCURY:
THE MERCURY IN THE AIR AS A RESULT OF BREAKING ONE OR A SMALL NUMBER
OF FLUORESCENT LAMPS SHOULD NOT RESULT IN SIGNIFICANT EXPOSURES TO AN
INDIVIDUAL. HOWEVER, WHEN BREAKING A LARGE NUMBER OF LAMPS FOR DISPOSAL,
APPROPRIATE INDUSTRIAL HYGIENE MONITORING AND CONTROLS SHOULD BE
IMPLEMENTED TO MINIMIZE AIRBORNE LEVELS OR SURFACE CONTAMINATION.
WE RECOMMEND A WELL-VENTILATED AREA, AND LOCAL EXHAUST VENTILATION
OR PERSONAL PROTECTIVE EQUIPMENT.

PHOSPHOR:
THERE HAVE BEEN NO SIGNIFICANT ADVERSE EFFECTS ON HUMANS BY INGESTION,
INHALATION, SKIN CONTACT, OR EYE CONTACT. ANTIMONY, MANGANESE, YTTRIUM AND
TIN COMPOUNDS ARE CHARACTERIZED BY OSHA AS HAZARDOUS CHEMICALS, HOWEVER,
DUE TO THEIR INSOLUBILITY, RELATIVELY LOW TOXICITY AND SMALL AMOUNT PRESENT
IN THE PHOSPHOR AND LAMP, THESE MATERIALS DO NOT PRESENT A SIGNIFICANT
HAZARD IN THE EVENT OF BREAKAGE OF THE LAMP.

GLASS:
GLASS DUST IS CONSIDERED TO BE PHYSIOLOGICALLY INERT AND AS SUCH HAS AN
OSHA EXPOSURE LIMIT OF 15-MG/CUBIC METER FOR TOTAL DUST AND 5-MG/CUBIC
METER FOR RESPIRABLE DUST. PERFORM NORMAL FIRST AID PROCEDURES.
SEEK MEDICAL ATTENTION AS REQUIRED.

INHALATION:
IF DISCOMFORT, IRRITATION OR SYMPTOMS OF PULMONARY INVOLVEMENT SHOULD
DEVELOP, REMOVE FROM EXPOSURE AND SEEK MEDICAL ATTENTION.

INGESTION:
IN THE UNLIKELY EVENT OF INGESTION OF A LARGE QUANTITY OF MATERIAL, SEEK
MEDICAL ATTENTION.

CONTACT EYE/SKIN:
WASH EYES/SKIN, INCLUDING UNDER EYELIDS, IMMEDIATELY WITH COPIOUS AMOUNTS
OF WATER AND SEEK MEDICAL ATTENTION.


PROCEDURES FOR DISPOSAL OF LAMPS 


TAKE USUAL PRECAUTIONS FOR COLLECTION OF BROKEN GLASS. PLACE MATERIALS
IN CLOSED CONTAINERS TO AVOID GENERATING DUST. A TOXICITY CHARACTERISTIC
LEACHING PROCEDURE (TCLP) WAS CONDUCTED ON THESE PRODUCTS SHOWING A RESULT
OF MERCURY CONTENT THAT IS NOT CONSIDERED HAZARDOUS WASTE. FOR FIELD
DISPOSAL THE LEAD IN THE SOLDERING IS CONSIDERED HAZARDOUS WASTE AND
MUST BE DISPOSED OF BY APPLICABLE FEDERAL, STATE AND LOCAL REGULATIONS.

ALTHOUGH TECHNICAL CONSUMER PRODUCTS, INC. ATTEMPTS TO PROVIDE CURRENT
AND ACCURATE INFORMATION HEREIN, IT MAKES NO REPRESENTATION REGARDING THE
ACCURACY OF COMPLETENESS OF THE INFORMATION AND ASSUMES NO LIABILITY FOR
ANY LOSS, DAMAGE OR INJURY OF ANY KIND WHICH MAY RESULT FROM OR ARISE OUT
OF THE USE OF/OR RELIANCE ON THE INFORMATION BY ANY PERSON.

TECHNICAL CONSUMER PRODUCTS, INC
300 LENA DRIVE
AURORA, OHIO 44202

P: 800-324-1496

F: 330-995-6188

WWW.TCPI.COM

(C)TCP, INC. 03/06 00369 SS