Common Name: SEALED LEAD BATTERY, CYCLON, GENESIS, SBS, SBS J, HAWKER XE ODYSSEY OR TROLLING
Manufacturer: ENERSYS ENERGY PRODUCTS
MSDS Revision Date: 9/7/2006
   
Grainger Item Number(s): 1TC12, 3CA66, 3UVX5, 3WDE4, 4KF51, 4XL89, 6348183, 6348184, 6348186, 6348189, 6348190, 6348191, 6348192, 6348195, 6348221, 6348226, 6348230, 9FC76, 9NMD5
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION I - PRODUCT AND MANUFACTURER IDENTITY 
SECTION II - INGREDIENTS 
SECTION III - PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION IV - FIRE & EXPLOSION HAZARD DATA 
SECTION V - REACTIVITY DATA AND SHIPPING/HANDLING 
SECTION VI - HEALTH HAZARD DATA 
SECTION VII - PRECAUTIONS FOR SAFE HANDLING & USE 
SECTION VIII - CONTROL MEASURES 
SECTION IX - TRANSPORTATION, SHIPPING AND HANDLING 
SECTION X - ADDITIONAL INFORMATION 



ENERSYS(TM)
POWER/FULL SOLUTIONS(TM)

INFORMATION ONLY - PLEASE READ SECTION X

NFPA 704 RATING:
H 1
F 1
R 0


SECTION I - PRODUCT AND MANUFACTURER IDENTITY 


PRODUCT IDENTITY:
SEALED LEAD BATTERY
CYCLON(R*), GENESIS(R*), SBS, SBS J, HAWKER XE(TM) ODYSSEY(R*) OR TROLLING
THUNDER(TM)

REVISION DATE: SEPTEMBER 7, 2006

SUPERSEDES: MAY 7, 2004

MANUFACTURER'S NAME AND ADDRESS:
ENERSYS ENERGY PRODUCTS INC.
(FORMERLY HAWKER ENERGY PRODUCTS INC.)
617 NORTH RIDGEVIEW DRIVE
WARRENSBURG, MO 64093-9301

EMERGENCY TELEPHONE NUMBER: (660) 429-2165

CUSTOMER SERVICE TELEPHONE NUMBER: 800-964-2837


SECTION II - INGREDIENTS 


HAZARDOUS COMPONENTS          CAS #         OSHA PEL-TWA      % (BY WEIGHT)

LEAD                          7439-92-1     50 (MICRO)G/M3    45 - 60%

LEAD DIOXIDE                  1309-60-0     50 (MICRO)G/M3    15 - 25%

SULFURIC ACID ELECTROLYTE     7664-93-9     1.0 MG/M3         15 - 20%

NON-HAZARDOUS MATERIALS       N/A           N/A                5 - 10%


SECTION III - PHYSICAL/CHEMICAL CHARACTERISTICS 


BOILING POINT: N/A

SPECIFIC GRAVITY (H2O=1): NA

VAPOR PRESSURE (MMHg.): N/A

MELTING POINT: N/A

SOLUBILITY IN WATER: N/A

APPEARANCE & COLOR: N/A


SECTION IV - FIRE & EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): N/A

FLAMMABLE LIMITS: N/A
LEL: N/A
UEL: N/A

EXTINGUISHING MEDIA: MULTIPURPOSE DRY CHEMICAL, CO2 OR WATER SPRAY.

SPECIAL FIRE FIGHTING PROCEDURES:
COOL BATTERY EXTERIOR TO PREVENT RUPTURE. ACID MISTS AND VAPORS IN A FIRE
ARE TOXIC AND CORROSIVE.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
HYDROGEN GAS MAY BE PRODUCED AND MAY EXPLODE IF IGNITED. REMOVE ALL SOURCES
OF IGNITION.


SECTION V - REACTIVITY DATA AND SHIPPING/HANDLING 

                          ELECTRICAL SAFETY

CONDITIONS TO AVOID:
AVOID SHORTING, HIGH LEVELS OF SHORT CIRCUIT CURRENT CAN BE DEVELOPED
ACROSS THE BATTERY TERMINALS. DO NOT REST TOOLS OR CABLES ON THE BATTERY.
AVOID OVER-CHARGING. USE ONLY APPROVED CHARGING METHODS. DO NOT CHARGE IN
GAS TIGHT CONTAINERS.

REQUIREMENTS FOR SAFE SHIPPING AND HANDLING OF CYCLON(R*) CELLS:
WARNING: ELECTRICAL FIRE HAZARD - PROTECT AGAINST SHORTING

TERMINALS CAN SHORT AND CAUSE A FIRE IF NOT INSULATED DURING SHIPPING.

CYCLON(R*) PRODUCT MUST BE LABELED "NONSPILLABLE" DURING SHIPPING. FOLLOW
ALL FEDERAL SHIPPING REGULATIONS. SEE SECTION IX OF THIS SHEET AND CFR 49
PARTS 171 THROUGH 180, AVAILABLE ANYTIME ONLINE AT WWWW.GPOACCESS.GOV.

REQUIREMENTS FOR SHIPPING CYCLON(R*) PRODUCT AS SINGLE CELLS:
PROTECTIVE CAPS OR OTHER DURABLE INERT MATERIAL MUST BE USED TO INSULATE
EACH TERMINAL OF EACH CELL UNLESS CELLS ARE SHIPPING IN THE ORIGINAL
PACKAGING FROM ENERSYS, IN FULL BOX QUANTITIES.

PROTECTIVE CAPS ARE AVAILABLE FOR ALL CELL SIZES BY CONTACTING ENERSYS
CUSTOMER SERVICE AT 1-800-964-2837.

REQUIREMENTS FOR SHIPPING CYCLON(R*) PRODUCT ASSEMBLED INTO MULTICELL
BATTERIES:
ASSEMBLED BATTERIES MUST HAVE SHORT CIRCUIT PROTECTION DURING SHIPPING.

EXPOSED TERMINALS, CONNECTORS, OR LEAD WIRES MUST BE INSULATED WITH A
DURABLE INERT MATERIAL TO PREVENT EXPOSURE DURING SHIPPING.


SECTION VI - HEALTH HAZARD DATA 


ROUTES OF ENTRY: N/A

HEALTH HAZARDS (ACUTE & CHRONIC): N/A

EMERGENCY & FIRST AID PROCEDURES:
BATTERY CONTAINS ACID ELECTROLYTE WHICH IS ABSORBED IN THE SEPARATOR
MATERIAL. IF BATTERY CASE IS PUNCTURED, COMPLETELY FLUSH ANY RELEASED
MATERIAL FROM SKIN OR EYES WITH WATER.

PROPOSITION 65:

WARNING:
BATTERY POSTS, TERMINALS AND RELATED ACCESSORIES CONTAIN LEAD AND LEAD
COMPOUNDS, CHEMICALS KNOWN TO THE STATE OF CALIFORNIA TO CAUSE CANCER AND
REPRODUCTIVE HARM. BATTERIES ALSO CONTAIN OTHER CHEMICALS KNOWN TO THE
STATE OF CALIFORNIA TO CAUSE CANCER. WASH HANDS AFTER HANDLING.


SECTION VII - PRECAUTIONS FOR SAFE HANDLING & USE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
AVOID CONTACT WITH ACID MATERIALS. USE SODA ASH OR LIME TO NEUTRALIZE.
FLUSH WITH WATER.

WASTE DISPOSAL METHOD:
DISPOSE OF IN ACCORDANCE WITH FEDERAL, STATE, & LOCAL REGULATIONS. DO NOT
INCINERATE. BATTERIES SHOULD BE SHIPPED TO A RECLAMATION FACILITY FOR
RECOVERY OF THE METAL AND PLASTIC COMPONENTS AS THE PROPER METHOD OF WASTE
MANAGEMENT. CONTACT DISTRIBUTOR FOR APPROPRIATE PRODUCT RETURN PROCEDURES.


SECTION VIII - CONTROL MEASURES 


NOT APPLICABLE


SECTION IX - TRANSPORTATION, SHIPPING AND HANDLING 


ENERSYS ENERGY PRODUCTS INC. BATTERIES ARE STARVED ELECTROLYTE BATTERIES
WHICH MEANS THE ELECTROLYTE IS ABSORBED IN THE SEPARATOR MATERIAL. THE
BATTERIES ARE ALSO SEALED. AS OF SEPTEMBER 30, 1995, ENERSYS ENERGY
PRODUCTS INC. BATTERIES WERE CLASSIFIED AS "NONSPILLABLE BATTERIES", AND AS
SUCH ARE NOT SUBJECT TO THE FULL REQUIREMENTS OF 49 CFR SUBSECTION 173.159.
THE PREVIOUS EXEMPT CLASSIFICATION, "DRY BATTERIES, NOT RESTRICTED" WAS
DISCONTINUED EFFECTIVE SEPTEMBER 30, 1995. "NONSPILLABLE" BATTERIES ARE
EXCEPTED FROM THE REGULATION'S COMPREHENSIVE PACKAGING REQUIREMENTS IF THE
FOLLOWING CONDITIONS ARE SATISFIED:

(1) THE BATTERY IS PROTECTED AGAINST SHORT CIRCUITS AND IS SECURELY
PACKAGED.

(2) FOR BATTERIES MANUFACTURED AFTER SEPTEMBER 30, 1995, THE BATTERY AND
OUTER PACKAGING MUST BE PLAINLY AND DURABLY MARKED "NONSPILLABLE" OR
"NONSPILLABLE BATTERY".

(3) THE BATTERY IS CAPABLE OF WITHSTANDING VIBRATION AND PRESSURE
DIFFERENTIAL TESTS SPECIFIED IN 49 CFR SUBSECTION 173.159(D).

(4) AT A TEMPERATURE OF 55 DEG. C (131 DEG. F), THE BATTERY MUST NOT
CONTAIN ANY UNABSORBED FREE-FLOWING LIQUIDS, AND IS DESIGNED SO THAT
ELECTROLYTE WILL NOT FLOW FROM A RUPTURED OR CRACKED CASE.

ENERSYS ENERGY PRODUCTS INC. BATTERIES HAVE BEEN TESTED BY WYLE SCIENTIFIC
SERVICES & SYSTEMS LABORATORIES GROUP AND DETERMINED TO BE IN COMPLIANCE
WITH THE VIBRATION AND PRESSURE DIFFERENTIAL TESTS CONTAINED IN 49 CFR
SUBSECTION 173.159(D), AND THEREFORE AS OF SEPTEMBER 30, 1995, EXCEPTED
FROM THE DOT REQUIREMENTS SET FORTH IN 49 CFR SUBSECTION 173.159, OTHER
THAN PARAGRAPH (D).

BATTERY SHIPMENTS FROM ENERSYS ENERGY PRODUCTS INC. WARRENSBURG LOCATION,
WILL BE PROPERLY LABELED IN ACCORDANCE WITH APPLICABLE DOT REGULATIONS.

PACKAGING CHANGES PERFORMED AT OTHER LOCATIONS MAY REQUIRE ADDITIONAL
LABELING, SINCE IN ADDITION TO THE BATTERY ITSELF CONTAINING THE REQUIRED
MARKING, THE OUTER PACKAGING OF THE BATTERY MUST ALSO CONTAIN THE REQUIRED
MARKING:
"NONSPILLABLE" OR "NONSPILLABLE BATTERY". BECAUSE THE BATTERIES ARE
CLASSIFIED AS "NONSPILLABLE" AND MEET THE THREE CONDITIONS ABOVE, (FROM
SUBSECTION 173.159(D)) THEY DO NOT HAVE AN ASSIGNED UN NUMBER NOR DO THEY
REQUIRE ADDITIONAL DOT HAZARD LABELING.

THE REGULATION CHANGE EFFECTIVE SEPTEMBER, 1995, WAS TO CLARIFY AND
DISTINGUISH TO SHIPPERS AND TRANSPORTERS, ALL BATTERIES THAT HAVE BEEN
TESTED AND DETERMINED TO BE IN COMPLIANCE WITH THE DOT HAZARDOUS MATERIAL
REGULATIONS, THE INTERNATIONAL CIVIL AERONAUTICS ORGANIZATION (ICAO), AND
THE INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) PACKING INSTRUCTION 806
AND SPECIAL PROVISION A67, AND THEREFORE EXCEPTED FROM ALL OTHER
REQUIREMENTS OF THE REGULATIONS AND CLASSIFIED AS A "NONSPILLABLE BATTERY".

PER 42 USC SECTION 14322 (US CODE TITLE 42 - THE PUBLIC HEALTH AND
WELFARE), PACKAGING MUST BE MARKED WITH THE FOLLOWING:
"CONTAINS SEALED LEAD BATTERY" AND "BATTERY MUST BE RECYCLED".


SECTION X - ADDITIONAL INFORMATION 


THE ENERSYS ENERGY PRODUCTS INC. SEALED LEAD ACID BATTERY IS DETERMINED TO
BE AN "ARTICLE" ACCORDING TO THE OSHA HAZARD COMMUNICATION STANDARD AND IS
THEREBY EXCLUDED FROM ANY REQUIREMENTS OF THE STANDARD. THE MATERIAL SAFETY
DATA SHEET IS THEREFORE SUPPLIED FOR INFORMATIONAL PURPOSES ONLY.

THE INFORMATION AND RECOMMENDATIONS CONTAINED HEREIN HAVE BEEN COMPILED
FROM SOURCES BELIEVED TO BE RELIABLE AND REPRESENT CURRENT OPINION ON THE
SUBJECT. NO WARRANTY, GUARANTEE, OR REPRESENTATION IS MADE BY ENERSYS
ENERGY PRODUCTS INC., AS TO THE ABSOLUTE CORRECTNESS OR SUFFICIENCY OF ANY
REPRESENTATION CONTAINED HEREIN AND ENERSYS ENERGY PRODUCTS INC. ASSUMES NO
RESPONSIBILITY IN CONNECTION THEREWITH, NOR CAN IT BE ASSUMED THAT ALL
ACCEPTABLE SAFETY MEASURES ARE CONTAINED HEREIN, OR THAT ADDITIONAL
MEASURES MAY NOT BE REQUIRED UNDER PARTICULAR OR EXCEPTIONAL CONDITIONS OR
CIRCUMSTANCES.

N/A OR NOT APPLICABLE - NOT APPLICABLE FOR FINISHED PRODUCT USED IN NORMAL
CONDITIONS.

INFORMATIONAL MSDS PART NUMBER: 2602-0043

REV.: 2 (09/07/06)