Common Name: BAR'S LEAKS REAR MAIN SEAL REPAIR
Manufacturer: BAR'S PRODUCTS
SDS Revision Date: 12/11/2006
SDS Format: No Format Specified
   
Grainger Item Number(s): 2EXX5
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - CHEMICAL PRODUCT AND COMPANY INFORMATION 
SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 - PHYSICAL / CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL CONSIDERATIONS 
SECTION 14 - TRANSPORTATION INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET

MSDS


SECTION 1 - CHEMICAL PRODUCT AND COMPANY INFORMATION 


PRODUCT BRAND: BAR'S LEAKS(R*)

PRODUCT PART #: 1050

PRODUCT NAME: REAR MAIN SEAL REPAIR

BAR'S PRODUCTS
720 WEST ROSE STREET
P.O. BOX 187
HOLLY, MICHIGAN 48442

24-HOUR EMERGENCY:
(CHEMTREC): 1-800-424-9300

INFORMATION:
1-248-634-8278
WWW.BARSLEAKS.COM

DATE PREPARED: 12/11/06


SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 


HAZARDOUS COMPONENTS    CAS NUMBER    OSHA     ACGIH     OTHER    %
(SPECIFIC CHEMICAL                    PEL      TLV       LIMITS  (OPTIONAL)
IDENTITY, COMMON
NAME(S))

SEVERELY SOLVENT         64741-88-4   5 MG/M3  5 MG/M3   NONE    <50.0
REFINED HEAVY
PARAFFINIC PETROLEUM
OIL

SEVERELY SOLVENT         64742-01-4   5 MG/M3  5 MG/M3   NONE    <50.0
REFINED - RESIDUUM

POLYMERIC ESTER         CONFIDENTIAL  5 MG/M3  5 MG/M3   NONE    <10.0

ALKOXY HETEROCYCLIC     398141-87-2   5 MG/M3  13 MG/M3  NONE    <1.0
ETHER

OLEFIN COPOLYMER        CONFIDENTIAL  5 MG/M3  5 MG/M3   NONE    <20.0

ZINC ALKYL               68649-42-3   5 MG/M3  5 MG/M3   NONE    <<1.0
DITHIOPHOSPHATE

COPOLYMER ESTER         CONFIDENTIAL  5 MG/M3  5 MG/M3   NONE    <1.0

ALL OTHER COMPONENTS ARE CONSIDERED TO BE NON-HAZARDOUS AS PER OSHA
29 CFR 1910.1200.


SECTION 3 - HAZARDS IDENTIFICATION 


POTENTIAL HEALTH EFFECTS:

EYE:
DIRECT CONTACT WITH THE EYES CAN CAUSE IRRITATION, REDNESS OR BLURRED
VISION.

SKIN:
AVOID SKIN CONTACT. MINIMALLY IRRITATING TO THE SKIN UPON DIRECT CONTACT.
CONTACT WITH THE SKIN MAY CAUSE TRANSIENT DERMAL IRRITATION OR DRYNESS.

INHALATION: NOT A PROBABLE INHALATION HAZARD UNDER NORMAL USAGE.

INGESTION:
DO NOT INGEST. THIS PRODUCT HAS LAXATIVE PROPERTIES AND MAY RESULT IN
ABDOMINAL CRAMPS AND DIARRHEA.

ACUTE HEALTH HAZARDS:
PROLONGED AND REPEATED EXPOSURE TO OIL MIST MAY POSE A RISK OF PULMONARY
DISEASE SUCH AS CHRONIC LUNG INFLAMMATION. THIS CONDITION IS USUALLY
ASYMPTOMATIC AS A RESULT OF REPEATED SMALL ASPIRATIONS. SHORTNESS OF BREATH
AND COUGH ARE THE MOST COMMON SYMPTOMS.

CHRONIC HEALTH HAZARDS: NONE EXPECTED ON INDUSTRIAL LEVEL.

MEDICAL CONDITIONS AGGRAVATED BY EXPOSURE:
DISORDERS OR DISEASE OF THE SKIN, OR RESPIRATORY SYSTEM.

TARGET ORGAN EFFECTS: NO DATA AVAILABLE.

CARCINOGENICITY:
OSHA: NO
IARC: NO
NTP: NO


SECTION 4 - FIRST AID MEASURES 


EYE: FLUSH WITH CLEAR WATER FOR 15 MINUTES.

SKIN CONTACT:
REMOVE CONTAMINATED CLOTHING AND WASH SKIN WITH WATER AND MILD SOAP.
IF REDNESS OR IRRITATION PERSISTS, SEEK MEDICAL ATTENTION.

INHALATION:
NOT CONSIDERED TO BE AN INHALATION HAZARD. IF BREATHING BECOMES DIFFICULT,
REMOVE TO FRESH AIR IMMEDIATELY. SEEK MEDICAL ATTENTION.

INGESTION:
HAS LAXATIVE EFFECT RESULTING IN RAPID ELIMINATION. DO NOT INDUCE VOMITING.
GIVE SEVERAL GLASSES OF WATER. GET MEDICAL ATTENTION.

NOTE TO PHYSICIAN: TREAT FOR CLINICAL SYMPTOMS.


SECTION 5 - FIRE FIGHTING MEASURES 


FLASH POINT (METHOD USED): >380 DEG. F (ASTM D92)

FLAMMABLE LIMITS:
LEL (LOWER EXPLOSION LIMIT): NOT DETERMINED
UEL (UPPER EXPLOSION LIMIT): NOT DETERMINED

EXTINGUISHING MEDIA: FOAM, DRY CHEMICAL OR CARBON DIOXIDE

SPECIAL FIRE FIGHTING PROCEDURES:
WATER MAY BE INEFFECTIVE BUT CAN BE USED TO COOL CONTAINERS EXPOSED TO HEAT
OR FLAME. CAUTION SHOULD BE EXERCISED WHEN USING WATER OR FOAM AS FROTHING
MAY OCCUR. ESPECIALLY IF SPRAYED INTO CONTAINERS OF HOT BURNING LIQUID.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
EXTREME HEAT MAY CAUSE SEALED CONTAINERS TO RUPTURE. COOL FIRE EXPOSED
CONTAINERS WITH WATER SPRAY.

NFPA NATIONAL FIRE PROTECTION AGENCY:
HEALTH       1
FLAMMABILITY 1
REACTIVITY   0

HMIS HAZARDOUS MATERIAL IDENTIFICATION:
HEALTH       1
FLAMMABILITY 1
REACTIVITY   0
PP           B


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


SPILL OR LEAK PROCEDURES:
NOTIFY APPROPRIATE AUTHORITIES OF SPILL. CONTAIN SPILL IMMEDIATELY. DO NOT
ALLOW SPILL TO ENTER SEWERS OR WATERCOURSES. REMOVE ALL SOURCES OF
IGNITION. ABSORB WITH APPROPRIATE INERT MATERIAL SUCH AS SAND, CLAY ETC.
LARGE SPILLS MAY BE PICKED UP BY USING VACUUM PUMPS, SHOVELS, BUCKETS OR
OTHER MEANS AND PLACE IN DRUMS OR OTHER SUITABLE CONTAINERS. DISPOSE IN
ACCORDANCE WITH FEDERAL STATE, AND LOCAL REGULATIONS.


SECTION 7 - HANDLING AND STORAGE 


STORAGE TEMPERATURE (MIN/MAX): AMBIENT

SHELF LIFE: N/A

HANDLING/STORAGE PRECAUTIONS:
STORE IN CLOSED CONTAINERS AWAY FROM HEAT, SPARKS, FLAME OR OXIDIZING
MATERIALS. DO NOT TRANSFER TO UNMARKED CONTAINERS. USE IN WELL VENTILATED
AREAS.


SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 


ENGINEERING CONTROLS:

RESPIRATORY PROTECTION:
RESPIRATORY PROTECTION IS NOT REQUIRED UNDER CONDITIONS OF NORMAL USE IF
VAPOR OR MIST IS GENERATED WHEN MATERIAL IS HEATED OR HANDLED, USE A NIOSH
APPROVED ORGANIC VAPOR RESPIRATOR WITH A DUST AND MIST FILTER.

SKIN PROTECTION:
NONE REQUIRED IN NORMAL USE. FOR PROLONGED OR REPEATED CONTACT, USE
IMPERVIOUS CLOTHING (GLOVES, APRONS ETC.) TO COVER EXPOSED BODY PARTS.

EYE PROTECTION:
NOT REQUIRED UNDER NORMAL USE. USE SPLASH-PROOF SAFETY GLASSES OR PLASTIC
FACE SHIELDS IF SPLASHING MAY OCCUR.


SECTION 9 - PHYSICAL / CHEMICAL PROPERTIES 


PHYSICAL STATE: LIQUID

FREEZING POINT: N/D

APPEARANCE: AMBER LIQUID

MELTING POINT: N/A

ODOR: PETROLEUM ODOR

BOILING POINT DEG. F (DEG. C): >500 DEG. F

SOLUBILITY IN WATER: NIL

EVAPORATION RATE: <<1

SPECIFIC GRAVITY (H2O=1): 0.87 @ 60 DEG. F

VAPOR DENSITY (AIR = 1): N/D

pH: NO DATA

VAPOR PRESSURE (MMHg): N/D

PERCENT VOLATILES (VOC): 0%


SECTION 10 - STABILITY AND REACTIVITY 


CHEMICAL STABILITY: STABLE

INCOMPATIBILITY: NONE KNOWN

HAZARDOUS DECOMPOSITION PRODUCTS:
OXIDES OF CARBON, NITROGEN, AND SULFUR FROM COMBUSTION

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR

CONDITIONS TO AVOID: NONE KNOWN


SECTION 11 - TOXICOLOGICAL INFORMATION 


CONSUMPTION OF FOOD AND BEVERAGE SHOULD BE AVOIDED IN WORK AREAS WHERE
HYDROCARBONS ARE PRESENT. ALWAYS WASH HANDS AND FACE WITH SOAP AND WATER
BEFORE EATING, DRINKING OR SMOKING.


SECTION 12 - ECOLOGICAL INFORMATION 


ECOTOXICOLOGICAL INFORMATION: NO DATA AVAILABLE

ENVIRONMENTAL FATE: NO DATA AVAILABLE


SECTION 13 - DISPOSAL CONSIDERATIONS 


DISPOSE IN ACCORDANCE WITH FEDERAL, STATE AND LOCAL REGULATIONS.


SECTION 14 - TRANSPORTATION INFORMATION 


U.S. PROPER SHIPPING NAME: NOT REGULATED

DOT (DOMESTIC SURFACE) HAZARD CLASS OR DIVISION: NON-HAZARDOUS

IMO / IMDG (OCEAN) HAZARD CLASS DIVISION NUMBER: N/A

ICAO / IATA (AIR) HAZARD CLASS DIVISION NUMBER: N/A


SECTION 15 - REGULATORY INFORMATION 


SARA TITLE III SECTION 302 EXTREMELY HAZARDOUS SUBSTANCES: NONE

SARA TITLE III SECTION 311/312 HAZARD CATEGORIES: N/A

SARA TITLE III SECTION 313 TOXIC CHEMICALS:
ZINC ALKYL DITHIOPHOSPHATE <1.0%

OSHA STATUS: NOT REGULATED

TSCA STATUS: CHEMICAL COMPONENTS LISTED ON TSCA INVENTORY

CIRCLA REPORTABLE QUANTITY: N/A


SECTION 16 - OTHER INFORMATION 


N/A: NOT APPLICABLE

N/E: NOT ESTABLISHED

N/D: NOT DETERMINED