Common Name: ZINC AIR BATTERIES
Manufacturer: RAYOVAC
MSDS Revision Date: 3/5/2007
   
Grainger Item Number(s): 2CUR2, 2CUR3, 2CUR4, 2CUR5, 4LW12, 5AHD3, 5U008, 5U010, 5U012, 5U014
Manufacturer Model Number(s): 146A, L10ZA, L13, L13ZA, L312ZA, L675, L675ZA



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
1. IDENTIFICATION 
2. INGREDIENTS 
3. PHYSICAL DATA 
4. FIRE & EXPLOSION HAZARD DATA 
5. HEALTH HAZARD DATA 
6. REACTIVITY DATA 
7. SPILL OR LEAK PROCEDURES 
8. PROTECTION INFORMATION 
9. SPECIAL PRECAUTIONS 
10. SARA 313 



RAYOVAC(R*)

RAYOVAC CORPORATION
601 RAYOVAC DRIVE
MADISON WI 53711

PHONE: 608-275-3340

FAX: 608-275-4577

HTTP://WWW.RAYOVAC.COM

MATERIAL SAFETY DATA SHEET

1. WE WOULD LIKE TO INFORM OUR CUSTOMERS THAT THESE BATTERIES ARE EXEMPT
ARTICLES AND ARE NOT SUBJECT TO THE 29 CFR 1910.1200 OSHA REQUIREMENT, OR
TO THE CANADIAN WHMIS REQUIREMENTS AND THE SHEETS ARE SUPPLIED AS A SERVICE
TO YOU. FOR OTHER MSDSS AND RELATED INFORMATION, VISIT:

HTTP://WWW.RAYOVAC.COM/TECHNICAL/MSDS.HTM


1. IDENTIFICATION 


PRODUCT NAME: ZINC AIR BATTERIES

SIZES: ALL

EMERGENCY TELEPHONE NUMBER: 800-424-9300 (24 HR, CHEMTREC)

ENVIRONMENTAL HEALTH & SAFETY INFORMATION: 608-275-2482

EDITION DATE: 03/05/2007

APPROVED BY: KEVIN J. DOMACK


2. INGREDIENTS 


INGREDIENT NAME       CAS #         %            TLV*

ZINC                  7440-66-6     30 - 40      5.0 MG/M3 (ZnO, FUME, TWA)

STEEL                 7439-89-6     30 - 40

NICKEL                7440-02-0      3 - 7       1.0 MG/M3 (ELEMENTAL, TWA)

COPPER                 7440-50-8     1 - 5       1 MG/M3 (TWA)

CHROMIUM              7440-47-3      1 - 5       0.5 (MICRO)G/M3
                                                 (METAL, TWA)

GRAPHITE              7782-42-5      1 - 3       15 MPPCF (TWA)

POTASSIUM HYDROXIDE   1310-58-3      1 - 3       NOT LISTED

MERCURY               7439-97-6      <1**        0.025 MG/M3 (INORGANIC,
                                                 TWA)
WATER, PAPER,                        BALANCE
PLASTIC, OTHER

*SOURCE:
OSHA 29 CFR 1910.1000 TABLE Z-1 3-01-07
OSHA 29 CFR 1910.102.6 APP. A

** ZINC AIR BATTERIES CONTAIN LESS THAN 25 MG/CELL OF MERCURY.


3. PHYSICAL DATA 


BOILING POINT @ 760 MMHg (DEG. C): NA

VAPOR PRESSURE (MMHg @ 25 DEG. C): NA

VAPOR DENSITY (AIR = 1): NA

DENSITY (GRAMS/CC): NA

PERCENT VOLATILE BY VOLUME (%): NA

EVAPORATION RATE (BUTYL ACETATE = 1): NA

PHYSICAL STATE: NA

SOLUBILITY IN WATER (% BY WEIGHT): NA

pH: NA

APPEARANCE AND ODOR:
GEOMETRIC SOLID OBJECT, THIS BATTERY HAS SEVERAL HOLES IN THE POSITIVE
(+)END


4. FIRE & EXPLOSION HAZARD DATA 


FLASH POINT: NA

FLAMMABLE LIMITS IN AIR (%): NA
LOWER (LEL): NA
UPPER (UEL): NA

EXTINGUISHING MEDIA: USE WATER, FOAM OR DRY POWDER, AS APPROPRIATE.

AUTO-IGNITION: NA

SPECIAL FIRE FIGHTING PROCEDURES:
AS WITH ANY FIRE, WEAR SELF-CONTAINED BREATHING APPARATUS TO AVOID
INHALATION OF HAZARDOUS DECOMPOSITION PRODUCTS (SEE SECTION 2).

SPECIAL FIRE EXPLOSION HAZARDS:
LIKE ANY SEALED CONTAINER, BATTERY CELLS MAY RUPTURE WHEN EXPOSED TO
EXCESSIVE HEAT; THIS COULD RESULT IN THE RELEASE OF FLAMMABLE OR CORROSIVE
MATERIALS.


5. HEALTH HAZARD DATA 


THRESHOLD LIMIT VALUE (TLV) AND SOURCE: NA

EFFECTS OF OVEREXPOSURE:
NONE. (IN FIRE OR RUPTURE SITUATION SEE SECTION 2 AND SECTION 4)

EMERGENCY FIRST AID PROCEDURES:

SKIN AND EYES:
IN THE EVENT THAT BATTERY RUPTURES, FLUSH EXPOSED SKIN WITH COPIOUS
QUANTITIES OF FLOWING LUKEWARM WATER FOR A MINIMUM OF 15 MINUTES. GET
IMMEDIATE MEDICAL ATTENTION FOR EYES. WASH SKIN WITH SOAP AND WATER.

SWALLOWING:
INGESTION OF A BATTERY CAN BE HARMFUL. CALL THE NATIONAL CAPITAL POISON
CENTER (800-222-1222), DAY OR NIGHT, FOR ADVICE AND FOLLOW-UP.

FOR MORE INFORMATION, VISIT:
HTTP://WWW.NEMA.ORG/GOV/EHS/COMMITTEES/DRYBAT/.


6. REACTIVITY DATA 


STABLE OR UNSTABLE: STABLE

INCOMPATIBILITY (MATERIALS TO AVOID): NA

HAZARDOUS DECOMPOSITION PRODUCTS: NA

DECOMPOSITION TEMPERATURE (0 DEG. F): NA

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR

CONDITIONS TO AVOID: AVOID ELECTRICAL SHORTING.


7. SPILL OR LEAK PROCEDURES 


PROCEDURES TO CONTAIN AND CLEAN UP LEAKS OR SPILLS:
IN THE EVENT OF A BATTERY RUPTURE, PREVENT SKIN CONTACT AND COLLECT ALL
RELEASED MATERIAL IN A PLASTIC LINED METAL CONTAINER.

REPORTING PROCEDURE:
REPORT ALL SPILLS IN ACCORDANCE WITH FEDERAL, STATE AND LOCAL REPORTING
REQUIREMENTS.

WASTE DISPOSAL METHOD:
COMPLY WITH ALL FEDERAL, STATE AND LOCAL REGULATIONS. SOME STATE OR LOCAL
RULES MAY REQUIRE SPECIFIC WASTE MANAGEMENT METHODS. COLLECTION IS REQUIRED
IN EUROPEAN UNION COUNTRIES. FOR ADDITIONAL INFORMATION ON DISPOSAL/RECLAIM
OPTIONS, VISIT:

HTTP://WWW.NEMA.ORG/GOV/EHS/COMMITTEES/DRYBAT/.


8. PROTECTION INFORMATION 


RESPIRATORY PROTECTION (SPECIFY TYPE): NA

VENTILATION:
LOCAL EXHAUST: NA
MECHANICAL (GENERAL): NA
SPECIAL: NA
OTHER: NA

PROTECTIVE GLOVES: NA

EYE PROTECTION: NA

OTHER PROTECTIVE CLOTHING: NA


9. SPECIAL PRECAUTIONS 


HANDLING AND STORAGE:
STORE IN A DRY PLACE. STORING UNPACKAGED CELLS TOGETHER COULD RESULT IN
CELL SHORTING AND HEAT BUILD-UP.

TRANSPORTATION-SHIPPING:
THESE ARE "BATTERIES, DRY" AND ARE NOT CONSIDERED TO BE A "HAZARDOUS
MATERIAL" PER THE DEPT. OF TRANSPORTATION (USDOT) REGULATIONS OR "DANGEROUS
GOODS" PER THE INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) REGULATIONS.
SHIPMENTS MUST COMPLY WITH THE GENERAL DUTY CLAUSE OF USDOT 49 CFR 172.102
(A) (1) SPECIAL PROVISION 130, "TO PREVENT SHORTING POTENTIAL WHILE
TRANSPORTING."


10. SARA 313 


NOTIFICATION IS NOT REQUIRED BECAUSE THESE PRODUCTS ARE ARTICLE(S) THAT DO
NOT RELEASE A COVERED TOXIC CHEMICAL UNDER THE NORMAL CONDITIONS OF
PROCESSING OR USE.

NOTICE:
THE INFORMATION AND RECOMMENDATIONS SET FORTH ARE MADE IN GOOD FAITH AND
ARE BELIEVED TO BE ACCURATE AT THE DATE OF PREPARATION. RAYOVAC CORPORATION
MAKES NO WARRANTY EXPRESSED OR IMPLIED.

NA = NOT APPLICABLE