Common Name: AEROSOL PAN-SPRAY
Manufacturer: NU-CALGON WHOLESALER
MSDS Revision Date: 6/21/2006
MSDS Format: No Format Specified
   
Grainger Item Number(s): 1ANJ9
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
I - PRODUCT IDENTIFICATION 
II - HAZARDOUS INGREDIENTS OF MIXTURES 
III - PHYSICAL DATA 
IV - FIRE AND EXPLOSION 
V - REACTIVITY DATA 
VI - HEALTH HAZARD DATA 
VII - EMERGENCY AND FIRST AID PROCEDURES 
VIII - SPILL OR LEAK PROCEDURE 
IX - PROTECTION INFORMATION/CONTROL MEASURES 
X - SPECIAL PRECAUTIONS 



NU-CALGON WHOLESALER, INC.

MATERIAL SAFETY DATA SHEET

AEROSOL PAN-SPRAY


I - PRODUCT IDENTIFICATION 


COMPANY NAME: NU-CALGON WHOLESALER, INC.

ADDRESS:
2008 ALTOM COURT
ST. LOUIS, MO 63146-4151

TEL NO:
(314) 469-7000
(800) 554-5499

CHEMTREC: (800) 424-9300

PRODUCT NAME: AEROSOL PAN-SPRAY

PRODUCT NUMBER: 4296

SYNONYMS:


II - HAZARDOUS INGREDIENTS OF MIXTURES 


MATERIAL                      CAS#        % BY WT    TLV        PEL

HYDROCARBON PROPELLANT        68476-86-8             800 PPM    800

(POLY) BUTADIENE-CO-STYRENE    9003-55-8             N/E        N/E

N-TALLOWALKYL TRIMETHYLENE    61791-53-5             N/E        N/E
DIAMINES OLE.

XYLENE                         1330-20-7             100 PPM    100 PPM

TITANIUM OXIDE                13463-67-7             10 MG/M3   10 MG/M3

ALIPHATIC HYDROCARBON           110-54-3             50 PPM     500 PPM

ALL INGREDIENTS ARE TSCA LISTED.


III - PHYSICAL DATA 


VAPOR PRESSURE: <75 PSI @ 60 DEG. F

VAPOR DENSITY (AIR=1) 60-90 DEG. F: HEAVIER THAN AIR

EVAPORATION RATE: N/E

SOLUBILITY IN H2O: NIL

VOC CONTENT (% BY WT): 60.8

FREEZING POINT DEG. F: N/E

pH @ SOLUTION: N/E
pH AS DISTRIBUTED: N/E

BOILING POINT DEG. F: N/E

SPECIFIC GRAVITY H2O=1 @ 25 DEG. C: 0.85

APPEARANCE: WHITE COATING

ODOR: ASPHALT


IV - FIRE AND EXPLOSION 


FLASH POINT F: LEVEL 3 AEROSOL

FLAMMABLE LIMITS: N/D

EXTINGUISHING MEDIA:
DRY CHEMICAL, CARBON DIOXIDE, HALOGENATED EXTINGUISHING AGENT. STOP GAS
FLOW

SPECIAL FIRE FIGHTING PROCEDURES:
USE WATER SPRAY TO COOL FIRE EXPOSED SURFACES AND TO PROTECT PERSONNEL.
ISOLATE "FUEL" SUPPLY FROM FIRE. USE FOAM, DRY CHEMICAL OR WATER SPRAY TO
EXTINGUISH FIRE. AVOID SPRAYING WATER DIRECTLY INTO STORAGE CONTAINERS DUE
TO DANGER OF BOIL OVER. THIS LIQUID IS VOLATILE AND GIVES OFF INVISIBLE
VAPORS. EITHER THE LIQUID OR VAPOR MAY SETTLE IN LOW AREAS OR TRAVEL SOME
DISTANCE ALONG THE GROUND OR SURFACE TO IGNITION SOURCES WHERE THEY MAY
IGNITE OR EXPLODE.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
CONTENTS UNDER PRESSURE DO NOT EXPOSE AEROSOLS TO TEMPERATURES ABOVE
130 DEG. F OR THE CONTAINER MAY RUPTURE. GAS FIRES SHOULD NOT BE
EXTINGUISHED UNLESS THE GAS FLOW CAN BE STOPPED IMMEDIATELY. ALLOW THE
FIRE TO BURN ITSELF OUT. IF THE SOURCE CANNOT BE SHUT OFF IMMEDIATELY,
ALL EQUIPMENT AND SURFACES EXPOSED TO THE FIRE SHOULD BE COOLED WITH
WATER TO PREVENT OVER-HEATING, FLASH-BACKS OR EXPLOSIONS. CONTROL FIRE
UNTIL GAS SUPPLY CAN BE SHUT OFF. USE PROPER PROTECTIVE EQUIPMENT. USE
FRESH AIR RESPIRATOR WHILE EXPOSURE TO HAZARDOUS CONCENTRATIONS OF TOXIC
GASES IS POSSIBLE.


V - REACTIVITY DATA 


STABILITY - CONDITIONS TO AVOID:
STABLE - OPEN FLAME, WELDING ARCS, HEAT ABOVE 130 DEG. F.

INCOMPATIBILITY: STRONG OXIDIZING AGENTS.

HAZARDOUS DECOMPOSITION PRODUCTS: NONE

CONDITIONS CONTRIBUTING TO HAZARDOUS POLYMERIZATIONS: WILL NOT OCCUR


VI - HEALTH HAZARD DATA 


EFFECTS OF OVEREXPOSURE (MEDICAL CONDITIONS AGGRAVATED/TARGET ORGAN
EFFECTS):

A. ACUTE (PRIMARY ROUTE OF EXPOSURE):

INHALATION:
HIGH VAPOR/AEROSOL CONCENTRATIONS (GREATER THAN APPROXIMATELY 100 PPM) ARE
IRRITATING TO THE EYES AND THE RESPIRATORY TRACT, MAY CAUSE HEADACHES,
DIZZINESS, ANESTHESIA, DROWSINESS UNCONSCIOUSNESS AND OTHER CENTRAL NERVOUS
SYSTEM EFFECTS, INCLUDING DEATH.

EYES: SLIGHTLY IRRITATING BUT DOES NOT INJURE EYE TISSUE.

SKIN CONTACT:
LOW ORDER OF TOXICITY. FREQUENT OR PROLONGED CONTACT MAY IRRITATE AND CAUSE
DERMATITIS. SKIN CONTACT MAY AGGRAVATE AN EXISTING DERMATITIS CONDITION.

INGESTION:
SMALL AMOUNTS OF THIS PRODUCT ASPIRATED INTO THE RESPIRATORY SYSTEM DURING
INGESTION OR VOMITING MAY CAUSE MILD TO SEVERE PULMONARY INJURY, POSSIBLE
MINIMAL TOXICITY.

B. SUBCHRONIC, CHRONIC, OTHER:
HEALTH STUDIES HAVE SHOWN THAT MANY HYDROCARBONS POSE POTENTIAL HUMAN
HEALTH RISKS WHICH MAY VARY FROM PERSON TO PERSON. AS A PRECAUTION,
EXPOSURE TO LIQUIDS, VAPORS, MISTS OR FUMES SHOULD BE MINIMIZED.

C. MEDICAL CONDITIONS AGGRAVATED BY OVEREXPOSURE:
THIS MATERIAL IS AN ASPIRATION HAZARD AND DEFATS THE SKIN. BREATHING VAPORS
OF HIGH CONCENTRATIONS MAY CAUSE CNS DEPRESSION.


VII - EMERGENCY AND FIRST AID PROCEDURES 


INHALATION:
USING PROPER RESPIRATORY PROTECTION, IMMEDIATELY REMOVE THE AFFECTED VICTIM
FROM EXPOSURE. ADMINISTER ARTIFICIAL RESPIRATION IF BREATHING IS STOPPED.
KEEP AT REST. CALL FOR PROMPT MEDICAL ATTENTION.

EYES:
FLUSH EYES WITH LARGE AMOUNTS OF WATER UNTIL IRRITATION SUBSIDES.
IF IRRITATION PERSISTS, GET MEDICAL ATTENTION.

SKIN:
FLUSH WITH LARGE AMOUNTS OF WATER; USE SOAP IF AVAILABLE. REMOVE GROSSLY
CONTAMINATED CLOTHING, INCLUDING SHOES, AND LAUNDER BEFORE REUSE.

INGESTION:
IF SWALLOWED, DO NOT INDUCE VOMITING. KEEP AT REST. GET PROMPT MEDICAL
ATTENTION.


VIII - SPILL OR LEAK PROCEDURE 


SPILL MANAGEMENT:
CLEAN UP AREA BY MOPPING OR WITH ABSORBENT MATERIALS AND PLACE IN CLOSED
CONTAINER FOR DISPOSAL CONSULT FEDERAL, STATE, AND LOCAL DISPOSAL
AUTHORITIES FOR APPROVED PROCEDURES. CONSULT FEDERAL, STATE AND LOCAL
DISPOSAL AUTHORITIES.

WASTE DISPOSAL METHODS:
CONSULT LOCAL AUTHORITIES FOR PROPER WASTE DISPOSAL PROCEDURES. EMPTY
DE-PRESSURIZED CONTAINERS CANNOT BE REUSED. CANS WHICH ARE PRESSURIZED
OR CONTAIN LIQUID MUST BE DISPOSED OF IN A PERMITTED WASTE MANAGEMENT
FACILITY. CONSULT FEDERAL, STATE AND LOCAL DISPOSAL AUTHORITIES FOR
APPROVED PROCEDURES.


IX - PROTECTION INFORMATION/CONTROL MEASURES 


RESPIRATORY:
BASED ON CONTAMINATION LEVEL AND WORKING LIMITS OF THE RESPIRATOR, USE A
RESPIRATOR APPROVED BY NIOSH/MSHA, PARTICULARLY WHERE VAPOR CONCENTRATIONS
EXCEED THE RECOMMENDED EXPOSURE LIMITS. A NIOSH APPROVED ORGANIC VAPOR
CARTRIDGE OR AIR-SUPPLYING RESPIRATOR IS RECOMMENDED.

EYE PROTECTION: FACE SHIELD AND GOGGLES OR CHEMICAL GOGGLES SHOULD BE WORN.

GLOVE:
IMPERVIOUS GLOVES SHOULD BE WORN. GLOVES CONTAMINATED WITH PRODUCT SHOULD
BE DISCARDED. POLYFLUORINATED POLYEHTYLENE HAS BEEN SUGGESTED.

OTHER CLOTHING AND EQUIPMENT:
STANDARD WORK CLOTHING. STANDARD WORK SHOES; DISCARD IF SHOES CANNOT BE
DECONTAMINATED. STORE CONTAMINATED CLOTHING IN WELL VENTILATED CABINETS
OR CLOSED CONTAINERS. WASH CONTAMINATED CLOTHING AND DRY BEFORE REUSE.

VENTILATION:
USE ADEQUATE LEVEL EXHAUST VENTILATION. LOCAL EXHAUST RECOMMENDED WHEN
APPROPRIATE TO CONTROL EMPLOYEE EXPOSURE. THE USE OF MECHANICAL DILUTION
VENTILATION IS RECOMMENDED WHENEVER THIS PRODUCT IS USED IN A CONFINED
SPACE, HAS BECOME HEATED ABOVE AMBIENT TEMPERATURES, OR IS AGITATED.

NOTE:
WHERE CARBON MONOXIDE MAY BE GENERATED, SPECIAL VENTILATION MAY BE
REQUIRED.


X - SPECIAL PRECAUTIONS 


PRECAUTIONS TO BE TAKEN IN HANDLING AND STORING:
WHEN UTILIZING PRESSURIZED CONTAINERS FOLLOW STANDARD SAFETY PRACTICES FOR
HANDLING AEROSOLS. DO NOT PUNCTURE OR INCINERATE CONTAINERS. DO NOT STORE
AT TEMPERATURES ABOVE 120 DEGREES F. ODOR IS NOT AN ADEQUATE WARNING OF
POTENTIALLY HAZARDOUS CONCENTRATIONS IN AIR. RELEASES OF THESE GASES MAY
CAUSE A FLAMMABLE ATMOSPHERE WITH EXPLOSION POTENTIAL.

ADDITIONAL INFORMATION:
KEEP OUT OF THE REACH OF CHILDREN. AVOID FOOD CONTAMINATION. AVOID
BREATHING VAPORS. REMOVE IGNITION SOURCES. READ AND FOLLOW THE DIRECTIONS
ON THE PRODUCT LABEL.

NFPA:
HEALTH HAZARD   2
FIRE HAZARD     4
REACTIVITY      0
SPECIFIC HAZARD

HMIS RATING:
HEALTH HAZARD       2
FIRE HAZARD         4
REACTIVITY          0
PERSONAL PROTECTION X (SEC. 9)

REVISION DATE: 06/21/2006

SELLER MAKES NO WARRANTY, EXPRESSED OR IMPLIED, CONCERNING THE USE OF THIS
PRODUCT OTHER THAN INDICATED ON THE LABEL. BUYER ASSUMES ALL RISK OF USE
AND/OR HANDLING OF THIS MATERIAL WHEN SUCH USE AND/OR HANDLING IS CONTRARY
TO LABEL INSTRUCTIONS. WHILE SELLER BELIEVES THAT THE INFORMATION CONTAINED
HEREIN IS ACCURATE, SUCH INFORMATION IS OFFERED SOLELY FOR ITS CUSTOMERS'
CONSIDERATION AND VERIFICATION UNDER THEIR SPECIFIC USE CONDITIONS.

CATEGORY: AEROSOL