Common Name: 92211, EPDM TAPE PRIMER WASH
Manufacturer: PORTALS PLUS
SDS Revision Date: 2/19/2007
SDS Format: No Format Specified
   
Grainger Item Number(s): 4YN42
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1 PRODUCT INFORMATION 
2 HAZARDOUS INGREDIENTS INFORMATION 
3 PHYSICAL AND CHEMICAL DATA 
4 FIRE AND EXPLOSION HAZARD DATA 
5 HEALTH HAZARD DATA 
6 REACTIVITY DATA 
7 PRECAUTIONS FOR SAFE HANDLING AND USE 
8 REGULATORY INFORMATION 



PORTALS PLUS

SINCE 1977

MATERIAL SAFETY DATA SHEET

PRINTING DATE: 02/20/2007

REVISION NUMBER: 3

REVIEWED ON: 02/19/2007


1 PRODUCT INFORMATION 


PRODUCT INFORMATION:

TRADE NAME: 92211, EPDM TAPE PRIMER WASH

MANUFACTURER/SUPPLIER:
PORTALS PLUS, INC
484 N. THOMAS DRIVE
BENSENVILLE, IL 60106

(TEL): 630-595-7320

EMERGENCY INFORMATION:

CHEMTREC:
UNITED STATES: 1 (800) 424-9300

PROPER SHIPPING NAME: FLAMMABLE LIQUID (TOLUENE) UN1133


2 HAZARDOUS INGREDIENTS INFORMATION 


CHEMICAL NAME           CAS#        % BY WEIGHT    ACGIH TLV   OSHA PEL

LIGHT ALIPHATIC         64742-89-8  40-60          300 PPM     500 PPM
SOLVENT NAPHTHA

AROMATIC HYDRO-           108-88-3  25-45          100 PPM     200 PPM
CARBON SOLVENT 


3 PHYSICAL AND CHEMICAL DATA 


APPEARANCE & ODOR:
TRANSLUCENT GRAY LIQUID WITH CHARACTERISTIC ALIPHATIC SOLVENT ODOR

PHYSICAL STATE: LIQUID

BOILING POINT: 185 DEG. F

SPECIFIC GRAVITY(WATER = 1): 0.82

EVAPORATION RAT(ETHYL ETHER = 1)E: 3.5

PERCENT VOLATILES: 85%

SOLUBILITY IN WATER: INSOLUBLE

VAPOR PRESSURE: 38 MMHg @ 68 DEG. F, 20 DEG. C

VAPOR DENSITY:
(AIR = 1): 3.6

PERCENT SOLIDS (BY WEIGHT): 15%

MELTING POINT: N/A

VOC CONTENT: 645 GRAMS/LITER


4 FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT: 10 DEG. F
METHOD USED:
ESTIMATE BASED ON THE FLASH POINT OF THE MOST VOLATILE COMPONENT

FLAMMABLE LIMITS:
LEL: 1.2%
UEL: N/A

PROPER EXTINGUISHING MEDIA:
FOAM, DRY CHEMICAL OR CARBON DIOXIDE. WATER MAY BE INEFFECTIVE, BUT WATER
SHOULD BE USED TO KEEP FIRE-EXPOSED CONTAINERS COOL.

RECOMMENDED FIREFIGHTING PROCEDURES:
TREAT AS A CLASS "B" FIRE. LIMIT FIREFIGHTING TO THOSE TRAINED TO DO SO. IF
A LEAK OR SPILL HAS IGNITED, USE WATER SPRAY TO DISPERSE THE VAPORS AND
PROTECT THE MEN ATTEMPTING TO DO SO. IF A LEAK OR SPILL HAS IGNITED, USE
WATER SPRAY TO DISPERSE THE VAPORS AND TO PROTECT THE MEN ATTEMPTING TO STOP
THE LEAK. MINIMIZE BREATHING GASES, VAPOR, FUMES OR DECOMPOSITION PRODUCTS.
USE SUPPLIED-AIR BREATHING EQUIPMENT FOR ENCLOSED OR CONFINED SPACES OR AS
OTHERWISE NEEDED.

UNUSUAL FIRE & EXPLOSION HAZARDS:
VAPORS ARE HEAVIER THAN AIR AND MAY TRAVEL ALONG THE GROUND AND BE IGNITED
BY IGNITION SOURCES DISTANT FROM THE HANDLING POINT. RESIDUE IN "EMPTY"
CONTAINERS MAY BE EXPLOSIVE IF EXPOSED TO IGNITION SOURCE. TO PREVENT FIRE
OR EXPLOSION FROM STATIC ACCUMULATION AND DISCHARGE, EFFECTIVELY GROUND THE
PRODUCT TRANSFER SYSTEM.


5 HEALTH HAZARD DATA 


MEDICAL CONDITIONS AGGRAVATED BY EXPOSURE:
PRE-EXISTING EYE, SKIN AND PULMONARY DISORDERS MAY BE AGGRAVATED BY EXPOSURE
TO THIS PRODUCT.

PRIMARY ROUTE OF ENTRY:
SKIN ABSORPTION: YES
INHALATION: YES
INGESTION: YES
EYE CONTACT: YES

SIGNS AND SYMPTOMS OF EXPOSURE:

SKIN CONTACT: CAN CAUSE SEVERE REDNESS, IRRITATION, TEARING, BLURRED VISION.

INHALATION:
CAN CAUSE REDNESS, IRRITATION, DEFATTING, DERMATITIS. INTENTIONAL MISUSE BY
DELIBERATELY CONCENTRATING AND INHALING VAPOR MAY BE HARMFUL OR FATAL.

INGESTION:
CAN CAUSE GASTROINTESTINAL IRRITATION, NAUSEA, VOMITING, AND DIARRHEA.

EYE CONTACT: CAN CAUSE SEVER IRRITATION, REDNESS, TEARING BLURRED VISION

EMERGENCY AND FIRST AID PROCEDURES:

IN EYES:
FLUSH WITH LARGE AMOUNTS OF WATER, FREQUENTLY FLUSHING UNDER THE LIDS. SEEK
MEDICAL ATTENTION.

INHALED:
REMOVE AFFECTED PERSON TO FRESH AIR, GIVE OXYGEN OR ARTIFICIAL RESPIRATION
AS NECESSARY TO ASSIST BREATHING. GET MEDICAL ATTENTION.

INGESTED: DO NOT INDUCE VOMITING. GET MEDICAL ATTENTION.

ON SKIN:
WASH WITH SOAP AND WATER. GET MEDICAL ATTENTION IF IRRITATION PERSISTS.

ACUTE EFFECTS OF OVEREXPOSURE: IRRITATION, REDNESS

CHRONIC EFFECTS:

(INCLUDE ALL POTENTIAL CARCINOGENS PRESENT @.1% OR GREATER):
PROLONGED OR REPEATED CONTACT WITH THE SKIN CAN CAUSE MODERATE IRRITATION,
DEFATTING, DERMATITIS

CARCINOGENICITY:
NTEP?: NO
IARC MONOGRAPHS?: NO
OSHA REGULATED?: NO


6 REACTIVITY DATA 


STABILITY: STABLE

CONDITIONS TO AVOID: NONE KNOWN

HAZARDOUS DECOMPOSITION PRODUCTS:
IN THE EVENT OF PARTIAL COMBUSTION, FUMES, SMOKE, CARBON MONOXIDE, ALDEHYDES
AND OTHER DECOMPOSITION PRODUCTS MAY BE RELEASED.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR

INCOMPATIBILITY: AVOID CONTACT WITH STRONG OXIDIZING AGENTS


7 PRECAUTIONS FOR SAFE HANDLING AND USE 


VENTILATION:
GENERAL EXHAUST AS NEEDED TO KEEP TLV BELOW RECOMMENDED LEVELS IF
ENGINEERING OR ADMINISTRATIVE CONTROLS ARE NOT ADEQUATE.

PERSONAL PROTECTIVE EQUIPMENT:

RESPIRATOR:
FOR LARGE SPILLS OR ENTRY INTO ENCLOSED SMALL SPACES WITH INADEQUATE
VENTILATION, A PRESSURE DEMAND, SELF-CONTAINED BREATHING APPARATUS IS
RECOMMENDED. IF ENGINEERING OR ADMINISTRATIVE CONTROLS ARE NOT ADEQUATE TO
MAINTAIN SOLVENT TLV BELOW RECOMMENDED LEVELS, AN APPROPRIATE RESPIRATOR
SHOULD BE USED IN CONJUNCTION WITH A RESPIRATOR USE AND FIT TRAINING
PROGRAM.

GLOVES: BUNA-N, IF NEEDED

EYE PROTECTION: SAFETY GLASSES WITH SIDE SHIELDS IF NEEDED

OTHER PROTECTIVE CLOTHING/ARTICLES:
TO PREVENT REPEATED OR PROLONGED SKIN CONTACT, WEAR IMPERVIOUS CLOTHING AND
BOOTS IF CONTACT IS LIKELY.

WORK AND HYGIENIC MEASURES:
MINIMIZE BREATHING VAPOR. AVOID PROLONGED OR REPEATED CONTACT WITH THE SKIN.
REMOVE CONTAMINATED CLOTHING AND LAUNDER BEFORE REUSE. CLEANSE SKIN
THOROUGHLY AFTER CONTACT, BEFORE WORK BREAKS AND MEALS AND AT THE END OF THE
WORKDAY. PRODUCT IS READILY REMOVED FROM THE SKIN WITH WATERLESS HAND
CLEANERS FOLLOWED BY WASHING THOROUGHLY WITH SOAP AND WATER. EYE WASH
STATIONS SHOULD BE AVAILABLE WHERE PRODUCT MAY COME IN CONTACT WITH THE
EYES.

STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
ELIMINATE ALL IGNITION SOURCES. CONTROL THE SOURCE OF THE SPILL IF IT IS
SAFE TO DO SO. VENTILATE ENCLOSED AREAS TO PREVENT VAPOR ACCUMULATION.
RESTRICT ACCESS BY UNAUTHORIZED PERSONNEL. ABSORB SPILLED PRODUCT WITH
VERMICULITE OR OTHER ABSORBENT MATERIAL. SHOVEL OR SCOOP INTO A SEALABLE
CONTAINER FOR DISPOSAL.

WASTE DISPOSAL METHOD:
IF THIS PRODUCT BECOMES A WASTE, IT IS CONSIDERED A HAZARDOUS WASTE DUE TO
ITS IGNITABILITY. DISPOSE OF IN ACCORDANCE WITH LOCAL, STATE, AND FEDERAL
ENVIRONMENTAL WASTE REGULATIONS.

STORAGE AND HANDLING PROCEDURES:
DO NOT STORE OR HANDLE NEAR AN IGNITION SOURCE. KEEP CONTAINERS CLOSED.
EFFECTIVELY GROUND THE PRODUCT TRANSFER SYSTEM TO PREVENT FIRE OR EXPLOSION
FROM STATIC DISCHARGE. EMPTY CONTAINERS MAY CONTAIN RESIDUAL PRODUCT. DO NOT
REUSE CONTAINERS UNLESS PROPERLY RECONDITIONED.


8 REGULATORY INFORMATION 


ALL COMPONENTS ARE INCLUDED IN THE EPA TOXIC SUBSTANCE CONTROL ACT (TSCA)
CHEMICAL SUBSTANCE INVENTORY

IF THIS PRODUCT BECOMES A WASTE, IT MEETS THE CRITERIA OF A HAZARDOUS WASTE
AS DEFINED UNDER RCRA 40 CFR 261

HAZARDOUS MATERIAL IDENTIFICATION SYSTEM (HMIS):

HEALTH HAZARD RATING          1
                              CAUTION:
                              IRRITATION OR MINOR REVERSIBLE INJURY POSSIBLE

FLAMMABILITY HAZARD RATING    3
                              WARNING:
                              MATERIAL CAPABLE OF IGNITION UNDER ALMOST ALL
                              NORMAL TEMPERATURE CONDITIONS.

REACTIVITY HAZARD RATING      0
                              NORMALLY STABLE AND WILL NOT REACT WITH WATER

PERSONAL PROTECTIVE EQUIPMENT H 
                              SAFETY GLASSES, GLOVES, APRON, VAPOR
                              RESPIRATOR

EPA SARA TITLE III HAZARD CLASS (40 CFR 370):
ACUTE HEALTH HAZARD
CHRONIC HEALTH HAZARD
FIRE HAZARD

EPA SARA TITLE III SECTION 313 (40 CFR 372):

AROMATIC HYDROCARBON SOLVENT:
C.A.S. # 108-88-3 25 - 45%

EPA SARA TITLE III (40 CFR 355):
THERE ARE NO COMPONENTS PRESENT IN THIS PRODUCT AT A LEVEL WHICH WOULD
REQUIRE REPORTING

THIS PRODUCT CONTAINS A CHEMICAL THAT IS LISTED ON THE FOLLOWING STATES
HAZARDOUS MATERIAL LIST:

PENNSYLVANIA HAZARDOUS SUBSTANCE LIST: YES

NEW JERSEY WORKPLACE HAZARDOUS SUBSTANCE LIST: YES

MASSACHUSETTS SUBSTANCE LIST: YES

CANADA (WHMIS) INGREDIENT DISCLOSURE LSIT: YES

CALIFORNIA PROPOSITION 65 (SAFE DRINKING WATER AND TOXIC ENFORCEMENT ACT OF
1986):
THIS PRODUCTS CONTAINS A LISTED SUBSTANCE, WHICH THE STATE OF CALIFORNIA HAS
FOUND TO CAUSE CANCER, BIRTH DEFECTS, OR OTHER REPRODUCTIVE HARM, IN A FORM
WHICH WOULD REQUIRE A WARNING UNDER THE STATUTE. TOLUENE CAS 108-88-3

THIS INFORMATION RELATES TO SPECIFIC MATERIAL DESIGNATED AND MAY NOT BE
VALID FOR SUCH MATERIAL USED IN COMBINATION WITH ANY OTHER MATERIALS OR IN
ANY PROCESS. SUCH INFORMATION IS TO THE BEST OF OUR KNOWLEDGE AND BELIEF
ACCURATE AND RELIABLE AS OF THE DATE COMPILED. HOWEVER, NO REPRESENTATION,
WARRANTY OR GUARANTEE IS MADE TO ITS ACCURACY, RELIABILITY OR COMPLETENESS.
IT IS THE USER'S RESPONSIBILITY TO SATISFY HIMSELF AS TO THE SUITABILITY AND
COMPLETENESS OF SUCH INFORMATION FOR HIS OWN PARTICULAR USE. WE DO NOT
ACCEPT LIABILITY FOR ANY LOSS OR DAMAGE THAT MAY OCCUR FROM THE USE OF THIS
INFORMATION NOR DO WE OFFER WARRANTY AGAINST PATENT INFRINGEMENT.