Common Name: QR POWDER (PACKAGED IN INDIVIDUAL PACKAGES)
Manufacturer: BIOLIFE
SDS Revision Date: 3/25/2008
SDS Format: No Format Specified
   
Grainger Item Number(s): 3EWN5, 3EWN6
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. PRODUCT IDENTIFICATION 
2. IDENTIFICATION OF COMPONENTS 
3. HAZARD INFORMATION 
4. FIRST AID MEASURES 
5. FIRE FIGHTING INFORMATION 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 
9. PHYSICAL AND CHEMICAL PROPERTIES 
10. STABILITY AND REACTIVITY 
11. DISPOSAL MEASURES 
12. TOXICOLOGICAL INFORMATION 
13. MISCELLANEOUS ADDITIONAL INFORMATION 



MSDS

MATERIAL SAFETY DATA SHEET

EFFECTIVE DATE: MARCH 25, 2008

FROM:
BIOLIFE, LLC
1235 TALLEVAST RD
SARASOTA, FL 34243

PHONE:
941-360-1300 OR LOCAL POISON CONTROL

QR POWDER (PACKAGED IN INDIVIDUAL PACKAGES)


1. PRODUCT IDENTIFICATION 


SYNONYMS:
QR FOR CUTS AND LACERATIONS, QR FOR NOSEBLEEDS, SPORTS QR, NOSEBLEED QR,
KIDS QR, URGENT QR, POWDER TO STOP BLEEDING BY BIOLIFE LLC

MOLECULAR WEIGHT: N/A - IT IS A MIXTURE OF 2 COMPONENTS.

APPEARANCE:
THE POWDER IS DISTRIBUTED IN INDIVIDUAL PEEL TO OPEN TEAR DROP SHAPED
BLISTER PACKS. IT MAY ALSO BE DISTRIBUTED PACKAGED IN OR WITH AN
APPLICATOR.


2. IDENTIFICATION OF COMPONENTS 


IDENTIFICATION                                   PERCENT BY WT

POTASSIUM SALT                                   5 TO 20

ION EXCHANGE RESIN                               80 TO 95


3. HAZARD INFORMATION 


HEALTH RATING             1
FLAMMABILITY RATING       0
REACTIVITY RATING         2
PERSONAL EQUIPMENT NEEDED EYE PROTECTION, DUST MASK, GOWNING

A REACTIVITY RATING OF 2 IS DUE TO THE POWDER'S FRICTION BASED EXOTHERMIC
ABSORPTION OF WATER. THICKER LIQUIDS, SUCH AS BLOOD, ABSORB MORE SLOWLY
THUS REDUCING THE AMOUNT OF HEAT GENERATED. LARGE QUANTITIES OF POWDER WILL
GENERATE CONSIDERABLE HEAT WHEN MIXED WITH WATER.

POTENTIAL HEALTH EFFECTS:

INHALATION: THE POWDER IS A RESPIRATORY IRRITANT.

INGESTION:
THE MAJOR CONCERN WITH INGESTION IS IRON ABSORPTION BY THE PERSON. THE
POLYMER WILL PASS THRU THE DIGESTIVE TRACK.

SKIN CONTACT:
THE DRY POWDER WILL DEHYDRATE THE SKIN AND MAY REACT EXOTHERMICALLY WITH
ANY MOISTURE ON THE SKIN. (E.G. PERSPIRATION)

EYE CONTACT:
EVEN MINUTE QUANTITIES IN THE AIR ARE AN IRRITANT TO THE EYES AND SHOULD BE
AVOIDED. ACCIDENTAL EYE CONTACT COULD RESULT IN SEVERE BURNS TO THE EYE,
AND EVEN IRREPARABLE DAMAGE. THE POLYMER PORTION OF THE POWDER IS A SOLID
MATERIAL AND MAY SCRATCH OR CONTINUE TO IRRITATE THE SURFACE OF THE EYE.

CHRONIC EXPOSURE: N/D

OTHER:
QR POWDER REACTS EXOTHERMICALLY WHEN EXPOSED TO WATER. THIS COULD RESULT IN
A PHYSICAL BURN.

APPLICATION OF THE POWDER TO AN EXPOSED DRY WOUND WILL RESULT IN A STINGING
SENSATION, BECAUSE OF THE SALT PORTION OF THE POWDER.


4. FIRST AID MEASURES 


INHALATION:
REMOVE THE PERSON TO FRESH AIR.
SEEK MEDICAL ATTENTION AS NEEDED.

INGESTION:
DO NOT INDUCE VOMITING.
SEEK MEDICAL ATTENTION AS NEEDED.

EYE CONTACT:
MOVE VERY QUICKLY AND FLUSH THE EYE WITH RUNNING WATER FOR AT LEAST 15
MINUTES. BE SURE TO WASH UNDER THE EYELIDS.
SEEK MEDICAL ATTENTION AS NEEDED.

SKIN CONTACT:
REMOVE THE DRY POWDER FROM THE SKIN WITH A BRUSH OR VACUUM. THEN WASH THE
AREA WITH RUNNING WATER, OR A LARGE VOLUME OF WATER.

CAUTION:

USING A SMALL VOLUME OF WATER TO TRY TO REMOVE A LARGE QUANTITY OF POWDER
COULD RESULT IN A BURN, DUE TO THE POWDER'S EXOTHERMIC REACTION WITH
WATER.

SEEK MEDICAL ATTENTION AS NEEDED.

OTHER:


5. FIRE FIGHTING INFORMATION 


COMBUSTIBILITY:

FLASH POINT: NO FLASH

EXPLOSIVE NATURE:

EXPLOSIVE LIMITS: N/D

FIRE EXTINGUISHING MEDIA:
DO NOT USE FOAM OR WATER.

EXTINGUISH FIRES WITH CO2, DRY CHEMICALS, SAND, SODA ASH, OR EVACUATE THE
AREA AND ALLOW THE FIRE TO BURN.

OTHER:


6. ACCIDENTAL RELEASE MEASURES 


WEAR APPROPRIATE PERSONAL PROTECTIVE EQUIPMENT. REMOVE SOURCES OF IGNITION,
AND VENTILATE THE AREA. PICK UP MATERIAL IN A WAY TO AVOID CREATING DUST
AND DISPOSE IN AN APPROPRIATE CONTAINER. PROPERLY REPORT ANY SPILLS THAT
MAY BE AN ENVIRONMENTAL CONCERN.

DISPOSAL OF THE MATERIAL IS TO BE CONDUCTED IN COMPLIANCE WITH ALL
GOVERNMENTAL REGULATIONS.


7. HANDLING AND STORAGE 


KEEP THE PACKAGES IN A COOL DRY ENVIRONMENT. IF THE POWDER IS REMOVED FROM
IT'S PROTECTIVE PACKAGING DISPOSE OF IT BECAUSE IT WILL INACTIVATE ITSELF
BY ABSORBING MOISTURE FROM THE AIR. ONCE THE POWDER GOES FROM THE DARK
BROWN TO THE LIGHT TAN COLOR IT IS NO LONGER USEFUL.


8. EXPOSURE CONTROLS AND PERSONAL PROTECTION 


OSHA PERMISSIBLE EXPOSURE LIMIT (PEL): N/D

AGGIH THRESHOLD LIMIT VALUE (TLV): N/D

VENTILATION:
WORK IN A WELL VENTILATED FACILITY. AVOID CONCENTRATING THE DUST IN A
CONFINED WORK AREA.

RESPIRATORY PROTECTION: N/A

OTHER PERSONAL PROTECTION EQUIPMENT: N/A


9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: BROWN POWDER

ODOR: NONE

SOLUBILITY: POLYMER PORTION IS INSOLUBLE

DENSITY (G/ML): APPROXIMATELY 1

pH: N/A (SOLID POWDER)

VAPOR PRESSURE (MMHG): N/A (SOLID POWDER)

% VOLATILE BY VOLUME: N/A (SOLID POWDER)

FREEZING POINT: N/A (SOLID POWDER)

MELTING POINT: N/A (SOLID POWDER)

SUBLIMATION POINT:
POLYMER PORTION OF THE POWDER WILL SUBLIMATE AT >300 DEG. C


10. STABILITY AND REACTIVITY 


STABILITY:
IF THE MATERIAL IS KEPT DRY AND NEAR 25 DEG. C IT IS VERY STABLE. IT WILL
EXOTHERMICALLY REACT WITH WATER AND OTHER LIQUIDS, PRODUCING O2 (G) AS IT
DECOMPOSES.

DECOMPOSITION PRODUCTS:
THE POLYMER UNDER NORMAL CONDITIONS WILL NOT DECOMPOSE, BUT THE SALT
DECOMPOSES WHEN WETTED. THERE IS INTERACTION BETWEEN THE TWO SPECIES IN THE
MIXTURE WHEN WETTED. THE BYPRODUCTS ARE POLYMER, IRON OXIDE, AND OXYGEN.

INCOMPATIBILITIES: N/A UNDER DESIGNED USAGES

CONDITIONS TO AVOID: N/A UNDER DESIGNED USAGES


11. DISPOSAL MEASURES 


DISPOSAL OF THE MATERIAL IS TO BE CONDUCTED IN COMPLIANCE WITH ALL
GOVERNMENTAL REGULATIONS.


12. TOXICOLOGICAL INFORMATION 


N/D


13. MISCELLANEOUS ADDITIONAL INFORMATION 


STORAGE AND LABELING:
DO NOT REMOVE THE POWDER FROM THE PACKAGE UNTIL IT IS TO BE USED.

FIRST AID LABEL:

DISCLAIMER:
THE SUBMISSION OF THE MSDS IS REQUIRED BY LAW AND IS NOT AN ASSERTION THAT
THE PRODUCT IS HAZARDOUS WHEN USED IN THE PROPER CONDITIONS, BY TRAINED
INDIVIDUALS. THE INFORMATION HEREIN IS DEPENDABLE AND ACCURATE TO THE BEST
OF BIOLIFE L.L.C.'S KNOWLEDGE. THERE IS NO ASSERTION TO ANY CLAIMS IF THIS
PRODUCT IS COMBINED WITH ANY OTHER MATERIAL.

BIOLIFE L.L.C. IS PROVIDING THE CONTAINED HEREIN INFORMATION IN GOOD FAITH,
BUT IS MAKING NO ASSERTION OR CLAIM THAT IS IT ACCURATE OR IS
COMPREHENSIVE. THE AFOREMENTIONED INFORMATION IN THIS DOCUMENT IS SOLELY
MEANT AS A GUIDE TO THE PRECAUTIONARY HANDLING OF SAID PRODUCT BY A
PROPERLY TRAINED PERSON USING THIS PRODUCT. THE PROPERLY TRAINED INDIVIDUAL
USING THIS PRODUCT MUST US THEIR EXPERTISE AND INDEPENDENT JUDGMENT TO
DETERMINE THE APPROPRIATE USE FOR THIS PRODUCT. BIOLIFE L.L.C. MAKES NO
WARRANTY OR REPRESENTATION THAT THIS INFORMATION IS COMPLETE, AND IS
APPLICABLE TO ANY SITUATION. BIOLIFE L.L.C. WILL NOT BE HELD ACCOUNTABLE
FOR ANY DAMAGE RESULTING FROM THE USE OR RELIANCE ON THE AFOREMENTIONED
INFORMATION CONTAINED WITHIN THIS DOCUMENT.