Common Name: SUVA HP80 (R402A)
Manufacturer: DU PONT
SDS Revision Date: 5/7/2004
SDS Format: No Format Specified
   
Grainger Item Number(s): 4LFC6
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
CHEMICAL PRODUCT/COMPANY IDENTIFICATION 
COMPOSITION/INFORMATION ON INGREDIENTS 
HAZARDS IDENTIFICATION 
FIRST AID MEASURES 
FIRE FIGHTING MEASURES 
ACCIDENTAL RELEASE MEASURES 
HANDLING AND STORAGE 
EXPOSURE CONTROLS/PERSONAL PROTECTION 
PHYSICAL AND CHEMICAL PROPERTIES 
STABILITY AND REACTIVITY 
TOXICOLOGICAL INFORMATION 
ECOLOGICAL INFORMATION 
DISPOSAL CONSIDERATIONS 
TRANSPORTATION INFORMATION 
REGULATORY INFORMATION 
OTHER INFORMATION 



DU PONT(R*)

THE MSDS FORMAT ADHERES TO THE STANDARDS AND REGULATORY REQUIREMENTS OF THE
UNITED STATES AND MAY NOT MEET REGULATORY REQUIREMENTS IN OTHER COUNTRIES.

DUPONT

MATERIAL SAFETY DATA SHEET

"SUVA" HP80 (R402A)

6003FR

REVISED: 7-MAY-2004


CHEMICAL PRODUCT/COMPANY IDENTIFICATION 


MATERIAL IDENTIFICATION:

"SUVA" IS A REGISTERED TRADEMARK OF DUPONT.

CORPORATE MSDS NUMBER: DU005613

COMPANY IDENTIFICATION:

MANUFACTURER/DISTRIBUTOR:
DUPONT FLUOROPRODUCTS
1007 MARKET STREET
WILMINGTON, DE 19898

PHONE NUMBERS:
PRODUCT INFORMATION: 1-800-441-7515 (OUTSIDE THE U.S. 302-774-1000)
TRANSPORT EMERGENCY: CHEMTREC 1-800-424-9300 (OUTSIDE U.S. 703-527-3887)
MEDICAL EMERGENCY: 1-800-441-3637 (OUTSIDE THE U.S. 302-774-1000)


COMPOSITION/INFORMATION ON INGREDIENTS 


COMPONENTS:

MATERIAL                              CAS NUMBER   %

ETHANE, PENTAFLUORO- (HFC-125)        354-33-6     60

*METHANE, CHLORODIFLUORO- (HCFC-22)   75-45-6      38

PROPANE                               74-98-6      2

* DISCLOSURE AS A TOXIC CHEMICAL IS REQUIRED UNDER SECTION 313 OF TITLE III
OF THE SUPERFUND AMENDMENTS AND REAUTHORIZATION ACT OF 1986 AND 40 CFR PART
372.


HAZARDS IDENTIFICATION 


POTENTIAL HEALTH EFFECTS:
INHALATION OF HIGH CONCENTRATIONS OF VAPOR IS HARMFUL AND MAY CAUSE HEART
IRREGULARITIES, UNCONSCIOUSNESS, OR DEATH. INTENTIONAL MISUSE OR DELIBERATE
INHALATION MAY CAUSE DEATH WITHOUT WARNING. VAPOR REDUCES OXYGEN AVAILABLE
FOR BREATHING AND IS HEAVIER THAN AIR. LIQUID CONTACT CAN CAUSE FROSTBITE.

HUMAN HEALTH EFFECTS:
OVEREXPOSURE TO THE VAPORS BY INHALATION MAY INCLUDE TEMPORARY NERVOUS
SYSTEM DEPRESSION WITH ANESTHETIC EFFECTS SUCH AS DIZZINESS, HEADACHE,
CONFUSION, INCOORDINATION, AND LOSS OF CONSCIOUSNESS. HIGHER EXPOSURES TO
THE VAPORS MAY CAUSE TEMPORARY ALTERATION OF THE HEART'S ELECTRICAL ACTIVITY
WITH IRREGULAR PULSE, PALPITATIONS, OR INADEQUATE CIRCULATION. FATALITY MAY
OCCUR FROM GROSS OVEREXPOSURE. SKIN CONTACT WITH THE LIQUID MAY CAUSE
FROSTBITE.

INDIVIDUALS WITH PREEXISTING DISEASES OF THE CENTRAL NERVOUS OR
CARDIOVASCULAR SYSTEM MAY HAVE INCREASED SUSCEPTIBILITY TO THE TOXICITY OF
INCREASED EXPOSURES.

CARCINOGENICITY INFORMATION:
NONE OF THE COMPONENTS PRESENT IN THIS MATERIAL AT CONCENTRATIONS EQUAL TO
OR GREATER THAN 0.1% ARE LISTED BY IARC, NTP, OSHA OR ACGIH AS A CARCINOGEN.


FIRST AID MEASURES 


FIRST AID:

INHALATION:
IF INHALED, IMMEDIATELY REMOVE TO FRESH AIR. KEEP PERSON CALM. IF NOT
BREATHING, GIVE ARTIFICIAL RESPIRATION. IF BREATHING IS DIFFICULT, GIVE
OXYGEN. CALL A PHYSICIAN.

SKIN CONTACT:
FLUSH AREA WITH LUKEWARM WATER. DO NOT USE HOT WATER. IF FROSTBITE HAS
OCCURRED, CALL A PHYSICIAN.

EYE CONTACT:
IN CASE OF CONTACT, IMMEDIATELY FLUSH EYES WITH PLENTY OF WATER FOR AT LEAST
15 MINUTES. CALL A PHYSICIAN.

INGESTION:
NOT A PROBABLE ROUTE. HOWEVER, IN CASE OF ACCIDENTAL INGESTION, CALL A
PHYSICIAN.

NOTES TO PHYSICIANS:
THIS MATERIAL MAY MAKE THE HEART MORE SUSCEPTIBLE TO ARRHYTHMIAS.
CATECHOLAMINES SUCH AS ADRENALINE, AND OTHER COMPOUNDS HAVING SIMILAR
EFFECTS, SHOULD BE RESERVED FOR EMERGENCIES AND THEN USED ONLY WITH SPECIAL
CAUTION.


FIRE FIGHTING MEASURES 


FLAMMABLE PROPERTIES:

FLASH POINT: NO FLASH POINT

FLAMMABLE LIMITS IN AIR, % BY VOLUME:
LEL: NONE PER ASTM E681
UEL: NONE PER ASTM E681

AUTOIGNITION: NOT DETERMINED

FIRE AND EXPLOSION HAZARDS:
CYLINDERS MAY RUPTURE UNDER FIRE CONDITIONS. DECOMPOSITION MAY OCCUR.

CONTACT OF WELDING OR SOLDERING TORCH FLAME WITH HIGH CONCENTRATIONS OF
REFRIGERANT CAN RESULT IN VISIBLE CHANGES IN THE SIZE AND COLOR OF TORCH
FLAMES. THIS FLAME EFFECT WILL ONLY OCCUR IN CONCENTRATIONS OF PRODUCT WELL
ABOVE THE RECOMMENDED EXPOSURE LIMIT, THEREFORE STOP ALL WORK AND VENTILATE
TO DISPERSE REFRIGERANT VAPORS FROM THE WORK AREA BEFORE USING ANY OPEN
FLAMES.

R-402A IS NOT FLAMMABLE IN AIR AT TEMPERATURES UP TO 100 DEG C (212 DEG F)
AT ATMOSPHERIC PRESSURE. HOWEVER, MIXTURES OF R-402A WITH HIGH
CONCENTRATIONS OF AIR AT ELEVATED PRESSURE AND/OR TEMPERATURE CAN BECOME
COMBUSTIBLE IN THE PRESENCE OF AN IGNITION SOURCE. R-402A CAN ALSO BECOME
COMBUSTIBLE IN AN OXYGEN ENRICHED ENVIRONMENT (OXYGEN CONCENTRATIONS GREATER
THAN THAT IN AIR).
WHETHER A MIXTURE CONTAINING R-402A AND AIR, OR R-402A IN AN OXYGEN ENRICHED
ATMOSPHERE BECOMES COMBUSTIBLE DEPENDS ON THE INTER-RELATIONSHIP OF
1) THE TEMPERATURE
2) THE PRESSURE, AND
3) THE PROPORTION OF OXYGEN IN THE MIXTURE.
IN GENERAL, R-402A SHOULD NOT BE ALLOWED TO EXIST WITH AIR ABOVE ATMOSPHERIC
PRESSURE OR AT HIGH TEMPERATURES; OR IN AN OXYGEN ENRICHED ENVIRONMENT. FOR
EXAMPLE: R-402A SHOULD NOT BE MIXED WITH AIR UNDER PRESSURE FOR LEAK TESTING
OR OTHER PURPOSES.

EXPERIMENTAL DATA HAVE ALSO BEEN REPORTED WHICH INDICATE COMBUSTIBILITY OF
HCFC-22, A COMPONENT IN THIS BLEND, IN THE PRESENCE OF CHLORINE.

EXTINGUISHING MEDIA: AS APPROPRIATE FOR COMBUSTIBLES IN AREA.

FIRE FIGHTING INSTRUCTIONS:
KEEP CYLINDERS COOL WITH WATER SPRAY OR FOG. SELF-CONTAINED BREATHING
APPARATUS (SCBA) IS REQUIRED IF CYLINDERS RUPTURE AND CONTENTS ARE RELEASED
UNDER FIRE CONDITIONS. WATER RUNOFF SHOULD BE CONTAINED AND NEUTRALIZED
PRIOR TO RELEASE.


ACCIDENTAL RELEASE MEASURES 


SAFEGUARDS (PERSONNEL):
NOTE:
REVIEW FIRE FIGHTING MEASURES AND HANDLING (PERSONNEL) SECTIONS BEFORE
PROCEEDING WITH CLEAN-UP. USE APPROPRIATE PERSONAL PROTECTIVE EQUIPMENT
DURING CLEAN-UP.

ACCIDENTAL RELEASE MEASURES:
REMOVE OPEN FLAMES. USE SELF-CONTAINED BREATHING APPARATUS (SCBA) FOR LARGE
SPILLS OR RELEASES.


HANDLING AND STORAGE 


HANDLING (PERSONNEL):
AVOID BREATHING VAPORS. AVOID LIQUID CONTACT WITH SKIN OR EYES. USE WITH
SUFFICIENT VENTILATION TO KEEP EMPLOYEE EXPOSURE BELOW THE RECOMMENDED
LIMITS. AVOID PROLONGED OR REPEATED EXPOSURE. WASH THOROUGHLY AFTER
HANDLING.

STORAGE: CLEAN, DRY AREA. DO NOT HEAT ABOVE 52 DEG C (125 DEG F).


EXPOSURE CONTROLS/PERSONAL PROTECTION 


ENGINEERING CONTROLS:
REFRIGERANT CONCENTRATION MONITORS MAY BE NECESSARY TO DETERMINE VAPOR
CONCENTRATIONS IN WORK AREAS PRIOR TO USE OF TORCHES OR OTHER OPEN FLAMES,
OR IF EMPLOYEES ARE ENTERING ENCLOSED AREAS.

USE WITH SUFFICIENT VENTILATION TO KEEP EMPLOYEE EXPOSURE BELOW THE
RECOMMENDED EXPOSURE LIMIT. LOCAL EXHAUST SHOULD BE USED IF LARGE AMOUNTS
ARE RELEASED. MECHANICAL VENTILATION SHOULD BE USED IN LOW OR ENCLOSED
PLACES.

PERSONAL PROTECTIVE EQUIPMENT:
IMPERVIOUS GLOVES SHOULD BE USED TO AVOID PROLONGED OR REPEATED EXPOSURE.
CHEMICAL SPLASH GOGGLES SHOULD BE AVAILABLE FOR USE AS NEEDED TO PREVENT EYE
CONTACT. UNDER NORMAL MANUFACTURING CONDITIONS, NO RESPIRATORY PROTECTION IS
REQUIRED WHEN USING THIS PRODUCT. SELF-CONTAINED BREATHING APPARATUS (SCBA)
IS REQUIRED IF A LARGE RELEASE OCCURS.

| EXPOSURE GUIDELINES:

APPLICABLE EXPOSURE LIMITS:

ETHANE, PENTAFLUORO- (HFC-125):
PEL (OSHA): NONE ESTABLISHED
TLV (ACGIH): NONE ESTABLISHED
AEL * (DUPONT): 1000 PPM, 8 & 12 HR. TWA
WEEL (AIHA): 1000 PPM, 4900 MG/M3, 8 HR. TWA

METHANE, CHLORODIFLUORO- (HCFC-22):
PEL (OSHA): NONE ESTABLISHED
TLV (ACGIH): 1,000 PPM, 3,540 MG/M3, 8 HR. TWA, A4
AEL * (DUPONT): NONE ESTABLISHED

PROPANE:
PEL (OSHA): 1,000 PPM, 1,800 MG/M3, 8 HR. TWA
TLV (ACGIH): 1000 PPM, 8 HR. TWA
AEL * (DUPONT): NONE ESTABLISHED

* AEL IS DUPONT'S ACCEPTABLE EXPOSURE LIMIT. WHERE GOVERNMENTALLY IMPOSED
OCCUPATIONAL EXPOSURE LIMITS WHICH ARE LOWER THAN THE AEL ARE IN EFFECT,
SUCH LIMITS SHALL TAKE PRECEDENCE.


PHYSICAL AND CHEMICAL PROPERTIES 


PHYSICAL DATA:

BOILING POINT: -49.2 C (-56.6 F)

VAPOR PRESSURE: 193.6 PSIA AT 25 DEG C (77 DEG F)

% VOLATILES: 100 WT %

EVAPORATION RATE: (CCL4 = 1) GREATER THAN 1

SOLUBILITY IN WATER: NOT DETERMINED

ODOR: SLIGHT ETHEREAL

FORM: LIQUEFIED GAS

COLOR: CLEAR, COLORLESS

DENSITY: 1.152 GM/CC AT 25 DEG C (77 DEG F) - LIQUID


STABILITY AND REACTIVITY 


CHEMICAL STABILITY:
MATERIAL IS STABLE. HOWEVER, AVOID OPEN FLAMES AND HIGH TEMPERATURES.

INCOMPATIBILITY WITH OTHER MATERIALS:
INCOMPATIBLE WITH ALKALI OR ALKALINE EARTH METALS - POWDERED Al, Zn, Be,
ETC.

DECOMPOSITION:
DECOMPOSITION PRODUCTS ARE HAZARDOUS. "SUVA" HP80 CAN BE DECOMPOSED BY HIGH
TEMPERATURES (OPEN FLAMES, GLOWING METAL SURFACES, ETC.) FORMING
HYDROCHLORIC AND HYDROFLUORIC ACIDS, AND POSSIBLY CARBONYL HALIDES. THESE
MATERIALS ARE TOXIC AND IRRITATING. CONTACT SHOULD BE AVOIDED.

POLYMERIZATION: POLYMERIZATION WILL NOT OCCUR.


TOXICOLOGICAL INFORMATION 


ANIMAL DATA: THE BLEND IS UNTESTED.

ETHANE, PENTAFLUORO:
INHALATION 4 HOUR ALC: >709,000 PPM IN RATS

SINGLE, HIGH INHALATION EXPOSURES CAUSED LETHARGY, DECREASED ACTIVITY,
LABORED BREATHING AND WEIGHT LOSS. WEAK CARDIAC SENSITIZATION EFFECT, A
POTENTIALLY FATAL DISTURBANCE OF HEART RHYTHM CAUSED BY A HEIGHTENED
SENSITIVITY TO THE ACTION OF EPINEPHRINE.
LOWEST-OBSERVED-ADVERSE-EFFECT-LEVEL FOR CARDIAC SENSITIZATION: 100,000 PPM.
REPEATED EXPOSURE CAUSED: NO SIGNIFICANT TOXICOLOGICAL EFFECTS.
NO-OBSERVED-ADVERSE-EFFECT LEVEL(NOAEL): 50,000 PPM

NO ANIMAL DATA ARE AVAILABLE TO DEFINE CARCINOGENIC, DEVELOPMENTAL OR
REPRODUCTIVE HAZARDS. IN ANIMAL TESTING THIS MATERIAL HAS NOT CAUSED
DEVELOPMENTAL TOXICITY. HFC-125 DOES NOT PRODUCE GENETIC DAMAGE IN BACTERIAL
OR MAMMALIAN CELL CULTURES OR WHEN TESTED IN ANIMALS (NOT TESTED FOR
HERITABLE GENETIC DAMAGE).

METHANE, CHLORODIFLUORO:
INHALATION 4-HOUR LC50: 220,000 PPM IN RATS

THE COMPOUND IS A SKIN IRRITANT AND A SLIGHT EYE IRRITANT, BUT IS NOT A SKIN
SENSITIZER IN ANIMALS.

EFFECTS FROM SINGLE HIGH EXPOSURES INCLUDE CENTRAL NERVOUS SYSTEM
DEPRESSION, ANESTHESIA, RAPID BREATHING, LUNG CONGESTION AND MICROSCOPIC
LIVER CHANGES. CARDIAC SENSITIZATION OCCURRED IN DOGS AT 50,000 PPM OR
GREATER FROM THE ACTION OF EXOGENOUS EPINEPHRINE.

NO TOXIC EFFECTS OR ABNORMAL HISTOPATHOLOGICAL OBSERVATIONS OCCURRED IN RATS
REPEATEDLY EXPOSED TO CONCENTRATIONS RANGING FROM 10,000 TO 50,000 PPM
(V/V). LONG-TERM EXPOSURES TO 50,000 PPM (V/V) OF VAPORS PRODUCED ORGAN
WEIGHT INCREASES AND A DECREASE IN BODY WEIGHT GAIN, BUT NO INCREASED
MORTALITY OR ADVERSE HEMATOLOGICAL EFFECTS.

IN CHRONIC INHALATION STUDIES, HCFC-22, AT A CONCENTRATION OF 50,000 PPM
(V/V), PRODUCED A SMALL, BUT STATISTICALLY SIGNIFICANT INCREASE OF
LATE-OCCURRING TUMORS INVOLVING SALIVARY GLANDS IN MALE RATS, BUT NOT FEMALE
RATS OR MALE OR FEMALE MICE. IN THE SAME STUDIES, NO INCREASED INCIDENCE OF
TUMORS WAS SEEN IN EITHER SPECIES AT CONCENTRATIONS OF 10,000 PPM OR 1000
PPM (V/V).

LONG-TERM ADMINISTRATION IN CORN OIL PRODUCED NO EFFECTS ON BODY WEIGHT OR
MORTALITY.

HCFC-22 WAS MUTAGENIC IN SOME STRAINS OF BACTERIA IN BACTERIAL CELL
CULTURES, BUT NOT MAMMALIAN CELL CULTURES OR ANIMALS. IT DID NOT CAUSE
HERITABLE GENETIC DAMAGE IN MAMMALS.

A SLIGHT, BUT SIGNIFICANT INCREASE IN DEVELOPMENTAL TOXICITY WAS OBSERVED AT
HIGH CONCENTRATIONS (50,000 PPM) OF HCFC-22, A CONCENTRATION WHICH ALSO
PRODUCED TOXIC EFFECTS IN THE ADULT ANIMAL. BASED ON THESE FINDINGS, AND
OTHER NEGATIVE DEVELOPMENTAL STUDIES, HCFC-22 IS NOT CONSIDERED A UNIQUE
HAZARD TO THE CONCEPTS. STUDIES OF THE EFFECTS OF HCFC-22 ON MALE
REPRODUCTIVE PERFORMANCE HAVE BEEN NEGATIVE. SPECIFIC STUDIES TO EVALUATE
THE EFFECT ON FEMALE REPRODUCTIVE PERFORMANCE HAVE NOT BEEN CONDUCTED,
HOWEVER, LIMITED INFORMATION OBTAINED FROM STUDIES ON DEVELOPMENTAL TOXICITY
DO NOT INDICATE ADVERSE EFFECTS ON FEMALE REPRODUCTIVE PERFORMANCE AT
CONCENTRATIONS UP TO 50,000 PPM.

PROPANE:
TOXICITY IN ANIMALS OCCURRING ONLY WITH INHALATION EXPOSURES AT HIGH
CONCENTRATIONS (10% OR GREATER) INCLUDE CARDIAC SENSITIZATION, ANALGESIA,
IRREGULAR RESPIRATION AND HYPOTENSION. NO ANIMAL TEST REPORTS ARE AVAILABLE
TO DEFINE CARCINOGENIC, DEVELOPMENTAL, OR REPRODUCTIVE HAZARDS. TESTS IN
BACTERIA CELL CULTURES DEMONSTRATE NO MUTAGENIC ACTIVITY.


ECOLOGICAL INFORMATION 


ECOTOXICOLOGICAL INFORMATION:

AQUATIC TOXICITY:

HCFC-22:
48 HOUR EC50 - DAPHNIA MAGNA: 433 MG/L


DISPOSAL CONSIDERATIONS 


WASTE DISPOSAL:
COMPLY WITH FEDERAL, STATE, AND LOCAL REGULATIONS. RECLAIM BY DISTILLATION
OR REMOVE TO A PERMITTED WASTE DISPOSAL FACILITY.


TRANSPORTATION INFORMATION 


SHIPPING INFORMATION:

DOT/IMO/IATA:
PROPER SHIPPING NAME:
LIQUEFIED GAS N.O.S. (CHLORODIFLUOROMETHANE AND PENTAFLUOROETHANE)
HAZARD CLASS: 2.2
UN NO.: 3163
LABEL(S): NONFLAMMABLE GAS

SHIPPING CONTAINERS:
TANK CARS.
CYLINDERS
TON TANKS


REGULATORY INFORMATION 


U.S. FEDERAL REGULATIONS:

TSCA INVENTORY STATUS: REPORTED/INCLUDED.

TITLE III HAZARD CLASSIFICATIONS SECTIONS 311, 312:
ACUTE:      YES
CHRONIC:    NO
FIRE:       NO
REACTIVITY: NO
PRESSURE:   YES

HAZARDOUS CHEMICAL LISTS:
SARA EXTREMELY HAZARDOUS SUBSTANCE: NO
CERCLA HAZARDOUS SUBSTANCE:         NO

SARA TOXIC CHEMICAL - SEE COMPONENTS SECTION


OTHER INFORMATION 


NFPA, NPCA-HMIS:

NPCA-HMIS RATING:
HEALTH:       1
FLAMMABILITY: 0
REACTIVITY:   1

PERSONAL PROTECTION RATING TO BE SUPPLIED BY USER DEPENDING ON USE
CONDITIONS.

ADDITIONAL INFORMATION:

MEDICAL USE:
CAUTION:
DO NOT USE IN MEDICAL APPLICATIONS INVOLVING PERMANENT IMPLANTATION IN THE
HUMAN BODY. FOR OTHER MEDICAL APPLICATIONS SEE DUPONT CAUTION BULLETIN
NO. H-50102.

THE DATA IN THIS MATERIAL SAFETY DATA SHEET RELATES ONLY TO THE SPECIFIC
MATERIAL DESIGNATED HEREIN AND DOES NOT RELATE TO USE IN COMBINATION WITH
ANY OTHER MATERIAL OR IN ANY PROCESS.

RESPONSIBILITY FOR MSDS:
MSDS COORDINATOR
DUPONT FLUOROPRODUCTS

ADDRESS: WILMINGTON, DE 19898

TELEPHONE: (800) 441-7515

| INDICATES UPDATED SECTION.

THIS INFORMATION IS BASED UPON TECHNICAL INFORMATION BELIEVED TO BE
RELIABLE. IT IS SUBJECT TO REVISION AS ADDITIONAL KNOWLEDGE AND EXPERIENCE
IS GAINED.