Common Name: AUTORF SSPR 6PK AUT HIGH HEAT PRME 2000, 249340
Manufacturer: RUST-OLEUM
SDS Revision Date: 12/16/2008
SDS Format: No Format Specified
   
Grainger Item Number(s): 4YLC8
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - CHEMICAL PRODUCT / COMPANY INFORMATION 
SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS / PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL INFORMATION 
SECTION 14 - TRANSPORTATION INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



249340 AUTORF SSPR 6PK AUT HIGH HEAT PRME 2000

MATERIAL SAFETY DATA SHEET

24 HOUR ASSISTANCE:
1-847-367-7700
RUST-OLEUM CORP.

WWW.RUSTOLEUM.COM


SECTION 1 - CHEMICAL PRODUCT / COMPANY INFORMATION 


PRODUCT NAME: AUTORF SSPR 6PK AUT HIGH HEAT PRME 2000

IDENTIFICATION NUMBER: 249340

REVISION DATE: 12/16/2008

PRODUCT USE/CLASS: PRIMER/AEROSOLS

SUPPLIER:
RUST-OLEUM CORPORATION
11 HAWTHORN PARKWAY
VERNON HILLS, IL 60061
USA

MANUFACTURER:
RUST-OLEUM CORPORATION
11 HAWTHORN PARKWAY
VERNON HILLS, IL 60061
USA

PREPARER: REGULATORY DEPARTMENT


SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 


CHEMICAL NAME                        CAS NUMBER       WEIGHT % LESS THAN

ACETONE                                 67-64-1       45.0

LIQUEFIED PETROLEUM GAS              68476-86-8       30.0

XYLENE                                1330-20-7       10.0

TOLUENE                                108-88-3        5.0

ETHYLBENZENE                           100-41-4        5.0

TITANIUM DIOXIDE                     13463-67-7        5.0

COPPER CHROMITE BLACK                68186-91-4        5.0


CHEMICAL NAME                ACGIH        ACGIH       OSHA        OSHA PEL
                             TLV-TWA      TLV-STEL    PEL-TWA     CEILING

ACETONE                      500 PPM      750 PPM     750 PPM     N.E.

LIQUEFIED PETROLEUM GAS      1000 PPM     N.E.        1000 PPM    N.E.

XYLENE                       100 PPM      150 PPM     100 PPM     N.E.

TOLUENE                      50 PPM       150 PPM     200 PPM     300 PPM

ETHYLBENZENE                 100 PPM      125 PPM     100 PPM     N.E.

TITANIUM DIOXIDE             10 MG/M3     N.E.        10 MG/M3    N.E.

COPPER CHROMITE BLACK        0.5 MG/M3    N.E.        0.5 MG/M3   N.E.


SECTION 3 - HAZARDS IDENTIFICATION 


EMERGENCY OVERVIEW:
CONTAINS AROMATIC DISTILLATE, WHICH MAY CAUSE CANCER. CONTENTS UNDER
PRESSURE. HARMFUL IF INHALED. MAY AFFECT THE BRAIN OR NERVOUS SYSTEM
CAUSING DIZZINESS, HEADACHE OR NAUSEA. HARMFUL IF SWALLOWED. EXTREMELY
FLAMMABLE LIQUID AND VAPOR. VAPORS MAY CAUSE FLASH FIRE OR EXPLOSION.

EFFECTS OF OVEREXPOSURE - EYE CONTACT: CAUSES EYE IRRITATION.

EFFECTS OF OVEREXPOSURE - SKIN CONTACT:
PROLONGED OR REPEATED CONTACT MAY CAUSE SKIN IRRITATION. SUBSTANCE MAY
CAUSE SLIGHT SKIN IRRITATION.

EFFECTS OF OVEREXPOSURE - INHALATION:
HIGH VAPOR CONCENTRATIONS ARE IRRITATING TO THE EYES, NOSE, THROAT AND
LUNGS. HARMFUL IF INHALED. HIGH GAS, VAPOR, MIST OR DUST CONCENTRATIONS
MAY BE HARMFUL IF INHALED. AVOID BREATHING VAPORS OR MISTS.

EFFECTS OF OVEREXPOSURE - INGESTION:
ASPIRATION HAZARD IF SWALLOWED; CAN ENTER LUNGS AND CAUSE DAMAGE. SUBSTANCE
MAY BE HARMFUL IF SWALLOWED.

EFFECTS OF OVEREXPOSURE - CHRONIC HAZARDS:
IARC LISTS ETHYLBENZENE AS A POSSIBLE HUMAN CARCINOGEN (GROUP 2B).
CONTAINS TITANIUM DIOXIDE. TITANIUM DIOXIDE IS LISTED AS A GROUP
2B-"POSSIBLY CARCINOGENIC TO HUMANS" BY IARC. SIGNIFICANT EXPOSURE IS
NOT ANTICIPATED DURING BRUSH APPLICATION OR DRYING. RISK OF OVEREXPOSURE
DEPENDS ON DURATION AND LEVEL OF EXPOSURE TO DUST FROM REPEATED SANDING OF
SURFACES OR SPRAY MIST AND THE ACTUAL CONCENTRATION OF TITANIUM DIOXIDE IN
THE FORMULA.

MAY CAUSE CENTRAL NERVOUS SYSTEM DISORDER (E.G., NARCOSIS INVOLVING A LOSS
OF COORDINATION, WEAKNESS, FATIGUE, MENTAL CONFUSION, AND BLURRED VISION)
AND/OR DAMAGE. REPORTS HAVE ASSOCIATED REPEATED AND PROLONGED OCCUPATIONAL
OVEREXPOSURE TO SOLVENTS WITH PERMANENT BRAIN AND NERVOUS SYSTEM DAMAGE.
OVEREXPOSURE TO XYLENE IN LABORATORY ANIMALS HAS BEEN ASSOCIATED WITH LIVER
ABNORMALITIES, KIDNEY, LUNG, SPLEEN, EYE AND BLOOD DAMAGE AS WELL AS
REPRODUCTIVE DISORDERS. EFFECTS IN HUMANS, DUE TO CHRONIC OVEREXPOSURE,
HAVE INCLUDED LIVER, CARDIAC ABNORMALITIES AND NERVOUS SYSTEM DAMAGE.
OVEREXPOSURE TO TOLUENE IN LABORATORY ANIMALS HAS BEEN ASSOCIATED WITH
LIVER ABNORMALITIES, KIDNEY, LUNG AND SPLEEN DAMAGE. EFFECTS IN HUMANS
HAVE INCLUDED LIVER AND CARDIAC ABNORMALITIES.

PRIMARY ROUTE(S) OF ENTRY:
SKIN CONTACT, SKIN ABSORPTION, INHALATION, EYE CONTACT


SECTION 4 - FIRST AID MEASURES 


FIRST AID - EYE CONTACT:
IMMEDIATELY FLUSH EYES WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES HOLDING
EYELIDS OPEN. GET MEDICAL ATTENTION.

FIRST AID - SKIN CONTACT:
WASH WITH SOAP AND WATER. GET MEDICAL ATTENTION IF IRRITATION DEVELOPS OR
PERSISTS.

FIRST AID - INHALATION:
IF YOU EXPERIENCE DIFFICULTY IN BREATHING, LEAVE THE AREA TO OBTAIN FRESH
AIR. IF CONTINUED DIFFICULTY IS EXPERIENCED, GET MEDICAL ASSISTANCE
IMMEDIATELY.

FIRST AID - INGESTION:

ASPIRATION HAZARD:
DO NOT INDUCE VOMITING OR GIVE ANYTHING BY MOUTH BECAUSE THIS MATERIAL
CAN ENTER THE LUNGS AND CAUSE SEVERE LUNG DAMAGE. GET IMMEDIATE MEDICAL
ATTENTION.


SECTION 5 - FIRE FIGHTING MEASURES 


FLASH POINT (SETAFLASH): -156 F

LOWER EXPLOSIVE LIMIT: 1.0 %
UPPER EXPLOSIVE LIMIT: 12.8 %

EXTINGUISHING MEDIA: CARBON DIOXIDE, DRY CHEMICAL, FOAM, WATER FOG

UNUSUAL FIRE AND EXPLOSION HAZARDS:
WATER SPRAY MAY BE INEFFECTIVE. FLASH POINT IS LESS THAN 20 DEG. F. -
EXTREMELY FLAMMABLE LIQUID AND VAPOR!
CLOSED CONTAINERS MAY EXPLODE WHEN EXPOSED TO EXTREME HEAT. VAPORS MAY FORM
EXPLOSIVE MIXTURES WITH AIR. VAPORS CAN TRAVEL TO A SOURCE OF IGNITION AND
FLASH BACK. KEEP CONTAINERS TIGHTLY CLOSED. ISOLATE FROM HEAT, ELECTRICAL
EQUIPMENT, SPARKS AND OPEN FLAME. PERFORATION OF THE PRESSURIZED CONTAINER
MAY CAUSE BURSTING OF THE CAN.

SPECIAL FIREFIGHTING PROCEDURES:
EVACUATE AREA AND FIGHT FIRE FROM A SAFE DISTANCE.


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


STEPS TO BE TAKEN IF MATERIAL IS RELEASED OR SPILLED:
CONTAIN SPILLED LIQUID WITH SAND OR EARTH. DO NOT USE COMBUSTIBLE MATERIALS
SUCH AS SAWDUST. REMOVE ALL SOURCES OF IGNITION, VENTILATE AREA AND REMOVE
WITH INERT ABSORBENT AND NON-SPARKING TOOLS. DISPOSE OF ACCORDING TO LOCAL,
STATE (PROVINCIAL) AND FEDERAL REGULATIONS. DO NOT INCINERATE CLOSED
CONTAINERS.


SECTION 7 - HANDLING AND STORAGE 


HANDLING:
FOLLOW ALL MSDS/LABEL PRECAUTIONS EVEN AFTER CONTAINER IS EMPTIED BECAUSE
IT MAY RETAIN PRODUCT RESIDUES. AVOID BREATHING VAPOR OR MIST. WASH
THOROUGHLY AFTER HANDLING. USE ONLY IN A WELL-VENTILATED AREA. WASH HANDS
BEFORE EATING.

STORAGE:
KEEP CONTAINERS TIGHTLY CLOSED. ISOLATE FROM HEAT, ELECTRICAL EQUIPMENT,
SPARKS AND OPEN FLAME. DO NOT STORE ABOVE 120 DEG. F. STORE LARGE
QUANTITIES IN BUILDINGS DESIGNED AND PROTECTED FOR STORAGE OF NFPA CLASS I
FLAMMABLE LIQUIDS. CONTENTS UNDER PRESSURE. DO NOT EXPOSE TO HEAT OR STORE
ABOVE 120 DEG. F.


SECTION 8 - EXPOSURE CONTROLS / PERSONAL PROTECTION 


ENGINEERING CONTROLS:
PREVENT BUILD-UP OF VAPORS BY OPENING ALL DOORS AND WINDOWS TO ACHIEVE
CROSS-VENTILATION. USE PROCESS ENCLOSURES, LOCAL EXHAUST VENTILATION, OR
OTHER ENGINEERING CONTROLS TO CONTROL AIRBORNE LEVELS BELOW RECOMMENDED
EXPOSURE LIMITS. USE EXPLOSION-PROOF VENTILATION EQUIPMENT.

RESPIRATORY PROTECTION:
A RESPIRATORY PROTECTION PROGRAM THAT MEETS OSHA 1910.134 AND ANSI Z88.2
REQUIREMENTS MUST BE FOLLOWED WHENEVER WORKPLACE CONDITIONS WARRANT A
RESPIRATOR'S USE. A NIOSH/MSHA APPROVED AIR PURIFYING RESPIRATOR WITH AN
ORGANIC VAPOR CARTRIDGE OR CANISTER MAY BE PERMISSIBLE UNDER CERTAIN
CIRCUMSTANCES WHERE AIRBORNE CONCENTRATIONS ARE EXPECTED TO EXCEED EXPOSURE
LIMITS.

PROTECTION PROVIDED BY AIR PURIFYING RESPIRATORS IS LIMITED. USE A
POSITIVE PRESSURE AIR SUPPLIED RESPIRATOR IF THERE IS ANY POTENTIAL FOR
AN UNCONTROLLED RELEASE, EXPOSURE LEVELS ARE NOT KNOWN, OR ANY OTHER
CIRCUMSTANCES WHERE AIR PURIFYING RESPIRATORS MAY NOT PROVIDE ADEQUATE
PROTECTION.

SKIN PROTECTION:
USE IMPERVIOUS GLOVES TO PREVENT SKIN CONTACT AND ABSORPTION OF THIS
MATERIAL THROUGH THE SKIN. NITRILE OR NEOPRENE GLOVES MAY AFFORD ADEQUATE
SKIN PROTECTION.

EYE PROTECTION:
USE SAFETY EYEWEAR DESIGNED TO PROTECT AGAINST SPLASH OF LIQUIDS.

OTHER PROTECTIVE EQUIPMENT:
REFER TO SAFETY SUPERVISOR OR INDUSTRIAL HYGIENIST FOR FURTHER INFORMATION
REGARDING PERSONAL PROTECTIVE EQUIPMENT AND ITS APPLICATION.

HYGIENIC PRACTICES:
WASH THOROUGHLY WITH SOAP AND WATER BEFORE EATING, DRINKING OR SMOKING.


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


BOILING RANGE: -34 - 999 F

VAPOR DENSITY: HEAVIER THAN AIR

ODOR: SOLVENT LIKE

ODOR THRESHOLD: N.E.

APPEARANCE: LIQUID

EVAPORATION RATE: FASTER THAN ETHER

SOLUBILITY IN H2O: SLIGHT

FREEZE POINT: N.D.

SPECIFIC GRAVITY: 0.767

VAPOR PRESSURE: N.D.

pH: N.A.

PHYSICAL STATE: LIQUID

(SEE SECTION 16 FOR ABBREVIATION LEGEND)


SECTION 10 - STABILITY AND REACTIVITY 


CONDITIONS TO AVOID:
AVOID TEMPERATURES ABOVE 120 DEG. F. AVOID ALL POSSIBLE SOURCES OF
IGNITION.

INCOMPATIBILITY:
INCOMPATIBLE WITH STRONG OXIDIZING AGENTS, STRONG ACIDS AND STRONG
ALKALIES.

HAZARDOUS DECOMPOSITION:
WHEN HEATED TO DECOMPOSITION, IT EMITS ACRID SMOKE AND IRRITATING FUMES.
BY OPEN FLAME, CARBON MONOXIDE AND CARBON DIOXIDE.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR UNDER NORMAL CONDITIONS.

STABILITY: THIS PRODUCT IS STABLE UNDER NORMAL STORAGE CONDITIONS.


SECTION 11 - TOXICOLOGICAL INFORMATION 


PRODUCT LD50: N.D.
PRODUCT LC50: N.D.

CHEMICAL NAME                LD50                  LC50

ACETONE                      5800 MG/KG (RAT)      50100 MG/M3 (RAT, 8HR)

LIQUEFIED PETROLEUM GAS      N.E.                  N.E.

XYLENE                       4300 MG/KG            5000 PPM
                             (RAT, ORAL)           (RAT, INHALATION, 4HR)

TOLUENE                      636 MG/KG             49 G/M3
                             (RAT, ORAL)           (RAT, INHALATION)

ETHYLBENZENE                 3500 MG/KG            N.E.
                             (RAT, ORAL)

TITANIUM DIOXIDE             >7500 MG/KG           N.E.
                             (RAT, ORAL)

COPPER CHROMITE BLACK        >10000 MG/L           N.E.
                             (RAT, ORAL)


SECTION 12 - ECOLOGICAL INFORMATION 


ECOLOGICAL INFORMATION: PRODUCT IS A MIXTURE OF LISTED COMPONENTS.


SECTION 13 - DISPOSAL INFORMATION 


DISPOSAL INFORMATION:
DISPOSE OF MATERIAL IN ACCORDANCE TO LOCAL, STATE AND FEDERAL REGULATIONS
AND ORDINANCES. DO NOT ALLOW TO ENTER STORM DRAINS OR SEWER SYSTEMS.


SECTION 14 - TRANSPORTATION INFORMATION 


DOT PROPER SHIPPING NAME: AEROSOLS

DOT TECHNICAL NAME: N.A.

DOT HAZARD CLASS: 2.1

DOT UN/NA NUMBER: UN1950

PACKING GROUP: N.A.

HAZARD SUBCLASS: N.A.

RESP. GUIDE PAGE: 126


SECTION 15 - REGULATORY INFORMATION 


CERCLA - SARA HAZARD CATEGORY:
THIS PRODUCT HAS BEEN REVIEWED ACCORDING TO THE EPA "HAZARD CATEGORIES"
PROMULGATED UNDER SECTIONS 311 AND 312 OF THE SUPERFUND AMENDMENT AND
REAUTHORIZATION ACT OF 1986 (SARA TITLE III) AND IS CONSIDERED, UNDER
APPLICABLE DEFINITIONS, TO MEET THE FOLLOWING CATEGORIES:
IMMEDIATE HEALTH HAZARD, CHRONIC HEALTH HAZARD, FIRE HAZARD, PRESSURIZED
GAS HAZARD

SARA SECTION 313:
LISTED BELOW ARE THE SUBSTANCES (IF ANY) CONTAINED IN THIS PRODUCT THAT ARE
SUBJECT TO THE REPORTING REQUIREMENTS OF SECTION 313 OF TITLE III OF THE
SUPERFUND AMENDMENT AND REAUTHORIZATION ACT OF 1986 AND 40 CFR PART 372:

CHEMICAL NAME                     CAS NUMBER

XYLENE                             1330-20-7

TOLUENE                             108-88-3

ETHYLBENZENE                        100-41-4

COPPER CHROMITE BLACK             68186-91-4

TOXIC SUBSTANCES CONTROL ACT:
LISTED BELOW ARE THE SUBSTANCES (IF ANY) CONTAINED IN THIS PRODUCT THAT
ARE SUBJECT TO THE REPORTING REQUIREMENTS OF TSCA 12(B) IF EXPORTED FROM
THE UNITED STATES:

U.S. STATE REGULATIONS: AS FOLLOWS

NEW JERSEY RIGHT-TO-KNOW:
THE FOLLOWING MATERIALS ARE NON-HAZARDOUS, BUT ARE AMONG THE TOP FIVE
COMPONENTS IN THIS PRODUCT.
NONE

PENNSYLVANIA RIGHT-TO-KNOW:
THE FOLLOWING NON-HAZARDOUS INGREDIENTS ARE PRESENT IN THE PRODUCT AT
GREATER THAN 3%.
NONE

CALIFORNIA PROPOSITION 65:

WARNING!
THIS PRODUCT CONTAINS A CHEMICAL(S) KNOWN BY THE STATE OF CALIFORNIA TO
CAUSE CANCER.

WARNING!
THIS PRODUCT CONTAINS A CHEMICAL(S) KNOWN TO THE STATE OF CALIFORNIA TO
CAUSE BIRTH DEFECTS OR OTHER REPRODUCTIVE HARM.

INTERNATIONAL REGULATIONS: AS FOLLOWS

CANADIAN WHMIS:
THIS MSDS HAS BEEN PREPARED IN COMPLIANCE WITH CONTROLLED PRODUCT
REGULATIONS EXCEPT FOR THE USE OF THE 16 HEADINGS.

CANADIAN WHMIS CLASS:
AB5
D2A
D2B


SECTION 16 - OTHER INFORMATION 


HMIS RATINGS:
HEALTH              2*
FLAMMABILITY        4
REACTIVITY          0
PERSONAL PROTECTION X

REASON FOR REVISION: REGULATORY UPDATE

LEGEND:
N.A. - NOT APPLICABLE
N.E. - NOT ESTABLISHED
N.D. - NOT DETERMINED

THE INFORMATION CONTAINED ON THIS MSDS HAS BEEN CHECKED AND SHOULD BE
ACCURATE. HOWEVER, IT IS THE RESPONSIBILITY OF THE USER TO COMPLY WITH
ALL FEDERAL, STATE, AND LOCAL LAWS AND REGULATIONS.