Common Name: LITHIUM PRIMARY BATTERY
Manufacturer: ZHONGYIN (NINGBO) BATTERY CHINA
SDS Revision Date: (No Date)
SDS Format: No Format Specified
   
Grainger Item Number(s): 5PT96
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - PRODUCT IDENTIFICATION 
SECTION II - HAZARDOUS INGREDIENTS 
SECTION III - PHYSICAL / CHEMICAL CHARACTERISTICS 
SECTION IV - FIRE AND EXPLOSION HAZARD DATA 
SECTION V - REACTIVITY DATA 
SECTION VI - HEALTH HAZARD DATA 
SECTION VII - FIRST AID MEASURES 
SECTION VIII - FIRE AND EXPLOSION HAZARD DATA 
SECTION IX - ACCIDENTAL RELEASE OR SPILLAGE 
SECTION X - HANDLING AND STORAGE 
SECTION XI - EXPOSURE CONTROLS / PERSON PROTECTION 
SECTION XII - ECOLOGICAL INFORMATION 
SECTION XIII - DISPOSAL METHOD 
SECTION XIV - TRANSPORTATION INFORMATION 
SECTION XV - REGULATORY INFORMATION 
SECTION XVI - OTHER INFORMATION 
SECTION XVII - MEASURES FOR FIRE EXTINCTION 



PAIRDEER(R*)

MSDS

LITHIUM PRIMARY BATTERY

MATERIAL SAFETY DATA SHEET

ZHONGYIN NINGBO BATTERY CO., LTD.
128 XINGGUANG ROAD, HI-TECH PARK
NINGBO
P.R. CHINA

P.C.: 315011

TEL: +86 574 87491087/87493214

FAX: +86 574 87493903

WWW.SONLUK.COM


SECTION I - PRODUCT IDENTIFICATION 


PRODUCT NAME: LITHIUM PRIMARY BATTERY.

NOMINAL VOLTAGE: 3V

CHEMICAL SYSTEM: LITHIUM / MANGANESE DIOXIDE

DESIGNED FOR RECHARGE:
YES ( )
NO  (X)


SECTION II - HAZARDOUS INGREDIENTS 


THE BATTERY IS NOT DANGEROUS TO HUMAN OR ENVIRONMENT. CADMIUM, LEAD, AND
MERCURY OR OTHER DANGEROUS CHEMICALS ARE NOT INCLUDED IN THE BATTERY.

HAZARDOUS COMPONENTS:

DESCRIPTION          APPROXIMATE % OF TOTAL WEIGHT

MERCURY              NIL       WT%

CADMIUM              NIL       WT%

METALLIC LITHIUM     1.2-3.3   WT%

NOTE:
NIL MEANS NOT INCLUDED.
N.A. MEANS NOT APPLICABLE


SECTION III - PHYSICAL / CHEMICAL CHARACTERISTICS 


BOILING POINT: N.A.

SPECIFIC GRAVITY (H2O=1): N.A.

VAPOR PRESSURE (MMHg): N.A.

MELTING POINT: N.A.

VAPOR DENSITY (AIR=1): N.A.

EVAPORATION RATE (BUTYL ACETATE: N.A.

SOLUBILITY IN WATER: N.A.

APPEARANCE AND ODOR: CYLINDRICAL OR BUTTON SHAPE, ODORLESS


SECTION IV - FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): N.A.

FLAMMABLE LIMITS:
LEL: N.A.
UEL: N.A.

EXTINGUISHING MEDIA: N.A.

SPECIAL FIRE FIGHTING PROCEDURES: N.A.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
DO NOT DISPOSE OF BATTERY IN FIRE - MAY CAUSE EXPLOSION

DO NOT SHORT-CIRCUIT BATTERY - MAY CAUSE BURNS.


SECTION V - REACTIVITY DATA 


STABILITY:
UNSTABLE ( )
STABLE   (X)

CONDITIONS TO AVOID:

INCOMPATIBILITY (MATERIALS TO AVOID):

HAZARDOUS DECOMPOSTION OR BYPRODUCTS:

HAZARDOUS POLYMERIZATION:
MAY OCCUR      ( )
WILL NOT OCCUR (X)

CONDITIONS TO AVOID:


SECTION VI - HEALTH HAZARD DATA 


IN CASE OF ELECTROLYTE LEAKAGE, SKIN WILL BE ITCHY WHEN CONTAMINATED WITH
ELECTROLYTE.

IN CONTACT WITH ELECTROLYTE CAN CAUSE SEVERE IRRITATION AND CHEMICAL
BURNS

INHALATION OF ELECTROLYTE VAPORS MAY CAUSE IRRITATION OF THE UPPER
RESPIRATORY TRACT AND LUNGS.


SECTION VII - FIRST AID MEASURES 


FIRST AID PROCEDURES:
IF ELECTROLYTE LEAKAGE OCCURS AND MAKES CONTACT WITH SKIN, WASH WITH PLENTY
OF WATER IMMEDIATELY

IF ELECTROLYTE COMES INTO CONTACT WITH EYES, WASH WITH COPIOUS AMOUNTS OF
WATER FOR FIFTEEN (15) MINUTES, AND CONTACT A PHYSICIAN.

IF ELECTROLYTE VAPORS ARE INHALED, PROVIDE FRESH AIR AND SEEK MEDICAL
ATTENTION IF RESPIRATORY IRRITATION DEVELOPS. VENTILATE THE CONTAMINATED
AREA.


SECTION VIII - FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): N.A.

IGNITION TEMP.: N.A.

FLAMMABLE LIMITS: N.A.

LEL: N.A.
UEL: N.A.

EXTINGUISHING MEDIA: CARBON DIOXIDE, DRY CHEMICAL OR FOAM EXTINGUISHERS

SPECIAL FIRE FIGHTING PROCEDURES: N.A.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
DO NOT DISPOSE OF BATTERY IN FIRE - MAY EXPLODE.
DO NOT SHORT-CIRCUIT BATTERY - MAY CAUSE BURNS.


SECTION IX - ACCIDENTAL RELEASE OR SPILLAGE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
BATTERIES THAT ARE LEAKAGE SHOULD BE HANDLED WITH RUBBER GLOVES.

AVOID DIRECT CONTACT WITH ELECTROLYTE.

WEAR PROTECTIVE CLOTHING AND A POSITIVE PRESSURE SELF-CONTAINED BREATHING
APPARATUS (SCBA).


SECTION X - HANDLING AND STORAGE 


SAFE HANDLING AND STORAGE ADVICE:

BATTERIES SHOULD BE HANDLED AND STORED CAREFULLY TO AVOID SHORT CIRCUITS.

DO NOT STORE IN DISORDERLY FASHION, OR ALLOW METAL OBJECTS TO BE MIXED WITH
STORED BATTERIES.

NEVER DISASSEMBLE A BATTERY.

DO NOT BREATHE CELL VAPORS OR TOUCH INTERNAL MATERIAL WITH BARE HANDS.

KEEP BATTERIES BETWEEN -30 C AND 35 C FOR PROLONG STORAGE.


SECTION XI - EXPOSURE CONTROLS / PERSON PROTECTION 


OCCUPATIONAL EXPOSURE LIMITS:
LTEP: N.A.
STEP: N.A.

RESPIRATORY PROTECTION (SPECIFY TYPE): N.A.

VENTILATION:
LOCAL EXHAUSTS: N.A.
SPECIAL: N.A.
MECHANICAL(GENERAL): N.A.
OTHER: N.A.

PROTECTIVE GLOVE: N.A.

EYE PROTECTION: N.A.

OTHER PROTECTIVE CLOTHING OR EQUIPMENT: N.A.

WORK/HYGIENIC PRACTICE: N.A.


SECTION XII - ECOLOGICAL INFORMATION 


N.A


SECTION XIII - DISPOSAL METHOD 


DISPOSE OF THE BATTERIES ACCORDING TO THE GOVERNMENT REGULATIONS.


SECTION XIV - TRANSPORTATION INFORMATION 


PAIRDEER LITHIUM CELLS AND BATTERIES ARE NOT SUBJECT TO THE REQUIREMENTS OF
THE U.S. HAZARDOUS MATERIALS REGULATIONS PURSUANT TO 49 CFR 173.185(B),
IATA DANGEROUS GOODS REGULATIONS PURSUANT TO SPECIAL PROVISION A45, AND
IMDG CODE PURSUANT TO SPECIAL PROVISION 188. EACH PAIRDEER CELL OR BATTERY
HAS BEEN TESTED UNDER PROVISIONS OF THE UN MANUAL OF TESTS AND CRITERIA,
PART III, SUB-SECTION 38.3. IF PAIRDEER LITHIUM CELLS ARE USED TO CONSTRUCT
BATTERY PACKS, THE ASSEMBLER OF THAT PACK IS RESPONSIBLE TO ENSURE THE
BATTERY HAS BEEN TESTED IN ACCORDANCE WITH THE REQUIREMENTS CONTAINED IN
THE UN MANUAL OF TESTS AND CRITERIA AND SHIPPED IN ACCORDANCE WITH
APPLICABLE REGULATIONS. BATTERIES MUST BE PACKAGED AND OFFERED FOR
TRANSPORTATION IN A MANNER THAT PREVENTS THE DANGEROUS EVOLUTION OF HEAT
(FOR EXAMPLE, BY THE EFFECTIVE INSULATION OF EXPOSED TERMINALS) AND
PROTECTS AGAINST SHORT CIRCUITS.

THE INTERNATIONAL MARITIME DANGEROUS GOODS CODE (IMDG) REGULATE THEM FOR
OCEAN TRANSPORTATION UNDER SPECIAL PROVISION 304 WHICH SAYS:
BATTERIES, DRY, CONTAINING CORROSIVE ELECTROLYTE WHICH WILL NOT FLOW OUT OF
THE BATTERY IF THE BATTERY CASE IS CRACKED ARE NOT SUBJECT TO THE PROVISION
OF THIS CODE PROVIDED THE BATTERIES ARE SECURELY PACKED AND PROTECTED
AGAINST SHORT-CIRCUITS

NON-DANGEROUS GOODS.

SUCH BATTERIES HAVE BEEN PACKED IN INNER PACKAGING IN SUCH A MANNER AS TO
EFFECTIVELY PREVENT SHORT CIRCUIT AND MOVEMENT THAT COULD LEAD TO SHORT
CIRCUIT.


SECTION XV - REGULATORY INFORMATION 


SPECIAL REQUIREMENT BE ACCORDING TO THE LOCAL REGULATORY.


SECTION XVI - OTHER INFORMATION 


THE DATA IN THIS MATERIAL SAFETY DATA SHEET RELATES ONLY TO THE SPECIFIC
MATERIAL DESIGNATED HEREIN.


SECTION XVII - MEASURES FOR FIRE EXTINCTION 


IN CASE OF FIRE, IT IS PERMISSIBLE TO USE ANY CLASS OF EXTINGUISHING MEDIUM
ON THESE BATTERIES OR THEIR PACKING MATERIAL. COOL EXTERIOR OF BATTERIES IF
EXPOSED TO FIRE TO PREVENT RUPTURE.

FIRE FIGHTERS SHOULD WEAR SELF-CONTAINED BREATHING APPARATUS.

VERSION: 02