Common Name: INSTANT COLD PACK
Manufacturer: SHANGHAI INTCO MEDICAL SUPPLY CHINA
SDS Revision Date: 9/10/2003
SDS Format: No Format Specified
   
Grainger Item Number(s): 14N215, 5ELU9, 8LAF2
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 - COMPOSITION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIREFIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROL / PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL CONSIDERATIONS 



MATERIAL SAFETY DATA SHEET

(MSDS)

DATE: 09-10-2003


SECTION 1 - PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT IDENTIFIER: INSTANT COLD PACK

PRODUCT USE:
FOR RELIEF OF PAIN AND SWELLING CAUSED BY SPRAINS, STRAINS CONTUSIONS,
MINOR BURNS, TOOTHACHES AND INSECT BITES.

MANUFACTURER:
SHANGHAI INTCO MEDICAL SUPPLY CO., LTD.
1036 SOUTH PU DONG RD.
SUITE 1703-1704 SHANGHAI P.R. 200120
CHINA


SECTION 2 - COMPOSITION ON INGREDIENTS 


HAZARDOUS INGREDIENTS                %               CAS NUMBER

AMMONIUM NITRATE                     40 - 70         6484-52-2

WATER                                30 - 60         7732-18-5


SECTION 3 - HAZARDS IDENTIFICATION 


ROUTES OF ENTRY: SKIN CONTACT; SKIN ABSORPTION; EYE CONTACT; INGESTION

EMERGENCY OVERVIEW:
DANGEROUS IF INGESTED, MAY INTERFERE WITH THE CIRCULATION AND OXYGEN
CAPACITY OF THE BLOOD.

POTENTIAL HEALTH EFFECTS:
PRODUCT MAY IRRITATE EYES AND SKIN CONTACT BUT IS UNLIKELY TO INJURE
TISSUE.


SECTION 4 - FIRST AID MEASURES 


SKIN CONTACT:
MAY CAUSE SKIN IRRITATION. WASH CONTAMINATED SKIN WITH SOAP AND WATER.
COVER IRRITATED SKIN WITH AN EMOLLIENT. IF IRRITATION PERSISTS, SEEK
MEDICAL ATTENTION.

EYE CONTACT:
IMMEDIATELY FLUSH EYES WITH RUNNING WATER FOR AT LEAST 15 MINUTES, KEEPING
EYELIDS OPEN. OBTAIN MEDICAL ATTENTION IF IRRITATION PERSISTS.

INHALATION:
LIQUID PRODUCT IS DIFFICULT TO INHALE. IF INHALED SEEK IMMEDIATE MEDICAL
ATTENTION.

INGESTION:
IF CONSCIOUS, HAVE THE PERSON DRINK SEVERAL GLASSES OF WATER OR MILK AND
INDUCE VOMITING. NEVER GIVE ANYTHING BY MOUTH TO AN UNCONSCIOUS PERSON.
LOWER HEAD SO THE VOMIT WILL NOT REENTER THE MOUTH AND THROAT. OBTAIN
MEDICAL ATTENTION.


SECTION 5 - FIREFIGHTING MEASURES 


FLAMMABILITY: YES

MEANS OF EXTINCTION:
CONTAINS OXIDIZING MATERIAL, COOL CONTAINING VESSELS WITH WATER JET TO
PREVENT PRESSURE BUILD-UP OR EXPLOSION. MATERIALS WILL NOT BURN.

FIRE FIGHTING INSTRUCTIONS:
USE FLOODING QUANTITIES OF WATER. FIRE FIGHTERS SHOULD WEAR
POSITIVE-PRESSURE SELF-CONTAINED BREATH APPARATUS (SCBA) AND FULL FIRE
PROTECTIVE CLOTHING.


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


LEAK AND SPILL PROCEDURES:

SMALL SPILL:
USE APPROPRIATE TOOLS OR EQUIPMENTS TO CLEAN UP SPILLED LIQUID MATERIAL.
SMALL QUANTITIES CAN BE FLUSHED TO SANITARY SEWER.

LARGE SPILL:
PREVENT ADDITIONAL MATERIAL FROM BEING SPILLED. KEEP FROM ENTERING SEWERS,
WATERCOURSES, WELLS, ETC. PRODUCT WILL PROMOTE ALGAE GROWTH AND MAY DEGRADE
WATER QUALITY AND TASTE. NOTIFY DOWNSTREAM WATER USERS.


SECTION 7 - HANDLING AND STORAGE 


HANDLING PROCEDURES AND EQUIPMENT:
USE NO SHARP TOOLS TO HANDLE PACKAGES. DO NOT DROP PACKAGES. USE CARE WHEN
OPENING PACKAGES TO NOT DAMAGE INNER CONTAINERS.

KEEP AWAY FROM HEAT, COMBUSTIBLE MATERIALS AND REDUCING AGENTS. AVOID
CONTACT WITH SKIN AND EYES. DO NOT INGEST. KEEP AWAY FROM COMBUSTIBLE
MATERIALS. KEEP OUT OF REACH OF CHILDREN. KEEP AWAY FROM FOOD, DRINK AND
ANIMAL FEED.

STORAGE REQUIREMENTS:
STORE IN A COOL, DRY WELL VENTILATED AREA. KEEP AWAY FROM FOOD, DRINK AND
ANIMAL FEED. KEEP AWAY FROM COMBUSTIBLE MATERIALS. KEEP AWAY FROM
INCOMPATIBLE MATERIALS.


SECTION 8 - EXPOSURE CONTROL / PERSONAL PROTECTION 


EXPOSURE LIMITS: 10 MG/M3 FOR AMMONIUM NITRATE POWDER ACGIH TLV

SPECIFIC ENGINEERING CONTROLS (SUCH AS VENTILATION, ENCLOSED PROCESS):
USE APPROPRIATE PERSONAL PROTECTIVE EQUIPMENT AND CLOTHING TO AVOID SKIN
CONTACT WITH LIQUID PRODUCT. IF SPILLED PRODUCT DRIES OUT AVOID INHALING
THE DUST.

PERSONAL PROTECTIVE EQUIPMENT:
GLOVE; EYE; FOOTWEAR

IF CHECKED, SPECIFY TYPE

USE IMPERVIOUS GLOVES. WEAR SAFETY GLASSES OR SAFETY GOGGLES IF THERE IS A
RISK OF SPLASH AND SPILLAGE. USE SUITABLE WATERPROOF FOOTWEAR.


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


PHYSICAL STATE: LIQUID

ODOR AND APPEARANCE: LIQUID

ODOR THRESHOLD (PPM): ODORLESS

SOLUBILITY IN WATER: EASILY SOLUBLE IN WATER.


SECTION 10 - STABILITY AND REACTIVITY 


CHEMICAL STABILITY: YES

INCOMPATIBILITY WITH OTHER SUBSTANCES:

YES. HIGHLY REACTIVE WITH COMBUSTIBLE MATERIALS.

REACTIVE WITH REDUCING AGENTS, ORGANIC MATERIALS, METALS. SLIGHTLY REACTIVE
WITH ALKALIS.

NON-REACTIVE WITH ACIDS.

REACTIVITY, AND UNDER WHAT CONDITIONS?:
VERY SLIGHTLY TO SLIGHTLY CORROSIVE ALUMINUM, ZINC AND COOPER.
NON-CORROSIVE TO STEEL AND STAINLESS STEEL (304 AND 316)

HAZARDOUS DECOMPOSITION PRODUCTS:
THERE ARE NO HAZARDOUS DECOMPOSITION PRODUCTS. THE PRODUCTS DEGRADES TO
NITROGEN, HYDROGEN AND OXYGEN.


SECTION 11 - TOXICOLOGICAL INFORMATION 


EFFECTS OF ACUTE EXPOSURE:
TOXIC TO LIVESTOCK, WILDLIFE AND DOMESTIC ANIMALS IF DIRECTLY INGESTED. THE
PRODUCT ITSELF AND ITS PRODUCTS OF DEGRADATION ARE NOT HARMFUL UNDER NORMAL
CONDITIONS OF CAREFUL AND RESPONSIBLE USE.

EFFECTS OF CHRONIC EXPOSURE:
EXPOSURE CAN CAUSE HEADACHE, STOMACH PAINS, VOMITING AND DIARRHEA. PRODUCES
METHEMOGLOBINEMIA WHICH REDUCES OXYGEN SUPPLY TO CIRCULATING BLOOD.
ALTHOUGH PREDOMINATELY AFFECTING INFANTS, NITRATE INDUCED METHEMOGLOBINEMIA
HAS ALSO BEEN DOCUMENTED IN ADULTS.

IRRITANCY OF PRODUCT: CONTACT WITH SKIN AND EYES MAY BE IRRITATING.

SKIN SENSITIZATION: NOT EXPECTED

RESPIRATORY SENSITIZATION: NOT EXPECTED

CARCINOGENICITY-IARC:
DOES NOT DEMONSTRATE ANY RISK OF GASTROINTESTINAL CANCER.

CARCINOGENICITY-ACGIH:
DOES NOT DEMONSTRATE ANY RISK OF GASTROINTESTINAL CANCER.

REPRODUCTIVE TOXICITY: N/A

TERATOGENICITY: NOT EXPECTED

EMBRYOTOXICITY: N/A

MUTAGENICITY: NOT EXPECTED

NAME OF SYNERGISTIC PRODUCTS/EFFECTS: NONE KNOWN


SECTION 12 - ECOLOGICAL INFORMATION 


TOXICITY:
LOW TOXICITY FOR HUMANS OR ANIMALS UNDER NORMAL CONDITIONS OF USE. MAY BE
HARMFUL TO LIVESTOCK AND WILDLIFE IF INGESTED. CLEAN UP SPILLED MATERIAL TO
PREVENT ANIMAL EXPOSURE.

AQUATIC MARINE TOXICITY:
WILL RELEASE AMMONIUM IONS. AMMONIA IS A TOXIC HAZARD TO FISH. AVOID SPILLS
OR RELEASES TO WATERCOURSES. WILL DISPERSE WITH CURRENT. RELEASE TO
WATERCOURSES MAY CAUSE EFFECTS DOWNSTREAM FROM POINT OF RELEASE. THIS
MATERIAL IS NOT LISTED AS A MARINE POLLUTANT IN THE INTERNATIONAL MARITIME
DANGEROUS GOODS CODE.

BIOCHEMICAL OXYGEN DEMAND: N/A

CHEMICAL OXYGEN DEMAND: N/A

TOXICITY OF THE PRODUCTS OF DEGRADATION:
THE PRODUCT ITSELF AND IT PRODUCTS OF DEGRADATION ARE NOT HARMFUL UNDER
NORMAL CONDITION OF USE. AVOID SPILLS OR RELEASES TO WATERCOURSES.

SPECIAL REMARKS ON THE PRODUCTS OF DEGRADATION:
PRODUCT WILL PROMOTE ALGAE GROWTH AND MAY DEGRADE WATER QUALITY AND TASTE.
NOTIFY DOWNSTREAM WATER USERS. NITRATE IN POTABLE DRINKING WATER SHOULD BE
MAINTAINED BELOW 10 MG/L. WILL DISPERSE IN WATER.


SECTION 13 - DISPOSAL CONSIDERATIONS 


WASTE DISPOSAL OR RECYCLING:
RECYCLE TO PROCESS IN MANUFACTURING IF POSSIBLE. RECOVER AND PLACE MATERIAL
IN SUITABLE CONTAINER FOR INTENDED USE OR DISPOSAL. CALL FOR ASSISTANCE ON
DISPOSAL. ENSURE DISPOSAL IN COMPLIANCE WITH FEDERAL, PROVINCIAL AND LOCAL
REGULATIONS.