Common Name: IVY-RID
Manufacturer: TEXTILEASE MEDIQUE
MSDS Revision Date: 1/1/2001
   
Grainger Item Number(s): 3JNH9, 8ZLV5
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION I - PRODUCT IDENTIFICATION 
SECTION II - HAZARDOUS MATERIAL 
SECTION III - PHYSICAL DATA 
SECTION IV - FIRE AND EXPLOSION DATA 
SECTION V - HEALTH HAZARD INFORMATION 
SECTION VI - REACTIVITY DATA 
SECTION VII - SPILL OR LEAK PROCEDURES 
SECTION VIII - INDUSTRIAL HYGIENE CONTROL MEASURES 
SECTION IX - SPECIAL PRECAUTIONS 



TM
TEXTILEASE MEDIQUE
900 LIVELY BLVD
WOOD DALE, IL 60191
(630) 694-4100
1-800-634-7680

FAX: (630) 694-4140

MATERIAL SAFETY DATA SHEET

DATE: 2001


SECTION I - PRODUCT IDENTIFICATION 


TEXTILEASE MEDIQUE

ADDRESS:
900 LIVELY BLVD
WOOD DALE, IL 60191

EMERGENCY PHONE: 1-800-634-7680

TRADE NAME: IVY-RID

SYNONYMS: POISON IVY SPRAY


SECTION II - HAZARDOUS MATERIAL 


COMPONENT OR MATERIAL        % OF MIXTURE     CAS #               TWA
CHEMICAL NAME

BENZOCAINE, USP              2.0%                 94-09-7

BENZETHONIUM CHLORIDE         .065%              121-54-0

PVP/VA - 535                 4.5%              25086-89-9

SDA 40-2                    43.43%                64-17-5

A-46 HYDROCARBON            50.00%            68-476-86-8         1000 PPM

THIS PRODUCT CONTAINS THE FOLLOWING TOXIC CHEMICALS SUBJECT TO THE
REPORTING AND REQUIREMENTS OF SECTION 313 OF THE EMERGENCY PLANNING
AND COMMUNITY RIGHT-TO-KNOW ACT OF 1986 AND 40 CFR

CAS#                   CHEMICAL NAME              % BY WEIGHT


SECTION III - PHYSICAL DATA 


BOILING POINT: NA

SOLUBILITY IN H2O % BY WT.: DISPERSES WITH WATER

SPECIFIC GRAVITY H2O=1: 1.35

VAPOR PRESSURE IN CAN PSI AT 70F: 35

% VOLATILES BY VOL.: 78

pH: NA

APPEARANCE AND ODOR: COLORLESS LIQUID


SECTION IV - FIRE AND EXPLOSION DATA 


FLASH POINT (CLOSED CUP): N/A

FLAMMABLE EXPLOSIVE LIMITS:
LOWER: N/A
UPPER: 120F

EXTINGUISHING METHODS: USE WATER FOG, ALCOHOL FOAM, DRY CHEMICAL OR CO2

SPECIAL FIRE AND EXPLOSION PROCEDURES:
CLEAR FIRE AREA OF PROTECTED PERSONNEL. DO NOT ENTER CONFINED FIRE SPACE
WITHOUT FULL BUNKER GEAR, INCLUDING A POSITIVE PRESSURE NIOSH APPROVED
BREATHING APPARATUS. COOL FIRE EXPOSED CONTAINERS WITH WATER.

UNUSUAL FIRE AND EXPLOSION HAZARD:
MATERIAL IS HIGHLY VOLATILE. CONTAINERS EXPOSED TO INTENSE HEAT FROM FIRES
SHOULD BE COOLED WITH WATER TO PREVENT VAPOR PRESSURE BUILD-UP WHICH COULD
RESULT IN CONTAINER RUPTURE.


SECTION V - HEALTH HAZARD INFORMATION 


HEALTH HAZARD DATA:

ROUTES OF EXPOSURE:

INHALATION:
EXCESSIVE BREATHING OF VAPORS CAN CAUSE NASAL AND RESPIRATORY IRRITATION,
DIZZINESS, WEAKNESS, FATIGUE, NAUSEA, HEADACHE, POSSIBLE UNCONSCIOUSNESS,
AND EVEN ASPHYXIATION.

SKIN CONTACT:
PROLONGED CONTACT MAY CAUSE IRRITATION AND REDDENING OF THE SKIN.

EYE CONTACT: MAY CAUSE SEVERE IRRITATION WITH TEARING AND BLURRED VISION.

INGESTION:
CAN CAUSE SEVERE IRRITATION OF STOMACH AND INTESTINES, POSSIBLY RESULTING
IN NAUSEA AND VOMITING. ASPIRATION OF THIS MATERIAL INTO THE LUNGS CAN
OCCUR DURING SWALLOWING OR VOMITING.

EFFECTS OF OVEREXPOSURE:
OCCUPATIONAL EXPOSURE LIMIT NOT ESTABLISHED. NONE OF THE INGREDIENTS ARE
CONSIDERED CARCINOGENIC.

EMERGENCY AND FIRST AID PROCEDURES:

EYE:
FLUSH EYES WITH LARGE AMOUNTS OF WATER FOR AT LEAST 15 MINUTES.
IF IRRITATION PERSISTS, GET MEDICAL ATTENTION.

SKIN:
WASH OFF SKIN WITH SOAP AND WATER. REMOVE CONTAMINATED CLOTHING. LAUNDER
CONTAMINATED CLOTHING BEFORE RE-USE.

INGESTION:

ASPIRATION HAZARD:
DO NOT INDUCE VOMITING OR GIVE ANYTHING BY MOUTH BECAUSE THIS MATERIAL
CAN ENTER THE LUNGS AND CAUSE SEVERE LUNG DAMAGE. IF VICTIM IS DROWSY
OR UNCONSCIOUS, PLACE ON THE LEFT SIDE WITH THE HEAD DOWN. IF POSSIBLE,
DO NOT LEAVE VICTIM UNATTENDED. SEEK MEDICAL ATTENTION

INHALATION:
REMOVE AFFECTED PERSON TO FRESH AIR. IF BREATHING IS DIFFICULT, ADMINISTER
OXYGEN. IF BREATHING HAS STOPPED GIVE ARTIFICIAL RESPIRATION. KEEP PERSON
WARM, QUIET AND GET MEDICAL ATTENTION.

NOTES TO PHYSICIAN:


SECTION VI - REACTIVITY DATA 


CONDITION CONTRIBUTING TO INSTABILITY: STABLE

INCOMPATIBILITY: AVOID CONTACTS WITH STRONG OXIDIZING AGENTS

HAZARDOUS DECOMPOSITION PRODUCTS: OXIDES OF CARBON, ALDEHIDES, AND ACIDS

CONDITIONS CONTRIBUTING TO HAZARDOUS POLYMERIZATION:
HAZARDOUS POLYMERIZATION WILL NOT OCCUR.


SECTION VII - SPILL OR LEAK PROCEDURES 


STEPS TO BE TAKEN IF MATERIAL IS RELEASED OR SPILLED:

NEUTRALIZING CHEMICAL:
SOAK UP ON ABSORBENT MATERIAL (SAND, CLAY, FLOOR ABSORBENT, ETC.)

WASTE DISPOSAL METHOD:
AEROSOL CONTAINER, MAKE SURE EMPTY BEFORE DISPOSING CONSULT CURRENT LOCAL,
STATE AND FEDERAL REGULATIONS


SECTION VIII - INDUSTRIAL HYGIENE CONTROL MEASURES 


VENTILATION REQUIREMENTS:
MECHANICAL VENTILATION SHOULD BE USED TO MAINTAIN EXPOSURE BELOW OSHA TWA'S

SPECIFIC PERSONAL PROTECTIVE EQUIPMENT:

RESPIRATORY (SPECIFIC IN DETAIL):
IF TWA IS EXCEEDED, USE A NIOSH/MSHA APPROVED RESPIRATOR

EYE: OSHA-APPROVED SAFETY GLASSES, GOGGLES, OR FACE SHIELD

GLOVES: YES, CHEMICAL RESISTANT GLOVES.

OTHER CLOTHING AND EQUIPMENT:
TO PREVENT REPEATED OR PROLONGED SKIN CONTACT, WEAR IMPERVIOUS CLOTHING AND
BOOTS.


SECTION IX - SPECIAL PRECAUTIONS 


PRECAUTIONARY STATEMENTS: DO NOT SPRAY TOWARD EYES OR MOUTH.

OTHER HANDLING AND STORAGE REQUIREMENTS:
CONTENTS UNDER PRESSURE. DO NOT EXPOSE TO OPEN FLAME OR TEMPERATURES
EXCEEDING 120F

DEPARTMENT OF TRANSPORTATION INFORMATION:
PROPER NAME: MEDIQUE IVY-RID SPRAY
HAZARD CLASS: ORM-D