Common Name: LITHIUM ION BATTERY
Manufacturer: SANYO ELECTRIC JAPAN
SDS Revision Date: 3/1/2006
SDS Format: No Format Specified
   
Item Number(s): 36H082, 36H083, 36H084, 36H085, 38D144, 38D146, 38D147, 38D148, 38D149, 38D150, 38D151, 38D152, 38D153, 38D154, 38D155, 8F868
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - PRODUCT INFORMATION 
SECTION II - COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION III - PHYSICAL DATA 
SECTION IV - FIRE AND EXPLOSION HAZARD DATA 
SECTION V - HEALTH HAZARD DATA 
SECTION VI - REACTIVITY DATA 
SECTION VII - SAFE HANDLING AND USE 
SECTION VIII CONTROL MEASURES 
SECTION IX - RECYCLING AND DISPOSAL 
SECTION X - TRANSPORTATION 



PRODUCT INFORMATION AND DATA SHEET

THIS PRODUCT IS A MANUFACTURED ARTICLE AS DESCRIBED IN 29 CFR 1910.1200
AND IS NOT SUBJECT TO OSHA'S HAZARD COMMUNICATION STANDARD REQUIREMENTS
FOR PREPARATION OF MATERIAL SAFETY DATA SHEETS (MSDS).

SANYO BATTERIES
SANYO ENERGY (USA) CORP.
2055 SANYO AVE.
SAN DIEGO, CA 92154

TELEPHONE NO.: (619) 661-4888

WWW.SANYOBATTERIES.COM

MANUFACTURER'S NAME:
SANYO ELECTRIC CO., LTD.
TOKONABE-CHO KASAI-CITY, HYOGO 675-2332
JAPAN

TELEPHONE NO.: 0790-43-2043

IN CASE OF EMERGENCY CONTACT:
CHEMTREC AT: (800) 424-9300


SECTION I - PRODUCT INFORMATION 


PRODUCT: LITHIUM ION BATTERY

DESIGNATED FOR RECHARGE?:
(X) YES
( ) NO

CHEMICAL SYSTEM: LITHIUM ION

MODEL: CYLINDRICAL AND PRISMATIC TYPE CELLS


SECTION II - COMPOSITION / INFORMATION ON INGREDIENTS 


THE INGREDIENTS ARE CONTAINED IN A HERMETICALLY SEALED CASE, DESIGNED TO
WITHSTAND TEMPERATURES AND PRESSURES ENCOUNTERED DURING NORMAL USE. AS A
RESULT, DURING NORMAL USE, HAZARDOUS MATERIALS ARE FULLY CONTAINED INSIDE
THE BATTERY. THE BATTERY SHOULD NOT BE OPENED OR EXPOSED TO HEAT BECAUSE
EXPOSURE TO THE FOLLOWING INGREDIENTS CONTAINED WITHIN COULD BE HARMFUL
UNDER SOME CIRCUMSTANCES. THE FOLLOWING INFORMATION IS PROVIDED FOR THE
USER'S INFORMATION ONLY.

CHEMICAL NAME            CAS NO.      PEL               TLV

LITHIUM COBALTATE        12190-79-3   NONE ESTABLISHED  NONE ESTABLISHED
(LiCoO2)

GRAPHITE (C)              7782-42-5   2.5 MG/M3         2.5 MG/M3
                                      (AS DUST)         (AS DUST)

ORGANIC SOLVENT                       NONE ESTABLISHED  NONE ESTABLISHED

LITHIUM SALT                          NONE ESTABLISHED  NONE ESTABLISHED

POLYVYNILIDENE           24937-79-9   NONE ESTABLISHED  NONE ESTABLISHED
DIFLUORIDE (PVdF)

WEIGHT OF LITHIUM PER CELL: 0g.
THERE IS NO METALLIC LITHIUM IN THE LITHIUM ION BATTERY.


SECTION III - PHYSICAL DATA 


SPECIFIC GRAVITY (H2O=1):
LiCoO2: 4.95
GRAPHITE: 2.09-2.2

APPEARANCE AND ODOR:
LiCoO2 IS A BLACK, ODORLESS POWDER.
C IS A BLACK, ODORLESS POWDER.
ORGANIC SOLVENT IS A COLORLESS OR LIGHT YELLOW LIQUID.
LITHIUM SALT IS A WHITE, CRYSTALLINE AND ODORLESS POWDER.

MELTING POINT (DEG. C): LiCoO2 ABOUT 1130 C


SECTION IV - FIRE AND EXPLOSION HAZARD DATA 


EXTINGUISHING MEDIA: WATER

FLAMMABLE LIMITS: NOT AVAILABLE


SECTION V - HEALTH HAZARD DATA 


ROUTES OF ENTRY:
INHALATION: YES
SKIN: YES
INGESTION: YES

HEALTH HAZARDS (ACUTE AND CHRONIC):
THESE CHEMICALS ARE CONTAINED IN A SEALED CAN. RISK OF EXPOSURE OCCURS
ONLY IF THE BATTERY IS MECHANICALLY OR ELECTRICALLY ABUSED. THE MOST
LIKELY RISK IS AN ACUTE EXPOSURE WHEN THE GAS RELEASE VENT WORKS.
ORGANIC SOLVENT HAS SLIGHT TOXICITY AND CAN IRRITATE SKIN AND EYES.
LITHIUM SALT IS IRRITATING TO SKIN, EYES AND MUCOUS MEMBRANES AND
SHOULD BE AVOIDED.

CARCINOGENICITY:
NTP: NONE
IARC MONOGRAPH: NONE
OSHA REGULATED: NONE

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
AN ACUTE EXPOSURE WILL NOT GENERALLY AGGRAVATE ANY MEDICAL CONDITION.

EMERGENCY AND FIRST AID PROCEDURES:
IN CASE OF SKIN CONTACT WITH CONTENTS OF BATTERY, FLUSH IMMEDIATELY WITH
WATER. FOR EYE CONTACT, FLUSH WITH COPIOUS AMOUNTS OF WATER FOR 15
MINUTES. DO NOT INHALE LEAKED MATERIAL. IF IRRITATION PERSISTS, GET
MEDICAL HELP.


SECTION VI - REACTIVITY DATA 


STABILITY: STABLE

CONDITIONS TO AVOID: DO NOT HEAT, DISASSEMBLE OR OVERCHARGE.

HAZARDOUS DECOMPOSITION OR BY-PRODUCTS: N/A

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.


SECTION VII - SAFE HANDLING AND USE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
THE PREFERRED RESPONSE IS TO LEAVE THE AREA AND ALLOW THE BATTERIES TO COOL
AND THE VAPORS TO DISSIPATE. AVOID SKIN AND EYE CONTACT OR INHALATION OF
VAPORS. REMOVE SPILLED LIQUID WITH ABSORBENT AND INCINERATE.

WASTE DISPOSAL METHOD:
OPEN CELLS SHOULD BE DISPOSED OF IN ACCORDANCE WITH LOCAL REGULATIONS

PRECAUTIONS TO BE TAKEN IN HANDLING AND STORING:
AVOID MECHANICAL OR ELECTRICAL ABUSE. BATTERIES MAY EXPLODE OR CAUSE BURNS,
IF DISASSEMBLED, CRUSHED OR EXPOSED TO FIRE OR HIGH TEMPERATURES. DO NOT
SHORT OR INSTALL WITH INCORRECT POLARITY.


SECTION VIII CONTROL MEASURES 


RESPIRATORY PROTECTION (SPECIFY TYPE):
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

VENTILATION: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

PROTECTIVE GLOVES: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

EYE PROTECTION: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

OTHER PROTECTIVE CLOTHING OR EQUIPMENT:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.


SECTION IX - RECYCLING AND DISPOSAL 


SANYO ENCOURAGES BATTERY RECYCLING. OUR LITHIUM ION BATTERIES ARE
RECYCLABLE THROUGH THE RECHARGEABLE BATTERY RECYCLING CORPORATION'S
(RBRC) CHARGE UP TO
RECYCLE!
PROGRAM. FOR INFORMATION CALL 1-800-8-BATTERY OR SEE THEIR WEBSITE AT
WWW.RBRC.ORG. LITHIUM ION BATTERIES MUST BE HANDLED IN ACCORDANCE WITH
ALL APPLICABLE STATE AND FEDERAL LAWS AND REGULATIONS.

RECYCLE
RBRC
NI-Cd
1.800.822.8837

DO NOT INCINERATE OR SUBJECT BATTERY CELLS TO TEMPERATURES IN EXCESS OF
212 F. SUCH TREATMENT CAN VAPORIZE THE LIQUID ELECTROLYTE CAUSING CELL
RUPTURE. INCINERATION MAY RESULT IN CADMIUM EMISSIONS.


SECTION X - TRANSPORTATION 


SANYO LITHIUM ION CELLS AND BATTERIES ARE NOT SUBJECT TO THE
REQUIREMENTS OF THE U.S. HAZARDOUS MATERIALS REGULATIONS PURSUANT
TO 49 CFR 173.185(B), IATA DANGEROUS GOODS REGULATIONS PURSUANT TO
SPECIAL PROVISION A45, AND IMDG CODE PURSUANT TO SPECIAL PROVISION 188.
EACH SANYO CELL OR BATTERY HAS BEEN TESTED UNDER PROVISIONS OF THE UN
MANUAL OF TESTS AND CRITERIA, PART III, SUB-SECTION 38.3. IF SANYO
LITHIUM ION CELLS ARE USED TO CONSTRUCT BATTERY PACKS, THE ASSEMBLER
OF THAT PACK IS RESPONSIBLE TO ENSURE THE BATTERY HAS BEEN TESTED IN
ACCORDANCE WITH THE REQUIREMENTS CONTAINED IN THE UN MANUAL
OF TESTS AND CRITERIA AND SHIPPED IN ACCORDANCE WITH APPLICABLE
REGULATIONS.

BATTERIES MUST BE PACKAGED AND OFFERED FOR TRANSPORTATION IN A MANNER
THAT PREVENTS THE DANGEROUS EVOLUTION OF HEAT (FOR EXAMPLE, BY THE
EFFECTIVE INSULATION OF EXPOSED TERMINALS) AND PROTECTS AGAINST SHORT
CIRCUITS.

THE INFORMATION AND RECOMMENDATIONS SET FORTH ARE MADE IN GOOD FAITH AND
BELIEVED TO BE ACCURATE AS OF THE DATE OF PREPARATION. SANYO ENERGY CORP.
MAKES NO WARRANTY, EXPRESSED OR IMPLIED, WITH RESPECT TO THIS INFORMATION
AND DISCLAIMS ALL LIABILITIES FROM RELIANCE ON IT.

DATE OF LAST REVISION: MARCH 2006