Common Name: AA ALKALINE
Manufacturer: ZHONGYIN (NINGBO) BATTERY
SDS Revision Date: 4/4/2002
SDS Format: No Format Specified
   
Item Number(s): 1AGR7, 4FZK6
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. INGREDIENTS 
2. SAFETY GUIDELINES 



MATERIAL SAFETY DATA SHEET

80.116

EDITION: 29.05.2001

REPLACE EDITION: 04.04.2002

IEC: LR6

SYSTEM: Zn / MnO2 / KOH

VOLTS: 1.5 V

WEIGHT: 24G


1. INGREDIENTS 


1.1 ACTIVE MATERIALS        APPROXIMATE PERCENT OF TOTAL WEIGHT %

MANGANESE DIOXIDE (MnO2)    40.17

ZINC POWDER (Zn)            17.15

WATER (H2O)                  8.25

POTASSIUM HYDROXIDE (KOH)    5.47

CONDUCTIVE MATERIAL          2.68

1.2 PASSIVE MATERIALS   APPROXIMATE PERCENT OF TOTAL WEIGHT %

PIGMENTS:

ZnO                      0.476

BASS METAL:

Fe                      19.49

Ni-PLATING               0.3

BINDER:

POLYMERE                 0.336

ALLOY:

BRASS                    1.94

Bi                       0.00517

In                       0.00517

OTHERS:

PLASTIC                  0.77

LABEL                    0.987

METALLIC TRACES:

Hg                      <0.00001

Pb                      <0.0040

Cd                      <0.0001

THIS PRODUCT CONFORMS TO THE REQUIREMENTS OF IEC PUBLICATION 86.


2. SAFETY GUIDELINES 


GENERAL:
CAUTIONARY USER ADVICE SHOULD BE PROVIDED WHERE CONSIDERED APPROPRIATE.

2.1. KEEP BATTERIES OUT OF THE REACH OF CHILDREN, ESPECIALLY THOSE
BATTERIES FITTING WITHIN HE LIMITS OF THE TRUNCATED CYLINDER AS DEFINED IN
ISO/DP 812/2.2 PAGE 17

2.2. IN THE CASE OF INGESTION OF A CELL OR BATTERY THE PERSON INVOLVED
SHOULD SEEK MEDICAL ASSISTANCE PROMPTLY.

2.3 EQUIPMENT INTENDED FOR USE BY CHILDREN SHOULD HAVE BATTERY COMPARTMENTS
WHICH ARE TAMPER-PROOF.

2.4. THE CIRCUITS OF EQUIPMENT DESIGNED TO USE ALTERNATIVE POWER SUPPLIES
SHOULD BE SUCH AS TO ELIMINATE THE POSSIBILITY OF THE BATTERY BEING
CHARGED.

2.5. IT IS OF EXTREME IMPORTANCE THAT BATTERIES ARE INSERTED INTO EQUIPMENT
CORRECTLY WITH REGARD TO POLARITY (+ AND -).

2.6. DO NOT ATTEMPT TO REVIVE USED BATTERIES BY HEATING, CHARGING OR OTHER
MEANS.

2.7 DO NOT DISPOSE OF BATTERIES IN FIRE.
DO NOT DISMANTLE BATTERIES.

2.8. REPLACE ALL BATTERIES OF A SET AT THE SAME TIME.

NEWLY PURCHASED BATTERIES SHOULD NOT BE MIXED WITH PARTIALLY EXHAUSTED
ONES.

BATTERIES OF DIFFERENT ELECTROCHEMICAL SYSTEMS, GRADES OR BRANDS SHOULD NOT
BE MIXED.

FAILURE TO OBSERVE THESE PRECAUTIONS MAY RESULT IN SOME BATTERIES IN A SET
BEING DRIVEN

BEYOND THEIR NORMAL EXHAUSTION POINT AND THUS INCREASE THE POSSIBILITY OF
LEAKAGE.

2.0. DO NOT SHORT-CIRCUIT BATTERIES.