Common Name: QUARTZ METAL HALIDE LAMPS - QMH
Manufacturer: GE CONSUMER & INDUSTRIAL LIGHTING
SDS Revision Date: 3/1/2009
SDS Format: No Format Specified
   
Item Number(s): 1C251, 1C263, 1C279, 1C344, 1C347, 1C854, 1E099, 1E279, 1E637, 1E639, 1E641, 1E643, 1E671, 1E674, 1E686, 1E690, 1E692, 1E694, 1F276, 1F278, 1F346, 1F348, 1F396, 1F398, 1G980, 1K015, 1K425, 1MM51, 1MM55, 1PCY8, 1PCY9, 1PCZ1, 1PCZ2, 1PCZ3, 1PCZ4, 1PCZ5, 1RD93, 1RF30, 1RF31, 1TJP9, 1TJR1, 1TJR2, 1TJR3, 1TJR4, 1TJR5, 1TJR6, 1TJR7, 1TJR8, 1TJT1, 1TJT2, 1TJT3, 1VZ60, 2DZW7, 2DZW8, 2DZW9, 2DZX1, 2DZX2, 2DZX3, 2DZX4, 2DZX5, 2DZX6, 2DZX7, 2DZX8, 2DZX9, 2F103, 2F105, 2F109, 2F111, 2F192, 2F196, 2F202, 2F942, 2F944, 2F968, 2F970, 2PB27, 2PB28, 2TJ25, 2TJ26, 2TJ27, 2TJ28, 2TJ29, 2V658, 2V659, 2V712, 2VAD8, 2VAD9, 2XKW9, 2XKX1, 2XKX2, 2XKX5, 2XKX6, 2XKX7, 2YGD2, 2YGD3, 2YGD4, 2YGD5, 2YGD6, 2YGD7, 2YGD8, 2YGD9, 2YGE1, 2YGE2, 2YGE3, 2YGE4, 2YGE5, 2YGE6, 2YGE7, 2YGE8, 2YGE9, 3APK1, 3APK2, 3APK3, 3APK4, 3DXR7, 3DXR8, 3DXR9, 3DXT1, 3DXT2, 3DXT3, 3DXT4, 3DXT5, 3JJ92, 3JJ96, 3JJ97, 3JK01, 3JK02, 3JK41, 4DA14, 4DA27, 4LV87, 4LV88, 4PL04, 4PL05, 4PL06, 4PL07, 4PL08, 4V484, 4V516, 4V518, 4V550, 4V561, 4V565, 4V596, 4V603, 4WW46, 4WW54, 4XMA5, 5CVK3, 5CVK4, 5CVK5, 5GTN0, 5GTN1, 5HB77, 5HB78, 5HB79, 5HB80, 5HB81, 5HB82, 5HB83, 5HB84, 5HB87, 5HB88, 5HB89, 5HB90, 5HB91, 5HB92, 5HB93, 5HB94, 5TB70, 5V658, 5V691, 5V978, 5XN33, 5XN44, 5XN58, 5XN59, 5XN60, 5XN61, 5XN64, 5XN65, 5XP29, 5XP46, 5XP47, 5XP48, 6V630, 6V698, 6V699, 6V746, 6V747, 6V748, 6V749, 6V751, 6V752, 6V753, 6V754, 6V755, 6V756, 6V757, 6V758, 6V759, 6XT44, 6XT76, 6XT77, 6XT89, 6XT90, 6XT91, 6XT92, 6XT93, 6XT94, 6XV24, 6XV25, 6XV27, 6XV28, 6XV41
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
I. PRODUCT IDENTIFICATION 
II. LAMP MATERIALS AND HAZARDOUS INGREDIENTS 
III. HEALTH CONCERNS 
IV. FIRE AND EXPLOSION DATA 
V. DISPOSAL CONCERNS 



MATERIAL SAFETY DATA SHEETS (MSDS)

GE

GE CONSUMER & INDUSTRIAL - LIGHTING

LAMP MATERIAL INFORMATION SHEET - QUARTZ METAL HALIDE LAMP

INFORMATION AND APPLICABILITY:
THE MATERIAL SAFETY DATA SHEET (MSDS) REQUIREMENTS OF THE OCCUPATIONAL
SAFETY AND HEALTH ADMINISTRATION (OSHA) FOR REGULATED CHEMICALS UNDER, 21
CFR 1900.1200 ARE NOT APPLICABLE TO MANUFACTURED ARTICLES. GE METAL HALIDE
LAMPS ARE CLASSIFIED AS ARTICLES, AND THEREFORE EXEMPT FROM THIS
REGULATION.

NO MATERIAL CONTAINED IN A LAMP IS RELEASED DURING NORMAL USE AND
OPERATION.

THE FOLLOWING INFORMATION IS PROVIDED AS A COURTESY SERVICE TO OUR
CUSTOMERS. THIS LAMP MATERIAL INFORMATION SHEET CONTAINS APPLICABLE
MATERIAL SAFETY DATA SHEET INFORMATION.


I. PRODUCT IDENTIFICATION 


GE QUARTZ METAL HALIDE LAMPS - QMH:
APPLICABLE LAMP TYPES: MVR, MVT, MPR AND MXR

GE CONSUMER & INDUSTRIAL - LIGHTING
1975 NOBLE ROAD
NELA PARK
CLEVELAND, OH 44112

(216) 266-2222


II. LAMP MATERIALS AND HAZARDOUS INGREDIENTS 


GLASS:
THESE LAMPS CONSIST OF AN INNER QUARTZ ARC TUBE ENCLOSED IN AN OUTER
ENVELOPE OF HEAT-RESISTANT GLASS. DEPENDING ON THE LAMP TYPE, THE ENVELOPE
IS EITHER CLEAR, OR COATED WITH ONE OF TWO DIFFERENT MATERIALS. THE "MVR,"
"MVT" AND "MPR" LAMPS ARE COATED WITH A PHOSPHOR MATERIAL ON THE INSIDE OF
THE BULB, WHILE "MXR" LAMPS ARE COATED WITH A DIFFUSING MATERIAL.

PHOSPHOR:
THE PHOSPHOR USED ON THE INSIDE SURFACE OF THE OUTER ENVELOPE OF COATED
LAMPS CONSISTS OF YTTRIUM VANADATE PHOSPHATE. THIS MATERIAL, LIKE MOST
VANADIUM COMPOUNDS, IS RELATIVELY INSOLUBLE, AND APPEARS TO HAVE A MUCH
LOWER TOXICITY THAN VANADIUM PENTOXIDE, BUT MAY ELICIT SOME SIMILAR
SYMPTOMS AT HIGH EXPOSURE LEVELS.

EXCESSIVE INHALATION EXPOSURE TO VANADIUM PENTOXIDE MAY RESULT IN
IRRITATION OF THE NASAL PASSAGES AND RESPIRATORY TRACT, COUGH, DIFFICULTY
IN BREATHING, AND BRONCHITIS. HOWEVER, THE YTTRIUM VANADIUM PHOSPHATE FROM
THE BREAKAGE OF ONE OR A SMALL NUMBER OF LAMPS SHOULD NOT RESULT IN A
SIGNIFICANT EXPOSURE.

THE PHOSPHOR USED ON SOME LAMPS MAY ALSO CONTAIN THE ADDITION OF A SMALL
AMOUNT OF MAGNESIUM GERMANATE PHOSPHOR, A TOXICOLOGICALLY RELATIVELY INERT
MATERIAL.

THE MATERIAL USED AS A DIFFUSER IN THE "MXR" LAMPS IS SPECIALLY PREPARED
KAOLIN CLAY THAT CONTAINS NO CRYSTALLINE SILICA OR ASBESTOS AS IMPURITIES.
THESE TYPES OF CLAYS ARE GENERALLY CONSIDERED TO BE TOXICOLOGICALLY
RELATIVELY INERT MATERIALS.

ARC TUBE:
THE QUARTZ ARC TUBE CONTAINS A SMALL AMOUNT OF MERCURY, RANGING FROM LESS
THAN 5 MILLIGRAMS IN LOW WATTAGE LAMPS, UP TO 165 MG IN A 1500-WATT LAMP.
FURTHER, THE ARC TUBE CONTAINS A SMALL AMOUNT OF INERT GAS, ARGON, USED AS
A FILL GAS. ARGON IS A STABLE, CHEMICALLY INERT GAS. A FEW LAMP TYPES MAY
ALSO MIX A SMALL QUANTITY OF KR-85 WITH ARGON INSIDE THE ARC TUBE.
KRYPTON-85 IS USED TO IMPROVED IONIZATION AND STARTABILITY OF THE LAMP. IF
PRESENT, THE ACTIVITY LEVEL OF KR-85 WILL RANGE FROM 0.04 - 0.86
MICROCURIES ((MICRO)Ci) (1.57-31.9KBQ). QUARTZ ARC TUBES ALSO CONTAIN A
SMALL AMOUNT OF THORIUM EMBEDDED WITHIN THE TUNGSTEN ELECTRODE TO IMPROVE
STARTING PERFORMANCE. IF THORIUM IS PRESENT IN EITHER THE ELECTRODE OR
DOSE, THE TOTAL ACTIVITY OF TH-232 IS LESS THAN 0.004 (MICRO)Ci (0.148KBQ).
THERE WOULD BE NO SIGNIFICANT EXPOSURE FROM LAMP BREAKAGE.

ALSO CONTAINED WITHIN THE ARC TUBE ARE SMALL AMOUNTS OF OTHER MATERIALS,
REFERRED TO AS THE DOSE. THE COMBINATION OF THESE MATERIALS WITHIN THE
PLASMA DISCHARGE CREATES THE "WHITE LIGHT" OF QMH LAMPS. THESE COMPOUNDS
INCLUDES SODIUM AND SCANDIUM IODIDE, AND IN SOME CASES THORIUM IODIDE AND
CADMIUM. NONE OF THESE MATERIALS IS EXPECTED TO BE A HAZARD IN THE SMALL
QUANTITIES PRESENT IN THE ARC TUBE. THE COATING ON THE END(S) OF THE ARC
TUBE IS ALUMINUM OXIDE, A MATERIAL GENERALLY CONSIDERED TO HAVE A LOW ORDER
OF TOXICITY.

METALS:
INTERNALLY, THE SUPPORT WIRES USED IN THE LAMP CONSTRUCTION ARE MADE FROM
NICKEL-COATED IRON OR STAINLESS STEEL WHILE THE ELECTRODES ARE TUNGSTEN.
MANY OF THE METAL HALIDE TYPES WILL USE A BRASS BASE AND HAVE LEAD-SOLDERED
CONNECTIONS TO THAT BASE.

GETTERS:
GETTERS EMPLOYED WITHIN THE OUTER ENVELOPE ARE USE TO EXTEND THE LIFE OF
THE LAMP. QUARTZ METAL HALIDE LAMPS TYPICALLY USE EITHER, ZIRCONIUM
ALUMINUM OR BARIUM PEROXIDE GETTERS. THESE GETTERS ARE IN SOLID FORM AND DO
NOT PRESENT AN EXPOSURE RISK ON INTACT OR BROKEN LAMPS.

GASES:
THE OUTER ENVELOPE OF THE QMH LAMP IS FILLED WITH ARGON TO A
SUB-ATMOSPHERIC PRESSURE. ARGON IS A STABLE, CHEMICALLY INERT GAS.


III. HEALTH CONCERNS 


MERCURY EXPOSURE:
THE AIR CONCENTRATION OF MERCURY RESULTING FROM THE BREAKAGE OF ONE OR A
SMALL NUMBER OF LAMPS SHOULD RESULT IN NO SIGNIFICANT EXPOSURE TO THE
INDIVIDUAL. HOWEVER, IF BREAKING A LARGE NUMBER OF LAMPS FOR DISPOSAL,
APPROPRIATE MONITORING, CONTROLS, AND EQUIPMENT SHOULD BE IMPLEMENTED TO
CONTROL AIRBORNE MERCURY AND DUST LEVELS OR SURFACE CONTAMINATION. SUCH
WORK SHOULD BE DONE IN A WELL-VENTILATED AREA, AND LOCAL EXHAUST
VENTILATION OR PERSONAL PROTECTIVE EQUIPMENT MAY BE NEEDED. COMPLY WITH ALL
APPLICABLE REGULATIONS.

ULTRAVIOLET (UV) RADIATION:
THE QUARTZ ARC TUBE, WHEN OPERATING, GENERATES A CONSIDERABLE AMOUNT OF
ULTRAVIOLET RADIATION. THE UV IS FILTERED TO ACCEPTABLE LEVELS BY THE GLASS
OUTER ENVELOPE DURING NORMAL USE. HOWEVER, IF THE OUTER ENVELOPE IS BROKEN,
THE UV FILTERING IS LOST.

LAMPS HAVING ORDERING CODES BEGINNING WITH THE LETTERS "MVR", "MPR" OR
"MXR" HAVE THE FOLLOWING R-WARNING NOTICE REQUIRED UNDER FEDERAL REGULATION
21 CFR 1040.30:

"WARNING:
THIS LAMP CAN CAUSE SERIOUS SKIN BURN AND EYE INFLAMMATION FROM SHORTWAVE
ULTRAVIOLET RADIATION IF OUTER ENVELOPE OF THE LAMP IS BROKEN OR PUNCTURED.
DO NOT USE WHERE PEOPLE WILL REMAIN FOR MORE THAN A FEW MINUTES UNLESS
ADEQUATE SHIELDING OR OTHER SAFETY PRECAUTIONS ARE USED. LAMPS THAT WILL
AUTOMATICALLY EXTINGUISH WHEN THE OUTER ENVELOPE IS BROKEN OR PUNCTURED ARE
COMMERCIALLY AVAILABLE.

THIS LAMP CERTIFIED TO COMPLY WITH FDA RADIATION PERFORMANCE STANDARDS, 21
CFR SUBCHAPTER J.

USA: 21 CFR 1040.30

CANADA: SOR/80-381"

THE SELF-EXTINGUISHING METAL HALIDE LAMPS REFERRED TO ABOVE HAVE ORDER
CODES BEGINNING WITH THE LETTERS "MVT." IF THE OUTER GLASS ENVELOPE OF A
SAF-T-GARD LAMP IS BROKEN, ALTHOUGH THE ARC TUBE WILL HAVE
SELF-EXTINGUISHED, ITS SUPPORT STRUCTURE WILL STILL BE ELECTRICALLY
CONNECTED AND COULD PRESENT AN ELECTRICAL SHOCK HAZARD. THEREFORE,
REGARDLESS OF THE TYPE, IF THE OUTER ENVELOPE OF THE LAMP IS BROKEN, TURN
THE POWER OFF BEFORE REPLACING THE LAMPS.

FOR ADDITIONAL INFORMATION ON PROTECTION FROM UV RADIATION, VISIT THE FDA
WEBSITE FOR MORE INFORMATION:
HTTP://WWW.FDA.GOV/CDRH/RADHEALTH/PRODUCTS/URBURNS.HTML


IV. FIRE AND EXPLOSION DATA 


WARNING:
UNEXPECTED LAMP RUPTURE MAY CAUSE INJURY, FIRE, OR PROPERTY DAMAGE. DO NOT
USE LAMP BEYOND RATED LIFE AND ADHERE TO ALL APPLICABLE CAUTION AND WARNING
NOTICES. TO FURTHER REDUCE THE POSSIBILITY OF RUPTURE, TURN LAMP OFF AT
LEAST ONCE FOR 15 MINUTES PER WEEK.

AN ARC TUBE RUPTURE CAN BURST AND SHATTER THE OUTER GLASS BULB RESULTING IN
THE DISCHARGE OF GLASS FRAGMENTS AND EXTREMELY HOT QUARTZ PARTICLES (AS
HIGH AS 1100 DEG. C). THERE IS A RISK OF PERSONAL INJURY, PROPERTY DAMAGE,
BURNS, AND FIRE.

CAUTION AND WARNING NOTICES FOR EACH GE PRODUCT MAY BE VIEWED ONLINE AT
HTTP://WWW.GELIGHTING.COM/

FURTHER GUIDANCE ON THE APPLICATION AND USE OF QUARTZ METAL HALIDE LAMPS IS
AVAILABLE FROM NEMA DOCUMENT LSD 25, BEST PRACTICES FOR METAL HALIDE
LIGHTING SYSTEM, PLUS QUESTIONS AND ANSWERS ABOUT LAMP RUPTURES IN METAL
HALIDE LIGHTING SYSTEMS. LSD 25 MAY BE VIEWED ONLINE AT
HTTP://WWW.NEMA.ORG/


V. DISPOSAL CONCERNS 


TCLP:
A TOXICITY CHARACTERISTIC LEACHING PROCEDURE (TCLP) TEST CONDUCTED ON THE
LAMP FOR LEAD OR MERCURY COULD CAUSE THE LAMP TO BE CLASSIFIED AS A
HAZARDOUS WASTE. METAL HALIDE LAMPS USE LEAD SOLDER ON THE LAMP BASE AND
MERCURY IN THE ARC TUBE. THE LEAD SOLDER OR MERCURY VAPOR SHOULD POSE
LITTLE RISK OF EXPOSURE UNDER NORMAL USE AND HANDLING. WHILE SMALL NUMBERS
OF THESE LAMPS PLACED IN THE ORDINARY HOUSEHOLD TRASH SHOULD NOT
APPRECIABLY AFFECT THE NATURE OR METHOD OF DISPOSAL OF THE TRASH IN MOST
STATES, UNDER SOME CIRCUMSTANCES DISPOSAL OF THESE LAMPS IS REGULATED. MANY
BUSINESSES IN THE UNITED STATES MANAGE THESE LAMPS AS UNIVERSAL WASTES. YOU
SHOULD REVIEW YOUR WASTE HANDLING PRACTICES TO ASSURE THAT YOU DISPOSE OF
WASTE LAMPS PROPERLY.

SOME STATES REQUIRE ALL MERCURY CONTAINING LAMPS TO BE RECYCLED, CONTACT
YOUR STATE ENVIRONMENTAL DEPARTMENT FOR ANY REGULATIONS THAT MAY APPLY. TO
CHECK STATE REGULATIONS OR TO LOCATE A RECYCLER, GO TO
HTTP://WWW.LAMPRECYCLE.ORG/ OR CALL 1-800-435-4448.

QUARTZ METAL HALIDE LAMPS - LMIS

MARCH 2009 - SUPERSEDES AUGUST 2004

GE2014-9281