Common Name: ARCAIR ARCWATER ELECTRODE
Manufacturer: TWECO PRODUCTS
MSDS Revision Date: 1/1/2010
   
Grainger Item Number(s): 6TNK0
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1 - PRODUCT IDENTIFICATION AND USE 
SECTION 2 - HAZARDOUS INGREDIENTS 
SECTION 3 - PHYSICAL DATA 
SECTION 4 - FIRE AND EXPLOSION DATA 
SECTION 5 - REACTIVITY DATA 
SECTION 6 - HEALTH HAZARD DATA 
SECTION 7 - PRECAUTIONS FOR SAFE HANDLING AND USE 
SECTION 8 - CONTROL MEASURES 



MATERIAL SAFETY DATA SHEET

89-250-819/B


SECTION 1 - PRODUCT IDENTIFICATION AND USE 


PRODUCT IDENTIFIER: ARCAIR ARCWATER ELECTRODE

CATALOG NUMBERS: 42-059-006

PRODUCT USE: UNDERWATER ARC METAL REMOVAL

MANUFACTURERS NAME: TWECO PRODUCTS, INC.

STREET ADDRESS: 2800 AIRPORT ROAD
CITY: DENTON
STATE: TEXAS
ZIP CODE: 76207

EMERGENCY PHONE #: (940) 566-2000

PHONE NUMBER: (940) 566-2000

PREPARED BY: TERRY FULKS

DATE PREPARED: JULY 1989

DATE REVISED: JANUARY 1, 2010


SECTION 2 - HAZARDOUS INGREDIENTS 


HAZARDOUS INGREDIENTS  %/RANGE    CAS NUMBER  OSHA PEL        ACGIH TLV

COPPER (COATING)       APPR. 15   7440-50-8   0.2 MG/M3 FUME  0.2 MG/M3 FUME

SYNTHETIC GRAPHITE     APPR. 84   7440-44-0   3.5 MG/M3       3.5 MG/M3

PLASTICIZED VINYL      APPR. 1    COMPOUND    N.AP.           N.AP.

WHEN PLACED INTO UNDERWATER SERVICE, AN ELECTRIC ARC IS FORMED AS IN
WELDING, GENERATING INTENSE HEAT, ULTRA-VIOLET (UV) RAYS, FUMES AND GASES AS
IN CONVENTIONAL WELDING. WHEN USED AS INTENDED FOR UNDERWATER WELDING,
EXPOSURE TO UV RAYS AND ELECTRICAL SHOCK POTENTIAL ARE THE MOST LIKELY
SOURCES OF RISK TO HEALTH. WHEN NOT IN SERVICE, THE ELECTRODES POSE NO
SIGNIFICANT HAZARD.

SECTION 313. SUPPLIER INFORMATION:

THIS PRODUCT:
DOES     (X)
DOES NOT ( )

CONTAIN TOXIC CHEMICALS SUBJECT TO THE REPORTING REQUIREMENTS OF SECTION 313
OF THE EMERGENCY PLANNING AND COMMUNITY RIGHT-TO-KNOW ACT OF 1986 AND OF
40 CFR 372.

CAS NUMBER              CHEMICAL NAME          %

7440-50-8               COPPER                 APPROXIMATELY 15


SECTION 3 - PHYSICAL DATA 


PHYSICAL STATE: SOLID

ODOR AND APPEARANCE:
WHITE PLASTIC OVER COPPER-COATED CARBON ROD. NO NOTICEABLE ODOR.

VAPOR PRESSURE: N.APP.

VAPOR DENSITY (AIR = 1): N.APP.

EVAPORATION RATE:

BOILING POINT (FREEZING POINT) (MMHg): N.APP.
(DEGREE)F/C):
(DEGREE)F/C): N.APP.

pH: N.APP.

SPECIFIC GRAVITY: N.APP.

SOLUBILITY: INSOLUBLE


SECTION 4 - FIRE AND EXPLOSION DATA 


FLAMMABILITY:
YES ( )
NO  (X)

IF YES, MEANS OF EXTINCTION: DOES NOT READILY BURN

FLASHPOINT ((DEGREE) FLAMMABLE LIMIT F/C) AND METHOD: N.APP.

LEL: N.APP.
UEL: N.APP.

UNUSUAL FIRE AND EXPLOSION HAZARDS: NONE

N.APP: NON APPLICABLE
N.AV.: NOT AVAILABLE
N.EST.: NOT ESTABLISHED

N.F.P.A. RATING SYSTEM:
HEALTH       1
FLAMMABILITY 0
REACTIVITY   0
SPECIAL      NONE

0 - INSIGNIFICANT
1 - SLIGHT
2 - MODERATE
3 - HIGH
4 - EXTREME

WHMIS CLASSIFICATION: CLASS "D" DIVISION 2 SUB-DIVISION "G"


SECTION 5 - REACTIVITY DATA 


CHEMICAL STABILITY:
YES (X)
NO  ( )

IF NO, CONDITIONS TO AVOID: N.AP.

INCOMPATIBILITY WITH OTHER SUBSTANCES:
YES ( )
NO  (X)

IF YES, WHICH ONES?: NONE KNOWN

HAZARDOUS POLYMERIZATION:
WILL OCCUR     ( )
WILL NOT OCCUR (X)

CONDITIONS TO AVOID: N.AP.

HAZARDOUS DECOMPOSITION PRODUCTS:
SMALL AMOUNTS OF COPPER FUME ARE GENERATED DURING CUTTING OPERATIONS, BUT
POSE NO PROBLEM FOR THE DIVER/WELDER.


SECTION 6 - HEALTH HAZARD DATA 


ROUTE OF ENTRY:
SKIN CONTACT    ( )
SKIN ABSORPTION ( )
EYE CONTACT     ( )
INHALATION      ( )
INGESTION       ( )
U.V. EXPOSURE   (X)

EFFECTS OF ACUTE/CHRONIC EXPOSURE TO PRODUCT:
EXPOSURE TO UV RADIATION FROM THE CUTTING ARC CAN RESULT IN
KERATOCONJUNCTIVITIS, ALSO KNOWN AS WELDERS FLASH.

TOXICITY:
CARBON:
INTRAVENOUS MOUSE; LD50: 440 MG/KG

COPPER (FUME):
HUMAN, ORAL LDLO: 120 (MICRO)G/KG

REPRODUCTION:
CARBON:
SUBCUTANEOUS RAT; TDLO: 167 MG/KG (8D PREG)

COPPER:
ORAL, RAT:
TDLO: 1520 (MICRO)G/KG (22W PRE)
TDLO: 1210 (MICRO)G/KG (35W PRE)

CARCINOGENICITY: NOT LISTED

SIGNS AND SYMPTOMS OF EXPOSURE:
INFLAMMATION, BLURRED VISION AND HEADACHE

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE: NONE KNOWN

EMERGENCY AND FIRST AID PROCEDURES:
SEEK MEDICAL ATTENTION, PREFERABLY AN EYE SPECIALIST.


SECTION 7 - PRECAUTIONS FOR SAFE HANDLING AND USE 


LEAK AND SPILL PROCEDURE: PICK UP SPENT ENDS WHEN COOL

WASTE DISPOSAL METHOD: SOLID LANDFILL IF LOCAL REGULATIONS ALLOW.

PRECAUTIONS TO BE TAKEN IN HANDLING AND STORING: STORE IN DRY AREA

OTHER PRECAUTIONS:

CUTTING WARNINGS:

CAUTION!

ELECTRIC SHOCK CAN KILL. ARC RAYS CAN INJURE EYES. TRAIN THE OPERATOR NOT TO
TOUCH ELECTRICAL PARTS. WEAR AN UNDERWATER SUIT.


SECTION 8 - CONTROL MEASURES 


RESPIRATORY PROTECTION (SPECIFY TYPE):

AS APPLICABLE FOR UNDERWATER OPERATION GLOVES (SPECIFY): BUTYL RUBBER

RESPIRATOR (SPECIFY): AS REQUIRED FOR UNDERWATER OPERATIONS

EYE (SPECIFY): FILTER LENS FOR U.V. PROTECTION, #12 OR DARKER

FOOTWEAR (SPECIFY): N.AP

CLOTHING (SPECIFY):
SUIT CONSTRUCTED OF RUBBER TO MINIMIZE LIKELYHOOD FOR SHOCK

OTHER (SPECIFY): N.AP.

VENTILATION: AS REQUIRED FOR UNDERWATER OPERATIONS

MECHANICAL: AS REQUIRED FOR UNDERWATER OPERATIONS

OTHER: N.APP

WORK/HYGIENIC PRACTICES: TOP WATER PERSONNEL SHOULD AVOID SURFACING FUMES

THIS DATA IS OFFERED IN GOOD FAITH AS TYPICAL VALUES. THIS IS NEITHER AN
EXPRESSED NOR IMPLIED PRODUCT SPECIFICATION. RECOMMENDED HANDLING PROCEDURES
AND HYGIENE ARE BELIEVED TO BE ACCURATE, HOWEVER, THESE RECOMMENDATIONS
SHOULD BE REVIEWED IN THE SPECIFIC CONTEXT OF INTENDED USE AND DETERMINED
APPROPRIATE BY THE USER.