Common Name: RANDO HD 22 - 68
Manufacturer: CHEVRON TEXACO
SDS Revision Date: 1/15/2007
SDS Format: No Format Specified
   
Grainger Item Number(s): 10H743, 10H744, 10H746, 10H748, 10H749
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 COMPOSITION/INFORMATION ON INGREDIENTS 
SECTION 3 HAZARDS IDENTIFICATION 
SECTION 4 FIRST AID MEASURES 
SECTION 5 FIRE FIGHTING MEASURES 
SECTION 6 ACCIDENTAL RELEASE MEASURES 
SECTION 7 HANDLING AND STORAGE 
SECTION 8 EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 STABILITY AND REACTIVITY 
SECTION 11 TOXICOLOGICAL INFORMATION 
SECTION 12 ECOLOGICAL INFORMATION 
SECTION 13 DISPOSAL CONSIDERATIONS 
SECTION 14 TRANSPORT INFORMATION 
SECTION 15 REGULATORY INFORMATION 
SECTION 16 OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET


SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 


TEXACO RANDO(R*) HD 22 - 68

PRODUCT NUMBER(S): CPS221655, CPS221657, CPS221658, CPS221659

SYNONYMS:
TEXACO RANDO(R*) HD 22, TEXACO RANDO(R*) HD 32, TEXACO RANDO(R*) HD 46,
TEXACO RANDO(R*) HD 68

COMPANY IDENTIFICATION:
CHEVRON PRODUCTS COMPANY
A DIVISION OF CHEVRON U.S.A. INC.
6001 BOLLINGER CANYON ROAD
SAN RAMON, CA 94583
UNITED STATES OF AMERICA

WWW.CHEVRONLUBRICANTS.COM

TRANSPORTATION EMERGENCY RESPONSE:
CHEMTREC: (800) 424-9300 OR (703) 527-3887

HEALTH EMERGENCY:

CHEVRON EMERGENCY INFORMATION CENTER:
LOCATED IN THE USA. INTERNATIONAL COLLECT CALLS ACCEPTED. (800) 231-0623 OR
(510) 231-0623

PRODUCT INFORMATION:
EMAIL: LUBEMSDS@CHEVRON.COM
PRODUCT INFORMATION: 800-LUBE-TEK
MSDS REQUESTS: 800-414-6737


SECTION 2 COMPOSITION/INFORMATION ON INGREDIENTS 


COMPONENTS                                   CAS NUMBER     AMOUNT

HIGHLY REFINED MINERAL OIL (C15 - C50)       MIXTURE        90 - 100 % 

WEIGHT


SECTION 3 HAZARDS IDENTIFICATION 


IMMEDIATE HEALTH EFFECTS:

EYE: NOT EXPECTED TO CAUSE PROLONGED OR SIGNIFICANT EYE IRRITATION.

SKIN:
CONTACT WITH THE SKIN IS NOT EXPECTED TO CAUSE PROLONGED OR SIGNIFICANT
IRRITATION. NOT EXPECTED TO BE HARMFUL TO INTERNAL ORGANS IF ABSORBED 
THROUGH THE SKIN.

HIGH-PRESSURE EQUIPMENT INFORMATION:
ACCIDENTAL HIGH-VELOCITY INJECTION UNDER THE SKIN OF MATERIALS OF THIS TYPE
MAY RESULT IN SERIOUS INJURY. SEEK MEDICAL ATTENTION AT ONCE SHOULD AN
ACCIDENT LIKE THIS OCCUR. THE INITIAL WOUND AT THE INJECTION SITE MAY NOT
APPEAR TO BE SERIOUS AT FIRST; BUT, IF LEFT UNTREATED, COULD RESULT IN
DISFIGUREMENT OR AMPUTATION OF THE AFFECTED PART.

INGESTION: NOT EXPECTED TO BE HARMFUL IF SWALLOWED.

INHALATION:
NOT EXPECTED TO BE HARMFUL IF INHALED. CONTAINS A PETROLEUM-BASED MINERAL
OIL. MAY CAUSE RESPIRATORY IRRITATION OR OTHER PULMONARY EFFECTS FOLLOWING
PROLONGED OR REPEATED INHALATION OF OIL MIST AT AIRBORNE LEVELS ABOVE THE
RECOMMENDED MINERAL OIL MIST EXPOSURE LIMIT. SYMPTOMS OF RESPIRATORY
IRRITATION MAY INCLUDE COUGHING AND DIFFICULTY BREATHING.


SECTION 4 FIRST AID MEASURES 


EYE:
NO SPECIFIC FIRST AID MEASURES ARE REQUIRED. AS A PRECAUTION, REMOVE CONTACT
LENSES, IF WORN, AND FLUSH EYES WITH WATER.

SKIN:
NO SPECIFIC FIRST AID MEASURES ARE REQUIRED. AS A PRECAUTION, REMOVE 
CLOTHING AND SHOES IF CONTAMINATED. TO REMOVE THE MATERIAL FROM SKIN, USE 
SOAP AND WATER. DISCARD CONTAMINATED CLOTHING AND SHOES OR THOROUGHLY CLEAN 
BEFORE REUSE.

INGESTION:
NO SPECIFIC FIRST AID MEASURES ARE REQUIRED. DO NOT INDUCE VOMITING. AS A
PRECAUTION, GET MEDICAL ADVICE.

INHALATION:
NO SPECIFIC FIRST AID MEASURES ARE REQUIRED. IF EXPOSED TO EXCESSIVE LEVELS
OF MATERIAL IN THE AIR, MOVE THE EXPOSED PERSON TO FRESH AIR. GET MEDICAL
ATTENTION IF COUGHING OR RESPIRATORY DISCOMFORT OCCURS.

NOTE TO PHYSICIANS:
IN AN ACCIDENT INVOLVING HIGH-PRESSURE EQUIPMENT, THIS PRODUCT MAY BE
INJECTED UNDER THE SKIN. SUCH AN ACCIDENT MAY RESULT IN A SMALL, SOMETIMES
BLOODLESS, PUNCTURE WOUND. HOWEVER, BECAUSE OF ITS DRIVING FORCE, MATERIAL
INJECTED INTO A FINGERTIP CAN BE DEPOSITED INTO THE PALM OF THE HAND. WITHIN
24 HOURS, THERE IS USUALLY A GREAT DEAL OF SWELLING, DISCOLORATION, AND
INTENSE THROBBING PAIN. IMMEDIATE TREATMENT AT A SURGICAL EMERGENCY CENTER 
IS RECOMMENDED.


SECTION 5 FIRE FIGHTING MEASURES 


LEAKS/RUPTURES IN HIGH PRESSURE SYSTEM USING MATERIALS OF THIS TYPE CAN
CREATE A FIRE HAZARD WHEN IN THE VICINITY OF IGNITION SOURCES (EG. OPEN
FLAME, PILOT LIGHTS, SPARKS, OR ELECTRIC ARCS).

FIRE CLASSIFICATION:

OSHA CLASSIFICATION (29 CFR 1910.1200):
NOT CLASSIFIED BY OSHA AS FLAMMABLE OR COMBUSTIBLE.

NFPA RATINGS:
HEALTH       0
FLAMMABILITY 1
REACTIVITY   0

FLAMMABLE PROPERTIES:

FLASHPOINT: (CLEVELAND OPEN CUP) 150 DEG. C (302 DEG. F) (MIN)

AUTOIGNITION: NO DATA AVAILABLE

FLAMMABILITY (EXPLOSIVE) LIMITS (% BY VOLUME IN AIR):
LOWER: NOT APPLICABLE
UPPER: NOT APPLICABLE

EXTINGUISHING MEDIA:
USE WATER FOG, FOAM, DRY CHEMICAL OR CARBON DIOXIDE (CO2) TO EXTINGUISH
FLAMES.

PROTECTION OF FIRE FIGHTERS:

FIRE FIGHTING INSTRUCTIONS:
THIS MATERIAL WILL BURN ALTHOUGH IT IS NOT EASILY IGNITED. FOR FIRES
INVOLVING THIS MATERIAL, DO NOT ENTER ANY ENCLOSED OR CONFINED FIRE SPACE
WITHOUT PROPER PROTECTIVE EQUIPMENT, INCLUDING SELF-CONTAINED BREATHING
APPARATUS.

COMBUSTION PRODUCTS:
HIGHLY DEPENDENT ON COMBUSTION CONDITIONS. A COMPLEX MIXTURE OF AIRBORNE
SOLIDS, LIQUIDS, AND GASES INCLUDING CARBON MONOXIDE, CARBON DIOXIDE, AND
UNIDENTIFIED ORGANIC COMPOUNDS WILL BE EVOLVED WHEN THIS MATERIAL UNDERGOES
COMBUSTION.


SECTION 6 ACCIDENTAL RELEASE MEASURES 


PROTECTIVE MEASURES:
ELIMINATE ALL SOURCES OF IGNITION IN VICINITY OF SPILLED MATERIAL.

SPILL MANAGEMENT:
STOP THE SOURCE OF THE RELEASE IF YOU CAN DO IT WITHOUT RISK. CONTAIN 
RELEASE TO PREVENT FURTHER CONTAMINATION OF SOIL, SURFACE WATER OR 
GROUNDWATER. CLEAN UP SPILL AS SOON AS POSSIBLE, OBSERVING PRECAUTIONS IN 
EXPOSURE CONTROLS/PERSONAL PROTECTION. USE APPROPRIATE TECHNIQUES SUCH AS 
APPLYING NON-COMBUSTIBLE ABSORBENT MATERIALS OR PUMPING. WHERE FEASIBLE AND
APPROPRIATE, REMOVE CONTAMINATED SOIL. PLACE CONTAMINATED MATERIALS IN
DISPOSABLE CONTAINERS AND DISPOSE OF IN A MANNER CONSISTENT WITH APPLICABLE
REGULATIONS.

REPORTING:
REPORT SPILLS TO LOCAL AUTHORITIES AND/OR THE U.S. COAST GUARD'S NATIONAL
RESPONSE CENTER AT (800) 424-8802 AS APPROPRIATE OR REQUIRED.


SECTION 7 HANDLING AND STORAGE 


PRECAUTIONARY MEASURES:
DO NOT USE IN HIGH PRESSURE SYSTEMS IN THE VICINITY OF FLAMES, SPARKS AND 
HOT SURFACES. USE ONLY IN WELL VENTILATED AREAS. KEEP CONTAINER CLOSED.

GENERAL HANDLING INFORMATION:
AVOID CONTAMINATING SOIL OR RELEASING THIS MATERIAL INTO SEWAGE AND DRAINAGE
SYSTEMS AND BODIES OF WATER.

STATIC HAZARD:
ELECTROSTATIC CHARGE MAY ACCUMULATE AND CREATE A HAZARDOUS CONDITION WHEN
HANDLING THIS MATERIAL. TO MINIMIZE THIS HAZARD, BONDING AND GROUNDING MAY 
BE NECESSARY BUT MAY NOT, BY THEMSELVES, BE SUFFICIENT. REVIEW ALL 
OPERATIONS WHICH HAVE THE POTENTIAL OF GENERATING AND ACCUMULATING AN 
ELECTROSTATIC CHARGE AND/OR A FLAMMABLE ATMOSPHERE (INCLUDING TANK AND 
CONTAINER FILLING, SPLASH FILLING, TANK CLEANING, SAMPLING, GAUGING, SWITCH 
LOADING, FILTERING, MIXING, AGITATION, AND VACUUM TRUCK OPERATIONS) AND USE 
APPROPRIATE MITIGATING PROCEDURES. FOR MORE INFORMATION, REFER TO OSHA 
STANDARD 29 CFR 1910.106, 'FLAMMABLE AND COMBUSTIBLE LIQUIDS', NATIONAL 
FIRE PROTECTION ASSOCIATION (NFPA 77, 'RECOMMENDED PRACTICE ON STATIC 
ELECTRICITY', AND/OR THE AMERICAN PETROLEUM INSTITUTE (API) RECOMMENDED 
PRACTICE 2003, 'PROTECTION AGAINST IGNITIONS ARISING OUT OF STATIC, 
LIGHTNING, AND STRAY CURRENTS'.

CONTAINER WARNINGS:
CONTAINER IS NOT DESIGNED TO CONTAIN PRESSURE. DO NOT USE PRESSURE TO EMPTY
CONTAINER OR IT MAY RUPTURE WITH EXPLOSIVE FORCE. EMPTY CONTAINERS RETAIN
PRODUCT RESIDUE (SOLID, LIQUID, AND/OR VAPOR) AND CAN BE DANGEROUS. DO NOT
PRESSURIZE, CUT, WELD, BRAZE, SOLDER, DRILL, GRIND, OR EXPOSE SUCH 
CONTAINERS TO HEAT, FLAME, SPARKS, STATIC ELECTRICITY, OR OTHER SOURCES OF 
IGNITION. THEY MAY EXPLODE AND CAUSE INJURY OR DEATH. EMPTY CONTAINERS 
SHOULD BE COMPLETELY DRAINED, PROPERLY CLOSED, AND PROMPTLY RETURNED TO A 
DRUM RECONDITIONER OR DISPOSED OF PROPERLY.


SECTION 8 EXPOSURE CONTROLS/PERSONAL PROTECTION 


GENERAL CONSIDERATIONS:
CONSIDER THE POTENTIAL HAZARDS OF THIS MATERIAL (SEE SECTION 3), APPLICABLE
EXPOSURE LIMITS, JOB ACTIVITIES, AND OTHER SUBSTANCES IN THE WORK PLACE WHEN
DESIGNING ENGINEERING CONTROLS AND SELECTING PERSONAL PROTECTIVE EQUIPMENT.
IF ENGINEERING CONTROLS OR WORK PRACTICES ARE NOT ADEQUATE TO PREVENT
EXPOSURE TO HARMFUL LEVELS OF THIS MATERIAL, THE PERSONAL PROTECTIVE
EQUIPMENT LISTED BELOW IS RECOMMENDED. THE USER SHOULD READ AND UNDERSTAND
ALL INSTRUCTIONS AND LIMITATIONS SUPPLIED WITH THE EQUIPMENT SINCE 
PROTECTION IS USUALLY PROVIDED FOR A LIMITED TIME OR UNDER CERTAIN 
CIRCUMSTANCES.

ENGINEERING CONTROLS: USE IN A WELL-VENTILATED AREA.

PERSONAL PROTECTIVE EQUIPMENT:

EYE/FACE PROTECTION:
NO SPECIAL EYE PROTECTION IS NORMALLY REQUIRED. WHERE SPLASHING IS POSSIBLE,
WEAR SAFETY GLASSES WITH SIDE SHIELDS AS A GOOD SAFETY PRACTICE.

SKIN PROTECTION:
NO SPECIAL PROTECTIVE CLOTHING IS NORMALLY REQUIRED. WHERE SPLASHING IS
POSSIBLE, SELECT PROTECTIVE CLOTHING DEPENDING ON OPERATIONS CONDUCTED,
PHYSICAL REQUIREMENTS AND OTHER SUBSTANCES IN THE WORKPLACE.

SUGGESTED MATERIALS FOR PROTECTIVE GLOVES INCLUDE:
4H (PE/EVAL), NITRILE RUBBER, SILVER SHIELD, VITON.

RESPIRATORY PROTECTION: NO RESPIRATORY PROTECTION IS NORMALLY REQUIRED.

IF USER OPERATIONS GENERATE AN OIL MIST, DETERMINE IF AIRBORNE 
CONCENTRATIONS ARE BELOW THE OCCUPATIONAL EXPOSURE LIMIT FOR MINERAL OIL 
MIST. IF NOT, WEAR AN APPROVED RESPIRATOR THAT PROVIDES ADEQUATE PROTECTION 
FROM THE MEASURED CONCENTRATIONS OF THIS MATERIAL. FOR AIR-PURIFYING 
RESPIRATORS USE A PARTICULATE CARTRIDGE.

USE A POSITIVE PRESSURE AIR-SUPPLYING RESPIRATOR IN CIRCUMSTANCES WHERE
AIR-PURIFYING RESPIRATORS MAY NOT PROVIDE ADEQUATE PROTECTION.


SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 


ATTENTION:
THE DATA BELOW ARE TYPICAL VALUES AND DO NOT CONSTITUTE A SPECIFICATION.

COLOR: YELLOW

PHYSICAL STATE: LIQUID

ODOR: PETROLEUM ODOR

pH: NOT APPLICABLE

VAPOR PRESSURE: <0.01 MMHg @ 37.8 DEG. C (100 DEG. F)

VAPOR DENSITY (AIR = 1): >1

BOILING POINT: >315.6 DEG. C (600 DEG. F)

SOLUBILITY: SOLUBLE IN HYDROCARBONS; INSOLUBLE IN WATER

FREEZING POINT: NOT APPLICABLE

MELTING POINT: NOT APPLICABLE

SPECIFIC GRAVITY:
0.86 - 0.87 @ 15.6 DEG. C (60.1 DEG. F) / 15.6 DEG. C (60.1 DEG. F)

DENSITY: 0.86 KG/L - 0.9 KG/L @ 15 DEG. C (59 DEG. F)

VISCOSITY: 22 CST - 61.2 CST @ 40 DEG. C (104 DEG. F) (MIN)


SECTION 10 STABILITY AND REACTIVITY 


CHEMICAL STABILITY:
THIS MATERIAL IS CONSIDERED STABLE UNDER NORMAL AMBIENT AND ANTICIPATED
STORAGE AND HANDLING CONDITIONS OF TEMPERATURE AND PRESSURE.

INCOMPATIBILITY WITH OTHER MATERIALS:
MAY REACT WITH STRONG ACIDS OR STRONG OXIDIZING AGENTS, SUCH AS CHLORATES,
NITRATES, PEROXIDES, ETC.

HAZARDOUS DECOMPOSITION PRODUCTS: NONE KNOWN (NONE EXPECTED)

HAZARDOUS POLYMERIZATION: HAZARDOUS POLYMERIZATION WILL NOT OCCUR.


SECTION 11 TOXICOLOGICAL INFORMATION 


IMMEDIATE HEALTH EFFECTS:

EYE IRRITATION:
THE EYE IRRITATION HAZARD IS BASED ON EVALUATION OF DATA FOR SIMILAR
MATERIALS OR PRODUCT COMPONENTS.

SKIN IRRITATION:
THE SKIN IRRITATION HAZARD IS BASED ON EVALUATION OF DATA FOR SIMILAR
MATERIALS OR PRODUCT COMPONENTS.

SKIN SENSITIZATION: NO PRODUCT TOXICOLOGY DATA AVAILABLE.

ACUTE DERMAL TOXICITY:
THE ACUTE DERMAL TOXICITY HAZARD IS BASED ON EVALUATION OF DATA FOR SIMILAR
MATERIALS OR PRODUCT COMPONENTS.

ACUTE ORAL TOXICITY:
THE ACUTE ORAL TOXICITY HAZARD IS BASED ON EVALUATION OF DATA FOR SIMILAR
MATERIALS OR PRODUCT COMPONENTS.

ACUTE INHALATION TOXICITY:
THE ACUTE INHALATION TOXICITY HAZARD IS BASED ON EVALUATION OF DATA FOR
SIMILAR MATERIALS OR PRODUCT COMPONENTS.

ADDITIONAL TOXICOLOGY INFORMATION:
THIS PRODUCT CONTAINS PETROLEUM BASE OILS WHICH MAY BE REFINED BY VARIOUS
PROCESSES INCLUDING SEVERE SOLVENT EXTRACTION, SEVERE HYDROCRACKING, OR
SEVERE HYDROTREATING. NONE OF THE OILS REQUIRES A CANCER WARNING UNDER THE
OSHA HAZARD COMMUNICATION STANDARD (29 CFR 1910.1200). THESE OILS HAVE NOT
BEEN LISTED IN THE NATIONAL TOXICOLOGY PROGRAM (NTP) ANNUAL REPORT NOR HAVE
THEY BEEN CLASSIFIED BY THE INTERNATIONAL AGENCY FOR RESEARCH ON CANCER
(IARC) AS; CARCINOGENIC TO HUMANS (GROUP 1), PROBABLY CARCINOGENIC TO HUMANS
(GROUP 2A), OR POSSIBLY CARCINOGENIC TO HUMANS (GROUP 2B).

THESE OILS HAVE NOT BEEN CLASSIFIED BY THE AMERICAN CONFERENCE OF
GOVERNMENTAL INDUSTRIAL HYGIENISTS (ACGIH) AS:
CONFIRMED HUMAN CARCINOGEN (A1)
SUSPECTED HUMAN CARCINOGEN (A2), OR
CONFIRMED ANIMAL CARCINOGEN WITH UNKNOWN RELEVANCE TO HUMANS (A3).


SECTION 12 ECOLOGICAL INFORMATION 


ECOTOXICITY:
THIS MATERIAL IS NOT EXPECTED TO BE HARMFUL TO AQUATIC ORGANISMS. THE
ECOTOXICITY HAZARD IS BASED ON AN EVALUATION OF DATA FOR THE COMPONENTS OR
A SIMILAR MATERIAL.

ENVIRONMENTAL FATE:
THIS MATERIAL IS NOT EXPECTED TO BE READILY BIODEGRADABLE.


SECTION 13 DISPOSAL CONSIDERATIONS 


USE MATERIAL FOR ITS INTENDED PURPOSE OR RECYCLE IF POSSIBLE. OIL COLLECTION
SERVICES ARE AVAILABLE FOR USED OIL RECYCLING OR DISPOSAL. PLACE 
CONTAMINATED MATERIALS IN CONTAINERS AND DISPOSE OF IN A MANNER CONSISTENT 
WITH APPLICABLE REGULATIONS. CONTACT YOUR SALES REPRESENTATIVE OR LOCAL 
ENVIRONMENTAL OR HEALTH AUTHORITIES FOR APPROVED DISPOSAL OR RECYCLING 
METHODS.


SECTION 14 TRANSPORT INFORMATION 


THE DESCRIPTION SHOWN MAY NOT APPLY TO ALL SHIPPING SITUATIONS. CONSULT
49CFR, OR APPROPRIATE DANGEROUS GOODS REGULATIONS, FOR ADDITIONAL 
DESCRIPTION REQUIREMENTS (E.G., TECHNICAL NAME) AND MODE-SPECIFIC OR 
QUANTITY-SPECIFIC SHIPPING REQUIREMENTS.

DOT SHIPPING DESCRIPTION:
PETROLEUM LUBRICATING OIL, NOT REGULATED AS A HAZARDOUS MATERIAL FOR
TRANSPORTATION UNDER 49 CFR

ADDITIONAL INFORMATION:
NOT HAZARDOUS BY U.S. DOT. ADR/RID HAZARD CLASS NOT APPLICABLE.

IMO/IMDG SHIPPING DESCRIPTION:
PETROLEUM LUBRICATING OIL; NOT REGULATED AS DANGEROUS GOODS FOR TRANSPORT
UNDER THE IMDG CODE

ICAO/IATA SHIPPING DESCRIPTION:
PETROLEUM LUBRICATING OIL
NOT REGULATED AS DANGEROUS GOODS FOR TRANSPORT UNDER ICAO


SECTION 15 REGULATORY INFORMATION 


EPCRA 311/312 CATEGORIES:
1. IMMEDIATE (ACUTE) HEALTH EFFECTS: NO
2. DELAYED (CHRONIC) HEALTH EFFECTS: NO
3. FIRE HAZARD: NO
4. SUDDEN RELEASE OF PRESSURE HAZARD: NO
5. REACTIVITY HAZARD: NO

REGULATORY LISTS SEARCHED:
01-1=IARC GROUP 1
01-2A=IARC GROUP 2A
01-2B=IARC GROUP 2B
02=NTP CARCINOGEN
03=EPCRA 313
04=CA PROPOSITION 65
05=MA RTK
06=NJ RTK
07=PA RTK

NO COMPONENTS OF THIS MATERIAL WERE FOUND ON THE REGULATORY LISTS ABOVE.

CHEMICAL INVENTORIES:

ALL COMPONENTS COMPLY WITH THE FOLLOWING CHEMICAL INVENTORY REQUIREMENTS:
AICS (AUSTRALIA), DSL (CANADA), ENCS (JAPAN), IECSC (CHINA), KECI (KOREA),
PICCS (PHILIPPINES), TSCA (UNITED STATES).

ONE OR MORE COMPONENTS IS LISTED ON ELINCS (EUROPEAN UNION). SECONDARY
NOTIFICATION BY THE IMPORTER MAY BE REQUIRED.

NEW JERSEY RTK CLASSIFICATION:

UNDER THE NEW JERSEY RIGHT-TO-KNOW ACT L. 1983 CHAPTER 315 N.J.S.A. 34:
5A-1 ET. SEQ.

THE PRODUCT IS TO BE IDENTIFIED AS FOLLOWS: PETROLEUM OIL (HYDRAULIC OIL)

WHMIS CLASSIFICATION:
THIS PRODUCT IS NOT CONSIDERED A CONTROLLED PRODUCT ACCORDING TO THE 
CRITERIA OF THE CANADIAN CONTROLLED PRODUCTS REGULATIONS.


SECTION 16 OTHER INFORMATION 


NFPA RATINGS:
HEALTH       0
FLAMMABILITY 1
REACTIVITY   0

HMIS RATINGS:
HEALTH       1
FLAMMABILITY 1
REACTIVITY   0

0-LEAST
1-SLIGHT
2-MODERATE
3-HIGH
4-EXTREME

PPE - PERSONAL PROTECTION EQUIPMENT INDEX RECOMMENDATION
* - CHRONIC EFFECT INDICATOR.

THESE VALUES ARE OBTAINED USING THE GUIDELINES OR PUBLISHED EVALUATIONS
PREPARED BY THE NATIONAL FIRE PROTECTION ASSOCIATION (NFPA) OR THE NATIONAL
PAINT AND COATING ASSOCIATION (FOR HMIS RATINGS).

LABEL RECOMMENDATION:
LABEL CATEGORY: INDUSTRIAL OIL 1 - IND1

REVISION STATEMENT:

THIS REVISION UPDATES THE FOLLOWING SECTIONS OF THIS MATERIAL SAFETY DATA
SHEET: 2.

REVISION DATE: JANUARY 15, 2007

ABBREVIATIONS THAT MAY HAVE BEEN USED IN THIS DOCUMENT:
TLV - THRESHOLD LIMIT VALUE
STEL - SHORT-TERM EXPOSURE LIMIT
ACGIH - AMERICAN CONFERENCE OF GOVERNMENT INDUSTRIAL HYGIENISTS
API - AMERICAN PETROLEUM INSTITUTE
CVX - CHEVRON
DOT - DEPARTMENT OF TRANSPORTATION (USA)
IARC - INTERNATIONAL AGENCY FOR RESEARCH ON CANCER
TWA - TIME WEIGHTED AVERAGE
PEL - PERMISSIBLE EXPOSURE LIMIT
CAS - CHEMICAL ABSTRACT SERVICE NUMBER
IMO/IMDG - INTERNATIONAL MARITIME DANGEROUS GOODS CODE
MSDS - MATERIAL SAFETY DATA SHEET
NFPA - NATIONAL FIRE PROTECTION ASSOCIATION (USA)
NTP - NATIONAL TOXICOLOGY PROGRAM (USA)
OSHA - OCCUPATIONAL SAFETY AND HEALTH ADMINISTRATION

PREPARED ACCORDING TO THE OSHA HAZARD COMMUNICATION STANDARD
(29 CFR 1910.1200) AND THE ANSI MSDS STANDARD (Z400.1) BY THE CHEVRON ENERGY
TECHNOLOGY COMPANY, 100 CHEVRON WAY, RICHMOND, CALIFORNIA 94802.

THE ABOVE INFORMATION IS BASED ON THE DATA OF WHICH WE ARE AWARE AND IS
BELIEVED TO BE CORRECT AS OF THE DATE HEREOF. SINCE THIS INFORMATION MAY
BE APPLIED UNDER CONDITIONS BEYOND OUR CONTROL AND WITH WHICH WE MAY BE
UNFAMILIAR AND SINCE DATA MADE AVAILABLE SUBSEQUENT TO THE DATE HEREOF MAY
SUGGEST MODIFICATIONS OF THE INFORMATION, WE DO NOT ASSUME ANY 
RESPONSIBILITY FOR THE RESULTS OF ITS USE. THIS INFORMATION IS FURNISHED 
UPON CONDITION THAT THE PERSON RECEIVING IT SHALL MAKE HIS OWN DETERMINATION
OF THE SUITABILITY OF THE MATERIAL FOR HIS PARTICULAR PURPOSE.