Common Name: PAIRDEER R14 BATTERY
Manufacturer: ZHONGYIN (NINGBO) BATTERY CHINA
SDS Revision Date: (No Date)
SDS Format: No Format Specified
   
Grainger Item Number(s): 6KWN4
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - PRODUCT IDENTIFICATION 
SECTION II - HAZARDOUS INGREDIENTS 
SECTION III - PHYSICAL / CHEMICAL CHARACTERISTICS 
SECTION IV - FIRE AND EXPLOSION HAZARD DATA 
SECTION V - REACTIVITY DATA 
SECTION VI - HEALTH HAZARD DATA 
SECTION VII - FIRST AID MEASURES 
SECTION VIII - FIRE AND EXPLOSION HAZARD DATA 
SECTION IX - ACCIDENTAL RELEASE OR SPILLAGE 
SECTION X - HANDLING AND STORAGE 
SECTION XI - EXPOSURE CONTROLS / PERSON PROTECTION 
SECTION XII - ECOLOGICAL INFORMATION 
SECTION XIII - DISPOSAL METHOD 
SECTION XIV - TRANSPORTATION INFORMATION 
SECTION XV - REGULATORY INFORMATION 
SECTION XVI - OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET

PAIRDEER(R*)

MSDS-R14

ZHONGYIN NINGBO BATTERY CO., LTD.
99.DAHETOU ST.DUAN TANG, NINGBO,
CHINA

P.C.: 315011

TEL: +86 574 87491087 87493214

FAX: +86 574 87493903

WWW.SONLUK.COM


SECTION I - PRODUCT IDENTIFICATION 


PRODUCT NAME: PAIRDEER R14 BATTERY.

NOMINAL VOLTAGE: 1.5V

CHEMICAL SYSTEM: ZINC / MANGANESE DIOXIDE

DESIGNED FOR RECHARGE:
YES ( )
NO  (X)


SECTION II - HAZARDOUS INGREDIENTS 


THE BATTERY IS NOT DANGEROUS TO HUMAN OR ENVIRONMENT. CADMIUM, LEAD, AND
MERCURY OR OTHER DANGEROUS CHEMICALS ARE NOT INCLUDED IN THE BATTERY.

HAZARDOUS COMPONENTS:

DESCRIPTION                                   APPROXIMATE % OF TOTAL WEIGHT

MANGANESE DIOXIDE                             23.1 WT%

ZINC                                          20.7 WT%

MERCURY                                       <0.0001 WT%

LEAD                                          <0.4 WT%

CADMIUM                                       <0.002 WT%

AMMONIUM CHLORIDE (NH4Cl)                     21.4 WT%
AND ZINC CHLORIDE (ZnNCl2)MIXTURE SOLUTION


SECTION III - PHYSICAL / CHEMICAL CHARACTERISTICS 


BOILING POINT: N.A.

VAPOR PRESSURE (MMHg): N.A.

VAPOR DENSITY (AIR=1): N.A.

SOLUBILITY IN WATER: N.A.

SPECIFIC GRAVITY (H2O=1): N.A.

MELTING POINT: N.A.

EVAPORATION RATE (BUTYL ACETATE=1): N.A.

APPEARANCE AND ODOR: CYLINDER AND ODORLESS.


SECTION IV - FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): N.A.

FLAMMABLE LIMITS: N.A.

LEL: N.A.
UEL: N.A.

EXTINGUISHING MEDIA: N.A.

SPECIAL FIRE FIGHTING PROCEDURES: N.A.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
DO NOT DISPOSE OF BATTERY IN FIRE - MAY CAUSE EXPLOSION
DO NOT SHORT-CIRCUIT BATTERY - MAY CAUSE BURNS.


SECTION V - REACTIVITY DATA 


STABILITY:
UNSTABLE ( )
STABLE   (X)

CONDITIONS TO AVOID:

INCOMPATIBILITY(MATERIALS TO AVOID):

HAZARDOUS DECOMPOSITION OR BYPRODUCTS:
WHEN HEATED, BATTERY MAY EMIT HAZARDOUS VAPOR OF KOH/NaOH AND Hg

HAZARDOUS POLYMERIZATION:
MAY OCCUR      ( )
WILL NOT OCCUR (X)

CONDITIONS TO AVOID:


SECTION VI - HEALTH HAZARD DATA 


IN CASE OF ELECTROLYTE LEAKAGE, SKIN WILL BE ITCHY WHEN CONTAMINATED WITH
ELECTROLYTE.

IN CONTACT WITH ELECTROLYTE CAN CAUSE SERVER IRRITATION AND CHEMICAL BURNS

INHALATION OF ELECTROLYTE VAPORS MAY CAUSE IRRITATION OF THE UPPER
RESPIRATORY TRACT AND LUNGS.


SECTION VII - FIRST AID MEASURES 


FIRST AID PROCEDURES:
IF ELECTROLYTE LEAKAGE OCCURS AND MAKES CONTACT WITH SKIN, WASH WITH PLENTY
OF WATER IMMEDIATELY

IF ELECTROLYTE COMES INTO CONTACT WITH EYES, WASH WITH COPIOUS AMOUNTS OF
WATER FOR FIFTEEN MINUTES, AND CONTACT A PHYSICIAN.

IF ELECTROLYTE VAPORS ARE INHALED, PROVIDE FRESH AIR AND SEEK MEDICAL
ATTENTION IF RESPIRATORY IRRITATION DEVELOPS. VENTILATE THE CONTAMINATED
AREA.


SECTION VIII - FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): N.A.

IGNITION TEMP.: N.A.

FLAMMABLE LIMITS: N.A.

LEL: N.A.
UEL: N.A.

EXTINGUISHING MEDIA: N.A

SPECIAL FIRE FIGHTING PROCEDURES: N.A.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
DO NOT DISPOSE OF BATTERY IN FIRE - MAY EXPLODE.
DO NOT SHORT-CIRCUIT BATTERY - MAY CAUSE BURNS.


SECTION IX - ACCIDENTAL RELEASE OR SPILLAGE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
BATTERIES THAT ARE LEAKAGE SHOULD BE HANDLED WITH RUBBER GLOVES.

AVOID DIRECT CONTACT WITH ELECTROLYTE.

WEAR PROTECTIVE CLOTHING AND A POSITIVE PRESSURE SELF-CONTAINED BREATHING
APPARATUS (SCBA).


SECTION X - HANDLING AND STORAGE 


SAFE HANDLING AND STORAGE ADVICE

THE BATTERY IS EXTREMELY SENSITIVE TO ADVERSE EFFECTS OF HUMIDITY. BE SURE
TO STORE THEM IN A PLACE THAT IS DRY AND SUBJECT TO LITTLE TEMPERATURE
CHANGE. DO NOT PLACE NEAR THE BOILER OR RADIATOR, NOR EXPOSE TO DIRECT SUN
LIGHT. DO NOT DISPOSE OF THE BATTERY IN FIRE. DO NOT CHARGE THE BATTERY. DO
NOT SHORT-CIRCUIT THE BATTERY. DO NOT PUT IN BACKWARD POSITION. DO NOT
STORE IN DISORDERLY FASHION, OR ALLOW METAL OBJECTS TO BE MIXED WITH STORED
BATTERIES. DO NOT DISASSEMBLE THE BATTERY, HANDING IN SUCH MANNER CAN CAUSE
THE BATTERY TO EXPLODE, LEAK AND INJURY.


SECTION XI - EXPOSURE CONTROLS / PERSON PROTECTION 


OCCUPATIONAL EXPOSURE LIMITS:
LTEP: N.A.
STEP: N.A.

RESPIRATORY PROTECTION (SPECIFY TYPE): N.A.

VENTILATION:
LOCAL EXHAUSTS: N.A.
MECHANICAL(GENERAL): N.A.
SPECIAL: N.A.
OTHER: N.A.

PROTECTIVE GLOVE: N.A.

EYE PROTECTION: N.A.

OTHER PROTECTIVE CLOTHING OR EQUIPMENT: N.A.

WORK/HYGIENIC PRACTICE: N.A.


SECTION XII - ECOLOGICAL INFORMATION 


N.A


SECTION XIII - DISPOSAL METHOD 


DISPOSE OF THE BATTERIES ACCORDING TO THE GOVERNMENT REGULATIONS.


SECTION XIV - TRANSPORTATION INFORMATION 


BATTERIES ARE CONSIDERED TO BE "DRY CELL" BATTERIES AND ARE UNREGULATED FOR
PURPOSES OF TRANSPORTATION BY THE U.S. DEPARTMENT OF TRANSPORTATION(DOT),
INTERNATIONAL CIVIL AVIATION ADMINISTRATION(ICAO), INTERNATIONAL AIR
TRANSPORT ASSOCIATION(IATA) AND INTERNATIONAL MARITIME DANGEROUS GOODS
REGULATIONS(IMDG).

THE ONLY DOT REQUIREMENT FOR SHIPPING THESE BATTERIES IS SPECIAL PROVISION
130 WHICH STATES:
BATTERIES, DRY ARE NOT SUBJECT TO THE REQUIREMENTS OF THIS SUBCHAPTER ONLY
WHEN THEY ARE OFFERED FOR TRANSPORTATION IN A MANNER THAT PREVENTS THE
DANGEROUS EVOLUTION OF HEAT(FOR EXAMPLE, BY THE EFFECTIVE INSULATION OF
EXPOSED TERMINALS). AS OF 1/1/97 IATA REQUIRES THAT BATTERIES BEING
TRANSPORTED BY AIR MUST BE PROTECTED FROM SHORT-CIRCUITING AND PROTECTED
FROM MOVEMENT THAT COULD LEAD TO SHORT-CIRCUITING.


SECTION XV - REGULATORY INFORMATION 


SPECIAL REQUIREMENT BE ACCORDING TO THE LOCAL REGULATORY.


SECTION XVI - OTHER INFORMATION 


THE INFORMATION ON THIS MATERIAL SAFETY DATE SHEET (MSDS) WAS OBTAINED FORM
CURRENT AND REPUTABLE SOURCES. HOWEVER, THE DATA IS PROVIDED WITHOUT ANY
WARRANTY; EXPRESSED OR IMPLIED, REGARDING ITS CORRECTNESS OR ACCURACY. IT
IS THE USER'S RESPONSIBILITY TO ASSUME LIABILITY ON LOSS, INJURY, DAMAGE,
OR EXPENSE RESULTING FROM IMPROPER USE OF THIS PRODUCT. ANY PREVIOUS MSDS
OF THIS PRODUCT MENTIONED ABOVE ARE HEREBY REPLACED WITH THIS NEW DOCUMENT.
WE URGE YOU TO MAKE THIS INFORMATION AVAILABLE AS APPROPRIATE IN YOUR
ORGANIZATION AND TO ANY OTHERS WITH WHOM YOU ARRANGE TO HANDLE THIS
PRODUCT.

VERSION: 01