Common Name: EVEREADY / ENERGIZER BATTERY
Manufacturer: ENERGIZER BATTERY
MSDS Revision Date: 1/1/2011
   
Grainger Item Number(s): 11U137, 11U139, 11V239, 11V240, 2LBJ7, 3KKG9, 3KKH2, 3KKH4, 3KKH6, 3KKH8, 3KKJ3, 8GMM7, 8GMM8, 8UYT7, 8WF10, 9GGY9, 9WAK7
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1 - MANUFACTURER INFORMATION 
SECTION 2 - HAZARDS IDENTIFICATION 
SECTION 3 - INGREDIENTS 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL CONSIDERATIONS 
SECTION 14 - TRANSPORT INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



PRODUCT SAFETY DATASHEET

ENERGIZER(R*)

ALKALINE BATTERIES

JANUARY, 2011

PRODUCT SAFETY DATA SHEET

PRODUCT NAME: EVEREADY / ENERGIZER BATTERY

TRADE NAMES:
ENERGIZER, ENERGIZER E(2), INDUSTRIAL ZMA, HERCULES, EVEREADY, WONDER

CHEMICAL SYSTEM: ALKALINE MANGANESE DIOXIDE-ZINC

APPROXIMATE WEIGHT:

TYPE NO.:

VOLTS:

DESIGNED FOR RECHARGE: NO


SECTION 1 - MANUFACTURER INFORMATION 


ENERGIZER BATTERY MANUFACTURING, INC.
25225 DETROIT RD.
WESTLAKE, OH 44145

TELEPHONE NUMBER FOR INFORMATION:
800-383-7323 (USA / CANADA)

DATE PREPARED: JANUARY, 2011


SECTION 2 - HAZARDS IDENTIFICATION 


UNDER NORMAL CONDITIONS OF USE, THE BATTERY IS HERMETICALLY SEALED.

INGESTION:
SWALLOWING A BATTERY CAN BE HARMFUL. CONTENTS OF AN OPEN BATTERY CAN CAUSE
SERIOUS CHEMICAL BURNS OF MOUTH, ESOPHAGUS, AND GASTROINTESTINAL TRACT.

INHALATION: CONTENTS OF AN OPEN BATTERY CAN CAUSE RESPIRATORY IRRITATION.

SKIN CONTACT:
CONTENTS OF AN OPEN BATTERY CAN CAUSE SKIN IRRITATION AND/OR CHEMICAL
BURNS.

EYE CONTACT:
CONTENTS OF AN OPEN BATTERY CAN CAUSE SEVERE IRRITATION AND CHEMICAL BURNS.


SECTION 3 - INGREDIENTS 


IMPORTANT NOTE:
THE BATTERY SHOULD NOT BE OPENED OR BURNED. EXPOSURE TO THE INGREDIENTS
CONTAINED WITHIN OR THEIR COMBUSTION PRODUCTS COULD BE HARMFUL.

MATERIAL OR INGREDIENT      PEL (OSHA)        TLV (ACGIH)           %/WT.

GRAPHITE                    15 MG/M3 TWA      2 MG/M3 TWA            2-6
(CAS# 7782-42-5)            (TOTAL DUST)      (RESPIRABLE
                            5 MG/M3 TWA       FRACTION)
                            (RESPIRABLE
                            FRACTION)

MANGANESE DIOXIDE           5 MG/M3 CEILING   0.2 MG/M3 TWA         30-45
(CAS# 1313-13-9)            (AS Mn)           (AS Mn)

POTASSIUM HYDROXIDE         NONE ESTABLISHED  2 MG/M3 CEILING        4-8
(CAS# 1310-58-3)

ZINC                        15 MG/M3 TWA      10 MG/M3 TWA          12-25
(CAS# 7440-66-6)            PNOR*             PNOC** (INHALABLE
                            (TOTAL DUST)      PARTICULATE)
                            5 MG/M3 TWA       3 MG/M3 TWA
                            PNOR*             PNOC** (RESPIRABLE
                            (RESPIRABLE       PARTICULATE)
                            FRACTION)

NON-HAZARDOUS COMPONENTS    NONE ESTABLISHED  NONE ESTABLISHED      18-22
STEEL
(IRON CAS# 7439-89-6)

WATER, PAPER, PLASTIC       NONE ESTABLISHED  NONE ESTABLISHED      BALANCE
AND OTHER

* PNOR: PARTICULATES NOT OTHERWISE REGULATED

**PNOC: PARTICULATES NOT OTHERWISE CLASSIFIED


SECTION 4 - FIRST AID MEASURES 


INGESTION:
DO NOT INDUCE VOMITING OR GIVE FOOD OR DRINK. SEEK MEDICAL ATTENTION
IMMEDIATELY. CALL NATIONAL BATTERY INGESTION HOTLINE FOR ADVICE AND
FOLLOW-UP (202-625-3333) COLLECT DAY OR NIGHT.

INHALATION: PROVIDE FRESH AIR AND SEEK MEDICAL ATTENTION.

SKIN CONTACT:
REMOVE CONTAMINATED CLOTHING AND WASH SKIN WITH SOAP AND WATER. IF A
CHEMICAL BURN OCCURS OR IF IRRITATION PERSISTS, SEEK MEDICAL ATTENTION.

EYE CONTACT:
IMMEDIATELY FLUSH EYES THOROUGHLY WITH WATER FOR AT LEAST 15 MINUTES,
LIFTING UPPER AND LOWER LIDS, UNTIL NO EVIDENCE OF THE CHEMICAL REMAINS.
SEEK MEDICAL ATTENTION.


SECTION 5 - FIRE FIGHTING MEASURES 


IN CASE OF FIRE, IT IS PERMISSIBLE TO USE ANY CLASS OF EXTINGUISHING MEDIUM
ON THESE BATTERIES OR THEIR PACKING MATERIAL. COOL EXTERIOR OF BATTERIES IF
EXPOSED TO FIRE TO PREVENT RUPTURE.

FIRE FIGHTERS SHOULD WEAR SELF-CONTAINED BREATHING APPARATUS.


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


TO CLEANUP LEAKING BATTERIES:

VENTILATION REQUIREMENTS:
ROOM VENTILATION MAY BE REQUIRED IN AREAS WHERE THERE ARE OPEN OR LEAKING
BATTERIES.

EYE PROTECTION:
WEAR SAFETY GLASSES WITH SIDE SHIELDS IF HANDLING AN OPEN OR LEAKING
BATTERY.

GLOVES:
USE NEOPRENE OR NATURAL RUBBER GLOVES IF HANDLING AN OPEN OR LEAKING
BATTERY.

BATTERY MATERIALS SHOULD BE COLLECTED IN A LEAK-PROOF CONTAINER.


SECTION 7 - HANDLING AND STORAGE 


STORAGE:
STORE IN A COOL, WELL VENTILATED AREA. ELEVATED TEMPERATURES CAN RESULT IN
SHORTENED BATTERY LIFE.

MECHANICAL CONTAINMENT:
IF POTTING OR SEALING THE BATTERY IN AN AIRTIGHT OR WATERTIGHT CONTAINER IS
REQUIRED, CONSULT YOUR ENERGIZER BATTERY MANUFACTURING, INC. REPRESENTATIVE
FOR PRECAUTIONARY SUGGESTIONS. BATTERIES NORMALLY EVOLVE HYDROGEN WHICH,
WHEN COMBINED WITH OXYGEN FROM THE AIR, CAN PRODUCE A COMBUSTIBLE OR
EXPLOSIVE MIXTURE UNLESS VENTED. IF SUCH A MIXTURE IS PRESENT, SHORT
CIRCUITS, HIGH TEMPERATURE, OR STATIC SPARKS CAN CAUSE AN IGNITION.

DO NOT OBSTRUCT SAFETY RELEASE VENTS ON BATTERIES. ENCAPSULATION (POTTING)
OF BATTERIES WILL NOT ALLOW CELL VENTING AND CAN CAUSE HIGH PRESSURE
RUPTURE.

HANDLING:
ACCIDENTAL SHORT CIRCUIT FOR A FEW SECONDS WILL NOT SERIOUSLY AFFECT THE
BATTERY. PROLONGED SHORT CIRCUIT WILL CAUSE THE BATTERY TO LOSE ENERGY, AND
CAN CAUSE THE SAFETY RELEASE VENT TO OPEN. SOURCES OF SHORT CIRCUITS
INCLUDE JUMBLED BATTERIES IN BULK CONTAINERS, METAL JEWELRY, METAL COVERED
TABLES OR METAL BELTS USED FOR ASSEMBLY OF BATTERIES INTO DEVICES.

IF SOLDERING OR WELDING TO THE BATTERY IS REQUIRED, CONSULT YOUR ENERGIZER
BATTERY MANUFACTURING, INC. REPRESENTATIVE FOR PROPER PRECAUTIONS TO
PREVENT SEAL DAMAGE OR SHORT CIRCUIT.

CHARGING:
THIS BATTERY IS MANUFACTURED IN A CHARGED STATE. IT IS NOT DESIGNED FOR
RECHARGING. RECHARGING CAN CAUSE BATTERY LEAKAGE OR, IN SOME CASES, HIGH
PRESSURE RUPTURE. INADVERTENT CHARGING CAN OCCUR IF A BATTERY IS INSTALLED
BACKWARDS.

LABELING:

IF THE EVEREADY / ENERGIZER BATTERY LABEL OR PACKAGE WARNINGS ARE NOT
VISIBLE, IT IS IMPORTANT TO PROVIDE A PACKAGE AND/OR DEVICE LABEL STATING:

WARNING:
DO NOT INSTALL BACKWARDS, CHARGE, PUT IN FIRE, OR MIX WITH OTHER BATTERY
TYPES. MAY EXPLODE OR LEAK CAUSING INJURY.

REPLACE ALL BATTERIES AT THE SAME TIME.

WHERE ACCIDENTAL INGESTION OF SMALL BATTERIES IS POSSIBLE, THE LABEL SHOULD
INCLUDE:
KEEP AWAY FROM SMALL CHILDREN. IF SWALLOWED, PROMPTLY SEE DOCTOR; HAVE
DOCTOR PHONE (202) 625-3333 COLLECT.


SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 


VENTILATION REQUIREMENTS: NOT NECESSARY UNDER NORMAL CONDITIONS.

RESPIRATORY PROTECTION: NOT NECESSARY UNDER NORMAL CONDITIONS.

EYE PROTECTION: NOT NECESSARY UNDER NORMAL CONDITIONS.

GLOVES: NOT NECESSARY UNDER NORMAL CONDITIONS.


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


BOILING POINT @ 760 MMHg (DEG. C): NOT APPLICABLE FOR AN ARTICLE

VAPOR PRESSURE (MMHg @ 25 DEG. C): NOT APPLICABLE FOR AN ARTICLE

VAPOR DENSITY (AIR = 1): NOT APPLICABLE FOR AN ARTICLE

DENSITY (G/CM3): 2.0 - 3.0

PERCENT VOLATILE BY VOLUME (%): NOT APPLICABLE FOR AN ARTICLE

EVAPORATION RATE (BUTYL ACETATE = 1): NOT APPLICABLE FOR AN ARTICLE

PHYSICAL STATE: SOLID

SOLUBILITY IN WATER (% BY WEIGHT): NOT APPLICABLE FOR AN ARTICLE

pH: NOT APPLICABLE FOR AN ARTICLE

APPEARANCE AND ODOR: SOLID OBJECT / NO ODOR


SECTION 10 - STABILITY AND REACTIVITY 


ALKALINE BATTERIES DO NOT MEET ANY OF THE CRITERIA ESTABLISHED IN 40 CFR
261.2 FOR REACTIVITY.


SECTION 11 - TOXICOLOGICAL INFORMATION 


ALKALINE BATTERIES ARE NOT HAZARDOUS WASTE. UNDER NORMAL CONDITIONS OF USE,
ALKALINE BATTERIES ARE NON-TOXIC.


SECTION 12 - ECOLOGICAL INFORMATION 


ISSUES SUCH AS ECOTOXICITY, PERSISTENCE AND BIOACCUMULATION ARE NOT
APPLICABLE FOR ARTICLES.


SECTION 13 - DISPOSAL CONSIDERATIONS 


DISPOSE OF IN ACCORDANCE WITH ALL APPLICABLE FEDERAL, STATE AND LOCAL
REGULATIONS. APPROPRIATE DISPOSAL TECHNOLOGIES INCLUDE INCINERATION AND
LAND FILLING.


SECTION 14 - TRANSPORT INFORMATION 


IN GENERAL, ALL BATTERIES IN ALL FORMS OF TRANSPORTATION (GROUND, AIR, OR
OCEAN) MUST BE PACKAGED IN A SAFE AND RESPONSIBLE MANNER. REGULATORY
CONCERNS FROM ALL AGENCIES FOR SAFE PACKAGING REQUIRE THAT BATTERIES BE
PACKAGED IN A MANNER THAT PREVENTS SHORT CIRCUITS AND BE CONTAINED IN
"STRONG OUTER PACKAGING" THAT PREVENTS SPILLAGE OF CONTENTS. ALL ORIGINAL
PACKAGING FOR ENERGIZER ALKALINE BATTERIES HAS BEEN DESIGNED TO BE
COMPLIANT WITH THESE REGULATORY CONCERNS.

ALKALINE BATTERIES (SOMETIMES REFERRED TO AS "DRY CELL" BATTERIES) ARE NOT
LISTED AS DANGEROUS GOODS UNDER THE IATA DANGEROUS GOODS REGULATIONS, ICAO
TECHNICAL INSTRUCTIONS AND THE U.S. HAZARDOUS MATERIALS REGULATIONS (49
CFR). THESE BATTERIES ARE NOT SUBJECT TO THE DANGEROUS GOODS REGULATIONS
PROVIDED THEY MEET THE REQUIREMENTS CONTAINED IN THE FOLLOWING SPECIAL
PROVISIONS.

REGULATORY BODY                          SPECIAL PROVISIONS

ADR                                      295 - 304, 598

IMDG                                     295 - 303

UN                                       295 - 303

US DOT                                   49 CFR 172.102 PROVISION 130

IATA                                     A123

ICAO                                     295 - 303

ALL ENERGIZER ALKALINE BATTERIES ARE PACKED IN SUCH A WAY TO PREVENT SHORT
CIRCUITS OR THE GENERATION DANGEROUS QUANTITIES OF HEAT AND MEET THE
SPECIAL PROVISIONS LISTED ABOVE. IN ADDITION, THE IATA DANGEROUS GOODS
REGULATIONS AND ICAO TECHNICAL INSTRUCTIONS REQUIRE THE WORDS "NOT
RESTRICTED" AND THE SPECIAL PROVISION NUMBER A123 BE PROVIDED ON THE AIR
WAYBILL, WHEN AN AIR WAYBILL IS ISSUED.


SECTION 15 - REGULATORY INFORMATION 


BATTERIES MARKETED BY ENERGIZER BATTERY MANUFACTURING, INC. ARE NOT
CLASSIFIED AS DANGEROUS GOODS BY THE US DEPARTMENT OF TRANSPORTATION OR THE
MAJOR INTERNATIONAL REGULATORY BODIES AND ARE THEREFORE NOT REGULATED.

SARA/TITLE III - AS AN ARTICLE, THIS BATTERY AND ITS CONTENTS ARE NOT
SUBJECT TO THE REQUIREMENTS OF THE EMERGENCY PLANNING AND COMMUNITY
RIGHT-TO-KNOW ACT.


SECTION 16 - OTHER INFORMATION 


NONE.

ENERGIZER HAS PREPARED COPYRIGHTED PRODUCT SAFETY DATASHEETS TO PROVIDE
INFORMATION ON THE DIFFERENT EVEREADY/ENERGIZER BATTERY SYSTEMS. AS DEFINED
IN OSHA HAZARD COMMUNICATION STANDARD, SECTION 1910.1200 (C),
EVEREADY/ENERGIZER BATTERIES ARE MANUFACTURED ARTICLES, WHICH DO NOT
RESULT IN EXPOSURE TO A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF USE.
THE INFORMATION AND RECOMMENDATIONS SET FORTH HEREIN ARE MADE IN GOOD
FAITH, FOR INFORMATION ONLY, AND ARE BELIEVED TO BE ACCURATE AS OF THE DATE
OF PREPARATION. HOWEVER, ENERGIZER BATTERY MANUFACTURING, INC., MAKES NO
WARRANTY, EITHER EXPRESS OR IMPLIED, WITH RESPECT TO THIS INFORMATION AND
DISCLAIMS ALL LIABILITY FROM REFERENCE ON IT.

(C)2011 ENERGIZER