Common Name: ULTIMATE (L91, L92); ADVANCED (EA91, EA92)
Manufacturer: ENERGIZER BATTERY
SDS Revision Date: 1/1/2011
SDS Format: No Format Specified
   
Grainger Item Number(s): 2LBJ6
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - MANUFACTURER INFORMATION 
SECTION 2 - HAZARDS IDENTIFICATION 
SECTION 3 - INGREDIENTS 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL CONSIDERATIONS 
SECTION 14 - TRANSPORT INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



ENERGIZER(R*)

PRODUCT SAFETY DATA SHEET

LITHIUM IRON DISULFIDE BATTERIES

JANUARY, 2011

PRODUCT SAFETY DATA SHEET

PRODUCT NAME: ENERGIZER BATTERY

TYPE NO.: L91, L92, EA91, EA92

VOLTS: 1.5

TRADE NAMES: ULTIMATE (L91, L92); ADVANCED (EA91, EA92)

APPROXIMATE WEIGHT: 7.6 G. (L92, EA92) - 14.5 G. (L91, EA91)

CHEMICAL SYSTEM: LITHIUM IRON

DISULFIDE DESIGNED FOR RECHARGE: NO


SECTION 1 - MANUFACTURER INFORMATION 


ENERGIZER BATTERY MANUFACTURING, INC.
25225 DETROIT RD.
WESTLAKE, OH 44145

TELEPHONE NUMBER FOR INFORMATION: 800-383-7323 (USA / CANADA)

DATE PREPARED: JANUARY, 2011


SECTION 2 - HAZARDS IDENTIFICATION 


UNDER NORMAL CONDITIONS OF USE, THE BATTERY IS HERMETICALLY SEALED.

INGESTION: SWALLOWING A BATTERY CAN BE HARMFUL.

INHALATION: CONTENTS OF AN OPEN BATTERY CAN CAUSE RESPIRATORY IRRITATION.

SKIN CONTACT: CONTENTS OF AN OPEN BATTERY CAN CAUSE SKIN IRRITATION.

EYE CONTACT: CONTENTS OF AN OPEN BATTERY CAN CAUSE SEVERE IRRITATION.


SECTION 3 - INGREDIENTS 


IMPORTANT NOTE:
THE BATTERY SHOULD NOT BE OPENED OR BURNED. EXPOSURE TO THE INGREDIENTS
CONTAINED WITHIN OR THEIR COMBUSTION PRODUCTS COULD BE HARMFUL.

MATERIAL OR INGREDIENT      PEL (OSHA)         TLV (ACGIH)        %/WT.

CARBON BLACK                3.5 MG/M3 TWA      3.5 MG/M3 TWA        0-4
(CAS# 1333-86-4)

1,2 DIEMETHOXYETHANE        NONE ESTABLISHED   NONE ESTABLISHED     2-4
(CAS# 110-71-4)

1,3 DIOXOLANE               NONE ESTABLISHED   20 PPM TWA           5-9
(CAS# 646-06-0)

GRAPHITE                    15 MG/M3 TWA       2 MG/M3 TWA          0-4
(CAS# 7782-42-5)            (TOTAL DUST)       (RESPIRABLE
                            5 MG/M3 TWA        FRACTION)
                            (RESPIRABLE
                            FRACTION)

IRON DISULFIDE              NONE ESTABLISHED   NONE ESTABLISHED    24-35
(CAS# 1309-36-0)

LITHIUM OR LITHIUM ALLOY    NONE ESTABLISHED   NONE ESTABLISHED   6.7/AA
                                                                  6.6/AAA

LITHIUM IODIDE              NONE ESTABLISHED   NONE ESTABLISHED   0.3-3

NON-HAZARDOUS COMPONENTS:

STEEL                       NONE ESTABLISHED   NONE ESTABLISHED    18-22
(IRON CAS# 7439-89-6)

PLASTIC AND OTHER           NONE ESTABLISHED   NONE ESTABLISHED   BALANCE


SECTION 4 - FIRST AID MEASURES 


INGESTION:
DO NOT INDUCE VOMITING OR GIVE FOOD OR DRINK. SEEK MEDICAL ATTENTION
IMMEDIATELY. CALL NATIONAL BATTERY INGESTION HOTLINE FOR ADVICE AND
FOLLOW-UP (202-625-3333) COLLECT DAY OR NIGHT.

INHALATION: PROVIDE FRESH AIR AND SEEK MEDICAL ATTENTION.

SKIN CONTACT:
REMOVE CONTAMINATED CLOTHING AND WASH SKIN WITH SOAP AND WATER.

EYE CONTACT:
IMMEDIATELY FLUSH EYES THOROUGHLY WITH WATER FOR AT LEAST 15 MINUTES,
LIFTING UPPER AND LOWER LIDS, UNTIL NO EVIDENCE OF THE CHEMICAL REMAINS.
SEEK MEDICAL ATTENTION.

NOTE:
CARBON BLACK IS LISTED AS A POSSIBLE CARCINOGEN BY INTERNATIONAL AGENCY
FOR RESEARCH ON CANCER (IARC).


SECTION 5 - FIRE FIGHTING MEASURES 


IN CASE OF FIRE WHERE LITHIUM BATTERIES ARE PRESENT, FLOOD AREA WITH
WATER OR SMOTHER WITH A CLASS D FIRE EXTINGUISHANT APPROPRIATE FOR
LITHIUM METAL, SUCH AS LITH-X. WATER MAY NOT EXTINGUISH BURNING BATTERIES
BUT WILL COOL THE ADJACENT BATTERIES AND CONTROL THE SPREAD OF FIRE.
BURNING BATTERIES WILL BURN THEMSELVES OUT. VIRTUALLY ALL FIRES
INVOLVING LITHIUM BATTERIES CAN BE CONTROLLED BY FLOODING WITH WATER.
HOWEVER, THE CONTENTS OF THE BATTERY WILL REACT WITH WATER AND FORM
HYDROGEN GAS. IN A CONFINED SPACE, HYDROGEN GAS CAN FORM AN EXPLOSIVE
MIXTURE. IN THIS SITUATION, SMOTHERING AGENTS ARE RECOMMENDED.
A SMOTHERING AGENT WILL EXTINGUISH BURNING LITHIUM BATTERIES.

EMERGENCY RESPONDERS SHOULD WEAR SELF-CONTAINED BREATHING APPARATUS.
BURNING LITHIUM-IRON DISULFIDE BATTERIES PRODUCE TOXIC AND CORROSIVE
LITHIUM HYDROXIDE FUMES AND SULFUR DIOXIDE GAS.


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


TO CLEANUP LEAKING BATTERIES:

VENTILATION REQUIREMENTS:
ROOM VENTILATION MAY BE REQUIRED IN AREAS WHERE THERE ARE OPEN OR
LEAKING BATTERIES.

RESPIRATORY PROTECTION:
AVOID EXPOSURE TO ELECTROLYTE FUMES FROM OPEN OR LEAKING BATTERIES.

EYE PROTECTION:
WEAR SAFETY GLASSES WITH SIDE SHIELDS IF HANDLING AN OPEN OR LEAKING
BATTERY.

GLOVES:
USE NEOPRENE OR NATURAL RUBBER GLOVES IF HANDLING AN OPEN OR LEAKING
BATTERY. BATTERY MATERIALS SHOULD BE DISPOSED OF IN A LEAK-PROOF CONTAINER.


SECTION 7 - HANDLING AND STORAGE 


STORAGE:
STORE IN A COOL, WELL VENTILATED AREA. ELEVATED TEMPERATURES CAN RESULT
IN SHORTENED BATTERY LIFE. IN LOCATIONS THAT HANDLE LARGE QUANTITIES OF
LITHIUM BATTERIES, SUCH AS WAREHOUSES, LITHIUM BATTERIES SHOULD BE
ISOLATED FROM UNNECESSARY COMBUSTIBLES.

MECHANICAL CONTAINMENT:
IF POTTING OR SEALING THE BATTERY IN AN AIRTIGHT OR WATERTIGHT CONTAINER
IS REQUIRED, CONSULT YOUR ENERGIZER BATTERY MANUFACTURING, INC.
REPRESENTATIVE FOR PRECAUTIONARY SUGGESTIONS. DO NOT OBSTRUCT SAFETY
RELEASE VENTS ON BATTERIES. ENCAPSULATION OF BATTERIES WILL NOT ALLOW
CELL VENTING AND CAN CAUSE HIGH PRESSURE RUPTURE.

HANDLING:
ACCIDENTAL SHORT CIRCUIT FOR A FEW SECONDS WILL NOT SERIOUSLY AFFECT THE
BATTERY. PROLONGED SHORT CIRCUIT WILL CAUSE THE BATTERY TO LOSE ENERGY,
GENERATE SIGNIFICANT HEAT AND CAN CAUSE THE SAFETY RELEASE VENT TO OPEN.
SOURCES OF SHORT CIRCUITS INCLUDE JUMBLED BATTERIES IN BULK CONTAINERS,
METAL JEWELRY, METAL COVERED TABLES OR METAL BELTS USED FOR ASSEMBLY OF
BATTERIES INTO DEVICES. DAMAGING A LITHIUM BATTERY MAY RESULT IN AN
INTERNAL SHORT CIRCUIT.

THE CONTENTS OF AN OPEN BATTERY, INCLUDING A VENTED BATTERY, WHEN EXPOSED
TO WATER, MAY RESULT IN A FIRE AND/OR EXPLOSION. CRUSHED OR DAMAGED
BATTERIES MAY RESULT IN A FIRE.

IF SOLDERING OR WELDING TO THE BATTERY IS REQUIRED, CONSULT YOUR
ENERGIZER REPRESENTATIVE FOR PROPER PRECAUTIONS TO PREVENT SEAL DAMAGE
OR SHORT CIRCUIT.

CHARGING:
THIS BATTERY IS MANUFACTURED IN A CHARGED STATE. IT IS NOT DESIGNED FOR
RECHARGING. RECHARGING CAN CAUSE BATTERY LEAKAGE OR, IN SOME CASES, HIGH
PRESSURE RUPTURE. INADVERTENT CHARGING CAN OCCUR IF A BATTERY IS
INSTALLED BACKWARDS.

LABELING:
IF THE ENERGIZER LABEL OR PACKAGE WARNINGS ARE NOT VISIBLE, IT IS
IMPORTANT TO PROVIDE A PACKAGE AND/OR DEVICE LABEL STATING:

WARNING:
BATTERY CAN EXPLODE OR LEAK AND CAUSE BURNS IF INSTALLED BACKWARDS,
DISASSEMBLED, CHARGED, OR EXPOSED TO WATER, FIRE OR HIGH TEMPERATURE.

WHERE ACCIDENTAL INGESTION OF SMALL BATTERIES IS POSSIBLE, THE LABEL
SHOULD INCLUDE:

WARNING:
(1) KEEP AWAY FROM SMALL CHILDREN. IF SWALLOWED, PROMPTLY SEE DOCTOR;
HAVE DOCTOR PHONE (202) 625-3333 COLLECT.

(2) BATTERY CAN EXPLODE OR LEAK AND CAUSE BURNS IF INSTALLED BACKWARDS,
DISASSEMBLED, CHARGED, OR EXPOSED TO WATER, FIRE OR HIGH TEMPERATURE.


SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 


VENTILATION REQUIREMENTS: NOT NECESSARY UNDER NORMAL CONDITIONS.

RESPIRATORY PROTECTION: NOT NECESSARY UNDER NORMAL CONDITIONS.

EYE PROTECTION: NOT NECESSARY UNDER NORMAL CONDITIONS.

GLOVES: NOT NECESSARY UNDER NORMAL CONDITIONS.


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


BOILING POINT @ 760 MMHg (DEG. C): NOT APPLICABLE FOR AN ARTICLE

VAPOR PRESSURE (MMHg @ 25 DEG. C): NOT APPLICABLE FOR AN ARTICLE

VAPOR DENSITY (AIR = 1): NOT APPLICABLE FOR AN ARTICLE

DENSITY (G/CM3): 1.7 - 2.0

PERCENT VOLATILE BY VOLUME (%): NOT APPLICABLE FOR AN ARTICLE

EVAPORATION RATE (BUTYL ACETATE = 1): NOT APPLICABLE FOR AN ARTICLE

PHYSICAL STATE: SOLID

SOLUBILITY IN WATER (% BY WEIGHT): NOT APPLICABLE FOR AN ARTICLE

pH: NOT APPLICABLE FOR AN ARTICLE

APPEARANCE AND ODOR: SOLID OBJECT / NO ODOR


SECTION 10 - STABILITY AND REACTIVITY 


LITHIUM IRON DISULFIDE BATTERIES DO NOT MEET ANY OF THE CRITERIA
ESTABLISHED IN 40 CFR 261.2 FOR REACTIVITY.


SECTION 11 - TOXICOLOGICAL INFORMATION 


LITHIUM IRON DISULFIDE BATTERIES ARE NOT HAZARDOUS WASTE. UNDER NORMAL
CONDITIONS OF USE, LITHIUM IRON DISULFIDE BATTERIES ARE NON-TOXIC.


SECTION 12 - ECOLOGICAL INFORMATION 


ISSUES SUCH AS ECOTOXICITY, PERSISTENCE AND BIOACCUMULATION ARE NOT
APPLICABLE FOR ARTICLES.


SECTION 13 - DISPOSAL CONSIDERATIONS 


DISPOSE OF IN ACCORDANCE WITH ALL APPLICABLE FEDERAL, STATE AND LOCAL
REGULATIONS.


SECTION 14 - TRANSPORT INFORMATION 


IN GENERAL, ALL BATTERIES IN ALL FORMS OF TRANSPORTATION (GROUND, AIR,
OR OCEAN) MUST BE PACKAGED IN A SAFE AND RESPONSIBLE MANNER. REGULATORY
CONCERNS FROM ALL AGENCIES FOR SAFE PACKAGING REQUIRE THAT BATTERIES BE
PACKAGED IN A MANNER THAT PREVENTS SHORT CIRCUITS AND BE CONTAINED IN
"STRONG OUTER PACKAGING" THAT PREVENTS SPILLAGE OF CONTENTS. ALL ORIGINAL
PACKAGING FOR ENERGIZER LITHIUM BATTERIES ARE COMPLIANT WITH THESE
REGULATORY CONCERNS.

ENERGIZER LITHIUM-IRON DISULFIDE BATTERIES ARE EXEMPT FROM THE
CLASSIFICATION AS DANGEROUS GOODS AS THEY MEET THE REQUIREMENTS OF
THE SPECIAL PROVISIONS LISTED BELOW. (ESSENTIALLY, THEY ARE PROPERLY
PACKAGED AND LABELED, CONTAIN LESS THAN 1 GRAM OF LITHIUM AND PASS THE
TESTS DEFINED IN UN MODEL REGULATION SECTION 38.3).

REGULATORY BODY               SPECIAL PROVISIONS

ADR                           188, 230, 310, 636

IMDG                          188, 230, 310, 957

UN                            UN 3090, UN 3091

US DOT                        29, A54, A55, 101, 102, A100

IATA, ICAO                    PACKAGING INSTRUCTIONS 968 - 970


SECTION 15 - REGULATORY INFORMATION 


OUTSIDE OF THE TRANSPORTATION REQUIREMENTS NOTED IN SECTION 14, LITHIUM
IRON DISULFIDE BATTERIES MARKETED BY ENERGIZER BATTERY MANUFACTURING,
INC. ARE NOT REGULATED.

SARA/TITLE III - AS AN ARTICLE, THIS BATTERY AND ITS CONTENTS ARE NOT
SUBJECT TO THE REQUIREMENTS OF THE EMERGENCY PLANNING AND COMMUNITY
RIGHT-TO-KNOW ACT.


SECTION 16 - OTHER INFORMATION 


NONE.

ENERGIZER HAS PREPARED COPYRIGHTED PRODUCT SAFETY DATASHEETS TO PROVIDE
INFORMATION ON THE DIFFERENT EVEREADY/ENERGIZER BATTERY SYSTEMS. AS
DEFINED IN OSHA HAZARD COMMUNICATION STANDARD, SECTION 1910.1200 (C),
EVEREADY/ENERGIZER BATTERIES ARE MANUFACTURED ARTICLES, WHICH DO NOT
RESULT IN EXPOSURE TO A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF
USE. THE INFORMATION AND RECOMMENDATIONS SET FORTH HEREIN ARE MADE IN
GOOD FAITH, FOR INFORMATION ONLY, AND ARE BELIEVED TO BE ACCURATE AS OF
THE DATE OF PREPARATION. HOWEVER, ENERGIZER BATTERY MANUFACTURING, INC.,
MAKES NO WARRANTY, EITHER EXPRESS OR IMPLIED, WITH RESPECT TO THIS
INFORMATION AND DISCLAIMS ALL LIABILITY FROM REFERENCE ON IT.

(C)2011 ENERGIZER