Common Name: PVTLBL SSPR 6PK TG ENAML ULTRA FLAT BLCK
Manufacturer: W.W. GRAINGER
SDS Revision Date: 1/11/2010
SDS Format: No Format Specified
   
Grainger Item Number(s): 4WGC1
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - CHEMICAL PRODUCT / COMPANY INFORMATION 
SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS / PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL INFORMATION 
SECTION 14 - TRANSPORTATION INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET

24 HOUR ASSISTANCE: 800-228-5635


SECTION 1 - CHEMICAL PRODUCT / COMPANY INFORMATION 


PRODUCT NAME: PVTLBL SSPR 6PK TG ENAML ULTRA FLAT BLCK

IDENTIFICATION NUMBER: 251834

PRODUCT USE/CLASS: TOUGH GUY AEROSOLS 4WGC1

SUPPLIER:
W.W. GRAINGER
100 GRAINGER PARKWAY
LAKE FOREST, IL 60045-5201
USA

MANUFACTURER:
W.W. GRAINGER
100 GRAINGER PARKWAY
LAKE FOREST, IL 60045-5201
USA

PREPARER: REGULATORY DEPARTMENT

REVISION DATE: 01/11/2010


SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 


CHEMICAL     CAS         WEIGHT  ACGIH    ACGIH     OSHA          OSHA PEL
NAME         NUMBER      % LESS  TLV-TWA  TLV-STEL  PEL-TWA       CEILING
                         THAN

ACETONE         67-64-1  35.0    500 PPM  750 PPM   1000 PPM      N.E.

LIQUEFIED    68476-86-8  30.0    N.E.     N.E.      N.E.          N.E.
PETROLEUM
GAS

MINERAL      64742-88-7  10.0    100 PPM  N.E.      100 PPM       N.E.
SPIRITS

ALIPHATIC    64742-89-8  10.0    N.E.     N.E.      300 PPM       N.E.
HYDROCARBON

XYLENE        1330-20-7  5.0     100 PPM  150 PPM   100 PPM       N.E.

NAPHTHA       8032-32-4  5.0     N.E.     N.E.      N.E.          N.E.

MAGNESIUM    14807-96-6  5.0     2 MG/M3  N.E.      0.1 MG/M3     N.E.
SILICATE                                            (RESPIRABLE)

PIGMENT       1333-86-4  5.0     3.5      N.E.      3.5 MG/M3     N.E.
BLACK 7                          MG/M3

ETHYL-         100-41-4  5.0     100 PPM  125 PPM   100 PPM       N.E.
BENZENE


SECTION 3 - HAZARDS IDENTIFICATION 


EMERGENCY OVERVIEW:
CONTENTS UNDER PRESSURE. HARMFUL IF INHALED. MAY AFFECT THE BRAIN OR
NERVOUS SYSTEM CAUSING DIZZINESS, HEADACHE OR NAUSEA. VAPORS MAY CAUSE
FLASH FIRE OR EXPLOSION. HARMFUL IF SWALLOWED. EXTREMELY FLAMMABLE
LIQUID AND VAPOR.

EFFECTS OF OVEREXPOSURE - EYE CONTACT: CAUSES EYE IRRITATION.

EFFECTS OF OVEREXPOSURE - SKIN CONTACT:
PROLONGED OR REPEATED CONTACT MAY CAUSE SKIN IRRITATION. SUBSTANCE MAY
CAUSE SLIGHT SKIN IRRITATION.

EFFECTS OF OVEREXPOSURE - INHALATION:
HIGH VAPOR CONCENTRATIONS ARE IRRITATING TO THE EYES, NOSE, THROAT AND
LUNGS. AVOID BREATHING VAPORS OR MISTS. HIGH GAS, VAPOR, MIST OR DUST
CONCENTRATIONS MAY BE HARMFUL IF INHALED. HARMFUL IF INHALED.

EFFECTS OF OVEREXPOSURE - INGESTION:
ASPIRATION HAZARD IF SWALLOWED; CAN ENTER LUNGS AND CAUSE DAMAGE.
SUBSTANCE MAY BE HARMFUL IF SWALLOWED.

EFFECTS OF OVEREXPOSURE - CHRONIC HAZARDS:
IARC LISTS ETHYLBENZENE AS A POSSIBLE HUMAN CARCINOGEN (GROUP 2B). MAY
CAUSE CENTRAL NERVOUS SYSTEM DISORDER (E.G., NARCOSIS INVOLVING A LOSS
OF COORDINATION, WEAKNESS, FATIGUE, MENTAL CONFUSION, AND BLURRED VISION)
AND/OR DAMAGE. REPORTS HAVE ASSOCIATED REPEATED AND PROLONGED OCCUPATIONAL
OVEREXPOSURE TO SOLVENTS WITH PERMANENT BRAIN AND NERVOUS SYSTEM DAMAGE.
OVEREXPOSURE TO XYLENE IN LABORATORY ANIMALS HAS BEEN ASSOCIATED WITH
LIVER ABNORMALITIES, KIDNEY, LUNG, SPLEEN, EYE AND BLOOD DAMAGE AS WELL
AS REPRODUCTIVE DISORDERS. EFFECTS IN HUMANS, DUE TO CHRONIC OVEREXPOSURE,
HAVE INCLUDED LIVER, CARDIAC ABNORMALITIES AND NERVOUS SYSTEM DAMAGE.

CONTAINS CARBON BLACK. CHRONIC INFLAMMATION, LUNG FIBROSIS, AND LUNG
TUMORS HAVE BEEN OBSERVED IN SOME RATS EXPERIMENTALLY EXPOSED FOR LONG
PERIODS OF TIME TO EXCESSIVE CONCENTRATIONS OF CARBON BLACK AND SEVERAL
INSOLUBLE FINE DUST PARTICLES. TUMORS HAVE NOT BEEN OBSERVED IN OTHER
ANIMAL SPECIES (I.E., MOUSE AND HAMSTER) UNDER SIMILAR CIRCUMSTANCES AND
STUDY CONDITIONS. EPIDEMIOLOGICAL STUDIES OF NORTH AMERICAN WORKERS SHOW
NO EVIDENCE OF CLINICALLY SIGNIFICANT ADVERSE HEALTH EFFECTS DUE TO
OCCUPATIONAL EXPOSURE TO CARBON BLACK.

CARBON BLACK IS LISTED AS A GROUP 2B-"POSSIBLY CARCINOGENIC TO HUMANS"
BY IARC AND IS PROPOSED TO BE LISTED AS A4- "NOT CLASSIFIED AS A HUMAN
CARCINOGEN" BY THE AMERICAN CONFERENCE OF GOVERNMENTAL INDUSTRIAL
HYGIENISTS. SIGNIFICANT EXPOSURE IS NOT ANTICIPATED DURING BRUSH
APPLICATION OR DRYING. RISK OF OVEREXPOSURE DEPENDS ON DURATION AND
LEVEL OF EXPOSURE TO DUST FROM REPEATED SANDING OF SURFACES OR SPRAY
MIST AND THE ACTUAL CONCENTRATION OF CARBON BLACK IN THE FORMULA.

PRIMARY ROUTE(S) OF ENTRY:
SKIN CONTACT, SKIN ABSORPTION, INHALATION, INGESTION, EYE CONTACT


SECTION 4 - FIRST AID MEASURES 


FIRST AID - EYE CONTACT:
IMMEDIATELY FLUSH EYES WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES
HOLDING EYELIDS OPEN. GET MEDICAL ATTENTION. DO NOT ALLOW RUBBING OF
EYES OR KEEPING EYES CLOSED.

FIRST AID - SKIN CONTACT:
WASH WITH SOAP AND WATER. GET MEDICAL ATTENTION IF IRRITATION DEVELOPS
OR PERSISTS.

FIRST AID - INHALATION:
IF YOU EXPERIENCE DIFFICULTY IN BREATHING, LEAVE THE AREA TO OBTAIN
FRESH AIR. IF CONTINUED DIFFICULTY IS EXPERIENCED, GET MEDICAL
ASSISTANCE IMMEDIATELY.

FIRST AID - INGESTION:

ASPIRATION HAZARD:
DO NOT INDUCE VOMITING OR GIVE ANYTHING BY MOUTH BECAUSE THIS MATERIAL
CAN ENTER THE LUNGS AND CAUSE SEVERE LUNG DAMAGE. GET IMMEDIATE MEDICAL
ATTENTION.


SECTION 5 - FIRE FIGHTING MEASURES 


FLASH POINT (SETAFLASH): -156 F

LOWER EXPLOSIVE LIMIT: 0.7%
UPPER EXPLOSIVE LIMIT: 12.8%

EXTINGUISHING MEDIA:
FILM FORMING FOAM, CARBON DIOXIDE, DRY CHEMICAL, WATER FOG

UNUSUAL FIRE AND EXPLOSION HAZARDS:
WATER SPRAY MAY BE INEFFECTIVE. CLOSED CONTAINERS MAY EXPLODE WHEN
EXPOSED TO EXTREME HEAT. VAPORS MAY FORM EXPLOSIVE MIXTURES WITH AIR.
VAPORS CAN TRAVEL TO A SOURCE OF IGNITION AND FLASH BACK.

FLASH POINT IS LESS THAN 20 DEG. .F. - EXTREMELY FLAMMABLE LIQUID AND
VAPOR!

KEEP CONTAINERS TIGHTLY CLOSED. ISOLATE FROM HEAT, ELECTRICAL EQUIPMENT,
SPARKS AND OPEN FLAME. PERFORATION OF THE PRESSURIZED CONTAINER MAY
CAUSE BURSTING OF THE CAN.

SPECIAL FIREFIGHTING PROCEDURES:
EVACUATE AREA AND FIGHT FIRE FROM A SAFE DISTANCE.


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


STEPS TO BE TAKEN IF MATERIAL IS RELEASED OR SPILLED:
CONTAIN SPILLED LIQUID WITH SAND OR EARTH. DO NOT USE COMBUSTIBLE
MATERIALS SUCH AS SAWDUST. DISPOSE OF ACCORDING TO LOCAL, STATE
(PROVINCIAL) AND FEDERAL REGULATIONS. DO NOT INCINERATE CLOSED
CONTAINERS. REMOVE ALL SOURCES OF IGNITION, VENTILATE AREA AND REMOVE
WITH INERT ABSORBENT AND NON-SPARKING TOOLS.


SECTION 7 - HANDLING AND STORAGE 


HANDLING:
WASH THOROUGHLY AFTER HANDLING. FOLLOW ALL MSDS/LABEL PRECAUTIONS EVEN
AFTER CONTAINER IS EMPTIED BECAUSE IT MAY RETAIN PRODUCT RESIDUES.
AVOID BREATHING VAPOR OR MIST. USE ONLY IN A WELL-VENTILATED AREA.
WASH HANDS BEFORE EATING.

STORAGE:
KEEP CONTAINERS TIGHTLY CLOSED. ISOLATE FROM HEAT, ELECTRICAL EQUIPMENT,
SPARKS AND OPEN FLAME. DO NOT STORE ABOVE 120 DEG. F. STORE LARGE
QUANTITIES IN BUILDINGS DESIGNED AND PROTECTED FOR STORAGE OF NFPA CLASS I
FLAMMABLE LIQUIDS. CONTENTS UNDER PRESSURE. DO NOT EXPOSE TO HEAT OR
STORE ABOVE 120 DEG. F.


SECTION 8 - EXPOSURE CONTROLS / PERSONAL PROTECTION 


ENGINEERING CONTROLS:
PREVENT BUILD-UP OF VAPORS BY OPENING ALL DOORS AND WINDOWS TO ACHIEVE
CROSS-VENTILATION. USE PROCESS ENCLOSURES, LOCAL EXHAUST VENTILATION,
OR OTHER ENGINEERING CONTROLS TO CONTROL AIRBORNE LEVELS BELOW
RECOMMENDED EXPOSURE LIMITS. USE EXPLOSION-PROOF VENTILATION EQUIPMENT.

RESPIRATORY PROTECTION:
A RESPIRATORY PROTECTION PROGRAM THAT MEETS OSHA 1910.134 AND ANSI Z88.2
REQUIREMENTS MUST BE FOLLOWED WHENEVER WORKPLACE CONDITIONS WARRANT A
RESPIRATOR'S USE. A NIOSH/MSHA APPROVED AIR PURIFYING RESPIRATOR WITH
AN ORGANIC VAPOR CARTRIDGE OR CANISTER MAY BE PERMISSIBLE UNDER CERTAIN
CIRCUMSTANCES WHERE AIRBORNE CONCENTRATIONS ARE EXPECTED TO EXCEED
EXPOSURE LIMITS.

PROTECTION PROVIDED BY AIR PURIFYING RESPIRATORS IS LIMITED. USE A
POSITIVE PRESSURE AIR SUPPLIED RESPIRATOR IF THERE IS ANY POTENTIAL FOR
AN UNCONTROLLED RELEASE, EXPOSURE LEVELS ARE NOT KNOWN, OR IN ANY OTHER
CIRCUMSTANCES WHERE AIR PURIFYING RESPIRATORS MAY NOT PROVIDE ADEQUATE
PROTECTION.

SKIN PROTECTION:
USE IMPERVIOUS GLOVES TO PREVENT SKIN CONTACT AND ABSORPTION OF THIS
MATERIAL THROUGH THE SKIN. NITRILE OR NEOPRENE GLOVES MAY AFFORD ADEQUATE
SKIN PROTECTION.

EYE PROTECTION:
USE SAFETY EYEWEAR DESIGNED TO PROTECT AGAINST SPLASH OF LIQUIDS.

OTHER PROTECTIVE EQUIPMENT:
REFER TO SAFETY SUPERVISOR OR INDUSTRIAL HYGIENIST FOR FURTHER INFORMATION
REGARDING PERSONAL PROTECTIVE EQUIPMENT AND ITS APPLICATION.

HYGIENIC PRACTICES:
WASH THOROUGHLY WITH SOAP AND WATER BEFORE EATING, DRINKING OR SMOKING.


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


BOILING RANGE: -34 - 999 F

VAPOR DENSITY: HEAVIER THAN AIR

ODOR: SOLVENT LIKE

ODOR THRESHOLD: N.E.

APPEARANCE: AEROSOLIZED MIST

EVAPORATION RATE: FASTER THAN ETHER

SOLUBILITY IN H2O: SLIGHT

FREEZE POINT: N.D.

SPECIFIC GRAVITY: 0.760

VAPOR PRESSURE: N.D.

pH: N.A.

PHYSICAL STATE: LIQUID

(SEE SECTION 16 FOR ABBREVIATION LEGEND)


SECTION 10 - STABILITY AND REACTIVITY 


CONDITIONS TO AVOID:
AVOID TEMPERATURES ABOVE 120 DEG. F. AVOID ALL POSSIBLE SOURCES OF
IGNITION.

INCOMPATIBILITY:
INCOMPATIBLE WITH STRONG OXIDIZING AGENTS, STRONG ACIDS AND STRONG
ALKALIES.

HAZARDOUS DECOMPOSITION:
WHEN HEATED TO DECOMPOSITION, IT EMITS ACRID SMOKE AND IRRITATING FUMES.
BY OPEN FLAME, CARBON MONOXIDE AND CARBON DIOXIDE.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR UNDER NORMAL CONDITIONS.

STABILITY: THIS PRODUCT IS STABLE UNDER NORMAL STORAGE CONDITIONS.


SECTION 11 - TOXICOLOGICAL INFORMATION 


PRODUCT LD50: N.D.

PRODUCT LC50: N.D.

CHEMICAL NAME            LD50                     LC50

ACETONE                  5800 MG/KG (RAT)         50100 MG/M3 (RAT, 8HR)

LIQUEFIED PETROLEUM GAS  N.E.                     N.E.

MINERAL SPIRITS          >8 MG/KG (RAT, ORAL)     >1400 PPM
                                                  (RAT, INHALATION, 4HR)

ALIPHATIC HYDROCARBON    >5000 MG/KG (RAT, ORAL)  N.E.

XYLENE                   4300 MG/KG (RAT, ORAL)   5000 PPM
                                                  (RAT, INHALATION, 4HR)

NAPHTHA                  >5000 MG/KG (RAT, ORAL)  N.E.

MAGNESIUM SILICATE       N.E.                     TCLO:
                                                  11 MG/M3 (INHALATION)

PIGMENT BLACK 7          >8000 MG/KG (RAT, ORAL)  N.E.

ETHYLBENZENE             3500 MG/KG (RAT, ORAL)   N.E.


SECTION 12 - ECOLOGICAL INFORMATION 


ECOLOGICAL INFORMATION: PRODUCT IS A MIXTURE OF LISTED COMPONENTS.


SECTION 13 - DISPOSAL INFORMATION 


DISPOSAL INFORMATION:
DISPOSE OF MATERIAL IN ACCORDANCE TO LOCAL, STATE AND FEDERAL REGULATIONS
AND ORDINANCES. DO NOT ALLOW TO ENTER STORM DRAINS OR SEWER SYSTEMS.


SECTION 14 - TRANSPORTATION INFORMATION 


DOT PROPER SHIPPING NAME: CONSUMER COMMODITY

DOT TECHNICAL NAME: N.A.

DOT UN/NA NUMBER: N.A.

DOT HAZARD CLASS: ORM-D

PACKING GROUP: N.A.

HAZARD SUBCLASS: N.A.

RESP. GUIDE PAGE: 126


SECTION 15 - REGULATORY INFORMATION 


CERCLA - SARA HAZARD CATEGORY:

THIS PRODUCT HAS BEEN REVIEWED ACCORDING TO THE EPA "HAZARD CATEGORIES"
PROMULGATED UNDER SECTIONS 311 AND 312 OF THE SUPERFUND AMENDMENT AND
REAUTHORIZATION ACT OF 1986 (SARA TITLE III) AND IS CONSIDERED, UNDER
APPLICABLE DEFINITIONS, TO MEET THE FOLLOWING CATEGORIES:
IMMEDIATE HEALTH HAZARD, CHRONIC HEALTH HAZARD, FIRE HAZARD, PRESSURIZED
GAS HAZARD

SARA SECTION 313:

LISTED BELOW ARE THE SUBSTANCES (IF ANY) CONTAINED IN THIS PRODUCT THAT
ARE SUBJECT TO THE REPORTING REQUIREMENTS OF SECTION 313 OF TITLE III OF
THE SUPERFUND AMENDMENT AND REAUTHORIZATION ACT OF 1986 AND
40 CFR PART 372:

CHEMICAL NAME                             CAS NUMBER

XYLENE                                    1330-20-7

ETHYLBENZENE                               100-41-4

TOXIC SUBSTANCES CONTROL ACT:

LISTED BELOW ARE THE SUBSTANCES (IF ANY) CONTAINED IN THIS PRODUCT THAT
ARE SUBJECT TO THE REPORTING REQUIREMENTS OF TSCA 12(B) IF EXPORTED FROM
THE UNITED STATES:

U.S. STATE REGULATIONS: AS FOLLOWS

NEW JERSEY RIGHT-TO-KNOW:
THE FOLLOWING MATERIALS ARE NON-HAZARDOUS, BUT ARE AMONG THE TOP FIVE
COMPONENTS IN THIS PRODUCT.

CHEMICAL NAME                             CAS NUMBER

MODIFIED ALKYD                            PROPRIETARY

PENNSYLVANIA RIGHT-TO-KNOW:
THE FOLLOWING NON-HAZARDOUS INGREDIENTS ARE PRESENT IN THE PRODUCT AT
GREATER THAN 3%.

CHEMICAL NAME                             CAS NUMBER

MODIFIED ALKYD                            PROPRIETARY

CALCIUM CARBONATE                         1317-65-3

CALIFORNIA PROPOSITION 65:

WARNING!

THIS PRODUCT CONTAINS A CHEMICAL(S) KNOWN BY THE STATE OF CALIFORNIA TO
CAUSE CANCER.

WARNING!

THIS PRODUCT CONTAINS A CHEMICAL(S) KNOWN TO THE STATE OF CALIFORNIA TO
CAUSE BIRTH DEFECTS OR OTHER REPRODUCTIVE HARM.

INTERNATIONAL REGULATIONS: AS FOLLOWS

CANADIAN WHMIS:
THIS MSDS HAS BEEN PREPARED IN COMPLIANCE WITH CONTROLLED PRODUCT
REGULATIONS EXCEPT FOR THE USE OF THE 16 HEADINGS.

CANADIAN WHMIS CLASS:
AB5
D2A
D2B


SECTION 16 - OTHER INFORMATION 


HMIS RATINGS:
HEALTH              2*
FLAMMABILITY        4
REACTIVITY          0
PERSONAL PROTECTION X

REASON FOR REVISION: REGULATORY UPDATE

LEGEND:
N.A. - NOT APPLICABLE
N.E. - NOT ESTABLISHED
N.D. - NOT DETERMINED

THE INFORMATION CONTAINED ON THIS MSDS HAS BEEN CHECKED AND SHOULD BE
ACCURATE. HOWEVER, IT IS THE RESPONSIBILITY OF THE USER TO COMPLY WITH
ALL FEDERAL, STATE, AND LOCAL LAWS AND REGULATIONS.