Common Name: BP-80
Manufacturer: ALEXANDER TECHNOLOGIES
SDS Revision Date: 3/1/2011
SDS Format: No Format Specified
   
Item Number(s): 13D361, 13D363, 13D365, 13D366, 13D367, 13D369, 13D370, 13D371, 13P969, 13P970, 13P971, 13P972, 13P973, 13P974, 13P975, 13P976, 13P981, 24Z215, 24Z216, 24Z217
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. PRODUCT IDENTIFICATION 
2. COMPOSITION / INFORMATION ON INGREDIENTS 
3. PHYSICAL DATA 
4. FIRE AND EXPLOSION HAZARD DATA 
5. REACTIVITY DATA 
6. HEALTH HAZARD DATA 
7. PRECAUTIONS FOR SAFE HANDLING AND USE 
8. CONTROL MEASURE 
9. RECYCLING AND DISPOSAL 
10. TRANSPORTATION 



MSDS - MATERIAL SAFETY DATA SHEET

BP-80

HUSKIE TOOLS

ALEXANDER(R*) TECHNOLOGIES

ALEXANDER TECHNOLOGIES
1511 S GARFIELD PLACE
MASON CITY, IA 50401
641-423-8955

FOR CHEMICAL EMERGENCY: SPILL, LEAK, FIRE, EXPOSURE, OR ACCIDENT

CALL ALEXANDER TECH: 800-323-3779


1. PRODUCT IDENTIFICATION 


PRODUCT NAME: BP-80

MODEL: 14.8V 3000MAH

CHEMICAL SYSTEM: LITHIUM ION

DESIGNATED FOR RECHARGE:
YES (X)
NO  ( )


2. COMPOSITION / INFORMATION ON INGREDIENTS 


IMPORTANT NOTE:
THE BATTERY CELL SHOULD NOT BE OPENED OR EXPOSED TO HEAT BECAUSE EXPOSURE
TO THE FOLLOWING INGREDIENTS CONTAINED WITHIN COULD BE HARMFUL UNDER SOME
CIRCUMSTANCES.

CHEMICAL NAME                 CAS NO.             PEL          TLV

DIMETHYL CARBONATE            (CAS NO. 616-38-6)  NONE         NONE
                                                  ESTABLISHED  ESTABLISHED

ETHYLENE CARBONATE             (CAS NO. 96-49-1)  NONE         NONE
                                                  ESTABLISHED  ESTABLISHED

LITHIUM HEXAFLUOROPHOSPHATE  (CAS NO 21324-40-3)  NONE         NONE
                                                  ESTABLISHED  ESTABLISHED

PROPYLENE CARBONATE           (CAS NO. 108-32-7)  NONE         NONE
                                                  ESTABLISHED  ESTABLISHED


3. PHYSICAL DATA 


PHYSICAL PHASE: SOLID

COLOR: CONTENTS SILVER IN COLOR.

ODOR: NONE

BOILING POINT/BOILING RANGE: NA DEG. C

MELTING POINT: NA DEG. C

pH VALUE: NA

DECOMPOSITION TEMPERATURE: NA DEG. C

FLASH POINT: NA DEG. C
TEST METHOD: OPEN CUP CLOSE CUP

IGNITION TEMPERATURE: NA DEG. C

EXPLOSION LIMITS:
(LEL): NA %
(UEL): NA %

VAPOR PRESSURE: 1.1-1.3 KPA @ 20 DEG. C

VAPOR DENSITY: 3.5

RELATIVE DENSITY: 1.2 KG/LITER

SOLUBILITY: MISCIBLE IN WATER


4. FIRE AND EXPLOSION HAZARD DATA 


EXTINGUISHING MEDIA: WATER

FLAMMABLE LIMITS: NOT AVAILABLE

SPECIAL FIRE FIGHTING PROCEDURE:
IN CASE OF FIRE IN AN ADJACENT AREA, USE WATER, CO2 OR DRY CHEMICAL
EXTINGUISHERS IF CELLS ARE PACKED IN THEIR ORIGINAL CONTAINERS SINCE THE
FUEL OF THE FIRE ARE BASICALLY PAPER PRODUCTS. FOR BULK QUANTITY OF
UNPACKAGED CELLS USE LITH-X (GRAPHITE BASE). IN THIS CASE DO NOT USE WATER.


5. REACTIVITY DATA 


STABILITY: STABLE

CONDITIONS TO AVOID: DO NOT HEAT, DISASSEMBLE OR OVERCHARGE.

HAZARDOUS DECOMPOSITION OR BY PRODUCTS: N/A

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.


6. HEALTH HAZARD DATA 


ROUTES OF ENTRY:
INHALATION: YES
SKIN: YES
INGESTION: YES

HEALTH HAZARDS (ACUTE AND CHRONIC):
THESE CHEMICALS ARE CONTAINED IN A SEALED CAN. RISK OF EXPOSURE OCCURS ONLY
IF THE BATTERY IS MECHANICALLY OR ELECTRICALLY ABUSED. THE MOST LIKELY RISK
IS AN ACUTE EXPOSURE WHEN THE GAS RELEASE VENT WORKS. ORGANIC SOLVENT HAS
SLIGHT TOXICITY AND CAN IRRITATE SKIN AND EYES. LITHIUM SALT IS IRRITATING
TO SKIN, EYES AND MUCOUS MEMBRANES AND SHOULD BE AVOIDED.

CARCINOGENICITY:
NTP: NONE
IARC MONOGRAPH: NONE
OSHA REGULATED: NONE

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
AN ACUTE EXPOSURE WILL NOT GENERALLY AGGRAVATE ANY MEDICAL CONDITION.

EMERGENCY AND FIRST AID PROCEDURES:
IN CASE OF SKIN CONTACT WITH CONTENTS OF BATTERY, FLUSH IMMEDIATELY WITH
WATER. FOR EYE CONTACT, FLUSH WITH COPIOUS AMOUNTS OF WATER FOR 15 MINUTES.
DO NOT INHALE LEAKED MATERIAL. IF IRRITATION PERSISTS, GET MEDICAL HELP.


7. PRECAUTIONS FOR SAFE HANDLING AND USE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:

THE PREFERRED RESPONSE IS TO LEAVE THE AREA AND ALLOW THE BATTERIES TO COOL
AND THE VAPORS TO DISSIPATE.

AVOID SKIN AND EYE CONTACT OR INHALATION OF VAPORS. REMOVE SPILLED LIQUID
WITH ABSORBENT AND INCINERATE.

WASTE DISPOSAL METHOD:
DISPOSE IN ACCORDANCE WITH APPROPRIATE REGULATIONS. OPEN CELLS SHOULD BE
TREATED AS HAZARDOUS WASTE.

PRECAUTIONS TO BE TAKEN IN HANDLING AND STORING:
AVOID MECHANICAL OR ELECTRICAL ABUSE.

OTHER PRECAUTIONS:
BATTERIES MAY EXPLODE OR CAUSE BURNS, IF DISASSEMBLED, CRUSHED OR EXPOSED
TO FIRE OR HIGH TEMPERATURES. DO NOT SHORT OR INSTALL WITH INCORRECT
POLARITY.


8. CONTROL MEASURE 


RESPIRATORY PROTECTION (SPECIFY TYPE):
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

VENTILATION: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

PROTECTIVE GLOVES: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

EYE PROTECTION: NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.

OTHER PROTECTIVE CLOTHING OR EQUIPMENT:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE.


9. RECYCLING AND DISPOSAL 


ALEXANDER TECHNOLOGIES ENCOURAGES BATTERY RECYCLING. LITHIUM ION BATTERIES
ARE SAFE FOR DISPOSAL IN THE NORMAL MUNICIPAL WASTE STREAM SINCE THEY ARE
NOT DEFINED BY THE FEDERAL GOVERNMENT AS HAZARDOUS WASTE. HOWEVER, LITHIUM
ION BATTERIES ARE RECYCLABLE. DO NOT INCINERATE OR SUBJECT BATTERY CELLS TO
TEMPERATURES IN EXCESS OF 212 DEG. F. SUCH TREATMENT CAN CAUSE CELL
RUPTURE.


10. TRANSPORTATION 


EFFECTIVE OCTOBER 1, 2008, ALL ALEXANDER TECHNOLOGIES LITHIUM ION BATTERIES
ARE NOT SUBJECTED TO THE REQUIREMENTS OF THE DEPARTMENT OF TRANSPORTATION
(DOT) SUBCHAPTER C, HAZARDOUS MATERIALS REGULATIONS IF SHIPPED IN
COMPLIANCE WITH 49 CFR 173.185 AND SPECIAL PROVISION 188.

CURRENTLY ALL ALEXANDER TECHNOLOGIES LITHIUM ION BATTERIES CAN BE
TRANSPORTED UNDER THE INTERNATIONAL CIVIL AVIATION ORGANIZATION (ICAO) AND
THE INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) UNDER SPECIAL PROVISION
A45. EFFECTIVE JANUARY 1, 2009 SPECIAL PROVISION A45 WILL BE REPLACED BY
PACKING INSTRUCTIONS (PI) 965 (BATTERIES), PI 966 (BATTERIES, PACKED WITH
EQUIPMENT) AND PI 967 (BATTERIES, CONTAINED IN EQUIPMENT).

CURRENTLY ALL ALEXANDER TECHNOLOGIES LITHIUM ION BATTERIES ARE REGULATED BY
THE INTERNATIONAL MARITIME ORGANIZATION (IMO) UNDER SPECIAL PROVISIONS 188
AND 230. THESE REGULATIONS WILL STAY IN EFFECT UNTIL JANUARY 1, 2010 WHEN
SPECIAL PROVISIONS 188 AND 230 WILL BE UPDATED.

IF YOU BUILD ANY OF OUR LITHIUM CELLS INTO A BATTERY PACK, YOU MUST ALSO
ASSURE THAT THEY ARE TESTED IN ACCORDANCE WITH THE UN MODEL REGULATIONS,
MANUAL OF TEST AND CRITERIA, PART III, SUBSECTION 38.3.

DATE ISSUED: MARCH 2011