Common Name: BLACK BUFFING COMPOUND
Manufacturer: BEILUN FUTUO MECHANICAL TOOLS CHINA
SDS Revision Date: 7/25/2011
SDS Format: No Format Specified
   
Grainger Item Number(s): 12U077, 12U091, 12U113
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 - HAZARDOUS INGREDIENTS / IDENTITY INFORMATION 
SECTION 3 - FIRST AID MEASURES 
SECTION 4 - FIRE AND EXPLOSION HAZARD DATA 
SECTION 5 - STABILITY AND REACTIVITY 
SECTION 6 - HANDLING AND STORAGE 
SECTION 7 - CONTROL MEASURES 
SECTION 8 - PHYSICAL AND CHEMICAL PROPERTIES 



COMMON NAME: BLACK BUFFING COMPOUND

MANUFACTURER: BEILUN FUTUO MECHANICAL TOOLS CO., LTD

MSDS REVISION DATE: 7/25/2011

GRAINGER ITEM NUMBER: 12U077, 12U091


SECTION 1 - PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT NAME: POLISHING COMPOUND

SYNONYMS: NOT AVAILABLE

PRODUCT USE: BUFFING AND / OR POLISHING

IF THIS PRODUCT IS USED IN COMBINATION WITH OTHER PRODUCTS, REFER TO THE
MATERIAL SAFETY DATA SHEET FOR THOSE PRODUCTS.

MANUFACTURER: BEILUN FUTUO MECHANICAL TOOLS CO., LTD

ADDRESS:
DAQI INDUSTRIAL ZONE
NINGBO ZHEJIANG

EMERGENCY TELEPHONE: (574) 86108314

TELEPHONE FOR INFORMATION: (574)86108314

DATE PREPARED: JULY 16, 2011

PREPARED BY: SUSAN MENG

CHEMICAL FAMILY: ORGANIC/INORGANIC MIXTURE

REPORTABLE QUANTITIES: NONE

FORMULA: PROPRIETARY FORMULA - ABRASIVE/GREASE MIXTURE


SECTION 2 - HAZARDOUS INGREDIENTS / IDENTITY INFORMATION 


HAZARDOUS COMPOSITION  %      OSHA PEL  CAS NO.     ACGIH TLV

TRIGLYCERIDE            8-10  NA        61789-97-7  NA

TALLOW                  2-4   NA        67701-27-3  NA

PLANT OIL              10-12  NA          8002-9-3  NA

ALUMINUM OXIDE         65-72  NA         1344-28-1  NA

APPEARANCE: WHITE PASTE, SOLVENT ODOR.

POTENTIAL IMPACT ON HEALTH:

INHALATION(BEARING): DUST MAY CAUSE RESPIRATORY IRRITATION.

INGESTION:
NONE EXPECTED UNDER NORMAL USE CONDITIONS. SWALLOWING LARGE PIECES MAY
CAUSE OBSTRUCTION OF THE GASTROINTESTINAL TRACT.

EYE:
DUST MAY CAUSE EYE IRRITATION. DUST PARTICLES OR FILLINGS MAY CAUSE INJURY
TO THE EYES

ALLERGY: NOT EXPECTED TO CAUSE ANY ALLERGY.

CHRONIC:
OVEREXPOSURE TO DUST MAY CAUSE DAMAGES TO LUNGS (FIBROSIS) WITH SYMPTOMS OF
COUGHING, SHORTNESS OF BREATH AND DIMINISHED BREATHING CAPACITY. CHRONIC
EFFECTS MAY BE AGGRAVATED BY SMOKING. PROLONGED EXPOSURE TO ELEVATED NOISE
LEVELS DURING OPERATIONS MAY AFFECT HEARING. A GREATER HAZARD, IN MOST
CASES, IS THE EXPOSURE TO THE DUST/FUMES FROM THE MATERIAL OR
PAINT/COATINGS BEING MACHINED. MOST OF THE DUST GENERATED DURING PROCESSING
IF FROM THE BASE MATERIAL BEING PROCESSED AND THE POTENTIAL HAZARD FROM
THIS EXPOSURE MUST BE EVALUATED.

CARCINOGENICITY:
NONE OF THE INGREDIENT IS LISTED AS A CARCINOGEN OR POTENTIAL CARCINOGEN BY
OSHA, NTP, ACGIH, OR IARC.

MEDICAL CONDITIONS AGGRAVATED BY EXPOSURE:
OPERATOR/MANIPULATOR WITH PRE-EXISTING RESPIRATORY DISEASE MAY BE AT RISK
DUE TO EXPOSURE.

ACUTE TOXICITY VALUES. THIS PRODUCT AND ITS INGREDIENTS ARE NOT ACUTELY
TOXIC.

WARNING:
EXPOSURE TO DUST PARTICLES SHOULD NOT EXCEED THE LIMIT OF ACGIH, TLV-TWA
RECOMMENDED CEILINGS FOR RESPIRABLE SILICA AND/OR TRIPOLI DUST AT 0.1
MG/M3. AVOID BREATHING IN AIR CONTAINING ABRASIVE MATERIALS, FOLLOWING OSHA
SAFETY AND HEALTH STANDARDS FOR DUST ACCUMULATION COLLECTION.


SECTION 3 - FIRST AID MEASURES 


INHALATION(BEARING): EVACUATE TO WHERE FRESH AIR IS AVAILABLE.

EYES:
IF IRRITATION OR REDNESS OCCUR, EVACUATE TO WHERE FRESH AIR IS AVAILABLE.
UPON CONTACT, IMMEDIATELY FLUSH EYES WITH PLENTY OF WATER, HOLDING EYELIDS
APART, FOR 15 MINUTES.

SKIN:
WASH WITH SOAP AND WATER. OBTAIN FIRST AID AND/OR MEDICAL ASSISTANCE IF
SYMPTOMS PERSIST

INGESTION: OBTAIN FIRST AID OR MEDICAL ASSISTANCE WHEN NEEDED.

OTHER POTENTIAL HEALTH RISKS:
(PROLONGED INHALATION OF DUST PARTICLES MAY RESULT IN PULMONARY FIBROSIS.

CARCINOGENICITY:
NTP: NOT REQUIRED
IARC: NOT REPORTED
OSHA: NOT REPORTED

REGULAR CONSTANT VIGILANCE IN SAFETY AND MAINTENANCE CHECK-UP PROGRAMS ARE
ADVISED TO REDUCE RISKS ASSOCIATED WITH BUFFING AND POLISHING OPERATIONS.


SECTION 4 - FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED): >300 DEGREES F C.O.C.

FLAMMABLE LIMITS: NOT ESTABLISHED

LEL:
UEL:

EXTINGUISHING MEDIA: CO2 - DRY CHEMICAL, FOAM, WATER FOG.

SPECIAL FIRE FIGHTING PROCEDURES:
DRY POLISHING COMPOUND AND BUFFING WHEEL LINT AND DEBRIS MAY MAKE THE MIX
COMBUSTIBLE. TREAT AS AN OIL FIRE.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
NONE FOR NEW AND UNUSED STORED MATERIAL.


SECTION 5 - STABILITY AND REACTIVITY 


STABILITY: STABLE

INCOMPATIBILITY (MATERIALS TO AVOID): STRONG OXIDIZERS OR REDUCING AGENTS

HAZARDOUS DECOMPOSITION OR BYPRODUCTS:
DUST FROM MACHINING COULD CONTAIN INGREDIENTS LISTED IN SECTION 2 AND
OTHER, POTENTIALLY MORE HAZARDOUS COMPONENTS OF THE BASE MATERIAL BEING
MACHINED OR COATINGS APPLIED TO THE BASE MATERIAL. COMBUSTION WILL FORM
OXIDES OF CARBON AND SMOKE.

HAZARDOUS POLYMERIZATION: NONE


SECTION 6 - HANDLING AND STORAGE 


KEEP AWAY FROM HEAT, SPARKS, OR FLAME. WHERE FLAMMABLE MIXTURES MAYBE
PRESENT, EQUIPMENT SAFETY FOR SUCH LOCATIONS SHOULD BE USED. USE CLEAN,
SPARK PROOF TOOLS AND EXPLOSION-PROOF EQUIPMENT. WHEN TRANSFERRING PRODUCT,
METAL CONTAINERS, INCLUDING TRUCKS AND TANK CARS, SHOULD BE GROUNDED AND
BONDED. DO NOT BREATHE VAPOR OR DUST. USE IN A WELL VENTILATED AREA. AVOID
CONTACT WITH EYES, SKIN, CLOTHING, AND SHOES. DO NOT SMOKE WHILE USING THIS
PRODUCT.

KEEP CONTAINER TIGHTLY CLOSED WHEN NOT IN USE AND DURING TRANSPORT. STORE
CONTAINERS IN A COOL, DRY PLACE. DO NO PRESSURIZE, CUT, WELD, BRAZE,
SOLDER, DRILL, OR GRIND CONTAINERS. KEEP CONTAINERS AWAY FROM HEAT, FLAME,
SPARKS, STATIC ELECTRICITY, OR OTHER SOURCES OF IGNITION. EMPTY PRODUCT
CONTAINERS MAY RETAIN PRODUCT RESIDUE AND CAN BE DANGEROUS.


SECTION 7 - CONTROL MEASURES 


RESPIRATORY PROTECTION (SPECIFY TYPE):
OSHA 24 CFR/134 NIOSH/MSHA APPROVED RESPIRATORS FOR PARTICULATES FROM
BUFFING DEBRIS.

VENTILATION:
LOCAL EXHAUST: GENERAL ROOM VENTILATION.
MECHANICAL (GENERAL): RECOMMEND VENTING TO DUST COLLECTORS.

PROTECTIVE GLOVES: WEAR HEAVY-DUTY WORK-TYPE GLOVES FOR HAND PROTECTION.

EYE PROTECTION:
WEAR SAFETY GLASSES AND/OR FACE SHIELD HELMETS (SEE OSHA 29 CFR 1910.122
(SAFETY GLASSES).

OTHER PROTECTIVE CLOTHING OR EQUIPMENT:
PROTECTIVE WORK CLOTHING, BODY APRON OR BELLY PADS, SAFETY SHOES, AS
NEEDED.

HEARING PROTECTION:

AVOID PROLONGED EXCESSIVE NOISE LEVELS CREATED BY BUFFING AND POLISHING
OPERATIONS (SEE OSHA 29 CFR 1910.215 (HEARING PROTECTION).

THE INFORMATION AND RECOMMENDATIONS SET FORTH HEREIN ARE TAKEN FROM SOURCES
BELIEVED TO BE ACCURATE AS OF THE DATE HEREOF; HOWEVER, BEILUN FUTUO MAKES
NO WARRANTY WITH RESPECT TO THE ACCURACY OF THE INFORMATION OR THE
SUITABILITY OF THE RECOMMENDATION, AND ASSUMES NO LIABILITY TO ANY USER
THEREOF.

NAIF = NO APPLICABLE INFORMATION FOUND
N/A = NOT APPLICABLE


SECTION 8 - PHYSICAL AND CHEMICAL PROPERTIES 


PHYSICAL STATE: BLACK PASTE, SOLVENT ODOR.

APPEARANCE, AND ODOR: 0.09 PPM (BASED ON KEROSENE)

MOLECULAR WEIGHT: NOT AVAILABLE.

SPECIFIC GRAVITY: 1.2(WATER=1) (APPROXIMATELY)

DENSITY: 10 LB/US GAL(1200 G/L) (APPROXIMATELY)

VAPOR DENSITY: GREATER THAN 1 (AIR = 1)

VAPOR PRESSURES: 5 MMHg AT 100 DEG. F(38 DEG. C) (MAXIMUM)

BOILING POINT: GREATER THAN 212 DEG. F(100 DEG. C)

FREEZING/MELTING POINT: NOT AVAILABLE

pH: NOT AVAILABLE

EVAPORATION RATE: LESS THAN 1 (BUTYL ACETATE=1)

SOLUBILITY IN WATER: SLIGHT

FLASH POINT: 195 DEG. F(91 DEG. C) PENSKY-MARTENS CLOSED CUP

FLAMMABLE LIMITS IN AIR:
LOWER: 0.7 VOL% (MINIMUM)
UPPER: 5.0 VOL% (MAXIMUM)

AUTOIGNITION TEMPERATURE: 410 DEG. F(210 DEG. C) (APPROXIMATELY)