Common Name: HIGH ENERGY LITHIUM BATTERY, OR SONNENSCHEIN LITHIUM INORGANIC LITHIUM BATTERY
Manufacturer: TADIRAN BATTERIES GERMANY
SDS Revision Date: 10/30/2007
SDS Format: No Format Specified
   
Grainger Item Number(s): 12M768
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. IDENTIFICATION 
2. COMPOSITION/INFORMATION ON INGREDIENTS 
3. HAZARDS IDENTIFICATION 
4. FIRST AID MEASURES 
5. FIRE - FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS / PERSONAL PROTECTION 
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
T
TADIRAN BATTERIES

SAFETY DATA SHEET LITHIUM BATTERIES

TADIRAN
BATTERIES GMBH
INDUSTRIESTRASSE 22
D-63654 BUDINGEN

LTN-065-26-1

REVISED: 2007-10-30

DISTRIBUTION CLASS 1 GENERAL

TECHNICAL NOTICE


1. IDENTIFICATION 


1.1 PRODUCT NAME:
TADIRAN HIGH ENERGY LITHIUM BATTERY, OR SONNENSCHEIN LITHIUM INORGANIC
LITHIUM BATTERY

VOLTAGE: 3.6 VOLTS

CHEMISTRY SYSTEM: LITHIUM THIONYL CHLORIDE

ANODE: LITHIUM METAL

CATHODE: LIQUID, THIONYL CHLORIDE

1.2 COMPANY:
TADIRAN BATTERIES GMBH
INDUSTRIESTR. 22
D-63654 BUDINGEN

1.3 EMERGENCY TELEPHONE NUMBER: +49(0)6042/954-599

NOTE:
THIS SAFETY DATA SHEETS REFERS TO CELLS AND BATTERIES ASSEMBLED FROM THEM


2. COMPOSITION/INFORMATION ON INGREDIENTS 


SUBSTANCE             CAS NO.    APPROXIMATE PERCENT   HAZARD   R-PHRASES
                                 OF TOTAL WEIGHT       SYMBOL

LITHIUM METAL         7439-93-2   2 - 6                F, C     14/15-34

THIONYL CHLORIDE      7719-09-7  18 - 47               C        14-34-37

ALUMINIUM CHLORIDE    7446-70-0   2 - 5

LITHIUM CHLORIDE      7447-41-8   1 - 2

CARBON                7440-44-0   2 - 5

STEEL, NICKEL PLATED             35 - 73

GLASS                             0 - 2

PVC                   9002-86-2   0 - 1

PMMA                  9011-14-7   0 - 1

PTFE                  9002-84-0   0 - 1

HAZARD SYMBOLS:
C: CORROSIVE
F: HIGHLY FLAMMABLE

R-PHRASES:
R 14: REACTS VIOLENTLY WITH WATER
R 14/15: REACTS VIOLENTLY WITH WATER LIBERATING EXTREMELY FLAMMABLE GASES
R 34: CAUSES BURNS
R 37: IRRITATING TO RESPIRATORY SYSTEM

IMPORTANT NOTE:
THE MATERIAL IN THIS SECTION MAY ONLY REPRESENT A HAZARD IF THE INTEGRITY
OF THE BATTERY IS COMPROMISED, OR IF THE BATTERY IS PHYSICALLY OR
ELECTRICALLY ABUSED.


3. HAZARDS IDENTIFICATION 


WARNING:
FIRE, EXPLOSION, AND SEVERE, BURN HAZARD. DO NOT RECHARGE, DISASSEMBLE,
HEAT ABOVE 100 DEG. C (SERIES SL-500: 150 DEG. C), INCINERATE, OR EXPOSE
CONTENTS TO WATER.

PROTECTION FROM CHARGING:
WHENEVER LITHIUM BATTERIES ARE NOT THE SINGLE POWER SOURCE IN A CIRCUIT
THE FOLLOWING MEASURES RECOMMENDED BY UNDERWRITERS LABORATORIES ARE
RELEVANT. THE CELLS SHOULD NOT BE CONNECTED IN SERIES WITH AN ELECTRICAL
POWER SOURCE THAT WOULD INCREASE THE FORWARD CURRENT THROUGH THE CELLS.

THE CIRCUIT FOR THESE CELLS SHALL INCLUDE ONE OF THE FOLLOWING:

A. TWO SUITABLE DIODES OR THE EQUIVALENT IN SERIES WITH THE CELLS TO
PREVENT ANY REVERSE (CHARGING) CURRENT. THE SECOND DIODE IS USED TO
PROVIDE PROTECTION IN THE EVENT THAT ONE SHOULD FAIL. QUALITY CONTROL,
OR EQUIVALENT PROCEDURES, SHALL BE ESTABLISHED BY THE DEVICE MANUFACTURER
TO ENSURE THE DIODE POLARITY IS CORRECT FOR EACH UNIT,

OR

B. A BLOCKING DIODE OR THE EQUIVALENT TO PREVENT ANY REVERSE (CHARGING)
CURRENT AND A RESISTOR TO LIMIT CURRENT IN CASE OF A DIODE FAILURE. THE
RESISTOR SHOULD BE SIZED TO LIMIT THE REVERSE CHARGING) CURRENT TO THE
MAXIMUMS GIVEN IN THE DATA SHEETS.


4. FIRST AID MEASURES 


A. ELECTROLYTE CONTACT:

SKIN:
IMMEDIATELY FLUSH WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES. IF
SYMPTOMS ARE PRESENT AFTER FLUSHING, GET MEDICAL ATTENTION.

EYES:
IMMEDIATELY FLUSH WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES AND GET
MEDICAL ATTENTION.

RESPIRATORY SYSTEM:
WITH LARGE QUANTITIES AND IRRITATION OF THE RESPIRATORY TRACT MEDICAL
SURVEILLANCE FOR 48 HOURS.

IMMEDIATELY INHALE CORTISONE SPRAY, E.G. PULMICORT.

B. LITHIUM METAL CONTACT:

SKIN:
REMOVE PARTICLES OF LITHIUM FROM SKIN AS RAPIDLY AS POSSIBLE. IMMEDIATELY
FLUSH WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES AND GET MEDICAL
ATTENTION.

EYES:
IMMEDIATELY FLUSH WITH PLENTY OF WATER FOR AT LEAST 15 MINUTES AND GET
IMMEDIATE MEDICAL ATTENTION.


5. FIRE - FIGHTING MEASURES 


A. EXTINGUISHING MEDIA:
DURING A FIRE WITH LITHIUM BATTERIES, COPIOUS AMOUNTS OF COLD WATER IS AN
EFFECTIVE MEDIUM TO PREVENT EXPANSION OF THE FIRE. DO NOT USE WARM WATER
OR HOT WATER.

LITH-X (CLASS D EXTINGUISHING MEDIA) IS EFFECTIVE ON FIRES INVOLVING ONLY
A FEW LITHIUM BATTERIES.

DO NOT USE CO2 OR HALON TYPE EXTINGUISHERS.

DRY CHEMICAL TYPE EXTINGUISHERS HAVE LIMITED EXTINGUISHING POTENTIAL

B. FIRE FIGHTING PROCEDURES:

USE A POSITIVE PRESSURE SELF-CONTAINED BREATHING APPARATUS IF BATTERIES
ARE INVOLVED IN A FIRE.

FULL PROTECTIVE CLOTHING IS NECESSARY.

DURING WATER APPLICATION CAUTION IS ADVISED AS BURNING PIECES OF LITHIUM
MAY BE EJECTED FROM THE FIRE.

WHERE THE CELLS OR BATTERIES ARE NOT AT THE CENTRE OF THE FIRE COPIOUS
AMOUNTS OF WATER MAY BE SUPPLIED TO THE CELLS USING A DIFFUSER TYPE NOZZLE
SO THAT THE CELLS REMAIN COOL DURING THE CONTAINMENT AND EXTINGUISHING OF
THE FIRE. A SPRINKLER SYSTEM SHOULD BE SUFFICIENT FOR THIS PURPOSE THE
CRITICAL FACTOR BEING THAT THE LITHIUM CELLS DO NOT EXPERIENCE
TEMPERATURES ABOVE THE MELTING POINT OF LITHIUM.

SMALL AMOUNTS OF WATER SHOULD NEVER BE USED SUCH AS THE VOLUMES CONTAINED
WITHIN PORTABLE FIRE EXTINGUISHERS. STANDARD DRY POWDER EXTINGUISHERS ARE
INEFFECTIVE. HALON EXTINGUISHERS MUST NOT BE USED WHEN FIGHTING LITHIUM
FIRES AS TOXIC GASES MAY BE GENERATED DURING FIRE FIGHTING. IT SHOULD BE
NOTED THAT A HAZARD OF HYDROGEN FORMATION EXISTS WHENEVER HOT LITHIUM
METAL COMES INTO CONTACT WITH WATER.


6. ACCIDENTAL RELEASE MEASURES 


WHEN THE BATTERY HOUSING IS DAMAGED, SMALL AMOUNTS OF ELECTROLYTE MAY
LEAK. SEAL BATTERY AIR TIGHT IN A PLASTIC BAG, ADDING SOME CHALK
(CaCO3) OR LIME (CaO) POWDER OR VERMICULITE.

ELECTROLYTE TRACES MAY BE WIPED OFF DRYLY USING HOUSEHOLD PAPER. RINSE
WITH WATER AFTERWARDS.


7. HANDLING AND STORAGE 


DO NOT ALLOW TERMINALS TO SHORT-CIRCUIT.

STORAGE PREFERABLY IN A COOL (BELOW 21 DEG. C), DRY AREA THAT IS SUBJECT
TO LITTLE TEMPERATURE CHANGE.

DO NOT PLACE NEAR HEATING EQUIPMENT, NOR EXPOSE TO DIRECT SUNLIGHT FOR
LONG PERIODS. ELEVATED TEMPERATURES CAN RESULT IN REDUCED BATTERY SERVICE
LIFE.


8. EXPOSURE CONTROLS / PERSONAL PROTECTION 


NOT APPLICABLE


9. PHYSICAL AND CHEMICAL PROPERTIES 


NOT APPLICABLE


10. STABILITY AND REACTIVITY 


MAY RUPTURE VIOLENTLY WHEN HEATED ABOVE 150 DEG. C OR WHEN CHARGED.


11. TOXICOLOGICAL INFORMATION 


NOT APPLICABLE

REFER TO INFORMATION UNDER ITEM 2.


12. ECOLOGICAL INFORMATION 


THE BATTERIES DO NOT CONTAIN MERCURY, CADMIUM OR OTHER HEAVY METALS.


13. DISPOSAL CONSIDERATIONS 


DISPOSE BY INCINERATION OR BURIAL AT PERMITTED WASTE TREATMENT AND/OR
DISPOSAL SITES.

BATTERIES DO NOT CONTAIN HAZARDOUS MATERIALS ACCORDING TO EC DIRECTIVES
91/157/EEC AND 93/86/EEC.

FOR LARGE QUANTITIES A DISPOSAL SERVICE IS OFFERED UPON REQUEST.


14. TRANSPORT INFORMATION 


CLASS 9:

UN3090: LITHIUM BATTERIES

UN3091:
LITHIUM BATTERIES CONTAINED IN EQUIPMENT, OR
LITHIUM BATTERIES PACKED WITH EQUIPMENT

PACKING GROUP: II

SPECIAL PROVISIONS AND PACKING INSTRUCTIONS:

ADR, RID: 188, 230, 310, 636, P903, P903A

IATA: A45, A88, A99, P903, P912, P918

IMDG-CODE:
188, 230, 310, P903
EMS: F-A, S-I
STORAGE AND SEGREGATION: CATEGORY A

FOR MORE INFORMATION SEE WWW.TADIRANBATTERIES.DE

SITE MAP

TRANSPORT REGULATIONS


15. REGULATORY INFORMATION 


NOT APPLICABLE


16. OTHER INFORMATION 


TADIRAN LITHIUM BATTERIES ARE REGISTERED BY UNDERWRITERS LABORATORIES,
NORTHBROOK, U.S.A. UNDER FILE MH 12827.

FURTHER INFORMATION IS GIVEN IN:
TADIRAN LITHIUM BATTERY PRODUCT DATA CATALOGUE
TADIRAN LITHIUM BATTERY TECHNICAL BROCHURE.

FOR LITHIUM BATTERIES IN GENERAL, SAFETY STANDARD IEC 60086-4 APPLIES. IT
CONTAINS DETAILED RECOMMENDATIONS FOR MANUFACTURERS OF EQUIPMENT AND
USERS.

VISIT OUR WEB SITE UNDER WWW.TADIRANBATTERIES.DE.

BATTERY PACKS

THE DESIGN AND ASSEMBLY OF BATTERY PACKS REQUIRE SPECIAL SKILLS, EXPERTISE
AND EXPERIENCE. THEREFORE IT IS NOT RECOMMENDED THAT THE END USER ATTEMPT
TO SELF-ASSEMBLE BATTERY PACKS. IT IS PREFERABLE THAT ANY BATTERY USING
LITHIUM CELLS BE FABRICATED BY TADIRAN TO ENSURE PROPER BATTERY DESIGN AND
CONSTRUCTION. A FULL BATTERY ASSEMBLY SERVICE IS AVAILABLE FROM TADIRAN
WHO CAN BE CONTACTED FOR FURTHER INFORMATION. IF FOR ANY REASON, THIS IS
NOT POSSIBLE, TADIRAN CAN REVIEW THE PACK DESIGN IN CONFIDENCE TO ENSURE
THAT THE DESIGN IS SAFE (IN ASSEMBLY AND USE) AND CAPABLE OF MEETING
STATED PERFORMANCE REQUIREMENTS.

THE INFORMATION CONTAINED HEREIN IS FURNISHED WITHOUT WARRANTY OF ANY
KIND. USERS SHOULD CONSIDER THESE DATA ONLY AS A SUPPLEMENT TO OTHER
INFORMATION GATHERED BY THEM AND MUST MAKE INDEPENDENT DETERMINATIONS OF
THE SUITABILITY AND COMPLETENESS OF INFORMATION FROM ALL SOURCES TO
ASSURE PROPER USE AND DISPOSAL OF THESE MATERIALS AND THE SAFETY AND
HEALTH OF EMPLOYEES AND CUSTOMERS.

TEL.: +49(0)6042/954-0

FAX: -190

E-MAIL: INFO@TADIRANBATTERIES.DE

INTERNET: WWW.TADIRANBATTERIES.DE