Common Name: MAN-MADE VITREOUS FIBER CEILINGS AND WALL PANELS (FIRE GUARD) - MSDS 2
Manufacturer: ARMSTRONG WORLD INDUSTRIES
SDS Revision Date: 9/1/2009
SDS Format: ANSI-OSHA
   
Item Number(s): 13Z990, 13Z991, 13Z992, 13Z993, 13Z994, 13Z995, 13Z996, 13Z997, 13Z998, 19H050, 22XJ43, 31LC01, 31LC02, 36N477, 5NGK2
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
I. PRODUCT INFORMATION 
II. INGREDIENT INFORMATION 
III. PHYSICAL DATA 
IV. FIRE AND EXPLOSION DATA 
V. HEALTH DATA 
VI. REACTIVITY DATA 
VII. SPILL OR LEAK PROCEDURES 
VIII. SPECIAL PROTECTION INFORMATION 



MATERIAL SAFETY DATA SHEET

ARMSTRONG

ARMSTRONG WORLD INDUSTRIES, INC.
ENVIRONMENT, HEALTH AND SAFETY
2500 COLUMBIA AVENUE, P.O. BOX 3001
LANCASTER, PA 17604

TELEPHONE: (717) 396-2328 OR 396-2935

DIVISION: BUILDING PRODUCTS

DATE: 9/09 (REPLACES 7/09)

N/A = NOT APPLICABLE OR NOT AVAILABLE

N/K = NONE KNOWN OR NOT KNOWN

ISSUED BY: SAFETY, HEALTH AND INDUSTRIAL HYGIENE DEPARTMENT

HMIS:
0 = MINIMAL HAZARD
4 = SEVERE HAZARD

HEALTH       1
FLAMMABILITY 0
REACTIVITY   0

DEPARTMENT OF TRANSPORTATION INFORMATION:
SHIPPING NAME: NOT CLASSIFIED
HAZARD CLASS: N/A
ID NO: N/A

EMERGENCY ONLY CONTACT:
CHEM-TEL: 800-255-3924


I. PRODUCT INFORMATION 


A. PRODUCT NAME:
MAN-MADE VITREOUS FIBER CEILINGS AND WALL PANELS (FIRE GUARD) - MSDS #2

B. CHEMICAL NAME AND SYNONYMS: N/A

C. CHEMICAL OR PRODUCT FAMILY: MAN-MADE VITREOUS FIBERS


II. INGREDIENT INFORMATION 


A. HAZARDOUS COMPONENTS     C.A.S NO.   %       OSHA PEL      ACGIH TLV
(CHEMICAL IDENTITY; COMMON
NAME)

MINERAL WOOL FIBER          N/A          0-60   RESPIRABLE    RESPIRABLE
                                                15 MG/M3 (AS  1 F/CC
                                                NUISANCE
                                                DUST)

FIBROUS GLASS               65997-17-3   0-5    5 MG/M3 (AS   1 F/CC
                                                RESPIRABLE
                                                NUISANCE
                                                DUST)

HYDROUS ALUMINUM SILICATE    1332-58-7  15-25   0.1 MG/M3     0.025 MG/M3
                                                (AS           (AS
                                                RESPIRABLE    RESPIRABLE
                                                CRYSTALLINE   CRYSTALLINE
                                                SILICA)       SILICA)

THIS PRODUCT FORMULATION DOES NOT CONTAIN ASBESTOS.


III. PHYSICAL DATA 


A. APPEARANCE AND COLOR:
GRAY, PRESSED MAN-MADE VITREOUS FIBER PANEL OF VARIOUS COLORS

B. BOILING POINT (DEGREES F): N/A

C. VAPOR PRESSURE (MMHg @ 20 DEGREES C): N/A

D. VAPOR DENSITY (AIR = 1): N/A

E. SOLUBILITY IN WATER: N/A

F. SPECIFIC GRAVITY (H2O = 1): N/A

G. PERCENT VOLATILE BY WEIGHT (30 MIN. @ 275 DEGREES F): N/A

H. EVAPORATION RATE (BUTYL ACETATE = 1): N/A

I. pH: N/A


IV. FIRE AND EXPLOSION DATA 


A. FLASH POINT: N/A

B. FLAMMABLE RANGE:
LEL: N/A
UEL: N/A

C. EXTINGUISHING MEDIA: WATER FOG, DRY CHEMICAL ABC RATED

D. SPECIAL FIRE FIGHTING PROCEDURES: NONE

E. UNUSUAL FIRE AND EXPLOSION HAZARDS: NONE


V. HEALTH DATA 


A. PRIMARY ROUTE (S) OF ENTRY: INHALATION, SKIN, AND EYE CONTACT

B. TARGET ORGANS: LUNGS, SKIN AND EYES

EFFECTS OF OVEREXPOSURE:

ACUTE HEALTH EFFECTS:
PRODUCTS ARE A TRANSIENT MECHANICAL IRRITANT TO THE SKIN, EYES AND UPPER
RESPIRATORY SYSTEM.

REFER TO SPECIAL PROTECTION INFORMATION FOR HANDLING INSTRUCTIONS.

MINERAL WOOL FIBER:
MINERAL WOOL FIBER HAS BEEN CLASSIFIED AS "NOT CLASSIFIABLE AS TO ITS
CARCINOGENICITY TO HUMAN" (GROUP 3) BY THE INTERNATIONAL AGENCY FOR
RESEARCH ON CANCER (IARC).

FIBROUS GLASS:
FIBROUS GLASS HAS BEEN CLASSIFIED AS "NOT CLASSIFIABLE AS TO ITS
CARCINOGENICITY TO HUMAN" (GROUP 3) BY THE INTERNATIONAL AGENCY FOR
RESEARCH ON CANCER (IARC). FIBROUS GLASS IS LISTED BY NTP AS 2, REASONABLY
ANTICIPATED TO BE A CARCINOGEN.

CRYSTALLINE SILICA:
LONG TERM EXPOSURE TO CRYSTALLINE SILICA DUST IN CONCENTRATIONS HIGHER THAN
THE RECOMMENDED PEL OR TLV MAY CAUSE SILICOSIS. NTP HAS CLASSIFIED
RESPIRABLE CRYSTALLINE SILICA AS A SUBSTANCE THAT MAY BE ANTICIPATED TO BE
A CARCINOGEN. IARC HAS ESTABLISHED A GROUP 1 CLASSIFICATION TO CRYSTALLINE
SILICA AS A KNOWN CARCINOGEN TO HUMANS.

C. CARCINOGENICITY:
NTP: YES
IARC MONOGRAPHS: YES
OSHA REGULATED: NO

D. MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
ANY CONDITION GENERALLY AGGRAVATED BY RESPIRATORY AND MECHANICAL IRRITANTS
IN THE AIR OR ON THE SKIN. PRE-EXISTING UPPER RESPIRATORY AND LUNG DISEASE
SUCH AS, BUT NOT LIMITED TO BRONCHITIS, EMPHYSEMA, AND ASTHMA.

E. FIRST AID PROCEDURES:
SKIN: WASH WITH MILD SOAP AND RUNNING WATER

EYES:
FLUSH WITH FLOWING WATER FOR AT LEAST 15 MINUTES AND IF SYMPTOMS PERSIST,
SEEK IMMEDIATE MEDICAL ATTENTION.


VI. REACTIVITY DATA 


A. STABILITY: MATERIAL IS STABLE

B. INCOMPATIBILITY: N/K

C. HAZARDOUS DECOMPOSITION PRODUCTS:
CARBON DIOXIDE, AND OTHER TRACE PYROLYSIS PRODUCTS TYPICAL OF DECOMPOSITION
OF ANY ORGANIC COMPOUND.

D. HAZARDOUS POLYMERIZATION: N/A


VII. SPILL OR LEAK PROCEDURES 


A. STEPS TO BE TAKEN IF MATERIAL IS RELEASED OR SPILLED: N/A

B. RECYCLING INFORMATION:
ARMSTRONG CEILINGS CAN BE RECYCLED THROUGH THE ARMSTRONG CEILING RECYCLING
PROGRAM. FOR MORE INFORMATION ON THE PROGRAM, REQUIREMENTS AND LOCAL
RESOURCES, PLEASE VISIT WWW.ARMSTRONG.COM/CEILINGS/RECYCLING OR CALL OUR
RECYCLING CENTER AT 877-276-7876, PRESS 1 (CEILINGS), THEN PRESS 8.

IF THE ARMSTRONG CEILNG RECYCLING PROGRAM CANNOT BE USED, PLEASE DISPOSE IN
ACCORDANCE WITH FEDERAL, STATE AND LOCAL WASTE DISPOSAL REGULATIONS


VIII. SPECIAL PROTECTION INFORMATION 


DURING THE INSTALLATION, BE CERTAIN THAT THE WORK SITE IS WELL VENTILATED,
AND AVOID BREATHING DUST.

WEAR LONG-SLEEVE, LOOSE FITTING CLOTHES, GLOVES AND EYE PROTECTION.

HANDLE THESE MATERIALS CAREFULLY TO MINIMIZE AIRBORNE DUST.

IF HIGH DUST LEVELS ARE ANTICIPATED DURING INSTALLATION, SUCH AS WITH THE
USE OF POWER TOOLS, USE THE APPROPRIATE NIOSH APPROVED DUST RESPIRATOR.

ALL POWER CUTTING TOOLS MUST BE EQUIPPED WITH DUST COLLECTORS.

AFTER USING THESE MATERIALS, WASH WITH WARM WATER AND MILD SOAP. DO NOT
SCRATCH OR RUB SKIN IF IT BECOMES IRRITATED.

WASH WORK CLOTHES SEPARATELY, AND THEN RINSE THE WASHER.

THE INFORMATION PRESENTED HEREIN IS SUPPLIED AS A GUIDE TO THOSE WHO HANDLE
OR USE THIS PRODUCT. SAFE WORK PRACTICES MUST BE EMPLOYED WHEN WORKING WITH
ANY MATERIALS. IT IS IMPORTANT THAT THE END USER MAKES A DETERMINATION
REGARDING THE ADEQUACY OF THE SAFETY PROCEDURES EMPLOYED DURING THE USE OF
THIS PRODUCT.