Common Name: LITHIUM METAL, THIONYL CHLORIDE (LI-SOCL2)
Manufacturer: PYRAMID TIME SYSTEMS
MSDS Revision Date: (No Date)
   
Grainger Item Number(s): 15F167, 15F564, 15F565, 15F568, 15F569
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
1. IDENTIFICATION OF THE PRODUCT AND SUPPLIER 
2. COMPOSITION AND INFORMATION ABOUT THE INGREDIENTS 
3. HAZARDS IDENTIFICATION 
4. FIRST AID MEASURES 
5. FIRE-FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS/PERSONAL PROTECTION 
9. PHYSICAL AND CHEMICAL PROPERTIES 
10. STABILITY AND REACTIVITY 
11. TOXICOLOGICAL INFORMATION 
12. ECOLOGICAL INFORMATION 
13. DISPOSAL CONSIDERATION 
14. TRANSPORT INFORMATION 
15. REGULATION INFORMATION 
16. OTHER INFORMATION 



MATERIAL SAFETY DATA SHEET

PYRAMID(R*)


1. IDENTIFICATION OF THE PRODUCT AND SUPPLIER 


IDENTIFICATION OF THE PRODUCT:
LITHIUM METAL
THIONYL CHLORIDE (Li-SOCl2)

MANUFACTURER ADDRESS:
PYRAMID TIME SYSTEMS
45 GRACEY AVENUE
MERIDEN, CT 06451

TELEPHONE: 203-535-0550

FAX: 203-634-1696

E-MAIL: PYRAMIDTIMESYSTEMS.COM


2. COMPOSITION AND INFORMATION ABOUT THE INGREDIENTS 


ACTIVE MATERIALS:

                                 APPR. PERCENT OF TOTAL WEIGHT (%)

LITHIUM (Li)                     4.72 (2.37 G)

CARBON BLACK (C)                 4.05

THIONYL CHLORIDE (SOCL2)         37.87

LITHIUM ALUMINUM TETRACHLORIDE   5.9
(LiAlCl4)

PASSIVE MATERIALS:

                                 APPR. PERCENT OF TOTAL WEIGHT (%)

BASE METAL  STEEL                44.73

OTHERS      PLASTIC              2.27

            GLASS FIBER          0.46


3. HAZARDS IDENTIFICATION 


THE LITHIUM-THIONYL CHLORIDE BATTERIES ARE NOT HAZARDOUS WHEN USED
ACCORDING TO THE RECOMMENDATIONS OF THE MANUFACTURER.

BUT IF THE DESIGN OF THE CIRCUIT DOESN'T FORECAST ALL THE NECESSARY CARES
TO PREVENT THE INVERSION OF POLARITY IN THE ASSEMBLY OF THE BATTERY OR THE
BATTERY AT PACKS, THERE IS THE RISK OF DANGERS DUE TO THE EXPLOSION OF THE
BATTERY.

DEFINE WITH CARE THE ASSEMBLING PROCESS TO ASSURE THAT ACCIDENTAL SHORT
CIRCUIT DON'T HAPPEN

DO NOT EXPOSE THE BATTERIES TO TEMPERATURES ABOVE 100 DEG C.

IF THE BATTERY LOSE ITS INTEGRITY AND SEALING, DUE TO BREAK OR DAMAGES
(MECHANICAL, THERMAL OR ELECTRICAL), LEAKAGE, EXPLOSION OR FIRE MAY
FOLLOW.

IN THIS CASE THERE IS THE RISK OF RELEASE OF CHEMICAL MATERIALS AS DEFINED
IN THE PARAGRAPH 2 (ACTIVE MATERIALS) OF THIS SAFETY SHEET.

HERE BELOW ARE SHOWN THE NATURE OF SPECIAL RISKS AND THE ADVICES OF
CAUTION.

NATURE OF SPECIAL RISKS:
R14/15: (REACTS WITH WATER AND YIELDS FLAMMABLE GASES)
R21: (HARMFUL IN CONTACT WITH SKIN)
R22: (HARMFUL IF SWALLOWED)
R35: (CAUSES SEVERE BURNS)
R41: (RISK OF SERIOUS DAMAGE TO THE EYE)
R42/43: (MAY CAUSE SENSITATION BY INHALATION AND SKIN CONTACT)

SAFETY ADVICES:
S2: (KEEP OUT OF REACH FROM CHILDREN)

S8: (KEEP AWAY FROM MOISTURE)

S22: (DO NOT BREATHE DUST)

S24: (AVOID CONTACT WITH SKIN)

S26:
(IN CASE OF CONTACT WITH EYES, RINSE IMMEDIATELY WITH PLENTY OF WATER AND
SEEK MEDICAL ATTENTION)

S36: (WEAR SUITABLE PROTECTIVE CLOTHING)

S37: (WEAR SUITABLE GLOVES)

S43: (IN CASE OF FIRE USE EXTINGUISHER TYPE D. DO NOT USE WATER)

S45: (IN CASE OF INCIDENT OR INDISPOSITION SEEK MEDICAL ATTENTION)


4. FIRST AID MEASURES 


ONLY IN CASE OF CONTACT WITH INTERNAL COMPONENTS OF THE BATTERY:

SKIN CONTACT: FLUSH WITH PLENTY OF WATER

EYE CONTACT: FLUSH WITH PLENTY OF WATER (EYELIDS HELD OPEN)

INHALATION:
BREATH FRESH AIR AND GIVE OXYGEN OR ARTIFICIAL RESPIRATION BY SPECIALIST
PEOPLE

INGESTION: DRINK MUCH WATER AND CONSULT A DOCTOR


5. FIRE-FIGHTING MEASURES 


EXTINGUISHING MEDIA: DO NOT USE WATER IN CASE OF BATTERY LEAKAGE

SPECIAL HAZARDS: IRRITATING VAPOR

SPECIAL PROTECTIVE EQUIPMENT:
WEAR PROTECTIVE CLOTHING, USE SELF-CONTAINED BREATHING APPARATUS WITH
FILTERED CARTRIDGE TYPE ABEK


6. ACCIDENTAL RELEASE MEASURES 


IN CASE OF BREAK OF A BATTERY, ALL THE PEOPLE MUST GO AWAY FROM THE PLACE
WHERE THE INCIDENT HAPPENED AND COME BACK ONLY AFTER THE DISSOLUTION OF THE
IRRITATING GAS.

BROKEN BATTERIES OR BATTERY PACKS MUST BE COVERED WITH SODIUM CARBONATE
(NA2CO3) OR DRY SAND, PLACE THEM IN APPROVED CONTAINER AND DISPOSE IN
ACCORDANCE WITH LOCAL REGULATION.

FOR THE EVENTUAL HANDLING USE GLOVES IN VITON(R*).


7. HANDLING AND STORAGE 


7.1 HANDLING:
DO NOT RECHARGE

DO NOT USE DIFFERENT TYPES AND BRANDS OF BATTERIES OR WITH DIFFERENT STATE
CHARGE

AVOID SHORT CIRCUIT

USE DESK OF WORK ELECTRICALLY INSULATED

AVOID TO WORK OVER WET SURFACE

USE PLASTIC CALIBRE TO VALUATE THE DIMENSIONS OF A LITHIUM BATTERY OR TO
INSULATE THE METALLIC SURFACE OF THE BATTERY

DO NOT HAVE RINGS ON THE FINGERS; OTHERWISE WEAR INSULATING GLOVES.

DO NOT CUT IN THE SAME TIME BOTH THE TERMINALS OF A BATTERY:
IT COULD BE A SHORT CIRCUIT TROUGH THE SHEARS

KEEP THE BATTERIES IN NON-CONDUCTIVE TRAYS (I.E. PLASTIC, WOOD OR CARTON)

DO NOT SOLDER DIRECTLY ON THE BATTERY

DO NOT DISASSEMBLE THE BATTERIES, DO NOT THROW THEM IN THE FIRE, DO NOT
HOLE, DO NOT OVERHEAT OR PLUNGE INTO WATER

7.2 STORAGE:
STORE THE LITHIUM CELLS IN A COOL, DRY AND VENTILATED AREA FAR FROM FIRES
AND HEATING SOURCES.

IT IS RECOMMENDED THE USE OF A NON-COMBUSTIBLE STRUCTURE, KEEP ADEQUATE
CLEARANCE BETWEEN WALLS AND BATTERIES.

THE MAXIMUM TEMPERATURE SUGGESTED FOR THE STORAGE IS +30 DEG. C

HIGHER TEMPERATURES ARE ALLOW BUT CAUSE AN INCREASE IN THE SELF DISCHARGE
OF THE BATTERY AND SPEED UP THE PROCESS OF PASSIVATION

IN ANY CASE, NEVER GO OVER 100 DEG. C, AS THE BATTERIES CAN BREAK AND CAUSE
A LEAKAGE

ARRANGE ADEQUATE PROTECTIONS TO AVOID POSSIBLE HURTS TO THE BATTERIES

KEEP THE BATTERIES IN THEIR ORIGINAL PACKAGES TILL WHEN THEY ARE USED

DO NOT EXPOSE THE BATTERIES DIRECTLY TO THE SUN LIGHT

DO NOT PUT AN HIGHER NUMBER OF CARTONS ONE ON ANOTHER (RESPECT WHAT
INDICATED)

IF IN THE SAME PLACE ARE STORAGE BATTERIES WITH A TOTAL CAPACITY >50,000
AH, IT IS SUGGESTED TO INSTALL AN ALARM FOR SMOKE AND GAS


8. EXPOSURE CONTROLS/PERSONAL PROTECTION 


IF THE BATTERY IS INTEGRAL, STORAGE AND HANDLE WITH CARE, THERE IS ANY
DANGERS.

IT IS SUGGESTED TO HANDLE THE BATTERIES IN A VENTILATED PLACE, TO DON'T
SMOKE, EAT OR DRINK DURING THE ASSEMBLING.


9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE:
THE BATTERIES ARE METAL CYLINDERS WITH DIFFERENT DIAMETERS AND HEIGHT,
FITTED WITH AN EXTERNAL PLASTIC SLEEVE.


10. STABILITY AND REACTIVITY 


10.1 CONDITIONS TO AVOID:
DO NOT EXPOSE AT TEMPERATURE HIGHER THAN 100 DEG. C.

AVOID SHORT CIRCUIT, CRUSH, EXPOSITION TO HEAT SOURCES.

DO NOT DISASSEMBLE THE BATTERIES OR THE BATTERY PACKS, DO NOT THROW THEM IN
THE FIRE, DO NOT PERFORATE THEM, DO NOT OVERHEAT OR WET THEM.

10.2 MATERIAL TO AVOID: WATER, OXIDIZING AGENTS, ALKALIS.


11. TOXICOLOGICAL INFORMATION 


THE RUPTURE OF A LITHIUM-THIONYL CHLORIDE BATTERIES CAN DEVELOPED THE
FOLLOWING SUBSTANCES:
HUYDROGEN (H2), LITHIUM OXIDE (Li2O) AND LITHIUM HYDROXIDE (LiOH) IN CASE
OF REACTION OF LITHIUM METAL WITH WATER

CHLORINE (Cl2), SULFUR DIOXIDE (SO2) AND DISULFUR DICHLORIDE (S2Cl2) IF THE
THYONIL CLORIDE GO ABOVE 140.5 DEG. C

HYDROCHLORIC ACID (HCl) AND SULFUR DIOXIDE (SO2) IN CASE OF REACTION OF
THIONYL CHLORIDE WITH WATER

HYDROCHLORIC ACID (HCl), LITHIUM OXIDE (Li2O), LITHIUM HYDROXIDE (LiOH) AND
ALUMINIUM HYDROXIDE (Al(OH)3) IN CASE OF REACTION OF LITHIUM
THETRACHLOROALUMINATE WITH WATER.


12. ECOLOGICAL INFORMATION 


WHEN PROPERLY USED OR DISPOSED, THE LITHIUM-THIONYL CHLORIDE BATTERIES DO
NOT PRESENT ENVIRONMENTAL HAZARD.


13. DISPOSAL CONSIDERATION 


FOR THE DISPOSAL APPLY TO SPECIALIZED ORGANISATION.


14. TRANSPORT INFORMATION 


RESTRICTION FOR THE TRANSPORT:
CLASS 9 IN ACCORDANCE TO THE UNITED NATION REGULATION.

INTERNATIONAL CONVENTION:
ROAD TRANSPORT: NOT HAZARDOUS IN ACCORDANCE TO ADR
RAIL TRANSPORT: NOT HAZARDOUS IN ACCORDANCE TO RID
SEA TRANSPORT: NOT HAZARDOUS IN ACCORDANCE TO IMDG
AIR TRANSPORT: NOT HAZARDOUS IN ACCORDANCE TO ICAO

NOTE:
THE BATTERIES WHICH CONTAIN FEW THAN 0.5 G OF METAL LITHIUM ARE NOT
RESTRICTED FOR TRANSPORT.


15. REGULATION INFORMATION 


LITHIUM BATTERIES ARE REGULATED DURING SHIPMENT BY THE DEPT. OF
TRANSPORTATION (USDOT) AND UNITED NATION, (INTERNATIONAL) REQUIREMENTS.
BATTERIES TESTED AND FOUND IN COMPLIANCE WITH UN CHAPTER 38.3 REQUIREMENTS
CAN BE SHIPPED WITHOUT DESIGNATION AS "CLASS 9" HAZARDOUS MATERIAL IF ALL
OTHER MARKING, LABELING, PACKING, AND UNIT VOLUMES ARE MET.

THE BATTERY COMPLIES WITH SECTION II OF PI968 OF IATA DGR 52ND ED. 2011
ACCORDINGLY.


16. OTHER INFORMATION 


THE LITHIUM BATTERIES OR BATTERY PACKS MUST BE HANDLE BY SPECIALIZE PEOPLE

THEY MUST BE KEPT OUT OF REACH FROM CHILDREN.

HANDLE WITH CARE. FLAMMABILITY HAZARD EXISTS IF THE PACKAGE IS DAMAGED.

ALLOW INSPECTION AND REPACKING IF NECESSARY.

THEY MUST BE USED FOLLOWING THE TECHNICAL SPECIFICATIONS, WITHOUT EXCEED
THE VALUES DEFINED, DOES NOT CONTAIN ANY RECALLED AND /OR DEFECTIVE
BATTERIES.

DO NOT ASSEMBLE BY ONE SELF A SERIAL OF BATTERIES, BUT REQUEST THE FINISHED
BATTERY TO THE SUPPLIER, WHO WILL PROVIDE FOR INSTALL PROTECTION COMPONENTS
(DIODES, ETC.)

THE INFORMATION CONTAINED IN THIS SHEET ARE BASED ON THE PRESENT KNOWLEDGE
AND THE CONDITIONS OF USE.

FOR EVERY USE NOT IN CONFORMITY TO THE SAFETY SHEET OR FOR THE USE IN
COMBINATION WITH ANY OTHER MATERIAL OR IN ANY OTHER PROCESS THE USER IS THE
RESPONSIBLE.

MSDS: LiSOCl, 2011