Common Name: WHITE DRY FAST SET
Manufacturer: JETOMES & ASSOCIATES
SDS Revision Date: 10/14/2009
SDS Format: No Format Specified
   
Grainger Item Number(s): 15F534
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - MANUFACTURER'S NAME 
SECTION II - PRODUCT IDENTIFICATION 
SECTION III - HAZARDOUS INGREDIENTS/IDENTITY INFORMATION 
SECTION IV - PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION V - FIRE AND EXPLOSION HAZARD DATA 
SECTION VI - REACTIVITY DATA 
SECTION VII - HEALTH HAZARD DATA 
SECTION VIII - PRECAUTIONS FOR SAFE HANDLING AND USE 
SECTION IX - CONTROL MEASURES/PERSONAL PROTECTION 



MATERIAL SAFETY DATA SHEET

(OSHA 29 CFR 1910.1200)

PRODUCT: WHITE DRY FAST SET

JE TOMES
PRODUCTS SINCE 1935


SECTION I - MANUFACTURER'S NAME 


JE TOMES & ASSOCIATES, INC.
2513 WEST 140TH PLACE
BLUE ISLAND, IL 60406

708-653-5100-PHONE

708-653-5101-FACSIMILE

EMERGENCY TELEPHONE NUMBER: N/A

DATE PREPARED: OCTOBER 30, 2006

DATE REVISED: OCTOBER 14, 2009


SECTION II - PRODUCT IDENTIFICATION 


PRODUCT NAME: WHITE DRY FAST SET

CODE#:


SECTION III - HAZARDOUS INGREDIENTS/IDENTITY INFORMATION 


HAZARDOUS COMPONENTS          CAS NO.      PEL (OSHA)    TLV (ACGIH)
                                           MG/M3         MG/M3

SILICA SAND, CRYSTALLINE      14808-60-7   10/%SiO2+2    0.05(RESPIRABLE)

PORTLAND CEMENT               65997-15-1   5             5

MAY CONTAIN ONE OR MORE OF THE FOLLOWING INGREDIENTS:

AMORPHOUS SILICA              07631-86-9   80 MG/M3/     10
                                           % SiO2

CALCIUM ALUMINATE CEMENT      65997-16-2   5             5

COPOLYMER POWDER              24937-78-8   NA            NA

OTHER LIMITS:
NATIONAL INSTITUTE FOR OCCUPATIONAL SAFETY AND HEALTH (NIOSH).
RECOMMENDED STANDARD MAXIMUM PERMISSIBLE CONCENTRATION:
005 MG/M3 (RESPIRABLE FREE SILICA) AS DETERMINED BY A FULL-SHIFT SAMPLE
UP TO 10-HOUR WORKING DAY, 40-HOUR WORK WEEK. SEE NIOSH CRITERIA FOR A
RECOMMENDED STANDARD OCCUPATIONAL EXPOSURE TO CRYSTALLINE


SECTION IV - PHYSICAL/CHEMICAL CHARACTERISTICS 


APPEARANCE:
GRAY TO FRAY-BROWN COLORED POWDER. SOME PRODUCTS CONTAIN COARSE AGGREGATE.

SPECIFIC GRAVITY: 2.6 TO 3.15

MELTING POINT: >2700F

BOILING POINT: >2700F

VAPOR PRESSURE: NONE

VAPOR DENSITY: NONE

EVAPORATION RATE: NONE

SOLUBILITY IN WATER: SLIGHT

ODOR: NONE

PRODUCT TYPES:
JE TOMES & ASSOCIATES, INC. DRY PACKED PORTLAND CEMENT BASED PRODUCTS MSDS


SECTION V - FIRE AND EXPLOSION HAZARD DATA 


FLAMMABILITY: NONCOMBUSTIBLE AND NOT EXPLOSIVE.


SECTION VI - REACTIVITY DATA 


STABILITY: STABLE.

INCOMPATIBILITY (MATERIALS TO AVOID):
CONTACT OF SILICA WITH POWERFUL OXIDIZING AGENTS SUCH AS FLUORINE, CHLORINE
TRIFLUORIDE, MANGANESE TRIOXIDE, OXYGEN DIFLUORIDE, MAY CAUSE FIRES.

HAZARDOUS DECOMPOSITION OR BY-PRODUCTS:
SILICA WILL DISSOLVE IN HYDROFLUORIC ACID AND PRODUCE A CORROSIVE
GASSILICON TETRAFLUORIDE.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.

CONDITION TO AVOID: KEEP DRY UNTIL USED TO PRESERVE PRODUCT UTILITY.


SECTION VII - HEALTH HAZARD DATA 


ROUTE(S) OF ENTRY: INHALATION, SKIN, INGESTION

ACUTE EXPOSURE:
PRODUCT BECOMES ALKALINE WHEN EXPOSED TO MOISTURE. EXPOSURE CAN DRY THE
SKIN, CAUSE ALKALI BURNS AND EFFECT THE MUCOUS MEMBRANES. DUST CAN IRRITATE
THE EYES AND UPPER RESPIRATORY SYSTEM. TOXIC EFFECTS NOTED IN ANIMALS
INCLUDE, FOR ACUTE EXPOSURES, ALVEOLAR DAMAGE WITH PULMONARY EDEMA.

CHRONIC EXPOSURE:
DUST CAN CAUSE INFLAMMATION OF THE LINING TISSUE OF THE INTERIOR OF THE
NOSE AND INFLAMMATION OF THE CORNEA. HYPERSENSITIVE INDIVIDUALS MAY DEVELOP
AN ALLERGIC DERMATITIS. RESPIRABLE CRYSTALLINE SILICA (QUARTZ) CAN CAUSE
SILICOSIS, A FIBROSIS (SCARRING) OF THE LUNGS AND POSSIBLY CANCER. THERE IS
EVIDENCE THAT EXPOSURE TO RESPIRABLE SILICA OR THE DISEASE SILICOSIS IS
ASSOCIATED WITH AN INCREASED INCIDENCE OF SCLERODERMA, TUBERCULOSIS AND
KIDNEY DISORDERS.

CARCINOGENICITY LISTINGS:
NTP: KNOWN CARCINOGEN
OSHA: NOT LISTED AS A CARCINOGEN
IARC MONOGRAPHS: GROUP 1 CARCINOGEN
CALIFORNIA PROPOSITION 65: KNOWN CARCINOGEN

NTP:
THE NATIONAL TOXICOLOGY PROGRAM, IN ITS "NINTH REPORT ON CARCINOGENS"
(RELEASED MAY 15, 2000) CONCLUDED THAT "RESPIRABLE CRYSTALLINE SILICA
(RCS), PRIMARILY QUARTZ DUSTS OCCURRING IN INDUSTRIAL AND OCCUPATIONAL
SETTINGS, IS KNOWN TO BE A HUMAN CARCINOGEN, BASED ON SUFFICIENT EVIDENCE
OF CARCINOGENICITY FROM STUDIES IN HUMANS INDICATING A CASUAL RELATIONSHIP
BETWEEN EXPOSURE TO RCS AND INCREASED LUNG CANCER RATES IN WORKERS EXPOSED
TO CRYSTALLINE SILICA DUST (REVIEWED IN IAC,, 1997; BROWN ET AL., 1997;
HIND ET AL., 1997)

IARC:
THE INTERNATIONAL AGENCY FOR RESEARCH ON CANCER ("IARC") CONCLUDED THAT
THERE WAS "SUFFICIENT EVIDENCE" IN HUMANS FOR THE CARCINOGENICITY OF
CRYSTALLINE SILICA IN THE FORMS OF QUARTZ OR CRISTOBALITE FROM OCCUPATIONAL
SOURCES", AND THAT THERE IS" SUFFICIENT EVIDENCE IN EXPERIMENTAL ANIMALS
FOR THE CARCINOGENICITY OF QUARTZ OR CRISTOBALITE." THE OVERALL IARC
EVALUATION WAS THAT "CRYSTALLINE SILICA INHALED IN THE FORM OF QUARTZ
OR CRISTOBALITE FROM OCCUPATIONAL SOURCES IS CARCINOGENIC TO HUMANS
(GROUP 1)." THE IARC EVALUATION NOTED THAT "CARCINOGENICITY WAS NOT
DETECTED IN ALL INDUSTRIAL CIRCUMSTANCES OR STUDIES. CARCINOGENICITY
MAY BE DEPENDENT ON INHERENT CHARACTERISTICS OF THE CRYSTALLINE SILICA
OR ON EXTERNAL FACTORS AFFECTING ITS BIOLOGICAL ACTIVITY OR DISTRIBUTION
OF ITS POLYMORPHS." FOR FURTHER INFORMATION ON THE IARC EVALUATION, SEE
IARC MONOGRAPHS ON THE EVALUATION OF CARCINOGENIC RISKS TO HUMANS, VOLUME
68, "SILICA, SOME SILICATES..."(1997)

SIGNS AND SYMPTOMS OF EXPOSURE:
SYMPTOMS OF EXCESSIVE EXPOSURE TO THE DUST INCLUDE SHORTNESS OF BREATH AND
REDUCED PULMONARY FUNCTION. EXCESSIVE EXPOSURE TO SKIN AND EYES ESPECIALLY
WHEN MIXED WITH WATER CAN CAUSE CAUSTIC BURNS AS SEVERE AS THIRD DEGREE.

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
INDIVIDUALS WITH SENSITIVE SKIN AND WITH PULMONARY AND/OR RESPIRATORY
DISEASE, INCLUDING, BUT NOT LIMITED TO, ASTHMA AND BRONCHITIS, OR SUBJECT
TO EYE IRRITATION, SHOULD BE PRECLUDED FROM EXPOSURE. EXPOSURE TO
CRYSTALLINE SILICA OR THE DISEASE SILICOSIS IS ASSOCIATED WITH INCREASED
INCIDENCE OF SCLERODERMA, TUBERCULOSIS AND POSSIBLY INCREASED INCIDENCE OF
KIDNEY LESIONS.

EMERGENCY FIRST AID PROCEDURES:
IRRIGATE (FLOOD) EYES IMMEDIATELY AND REPEATEDLY WITH CLEAN WATER. WASH
EXPOSED SKIN AREAS WITH SOAP AND WATER. IF IRRITATION OR INFLAMMATION
OCCURS SEEK PROMPT ATTENTION. FOR GROSS INHALATION, REMOVE PERSON
IMMEDIATELY TO FRESH AIR, GIVE ARTIFICIAL RESPIRATION AS NEEDED.
GET PROMPT MEDICAL ATTENTION.


SECTION VIII - PRECAUTIONS FOR SAFE HANDLING AND USE 


SPILLS:
IF SPILLED, USE DUSTLESS METHODS (VACUUM) AND PLACE INTO CLOSE ABLE
CONTAINER FOR DISPOSAL OR USE IF NOT CONTAMINATED OR WET. USE ADEQUATE
VENTILATION.

WASTE DISPOSAL METHOD:
THE PACKAGING AND MATERIAL MAY BE LAND FILLED; HOWEVER, MATERIAL SHOULD BE
COVERED TO MINIMIZE GENERATION OF AIRBORNE DUST. THIS PRODUCT IS NOT
CLASSIFIED AS A HAZARDOUS WASTE UNDER RCRA OR CERCLA.


SECTION IX - CONTROL MEASURES/PERSONAL PROTECTION 


INHALATION:
DO NOT BREATH DUST. IN DUSTY ENVIRONMENTS, THE USE OF OSHA, MSHA OR NIOSH
APPROVED RESPIRATOR IS RECOMMENDED. LOCAL EXHAUST CAN BE USED, IF
NECESSARY, TO CONTROL AIRBORNE DUST LEVELS.

EYES: WEAR TIGHT FITTING GOGGLES.

SKIN:
THE USE OF BARRIER CREAMS OR IMPERVIOUS GLOVES, BOOTS AND CLOTHING TO
PROTECT THE SKIN FROM CONTACT IS RECOMMENDED. FOLLOWING WORK, WORKERS
SHOULD SHOWER WITH SOAP AND WATER.

PRECAUTIONS MUST BE OBSERVED BECAUSE BURNS OCCUR WITH LITTLE WARNING:
LITTLE HEAT IS SENSED.

WARN EMPLOYEES AND/OR CUSTOMERS OF THE HAZARDS AND REQUIRED OSHA
PRECAUTIONS ASSOCIATED WITH THE USE OF THIS PRODUCT.

NOTE:
THE INFORMATION AND RECOMMENDATIONS CONTAINED HEREIN ARE BASED UPON DATE
BELIEVED TO BE CORRECT. HOWEVER, NO GUARANTEE OR WARRANTY OF ANY KIND,
EXPRESS OR IMPLIED, IS MADE WITH RESPECT TO THE INFORMATION CONTAINED
HEREIN. WE ACCEPT NO RESPONSIBILITY AND DISCLAIM ALL LIABILITY FOR ANY
HARMFUL EFFECTS WHICH MAY BE CAUSED BY EXPOSURE TO SILICA CONTAINED IN
OUR PRODUCTS. CUSTOMERS-USERS MUST COMPLY WITH ALL APPLICABLE HEALTH AND
SAFETY LAWS, REGULATIONS AND ORDERS COVERING SILICA.