Common Name: 2 COMPONENT FAST SET, LATEX POLYMER LIQUID
Manufacturer: JETOMES & ASSOCIATES
SDS Revision Date: 10/30/2006
SDS Format: No Format Specified
   
Grainger Item Number(s): 15F535
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - MANUFACTURER'S NAME 
SECTION II - PRODUCT IDENTIFICATION 
SECTION III - HAZARDOUS INGREDIENTS/IDENTITY INFORMATION 
SECTION IV - PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION V - FIRE AND EXPLOSION HAZARD DATA 
SECTION VI - REACTIVITY DATA 
SECTION VII - HEALTH HAZARD DATA 
SECTION VIII - PRECAUTIONS FOR SAFE HANDLING AND USE 
SECTION IX - CONTROL MEASURES/PERSONAL PROTECTION 
SECTION I: MANUFACTURER'S NAME 
SECTION II: PRODUCT IDENTIFICATION 
SECTION III: HAZARDOUS INGREDIENTS/IDENTIFY INFORMATION 
SECTION IV: PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION V: FIRE AND EXPLOSION HAZARD DATA 
SECTION VI: REACTIVITY DATA 
SECTION VII: HEALTH HAZARD DATA 
SECTION VIII: PRECAUTIONS FOR SAFE HANDLING OR USE 
SECTION IX: CONTROL MEASURES 



MATERIAL SAFETY DATA SHEET

(OSHA 29 CFR 1910.1200)

PRODUCT: 2 COMPONENT FAST SET

JE TOMES
PRODUCT SINCE 1935


SECTION I - MANUFACTURER'S NAME 


JE TOMES & ASSOCIATES, INC.
2513 WEST 140TH PLACE
BLUE ISLAND, IL 60406

708-653-5100 - PHONE

708-653-5101- FACSIMILE

EMERGENCY TELEPHONE NUMBER: N/A

DATE PREPARED: OCTOBER 30, 2006


SECTION II - PRODUCT IDENTIFICATION 


PRODUCT NAME                           CODE#

2 COMPONENT FAST SET


SECTION III - HAZARDOUS INGREDIENTS/IDENTITY INFORMATION 


HAZARDOUS COMPONENTS       CAS NO.       PEL (OSHA)      TLV (ACGIH)
                                         MG/M3           MG/M3

SILICA SAND, CRYSTALLINE   14808-60-7    10/%SiO2+ 2     0.05 (RESPIRABLE)

PORTLAND CEMENT            65997-15-1    5               5

MAY CONTAIN ONE OR MORE OF THE FOLLOWING INGREDIENTS:

AMORPHOUS SILICA           07631-86-9    80 MG/M3/       10
                                         % SiO2

CALCIUM SULFATE            10101-41-4    5               5
                           OR
                           13997-24-5

LIME                       01305-62-0    5               5

FLY ASH                    68131-74-8    5               5

CALCIUM ALUMINATE CEMENT   65997-16-2    5               5

COPOLYMER POWDER           24937-78-8    NA              NA

OTHER LIMITS:
NATIONAL INSTITUTE FOR OCCUPATIONAL SAFETY AND HEALTH (NIOSH). RECOMMENDED
STANDARD MAXIMUM PERMISSIBLE CONCENTRATION=005 MG/M3 (RESPIRABLE FREE
SILICA) AS DETERMINED BY A FULL-SHIFT SAMPLE UP TO 10-HOUR WORKING DAY,
40-HOUR WORK WEEK. SEE NIOSH CRITERIA FOR A RECOMMENDED STANDARD
OCCUPATIONAL EXPOSURE TO CRYSTALLINE


SECTION IV - PHYSICAL/CHEMICAL CHARACTERISTICS 


APPEARANCE:
GRAY TO FRAY-BROWN COLORED POWDER. SOME PRODUCTS CONTAIN COARSE AGGREGATE.

SPECIFIC GRAVITY: 2.6 TO 3.15

MELTING POINT: >2700F

BOILING POINT: >2700F

VAPOR PRESSURE: NONE

VAPOR DENSITY: NONE

EVAPORATION RATE: NONE

SOLUBILITY IN WATER: SLIGHT

ODOR: NONE

PRODUCT TYPES:
JE TOMES & ASSOCIATES, INC. DRY PACKED PORTLAND CEMENT BASED PRODUCTS MSDS


SECTION V - FIRE AND EXPLOSION HAZARD DATA 


FLAMMABILITY: NONCOMBUSTIBLE AND NOT EXPLOSIVE.


SECTION VI - REACTIVITY DATA 


STABILITY: STABLE.

INCOMPATIBILITY (MATERIALS TO AVOID):
CONTACT OF SILICA WITH POWERFUL OXIDIZING AGENTS SUCH AS FLUORINE, CHLORINE
TRIFLUORIDE, MANGANESE TRIOXIDE, OXYGEN DIFLUORIDE, MAY CAUSE FIRES.

HAZARDOUS DECOMPOSITION OR BY-PRODUCTS:
SILICA WILL DISSOLVE IN HYDROFLUORIC ACID AND PRODUCE A CORROSIVE
GASSILICON TETRAFLUORIDE.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.

CONDITION TO AVOID: KEEP DRY UNTIL USED TO PRESERVE PRODUCT UTILITY.


SECTION VII - HEALTH HAZARD DATA 


ROUTE(S) OF ENTRY: INHALATION, SKIN, INGESTION

ACUTE EXPOSURE:
PRODUCT BECOMES ALKALINE WHEN EXPOSED TO MOISTURE. EXPOSURE CAN DRY THE
SKIN, CAUSE ALKALI BURNS AND EFFECT THE MUCOUS MEMBRANES. DUST CAN IRRITATE
THE EYES AND UPPER RESPIRATORY SYSTEM. TOXIC EFFECTS NOTED IN ANIMALS
INCLUDE, FOR ACUTE EXPOSURES, ALVEOLAR DAMAGE WITH PULMONARY EDEMA.

CHRONIC EXPOSURE:
DUST CAN CAUSE INFLAMMATION OF THE LINING TISSUE OF THE INTERIOR OF THE
NOSE AND INFLAMMATION OF THE CORNEA. HYPERSENSITIVE INDIVIDUALS MAY DEVELOP
AN ALLERGIC DERMATITIS. RESPIRABLE CRYSTALLINE SILICA (QUARTZ) CAN CAUSE
SILICOSIS, A FIBROSIS (SCARRING) OF THE LUNGS AND POSSIBLY CANCER. THERE
IS EVIDENCE THAT EXPOSURE TO RESPIRABLE SILICA OR THE DISEASE SILICOSIS IS
ASSOCIATED WITH AN INCREASED INCIDENCE OF SCLERODERMA, TUBERCULOSIS AND
KIDNEY DISORDERS.

CARCINOGENICITY LISTINGS:
NTP: KNOWN CARCINOGEN
OSHA: NOT LISTED AS A CARCINOGEN
IARC MONOGRAPHS: GROUP 1 CARCINOGEN

CALIFORNIA PROPOSITION 65: KNOWN CARCINOGEN

NTP:
THE NATIONAL TOXICOLOGY PROGRAM, IN ITS "NINTH REPORT ON CARCINOGENS"
(RELEASED MAY 15, 2000) CONCLUDED THAT "RESPIRABLE CRYSTALLINE SILICA
(RCS), PRIMARILY QUARTZ DUSTS OCCURRING IN INDUSTRIAL AND OCCUPATIONAL
SETTINGS, IS KNOWN TO BE A HUMAN CARCINOGEN, BASED ON SUFFICIENT EVIDENCE
OF CARCINOGENICITY FROM STUDIES IN HUMANS INDICATING A CASUAL RELATIONSHIP
BETWEEN EXPOSURE TO RCS AND INCREASED LUNG CANCER RATES IN WORKERS EXPOSED
TO CRYSTALLINE SILICA DUST (REVIEWED IN IAC,, 1997; BROWN ET AL., 1997;
HIND ET AL., 1997)

IARC:
THE INTERNATIONAL AGENCY FOR RESEARCH ON CANCER ("IARC") CONCLUDED THAT
THERE WAS "SUFFICIENT EVIDENCE" IN HUMANS FOR THE CARCINOGENICITY OF
CRYSTALLINE SILICA IN THE FORMS OF QUARTZ OR CRISTOBALITE FROM OCCUPATIONAL
SOURCES", AND THAT THERE IS "SUFFICIENT EVIDENCE IN EXPERIMENTAL ANIMALS
FOR THE CARCINGOGENICITY OF QUARTZ OR CRISTOBALITE." THE OVERALL IARC
EVALUATION WAS THAT "CRYSTALLINE SILICA INHALED IN THE FORM OF QUARTZ OR
CRISTOBALITE FROM OCCUPATIONAL SOURCES IS CARCINOGENIC TO HUMANS (GROUP1)."
THE IARC EVALUATION NOTED THAT "CARCINOGENICITY WAS NOT DETECTED IN ALL
INDUSTRIAL CIRCUMSTANCES OR STUDIES. CARCINOGENICITY MAY BE DEPENDENT ON
INHERENT CHARACTERISTICS OF THE CRYSTALLINE SILICA OR ON EXTERNAL FACTORS
AFFECTING ITS BIOLOGICAL ACTIVITY OR DISTRIBUTION OF ITS POLYMORPHS." FOR
FURTHER INFORMATION ON THE IARC EVALUATION, SEE IARC MONOGRAPHS ON THE
EVALUATION OF CARCINOGENIC RISKS TO HUMANS, VOLUME 68, "SILICA, SOME
SILICATES..."(1997)

SIGNS AND SYMPTOMS OF EXPOSURE:
SYMPTOMS OF EXCESSIVE EXPOSURE TO THE DUST INCLUDE SHORTNESS OF BREATH AND
REDUCED PULMONARY FUNCTION. EXCESSIVE EXPOSURE TO SKIN AND EYES ESPECIALLY
WHEN MIXED WITH WATER CAN CAUSE CAUSTIC BURNS AS SEVERE AS THIRD DEGREE.

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
INDIVIDUALS WITH SENSITIVE SKIN AND WITH PULMONARY AND/OR RESPIRATORY
DISEASE, INCLUDING, BUT NOT LIMITED TO, ASTHMA AND BRONCHITIS, OR SUBJECT
TO EYE IRRITATION, SHOULD BE PRECLUDED FROM EXPOSURE. EXPOSURE TO
CRYSTALLINE SILICA OR THE DISEASE SILICOSIS IS ASSOCIATED WITH INCREASED
INCIDENCE OF SCLERODERMA, TUBERCULOSIS AND POSSIBLY INCREASED INCIDENCE
OF KIDNEY LESIONS.

EMERGENCY FIRST AID PROCEDURES:
IRRIGATE (FLOOD) EYES IMMEDIATELY AND REPEATEDLY WITH CLEAN WATER. WASH
EXPOSED SKIN AREAS WITH SOAP AND WATER. IF IRRITATION OR INFLAMMATION
OCCURS SEEK PROMPT ATTENTION. FOR GROSS INHALATION, REMOVE PERSON
IMMEDIATELY TO FRESH AIR, GIVE ARTIFICIAL RESPIRATION AS NEEDED. GET
PROMPT MEDICAL ATTENTION.


SECTION VIII - PRECAUTIONS FOR SAFE HANDLING AND USE 


SPILLS:
IF SPILLED, USE DUSTLESS METHODS (VACUUM) AND PLACE INTO CLOSE ABLE
CONTAINER FOR DISPOSAL OR USE IF NOT CONTAMINATED OR WET. USE ADEQUATE
VENTILATION.

WASTE DISPOSAL METHOD:
THE PACKAGING AND MATERIAL MAY BE LAND FILLED; HOWEVER, MATERIAL SHOULD BE
COVERED TO MINIMIZE GENERATION OF AIRBORNE DUST. THIS PRODUCT IS NOT
CLASSIFIED AS A HAZARDOUS WASTE UNDER RCRA OR CERCLA.


SECTION IX - CONTROL MEASURES/PERSONAL PROTECTION 


INHALATION:
DO NOT BREATH DUST. IN DUSTY ENVIRONMENTS, THE USE OF OSHA, MSHA OR NIOSH
APPROVED RESPIRATOR IS RECOMMENDED. LOCAL EXHAUST CAN BE USED, IF
NECESSARY, TO CONTROL AIRBORNE DUST LEVELS.

EYES: WEAR TIGHT FITTING GOGGLES.

SKIN:
THE USE OF BARRIER CREAMS OR IMPERVIOUS GLOVES, BOOTS AND CLOTHING TO
PROTECT THE SKIN FROM CONTACT IS RECOMMENDED. FOLLOWING WORK, WORKERS
SHOULD SHOWER WITH SOAP AND WATER.

PRECAUTIONS MUST BE OBSERVED BECAUSE BURNS OCCUR WITH LITTLE WARNING -
LITTLE HEAT IS SENSED.

WARN EMPLOYEES AND/OR CUSTOMERS OF THE HAZARDS AND REQUIRED OSHA
PRECAUTIONS ASSOCIATED WITH THE USE OF THIS PRODUCT.

NOTE:
THE INFORMATION AND RECOMMENDATIONS CONTAINED HEREIN ARE BASED UPON DATE
BELIEVED TO BE CORRECT. HOWEVER, NO GUARANTEE OR WARRANTY OF ANY KIND,
EXPRESS OR IMPLIED, IS MADE WITH RESPECT TO THE INFORMATION CONTAINED
HEREIN. WE ACCEPT NO RESPONSIBILITY AND DISCLAIM ALL LIABILITY FOR ANY
HARMFUL EFFECTS WHICH MAY BE CAUSED BY EXPOSURE TO SILICA CONTAINED IN
OUR PRODUCTS. CUSTOMERS-USERS MUST COMPLY WITH ALL APPLICABLE HEALTH AND
SAFETY LAWS, REGULATIONS AND ORDERS COVERING SILICA.


MATERIAL SAFETY DATA SHEET

(OSHA 29 CFR 1910.1200)

PRODUCT: LATEX POLYMER LIQUID

JE TOMES

PRODUCT SINCE 1935


SECTION I: MANUFACTURER'S NAME 


JETOMES & ASSOCIATES, INC.
2513 WEST 140TH PLACE
BLUE ISLAND, IL 60406

708-653-5100 - PHONE

708-653-5101 - FACSIMILE

EMERGENCY TELEPHONE NUMBER: N/A

DATE PREPARED: SEPTEMBER 23, 2004

UPDATED: OCTOBER 14, 2009


SECTION II: PRODUCT IDENTIFICATION 


PRODUCT NAME                      CODE #

LATEX POLYMER LIQUID              C133\C134


SECTION III: HAZARDOUS INGREDIENTS/IDENTIFY INFORMATION 


HAZARDOUS COMPONENTS (SPECIFIC CHEMICAL IDENTITY COMMON NAME):

OSHA PEL              ACGIA TLV         OTHER % (OPTIONAL)

AMMONIA, AQUA                           0.1


SECTION IV: PHYSICAL/CHEMICAL CHARACTERISTICS 


BOILING POINT: N/A

SPECIFIC GRAVITY (H2O=1): 2.54

VAPOR PRESSURE (MMHg.): N/A

MELTING POINT: N/A

VAPOR DENSITY (AIR=1): N/A

EVAPORATION RATE (BUTYL ACETATE=1): N/A

SOLUBILITY IN WATER: NON-SOLUBLE


SECTION V: FIRE AND EXPLOSION HAZARD DATA 


FLASH POINT (METHOD USED):

NON FLAMMABLE:

FLAMMABLE UNITS: N/A
LEL: N/A
UEL: N/A

EXTINGUISHING MEDIA: WILL NOT BURN.

SPECIAL FIRE FIGHTING PROCEDURES:
AVOID BREATHING SMOKE, FUMES, AND DECOMPOSITION PRODUCTS. AS IN ANY FIRE,
WEAR SELF-CONTAINED BREATHING APPARATUS PRESSURE-DEMAND MSHA/NIOSH
(APPROVED OR EQUIVALENT) AND FULL PROTECTIVE GEAR.

UNUSUAL FIRE AND EXPLOSION HAZARDS: NONE REQUIRED WITH THIS PRODUCT.


SECTION VI: REACTIVITY DATA 


UNSTABLE: STABLE

STABLE: YES

CONDITIONS TO AVOID: NONE

INCOMPATIBILITY (MATERIALS TO AVOID): NONE

HAZARDOUS DECOMPOSITION OR BYPRODUCTS: NONE.

HAZARDOUS POLYMERIZATION: MAY OCCUR

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.

CONDITIONS TO AVOID: NONE.


SECTION VII: HEALTH HAZARD DATA 


ROUTE(S) OF ENTRY:
INHALATION: YES
SKIN: YES
INGESTION: YES

HEALTH HAZARD (ACUTE AND CHRONIC) INHALATION:
EXCESSIVE OR LONG-TERM INHALATION MAY CAUSE PNEUMOCONIOSIS (SILICOSIS).
MAY CAUSE IRRITATION TO NOSE, THROAT, AND RESPIRATORY.

CARCINOGENICITY:
NTP?: YES
IARC MONOGRAPHS?: YES
OSHA REGULATED?: N/A

SIGNS AND SYMPTOMS OF EXPOSURE: MAY CAUSE RASH OR IRRITATION TO SKIN.

MEDICAL CONDITIONS GENERALLY AGGRAVATED BY EXPOSURE:
INDIVIDUALS WITH RESPIRATORY DISEASE, SUBJECT EYE IRRITATION AND OR
ALLERGIES TO CEMENTS.

EMERGENCY AND FIRST AID PROCEDURES:

LUNGS: MOVE TO FRESH AIR.

EYES: FLUSH WITH WATER.

SKIN: WASH WITH SOAP AND WATER.

INTERNAL/INGESTION:
IS NOT CONSIDERED A POTENTIAL ROUTE OF EXPOSURE IF SWALLOWED, IMMEDIATELY
GIVE 2 GLASSES OF WATER. GET MEDICAL ATTENTION IMMEDIATELY. NEVER GIVE
ANYTHING BY MOUTH TO AN UNCONSCIOUS PERSON.


SECTION VIII: PRECAUTIONS FOR SAFE HANDLING OR USE 


STEPS TO BE TAKEN IN CASE MATERIAL RELEASES OR SPILLS:
CONTAINED, SOLIDIFIED AND PLACE IN DISPOSAL CONTAINERS.

WASTE DISPOSAL METHOD:
DISPOSE IN ACCORDANCE WITH ALL LOCAL, STATE, PROVINCIAL, AND FEDERAL
REGULATIONS.

PRECAUTIONS TO BE TAKEN IN HANDLING AND STORAGE:
STORE IN A COOL DRY ENVIRONMENT. AVOID BAG OR CONTAINER BREAKAGE.

OTHER PRECAUTIONS: DO NOT BREATHE DUST.


SECTION IX: CONTROL MEASURES 


RESPIRATORY PROTECTION (SPECIFIC TYPE) NIOSH/MSHA: APPROVED

VENTILATION LOCAL EXHAUST: N/A, SPECIAL AS SUITABLE FOR JOB CONDITIONS

PROTECTIVE GLOVES: RECOMMENDED

EYE PROTECTION: RECOMMENDED

OTHER PROTECTIVE CLOTHING OR EQUIPMENT: BOOTS, COVERALLS TO PREVENT CONTACT

WORK/HYGIENIC PRACTICES:
WHEN FINISHED SHOWER TO REMOVE DUST. LAUNDER CLOTHING AFTER USE TO REMOVE
DUST BEFORE REUSE.