Common Name: POLY-CARBONMONOFLUORIDE (BR TYPE) LITHIUM BATTERIES
Manufacturer: PANASONIC INDUSTRIAL
MSDS Revision Date: 1/1/2010
   
Grainger Item Number(s): 36E896, 4EA49, 4EE37, 5RE39
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
DISPOSAL 
TRANSPORTATION 
FIRST AID 
GENERAL RECOMMENDATIONS 
FIRE SAFETY 



PRODUCT INFORMATION SHEET

PANASONIC BATTERIES

PANASONIC INDUSTRIAL COMPANY
A DIVISION PANASONIC CORPORATION OF NORTH AMERICA
5201 TOLLVIEW DRIVE, 1F-3
ROLLING MEADOWS, IL 60008

TOLL FREE: 877-726-2228

FAX: 847-637-4660

INTERNET: WWW.PANASONIC.COM/BATTERIES

E-MAIL: OEMBATTERIES@PANASONIC.COM

PRODUCT: POLY-CARBONMONOFLUORIDE (BR TYPE) LITHIUM BATTERIES

APPLICABLE MODELS/SIZES:
ALL BR TYPE CYLINDRICAL AND COIN BATTERIES, EXCEPT OUR BR-C.

REVISION: K JANUARY 1, 2010

THE BATTERIES REFERENCED HEREIN ARE EXEMPT ARTICLES AND ARE NOT SUBJECT
TO THE OSHA HAZARD COMMUNICATION STANDARD REQUIREMENT. THIS SHEET IS
PROVIDED AS A SERVICE TO OUR CUSTOMERS.

MSDS

MATERIAL SAFETY DATA SHEETS (MSDS) ARE A SUB-REQUIREMENT OF THE
OCCUPATIONAL SAFETY AND HEALTH ADMINISTRATION (OSHA) HAZARD
COMMUNICATION STANDARD, 29 CFR SUBPART 1910.1200. THIS HAZARD
COMMUNICATION STANDARD DOES NOT APPLY TO VARIOUS SUBCATEGORIES
INCLUDING ANYTHING DEFINED BY OSHA AS AN "ARTICLE". OSHA HAS
DEFINED "ARTICLE" AS A MANUFACTURED ITEM OTHER THAN A FLUID OR
PARTICLE
(I) WHICH IS FORMED TO A SPECIFIC SHAPE OR DESIGN DURING MANUFACTURE
(II) WHICH HAS END USE FUNCTION(S) DEPENDENT IN WHOLE OR IN PART UPON
ITS SHAPE OR DESIGN DURING END USE; AND
(III) WHICH UNDER NORMAL CONDITIONS OF USE DOES NOT RELEASE MORE THAN VERY
SMALL QUANTITIES, E.G. MINUTE OR TRACE AMOUNTS OF A HAZARDOUS CHEMICAL,
AND DOES NOT POSE A PHYSICAL HAZARD OR HEALTH RISK TO EMPLOYEES.

BECAUSE ALL OF OUR BATTERIES ARE DEFINED AS "ARTICLES", THEY ARE
EXEMPT FROM THE REQUIREMENTS OF THE HAZARD COMMUNICATION STANDARD;
HENCE A MSDS IS NOT REQUIRED.

THE FOLLOWING COMPONENTS ARE FOUND IN A PANASONIC POLY-CARBONMONOFLUORIDE
(BR) LITHIUM BATTERIES:

CYLINDRICAL CELL COMPONENTS   MATERIAL                           FORMULA

POSITIVE ELECTRODE            POLY-CARBONMONOFLUORIDE            (CF)n

NEGATIVE ELECTRODE            LITHIUM                            Li

ELECTROLYTE                   y-BUTYROLACTONE-SOLVENT            C4H6O2

                              1,2 DIMETHOXYETHANE-SOLVENT        C4H10O2

                              LITHIUM TETRAFLUROBORATE-SALT      LiBF4

COIN CELL COMPONENTS          MATERIAL                           FORMULA

POSITIVE ELECTRODE            POLY-CARBONMONOFLUORIDE            (CF)n

NEGATIVE ELECTRODE            LITHIUM                            Li

ELECTROLYTE                   y-BUTYROLACTONE-SOLVENT            C4H6O2

                              1,2 DIMETHOXYETHANE-SOLVENT        C4H10O2

                              LITHIUM TETRAFLUROBORATE-SALT      LiBF4


DISPOSAL 


LITHIUM BATTERIES ARE NEITHER SPECIFICALLY LISTED NOR EXEMPTED FROM
THE FEDERAL ENVIRONMENTAL PROTECTION AGENCY (EPA) HAZARDOUS WASTE
REGULATIONS AS PROMULGATED BY THE RESOURCE CONSERVATION AND RECOVERY
ACT (RCRA). THE ONLY METAL OF POSSIBLE CONCERN IN A LITHIUM BATTERY
IS LITHIUM THAT IS NOT A LISTED OR CHARACTERISTIC TOXIC HAZARDOUS WASTE.
WASTE LITHIUM BATTERIES CAN BE CONSIDERED A REACTIVE HAZARDOUS WASTE IF
THERE IS A SIGNIFICANT AMOUNT OF UNREACTED, OR UNCONSUMED LITHIUM
REMAINING IN THE SPENT BATTERY. THE KEY TO DISPOSING OF A LITHIUM
BATTERY AS A NON-HAZARDOUS WASTE IS TO GUARANTEE THAT IT IS FULLY OR
MOSTLY DISCHARGED. ONCE IT IS DISCHARGED IT CAN BE DISPOSED OF AS
NON-HAZARDOUS WASTE. YOU CAN DISPOSE OF A FULLY CHARGED OR PARTIALLY
DISCHARGED LITHIUM BATTERY AS A HAZARDOUS WASTE AFTER THEY ARE FIRST
NEUTRALIZED THROUGH AN APPROVED SECONDARY TREATMENT. THE NEED FOR A
SECONDARY TREATMENT PRIOR TO DISPOSAL IS A REQUIREMENT OF THE U.S. LAND
BAN RESTRICTIONS OF THE HAZARDOUS AND SOLID WASTE AMENDMENTS OF 1984.
A SECONDARY TREATMENT CENTER CAN ONLY RECEIVE THESE BATTERIES AS
MANIFESTED HAZARDOUS WASTE. THE WASTE CODE FOR CHARGED LITHIUM
BATTERIES IS D003, REACTIVE. IN EITHER CASE, BUTTON CELL BATTERIES
CONTAIN SO LITTLE LITHIUM THAT THEY NEVER QUALIFY AS A REACTIVE
HAZARDOUS WASTE. THESE BATTERIES ARE SAFE FOR DISPOSAL IN THE NORMAL
MUNICIPAL WASTE STREAM.

DISPOSAL OF LARGE QUANTITIES OF UNDISCHARGED LITHIUM BATTERIES SHOULD
BE PERFORMED BY PERMITTED, PROFESSIONAL DISPOSAL FIRMS KNOWLEDGEABLE IN
FEDERAL, STATE AND LOCAL HAZARDOUS MATERIALS AND HAZARDOUS WASTE
TRANSPORTATION AND DISPOSAL REQUIREMENTS. AS ALWAYS, HOUSEHOLDS ARE
EXEMPT FROM THE RCRA HAZARDOUS WASTE GUIDELINES.

IN CALIFORNIA, PACKAGES THAT CONTAIN CR LITHIUM COIN CELLS AND
THE OWNERS/OPERATING INSTRUCTIONS OF PRODUCTS THAT CONTAIN CR
LITHIUM COIN CELLS MUST INCLUDE THE FOLLOWING STATEMENT:
"PERCHLORATE MATERIAL - SPECIAL HANDLING MAY APPLY, SEE
WWW.DTSC.CA.GOV/HAZARDOUSWASTE/PERCHORATE". THE EFFECTIVE DATE FOR
THIS PERCHLORATE LABEL WAS JULY 1, 2006 FOR NON-CONSUMER PRODUCTS
AND JANUARY 1, 2007 FOR CONSUMER PRODUCTS.


TRANSPORTATION 


EFFECTIVE OCTOBER 1, 2008 ALL PANASONIC LITHIUM BATTERIES, EXCEPT FOR
OUR BR-C, ARE NOT SUBJECT TO THE REQUIREMENTS OF THE DEPARTMENT OF
TRANSPORTATION (DOT) SUBCHAPTER C, HAZARDOUS MATERIALS REGULATIONS IF
SHIPPED IN COMPLIANCE WITH 49 CFR 173.185 AND SPECIAL PROVISION 188.

EFFECTIVE JANUARY 1, 2010 ALL PANASONIC LITHIUM BATTERIES CAN BE
SHIPPED BY AIR IN ACCORDANCE WITH INTERNATIONAL CIVIL AVIATION
ORGANIZATION (ICAO), SECTION II OR INTERNATIONAL AIR TRANSPORT
ASSOCIATION (IATA), SECTION II PACKING INSTRUCTIONS
(PI) 968 (BATTERIES), PI 969 (BATTERIES, PACKED WITH EQUIPMENT)
AND PI 970 (BATTERIES, CONTAINED IN EQUIPMENT) AS APPROPRIATE

CURRENTLY ALL PANASONIC LITHIUM BATTERIES ARE REGULATED BY THE
INTERNATIONAL MARITIME ORGANIZATION (IMO), UNDER SPECIAL
PROVISIONS 188 AND 230.

IF YOU BUILD ANY OF OUR LITHIUM CELLS INTO A BATTERY PACK, YOU MUST
ALSO ASSURE THAT THEY ARE TESTED IN ACCORDANCE WITH THE UN MODEL
REGULATIONS, MANUAL OF TEST AND CRITERIA. PART III, SUBSECTION 38.3.

EFFECTIVE DECEMBER 29, 2004, THE DOT REQUIRES THAT THE OUTSIDE OF EACH
PACKAGE THAT CONTAINS PRIMARY LITHIUM BATTERIES, REGARDLESS OF SIZE OR
NUMBER OF BATTERIES, BE LABELED WITH THE FOLLOWING STATEMENT:
"PRIMARY LITHIUM BATTERIES - FORBIDDEN FOR TRANSPORT ABOARD PASSENGER
AIRCRAFT". THE LABELING REQUIREMENT COVERS SHIPMENTS VIA HIGHWAY, RAIL,
VESSEL OR CARGO-ONLY AIRCRAFT AND COVERS ALL SHIPMENTS INSIDE, INTO OR
OUT OF THE US. THE LABEL MUST BE IN CONTRASTING COLOR AND THE LETTERS
MUST BE 12 MM (0.5 IN) IN HEIGHT FOR PACKAGES WEIGHING MORE THAN 30 KG
AND 6 MM (0.25 IN) IN HEIGHT FOR PACKAGES WEIGHTING LESS THAN 30 KG.

IF YOU PLAN ON TRANSPORTING ANY UNTESTED PROTOTYPE BATTERY PACKS CONTACT
YOUR PANASONIC SALES REPRESENTATIVE FOR REGULATORY INFORMATION.


FIRST AID 


IF YOU GET ELECTROLYTE IN YOUR EYES, FLUSH WITH WATER FOR 15 MINUTES
WITHOUT RUBBING AND IMMEDIATELY CONTACT A PHYSICIAN. IF YOU GET
ELECTROLYTE ON YOUR SKIN WASH THE AREA IMMEDIATELY WITH SOAP AND WATER.
IF IRRITATION CONTINUES, CONTACT A PHYSICIAN. IF A BATTERY IS INGESTED,
CALL THE NATIONAL CAPITAL POISON CENTER (NCPC) AT 202-625-3333
(COLLECT) OR YOUR LOCAL POISON CENTER IMMEDIATELY. LITHIUM COIN
BATTERIES LODGED IN THE ESOPHAGUS SHOULD BE REMOVED IMMEDIATELY.
LEAKAGE, CHEMICAL BURNS AND PERFORATION CAN OCCUR WITHIN HOURS OF
INGESTION.


GENERAL RECOMMENDATIONS 


CAUTION:
RISK OF FIRE, EXPLOSION AND BURNS. DO NOT RECHARGE, CRUSH, HEAT
ABOVE 212 DEG. F (100 DEG. C) OR INCINERATE.


FIRE SAFETY 


IN CASE OF FIRE, YOU CAN USE A CLASS "D" FIRE EXTINGUISHER OR OTHER
SMOTHERING AGENT SUCH AS LITH-X, COPPER POWDER OR DRY SAND. IF YOU
USE WATER, USE ENOUGH TO SMOTHER THE FIRE. USING AN INSUFFICIENT AMOUNT
OF WATER WILL ONLY MAKE THE FIRE WORSE. COOLING THE EXTERIOR OF THE
BATTERIES WILL HELP PREVENT RUPTURING. BURNING OF THESE BATTERIES WILL
GENERATE TOXIC AND CORROSIVE LITHIUM HYDROXIDE FUMES. FIRE FIGHTERS
SHOULD USE SELF-CONTAINED BREATHING APPARATUS. DETAILED INFORMATION ON
FIGHTING A LITHIUM METAL BATTERY FIRE CAN BE FOUND IN GUIDE 138
(SUBSTANCES - WATER - REACTIVE) OF THE US DOT EMERGENCY RESPONSE GUIDE.

NOTICE:
THE INFORMATION AND RECOMMENDATIONS SET FORTH ARE MADE IN GOOD FAITH
AND ARE BELIEVED TO BE ACCURATE AT THE DATE OF PREPARATION. PANASONIC
INDUSTRIAL COMPANY MAKES NO WARRANTY EXPRESSED OR IMPLIED.

007-10