Common Name: SUPERCOOL R-134A REFRIGERANT PLUS, 24261
Manufacturer: TIRE SEAL
SDS Revision Date: 9/9/2011
SDS Format: No Format Specified
   
Grainger Item Number(s): 5DPW6
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 COMPANY IDENTIFICATION AND CHEMICAL PRODUCT 
SECTION 2 HAZARDOUS INGREDIENTS 
SECTION 3 PHYSICAL INGREDIENTS 
SECTION 4 FIRST AID MEASURES 
SECTION 5 FIRE FIGHTING MEASURES 
SECTION 6 ACCIDENTAL RELEASE MEASURES 
SECTION 7 HANDLING AND STORAGE 
SECTION 8 EXPOSURE CONTROL / PERSONAL PROTECTION 
SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 REACTIVITY 
SECTION 11 TOXICOLOGICAL INFORMATION 
SECTION 12 ECOLOGICAL INFORMATION 
SECTION 13 DISPOSAL CONSIDERATIONS 
SECTION 14 TRANSPORTATION INFORMATION 
SECTION 15 REGULATORY INFORMATION 
SECTION 16 OTHER INFORMATION 



SUPERCOOL R-134A REFRIGERANT PLUS

PART #: 24261

MATERIAL SAFETY DATA SHEET

EMERGENCY PHONE NUMBER: 904-378-3232

DATE: SEPTEMBER 9, 2011


SECTION 1 COMPANY IDENTIFICATION AND CHEMICAL PRODUCT 


COMPANY NAME: TIRE SEAL, INC.

ADDRESS:
3574 CORONA STREET
LAKE WORTH, FL 33461

PHONE/FAX: 561-582-2245 / 561-582-1499

TRADE NAME: SUPERCOOL R-134A REFRIGERANT PLUS

CHEMICAL NAME: SYNTHETIC HYDROCARBON BLEND AND R134A

CHEMICAL FAMILY: SYNTHETIC HYDROCARBON BLEND AND R134A

FORMULA: PROPRIETARY

CAS#: PROPRIETARY

APPLICATIONS:
SUPERCOOL R-134A REFRIGERANT PLUS IS USED AS OIL CHARGE, PERFORMANCE
ENHANCER, AND LEAK STOP IN R-134A REFRIGERATION SYSTEMS.


SECTION 2 HAZARDOUS INGREDIENTS 


INGREDIENTS                  OSHA PEL / ACGIH TLV  CAS NUMBER  PERCENT

1,1,1,2-TETRAFLUOROETHANE    1000 PPM: TWA         811-97-2    86%

SYNTHETIC HYDROCARBON BLEND  NON-HAZARDOUS         NA          14%


SECTION 3 PHYSICAL INGREDIENTS 


APPEARANCE: CLEAR LIQUID & GAS, YELLOW/GREEN TINT


SECTION 4 FIRST AID MEASURES 


EYES:
FLUSH WITH CLEAN, LUKEWARM WATER (LOW PRESSURE) OCCASIONALLY LIFTING
EYELIDS. HAVE EYES EXAMINED AND TREATED BY MEDICAL PERSONNEL. R134A LIQUID
SPLASHES OR VAPOR MAY CAUSE FREEZE BURNS.

SKIN:
R134A IN LIQUID FORM IN THIS PRODUCT MAY CAUSE FREEZE BURNS (FROST-LIKE
LESIONS. THAW AFFECTED AREA WITH WARM WATER. REMOVE OIL FROM SKIN BY
WASHING AFFECTED AREAS THOROUGHLY WITH SOAP AND WATER. WASH CONTAMINATED
CLOTHING BEFORE REUSE. IF SYMPTOMS (IRRITATIONS OR BLISTERING) DEVELOP, GET
MEDICAL ATTENTION.

INHALATION:
EXPOSURE TO VERY HIGH VAPOR CONCENTRATIONS CAN INDUCE ANESTHETIC EFFECTS
PROGRESSING FROM DIZZINESS, WEAKNESS, NAUSEA, TO UNCONSCIOUSNESS. IT CAN
ACT AS AN ASPHYXIANT BY LIMITING AVAILABLE OXYGEN, AT VERY HIGH DOSES,
CARDIAC SENSITIZATION TO THE CIRCULATING EPINEPHRINE LIKE - COMPOUNDS CAN
RESULT IN FATAL CARDIAC ARRHYTHMIAS. AVOID BREATHING OIL MISTS. REMOVE
VICTIM TO FRESH AIR. GIVE ARTIFICIAL RESPIRATION IF NOT BREATHING. OXYGEN
MAY BE GIVEN BY QUALIFIED PERSONNEL IF BREATHING IS DIFFICULT. IN THE EVENT
OF CARDIAC ARREST, APPLY EXTERNAL CARDIAC MASSAGE. DO NOT ADMINISTER
ADRENALINE OR SIMILAR SYMPATHOMIMETIC DRUGS AS CARDIAC ARRHYTHMIAS MAY
RESULT. GET IMMEDIATE MEDICAL ATTENTION.

INGESTION:
DO NOT INDUCE VOMITING. FORCE LIQUIDS. HAS LAXATIVE EFFECT. R134A LIQUID
MIXED WITH LUBRICANT MOST UNLIKELY TO DIGEST.


SECTION 5 FIRE FIGHTING MEASURES 


FLASH POINT: 425 DEG. F MIN

FLAMMABLE LIMITS: N/A

AUTO IGNITION TEMP: N/A

FIRE & EXPOSURE HAZARDS:
LOW FIRE HAZARD - DO NOT CUT, DRILL, OR WELD CONTAINERS.

EXTINGUISHING MEDIA:
DRY CHEMICAL FOAM, WATER SPRAY, CARBON DIOXIDE FOR SMALL FIRES.

FIRE FIGHTING PROCEDURES:
CONTAIN LIQUID, COVER WITH EXTINGUISHING AGENT, USE WATER SPRAY TO COOL
FIRE EXPOSED CONTAINERS AND AS PROTECTIVE SCREEN. DO NOT POINT SOLID WATER
STREAM DIRECTLY INTO BURNING FLUID TO AVOID SPREADING


SECTION 6 ACCIDENTAL RELEASE MEASURES 


SPILL OR LEAK:
CONTAIN SPILL, ABSORB WITH INERT ABSORBENT SUCH DRY CLAY, SAND,
DIATOMACEOUS EARTH, COMMERCIAL SORBENTS OR RECOVER USING PUMPS. SCOOP UP
USED ABSORBENTS INTO APPROVED RECEPTACLES.

WASTE DISPOSAL:
DISPOSE IN APPROVED, SECURE LANDFILL SITE OR THROUGH A LICENSED WASTE
RECLAIMER.


SECTION 7 HANDLING AND STORAGE 


MAX. STORAGE TEMP.: 120 DEG. F

SHELF LIFE: INDEFINITE IN ORIGINAL CONTAINER

PRECAUTIONS:
NOT FOR INTERNAL USE. AVOID CONTACT WITH SKIN, EYES, CLOTHING


SECTION 8 EXPOSURE CONTROL / PERSONAL PROTECTION 


EYE PROTECTION:
CHEMICAL GOGGLES IF SPLASHING IS LIKELY OR HIGH PRESSURE SYSTEMS ARE USED.
PVC OR NITRILE GLOVES ARE RECOMMENDED IF PROLONGED CONTACT WITH SKIN IS TO
OCCUR. NORMALLY NOT NECESSARY. IF MIST IS GENERATED, WEAR APPROVED ORGANIC
RESPIRATOR SUITABLE FOR OIL MIST AREAS WITH SUFFICIENT OXYGEN.

VENTILATION: GENERAL VENTILATION.

EXPOSURE LIMITS:
ACUTE LD50: >5000 MG/KG (RAT: ORAL)


SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: CLEAR LIQUID & GAS, YELLOW/GREEN TINT.

BOILING POINT: -40 DEG. F (R134A), >570 DEG. F SYNTHETIC HYDROCARBON BLEND

VAPOR PRESSURE: 79 PSIG @ 25 DEG. C (R134A), <0.001 KPA @ 25 DEG. C

SPECIFIC GRAVITY: 0.85-.097 SYNTHETIC HYDROCARBON BLEND

VOLATILES, % VOLUME: 0%

ODOR: VERY SLIGHT HYDROCARBON ODOR

SOLUBILITY IN WATER: NEGLIGIBLE

EVAPORATION RATE: NIL

VISCOSITY: @40 DEG. C VARIES DEPENDING ON GRADE


SECTION 10 REACTIVITY 


STABILITY: PRODUCT IS STABLE

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.

INCOMPATIBILITIES: STRONG OXIDIZERS.

DECOMPOSITION PRODUCTS:
R134A - HIGHLY TOXIC DECOMPOSITION PRODUCTS OCCUR WHEN BURNED. SYNTHETIC
HYDROCARBON BLEND - ANALOGOUS COMPOUNDS EVOLVE, CARBON MONOXIDE, CARBON
DIOXIDE, AND OTHER UNDEFINED FRAGMENTS WHEN BURNED.


SECTION 11 TOXICOLOGICAL INFORMATION 


GENERAL:
ACUTE LD50: >2000 MG/KG (RAT: ORAL)


SECTION 12 ECOLOGICAL INFORMATION 


GENERAL: BIODEGRADABLE CEC L33A93 >80% @ 45 DAYS.


SECTION 13 DISPOSAL CONSIDERATIONS 


WASTE DISPOSAL:
USED PRODUCT MUST BE DISPOSED OF IN ACCORDANCE WITH FEDERAL, STATE, AND
LOCAL ENVIRONMENTAL CONTROL REGULATIONS. INCINERATION IS PREFERRED. DO NOT
HEAT OR CUT EMPTY CONTAINERS WITH ELECTRIC OR GAS TORCH.


SECTION 14 TRANSPORTATION INFORMATION 


DOT SHIP NAME: AEROSOL A/C OIL CHARGE

D.O.T. HAZARD CLASS: ORMD

UN / ID #: 1950 AEROSOLS

IMDG HAZARD CLASS: 2.2

UN / ID #: 1950 AEROSOLS

IATA HAZARD CLASS: 2.2

PRODUCT LABEL: SUPERCOOL R-134A REFRIGERANT PLUS


SECTION 15 REGULATORY INFORMATION 


OSHA STATUS: NON-HAZARDOUS UNDER 29 CFR 1910.1200

TSCA STATUS: N/A

RCRA STATUS:
IF DISCARDED IN ITS PURCHASED FORM THIS PRODUCT WOULD NOT BE A HAZARDOUS
WASTE EITHER BY LISTING OR CHARACTERISTIC. HOWEVER, IT IS THE
RESPONSIBILITY OF THE PRODUCT USER TO DETERMINE AT THE TIME OF DISPOSAL,
WHETHER THE MATERIAL BEING DISPOSED OF IS A HAZARDOUS WASTE (40 CFR
261.20-24).


SECTION 16 OTHER INFORMATION 


GENERAL:
THIS INFORMATION IS FURNISHED WITHOUT WARRANTY, EXPRESSED OR IMPLIED,
EXCEPT THAT IS ACCURATE TO THE BEST KNOWLEDGE OF TIRE SEAL, INC. THE DATA
ON THIS SHEET RELATED ONLY TO THE SPECIFIC MATERIAL DESIGNED HEREIN. TIRE
SEAL, INC. ASSUMES NO LEGAL RESPONSIBILITY FOR THE USE OR RELIANCE UPON
THESE DATA.

TSI-9473

NR: NOT REGULATED
N/A: NOT APPLICABLE
U: UNKNOWN