Common Name: SHELL GADUS S3 V220 1.5
Manufacturer: UNIVAR FINLAND
SDS Revision Date: 12/22/2010
SDS Format: No Format Specified
   
Grainger Item Number(s): 19H304, 19H305
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. IDENTIFICATION OF THE SUBSTANCE/PREPARATION AND 
2. HAZARDS IDENTIFICATION 
3. COMPOSITION/INFORMATION ON INGREDIENTS 
4. FIRST AID MEASURES 
5. FIRE FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS/PERSONAL PROTECTION 
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
REGULATION 1907/2006/EC

SHELL GADUS S3 V220 1.5

VERSION: 1.0

EFFECTIVE DATE: 22.12.2010


1. IDENTIFICATION OF THE SUBSTANCE/PREPARATION AND 

                   COMPANY/UNDERTAKING

MATERIAL NAME: SHELL GADUS S3 V220 1.5

USES: AUTOMOTIVE AND INDUSTRIAL GREASE.

PRODUCT CODE: 001D8436

MANUFACTURER/SUPPLIER:
UNIVAR OY
Y-TUNNUS (COMPANY NUMBER): 0536122-7
FI-01670
VANHA NURMIJARVENTIE 62 E 28
VANTAA

TELEPHONE: 09-3508650

FAX: 09-35086550

EMAIL CONTACT FOR MSDS: SDS.FI@UNIVAREUROPE.COM

EMERGENCY TELEPHONE NUMBER: 09-471 977

OTHER INFORMATION:
KT CODE: 35 LUBRICANTS AND ADDITIVES
TOL CODE: C INDUSTRY.


2. HAZARDS IDENTIFICATION 


EC CLASSIFICATION: DANGEROUS FOR THE ENVIRONMENT.

HEALTH HAZARDS:
NOT EXPECTED TO BE A HEALTH HAZARD WHEN USED UNDER NORMAL CONDITIONS.
PROLONGED OR REPEATED SKIN CONTACT WITHOUT PROPER CLEANING CAN CLOG THE
PORES OF THE SKIN RESULTING IN DISORDERS SUCH AS OIL ACNE/FOLLICULITIS.
HIGH-PRESSURE INJECTION UNDER THE SKIN MAY CAUSE SERIOUS DAMAGE INCLUDING
LOCAL NECROSIS. USED GREASE MAY CONTAIN HARMFUL IMPURITIES.

SIGNS AND SYMPTOMS:
LOCAL NECROSIS IS EVIDENCED BY DELAYED ONSET OF PAIN AND TISSUE DAMAGE A
FEW HOURS FOLLOWING INJECTION. OIL ACNE/FOLLICULITIS SIGNS AND SYMPTOMS
MAY INCLUDE FORMATION OF BLACK PUSTULES AND SPOTS ON THE SKIN OF EXPOSED
AREAS. INGESTION MAY RESULT IN NAUSEA, VOMITING AND/OR DIARRHOEA.

SAFETY HAZARDS: NOT CLASSIFIED AS FLAMMABLE BUT WILL BURN.

ENVIRONMENTAL HAZARDS:
HARMFUL TO AQUATIC ORGANISMS, MAY CAUSE LONG-TERM ADVERSE EFFECTS IN THE
AQUATIC ENVIRONMENT.


3. COMPOSITION/INFORMATION ON INGREDIENTS 


PREPARATION DESCRIPTION:
A LUBRICATING GREASE CONTAINING HIGHLY-REFINED MINERAL OILS AND ADDITIVES.

HAZARDOUS COMPONENTS:

CHEMICAL       CAS         EINECS     SYMBOL(S)  R-PHRASE(S)  CONC.
IDENTITY

ZINC           12001-85-3  234-409-2  XI, N      R36/38;      1.00 - 5.00%
NAPHTHENATE                                      R51/53

ZINC DIALKYL   68649-42-3  272-028-3  XI, N      R36; R51/53  1.00 - 5.00%
DITHIO-
PHOSPHATE

ADDITIONAL INFORMATION:
THE HIGHLY REFINED MINERAL OIL CONTAINS <3% (W/W) DMSO-EXTRACT, ACCORDING
TO IP346. REFER TO CHAPTER 16 FOR FULL TEXT OF EC R-PHRASES.

EXPOSURE LIMITS APPLY TO THE FOLLOWING COMPONENTS:
HIGHLY REFINED MINERAL OIL.


4. FIRST AID MEASURES 


GENERAL INFORMATION:
NOT EXPECTED TO BE A HEALTH HAZARD WHEN USED UNDER NORMAL CONDITIONS.

INHALATION:
NO TREATMENT NECESSARY UNDER NORMAL CONDITIONS OF USE. IF SYMPTOMS
PERSIST, OBTAIN MEDICAL ADVICE.

SKIN CONTACT:
REMOVE CONTAMINATED CLOTHING. FLUSH EXPOSED AREA WITH WATER AND FOLLOW BY
WASHING WITH SOAP IF AVAILABLE. IF PERSISTENT IRRITATION OCCURS, OBTAIN
MEDICAL ATTENTION. WHEN USING HIGH PRESSURE EQUIPMENT, INJECTION OF
PRODUCT UNDER THE SKIN CAN OCCUR. IF HIGH PRESSURE INJURIES OCCUR, THE
CASUALTY SHOULD BE SENT IMMEDIATELY TO A HOSPITAL. DO NOT WAIT FOR
SYMPTOMS TO DEVELOP. OBTAIN MEDICAL ATTENTION EVEN IN THE ABSENCE OF
APPARENT WOUNDS.

EYE CONTACT:
FLUSH EYE WITH COPIOUS QUANTITIES OF WATER. IF PERSISTENT IRRITATION
OCCURS, OBTAIN MEDICAL ATTENTION.

INGESTION:
IN GENERAL NO TREATMENT IS NECESSARY UNLESS LARGE QUANTITIES ARE
SWALLOWED, HOWEVER, GET MEDICAL ADVICE.

ADVICE TO PHYSICIAN:
TREAT SYMPTOMATICALLY. HIGH PRESSURE INJECTION INJURIES REQUIRE PROMPT
SURGICAL INTERVENTION AND POSSIBLY STEROID THERAPY, TO MINIMISE TISSUE
DAMAGE AND LOSS OF FUNCTION. BECAUSE ENTRY WOUNDS ARE SMALL AND DO NOT
REFLECT THE SERIOUSNESS OF THE UNDERLYING DAMAGE, SURGICAL EXPLORATION TO
DETERMINE THE EXTENT OF INVOLVEMENT MAY BE NECESSARY. LOCAL ANAESTHETICS
OR HOT SOAKS SHOULD BE AVOIDED BECAUSE THEY CAN CONTRIBUTE TO SWELLING,
VASOSPASM AND ISCHAEMIA. PROMPT SURGICAL DECOMPRESSION, DEBRIDEMENT AND
EVACUATION OF FOREIGN MATERIAL SHOULD BE PERFORMED UNDER GENERAL
ANAESTHETICS, AND WIDE EXPLORATION IS ESSENTIAL.

IF THE PATIENT IS NOT FEELING ILL, GIVE HIM AS SOON AS POSSIBLE 1-2 DL
CREAM OR ICE-CREAM FOLLOWED BY 50 - 100 G MEDICINAL CARBON SUSPENDED IN
WATER.


5. FIRE FIGHTING MEASURES 


CLEAR FIRE AREA OF ALL NON-EMERGENCY PERSONNEL.

SPECIFIC HAZARDS:

HAZARDOUS COMBUSTION PRODUCTS MAY INCLUDE:
A COMPLEX MIXTURE OF AIRBORNE SOLID AND LIQUID PARTICULATES AND GASES
(SMOKE). CARBON MONOXIDE. UNIDENTIFIED ORGANIC AND INORGANIC COMPOUNDS.

SUITABLE EXTINGUISHING MEDIA:
FOAM, WATER SPRAY OR FOG. DRY CHEMICAL POWDER, CARBON DIOXIDE, SAND OR
EARTH MAY BE USED FOR SMALL FIRES ONLY.

UNSUITABLE EXTINGUISHING MEDIA: DO NOT USE WATER IN A JET.

PROTECTIVE EQUIPMENT FOR FIREFIGHTERS:
PROPER PROTECTIVE EQUIPMENT INCLUDING BREATHING APPARATUS MUST BE WORN
WHEN APPROACHING A FIRE IN A CONFINED SPACE.


6. ACCIDENTAL RELEASE MEASURES 


AVOID CONTACT WITH SPILLED OR RELEASED MATERIAL. FOR GUIDANCE ON SELECTION
OF PERSONAL PROTECTIVE EQUIPMENT SEE CHAPTER 8 OF THIS MATERIAL SAFETY
DATA SHEET. SEE CHAPTER 13 FOR INFORMATION ON DISPOSAL. OBSERVE THE
RELEVANT LOCAL AND INTERNATIONAL REGULATIONS.

PROTECTIVE MEASURES:
AVOID CONTACT WITH SKIN AND EYES. USE APPROPRIATE CONTAINMENT TO AVOID
ENVIRONMENTAL CONTAMINATION. PREVENT FROM SPREADING OR ENTERING DRAINS,
DITCHES OR RIVERS BY USING SAND, EARTH, OR OTHER APPROPRIATE BARRIERS.

CLEAN UP METHODS:
SHOVEL INTO A SUITABLE CLEARLY MARKED CONTAINER FOR DISPOSAL OR
RECLAMATION IN ACCORDANCE WITH LOCAL REGULATIONS.


7. HANDLING AND STORAGE 


GENERAL PRECAUTIONS:
USE LOCAL EXHAUST VENTILATION IF THERE IS RISK OF INHALATION OF VAPOURS,
MISTS OR AEROSOLS. PROPERLY DISPOSE OF ANY CONTAMINATED RAGS OR CLEANING
MATERIALS IN ORDER TO PREVENT FIRES. USE THE INFORMATION IN THIS DATA
SHEET AS INPUT TO A RISK ASSESSMENT OF LOCAL CIRCUMSTANCES TO HELP
DETERMINE APPROPRIATE CONTROLS FOR SAFE HANDLING, STORAGE AND DISPOSAL OF
THIS MATERIAL.

HANDLING:
AVOID PROLONGED OR REPEATED CONTACT WITH SKIN. AVOID INHALING VAPOUR
AND/OR MISTS. WHEN HANDLING PRODUCT IN DRUMS, SAFETY FOOTWEAR SHOULD BE
WORN AND PROPER HANDLING EQUIPMENT SHOULD BE USED.

STORAGE:
KEEP CONTAINER TIGHTLY CLOSED AND IN A COOL, WELL-VENTILATED PLACE. USE
PROPERLY LABELLED AND CLOSEABLE CONTAINERS.

STORAGE TEMPERATURE: 0 - 50 DEG. C / 32 - 122 DEG. F

RECOMMENDED MATERIALS:
FOR CONTAINERS OR CONTAINER LININGS, USE MILD STEEL OR HIGH DENSITY
POLYETHYLENE.

UNSUITABLE MATERIALS: PVC.

ADDITIONAL INFORMATION:
POLYETHYLENE CONTAINERS SHOULD NOT BE EXPOSED TO HIGH TEMPERATURES BECAUSE
OF POSSIBLE RISK OF DISTORTION.


8. EXPOSURE CONTROLS/PERSONAL PROTECTION 


IF THE AMERICAN CONFERENCE OF GOVERNMENTAL INDUSTRIAL HYGIENISTS (ACGIH)
VALUE IS PROVIDED ON THIS DOCUMENT, IT IS PROVIDED FOR INFORMATION ONLY.

OCCUPATIONAL EXPOSURE LIMITS:

MATERIAL           SOURCE     TYPE         PPM  MG/M3    NOTATION

OIL MIST, MINERAL  HTP-ARVOT  HTP 8H            5 MG/M3  KNOWN HARMFUL
                              [MIST.]                    CONCENTRATION
                                                         (LIITE 1).

                   ACGIH      TWA               5 MG/M3
                              [INHALABLE
                              FRACTION.]

ADDITIONAL INFORMATION:
DUE TO THE PRODUCT'S SEMI-SOLID CONSISTENCY, GENERATION OF MISTS AND DUSTS
IS UNLIKELY TO OCCUR.

EXPOSURE CONTROLS:
THE LEVEL OF PROTECTION AND TYPES OF CONTROLS NECESSARY WILL VARY
DEPENDING UPON POTENTIAL EXPOSURE CONDITIONS. SELECT CONTROLS BASED ON A
RISK ASSESSMENT OF LOCAL CIRCUMSTANCES.

APPROPRIATE MEASURES INCLUDE:
ADEQUATE VENTILATION TO CONTROL AIRBORNE CONCENTRATIONS. WHERE MATERIAL IS
HEATED, SPRAYED OR MIST FORMED, THERE IS GREATER POTENTIAL FOR AIRBORNE
CONCENTRATIONS TO BE GENERATED.

PERSONAL PROTECTIVE EQUIPMENT:
PERSONAL PROTECTIVE EQUIPMENT (PPE) SHOULD MEET RECOMMENDED NATIONAL
STANDARDS. CHECK WITH PPE SUPPLIERS.

RESPIRATORY PROTECTION:
NO RESPIRATORY PROTECTION IS ORDINARILY REQUIRED UNDER NORMAL CONDITIONS
OF USE. IN ACCORDANCE WITH GOOD INDUSTRIAL HYGIENE PRACTICES, PRECAUTIONS
SHOULD BE TAKEN TO AVOID BREATHING OF MATERIAL. IF ENGINEERING CONTROLS DO
NOT MAINTAIN AIRBORNE CONCENTRATIONS TO A LEVEL WHICH IS ADEQUATE TO
PROTECT WORKER HEALTH, SELECT RESPIRATORY PROTECTION EQUIPMENT SUITABLE
FOR THE SPECIFIC CONDITIONS OF USE AND MEETING RELEVANT LEGISLATION.
CHECK WITH RESPIRATORY PROTECTIVE EQUIPMENT SUPPLIERS. WHERE AIR-FILTERING
RESPIRATORS ARE SUITABLE, SELECT AN APPROPRIATE COMBINATION OF MASK AND
FILTER. SELECT A FILTER SUITABLE FOR COMBINED PARTICULATE/ORGANIC GASES
AND VAPOURS [BOILING POINT >65 DEG. C (149 DEG. F)] MEETING EN14387.

HAND PROTECTION:

WHERE HAND CONTACT WITH THE PRODUCT MAY OCCUR THE USE OF GLOVES APPROVED
TO RELEVANT STANDARDS (E.G. EUROPE: EN374, US: F739) MADE FROM THE
FOLLOWING MATERIALS MAY PROVIDE SUITABLE CHEMICAL PROTECTION:
PVC, NEOPRENE OR NITRILE RUBBER GLOVES. SUITABILITY AND DURABILITY OF A
GLOVE IS DEPENDENT ON USAGE, E.G. FREQUENCY AND DURATION OF CONTACT,
CHEMICAL RESISTANCE OF GLOVE MATERIAL, GLOVE THICKNESS, DEXTERITY. ALWAYS
SEEK ADVICE FROM GLOVE SUPPLIERS. CONTAMINATED GLOVES SHOULD BE REPLACED.
PERSONAL HYGIENE IS A KEY ELEMENT OF EFFECTIVE HAND CARE. GLOVES MUST ONLY
BE WORN ON CLEAN HANDS. AFTER USING GLOVES, HANDS SHOULD BE WASHED AND
DRIED THOROUGHLY. APPLICATION OF A NON-PERFUMED MOISTURIZER IS
RECOMMENDED.

EYE PROTECTION:
WEAR SAFETY GLASSES OR FULL FACE SHIELD IF SPLASHES ARE LIKELY TO OCCUR.
APPROVED TO EU STANDARD EN166.

PROTECTIVE CLOTHING:
SKIN PROTECTION NOT ORDINARILY REQUIRED BEYOND STANDARD ISSUE WORK
CLOTHES.

MONITORING METHODS:
MONITORING OF THE CONCENTRATION OF SUBSTANCES IN THE BREATHING ZONE OF
WORKERS OR IN THE GENERAL WORKPLACE MAY BE REQUIRED TO CONFIRM COMPLIANCE
WITH AN OEL AND ADEQUACY OF EXPOSURE CONTROLS. FOR SOME SUBSTANCES
BIOLOGICAL MONITORING MAY ALSO BE APPROPRIATE.

ENVIRONMENTAL EXPOSURE CONTROLS:
MINIMISE RELEASE TO THE ENVIRONMENT. AN ENVIRONMENTAL ASSESSMENT MUST BE
MADE TO ENSURE COMPLIANCE WITH LOCAL ENVIRONMENTAL LEGISLATION.


9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: LIGHT BROWN. SEMI-SOLID AT AMBIENT TEMPERATURE.

ODOUR: SLIGHT HYDROCARBON.

PH: NOT APPLICABLE.

INITIAL BOILING POINT AND BOILING RANGE: DATA NOT AVAILABLE

DROPPING POINT: TYPICAL 260 DEG. C / 500 DEG. F

FLASH POINT: >150 DEG. C / 302 DEG. F (COC)

LOWER / UPPER FLAMMABILITY OR EXPLOSION LIMITS:
TYPICAL 1 - 10%(V) (BASED ON MINERAL OIL)

AUTO-IGNITION TEMPERATURE: >320 DEG. C / 608 DEG. F

VAPOUR PRESSURE: <0.5 PA AT 20 DEG. C / 68 DEG. F (ESTIMATED VALUE(S))

DENSITY: TYPICAL 900 KG/M3 AT 15 DEG. C / 59 DEG. F

WATER SOLUBILITY: NEGLIGIBLE.

N-OCTANOL/WATER PARTITION COEFFICIENT (LOG POW):
>6 (BASED ON INFORMATION ON SIMILAR PRODUCTS)

KINEMATIC VISCOSITY: NOT APPLICABLE.

VAPOUR DENSITY (AIR=1): >1 (ESTIMATED VALUE(S))

EVAPORATION RATE (NBUAC=1): DATA NOT AVAILABLE


10. STABILITY AND REACTIVITY 


STABILITY: STABLE.

CONDITIONS TO AVOID: EXTREMES OF TEMPERATURE AND DIRECT SUNLIGHT.

MATERIALS TO AVOID: STRONG OXIDISING AGENTS.

HAZARDOUS DECOMPOSITION PRODUCTS:
HAZARDOUS DECOMPOSITION PRODUCTS ARE NOT EXPECTED TO FORM DURING NORMAL
STORAGE.


11. TOXICOLOGICAL INFORMATION 


BASIS FOR ASSESSMENT:
INFORMATION GIVEN IS BASED ON DATA ON THE COMPONENTS AND THE TOXICOLOGY OF
SIMILAR PRODUCTS.

ACUTE ORAL TOXICITY:

EXPECTED TO BE OF LOW TOXICITY:
LD50: >5000 MG/KG, RAT

ACUTE DERMAL TOXICITY:

EXPECTED TO BE OF LOW TOXICITY:
LD50: >5000 MG/KG, RABBIT

ACUTE INHALATION TOXICITY:
NOT CONSIDERED TO BE AN INHALATION HAZARD UNDER NORMAL CONDITIONS OF USE.

SKIN IRRITATION:
EXPECTED TO BE SLIGHTLY IRRITATING. PROLONGED OR REPEATED SKIN CONTACT
WITHOUT PROPER CLEANING CAN CLOG THE PORES OF THE SKIN RESULTING IN
DISORDERS SUCH AS OIL ACNE/FOLLICULITIS.

EYE IRRITATION: EXPECTED TO BE SLIGHTLY IRRITATING.

RESPIRATORY IRRITATION:
INHALATION OF VAPOURS OR MISTS MAY CAUSE IRRITATION.

SENSITISATION: NOT EXPECTED TO BE A SKIN SENSITISER.

REPEATED DOSE TOXICITY: NOT EXPECTED TO BE A HAZARD.

MUTAGENICITY: NOT CONSIDERED A MUTAGENIC HAZARD.

CARCINOGENICITY:
PRODUCT CONTAINS MINERAL OILS OF TYPES SHOWN TO BE NON-CARCINOGENIC IN
ANIMAL SKIN-PAINTING STUDIES. HIGHLY REFINED MINERAL OILS ARE NOT
CLASSIFIED AS CARCINOGENIC BY THE INTERNATIONAL AGENCY FOR RESEARCH ON
CANCER (IARC). OTHER COMPONENTS ARE NOT KNOWN TO BE ASSOCIATED WITH
CARCINOGENIC EFFECTS.

REPRODUCTIVE AND DEVELOPMENTAL TOXICITY: NOT EXPECTED TO BE A HAZARD.

ADDITIONAL INFORMATION:
USED GREASE MAY CONTAIN HARMFUL IMPURITIES THAT HAVE ACCUMULATED DURING
USE. THE CONCENTRATION OF SUCH HARMFUL IMPURITIES WILL DEPEND ON USE AND
THEY MAY PRESENT RISKS TO HEALTH AND THE ENVIRONMENT ON DISPOSAL. ALL USED
GREASE SHOULD BE HANDLED WITH CAUTION AND SKIN CONTACT AVOIDED AS FAR AS
POSSIBLE. HIGH PRESSURE INJECTION OF PRODUCT INTO THE SKIN MAY LEAD TO
LOCAL NECROSIS IF THE PRODUCT IS NOT SURGICALLY REMOVED.


12. ECOLOGICAL INFORMATION 


ECOTOXICOLOGICAL DATA HAVE NOT BEEN DETERMINED SPECIFICALLY FOR THIS
PRODUCT. INFORMATION GIVEN IS BASED ON A KNOWLEDGE OF THE COMPONENTS AND
THE ECOTOXICOLOGY OF SIMILAR PRODUCTS.

ACUTE TOXICITY:
POORLY SOLUBLE MIXTURE. MAY CAUSE PHYSICAL FOULING OF AQUATIC ORGANISMS.

EXPECTED TO BE HARMFUL:

LL/EL/IL50:
10-100 MG/L (TO AQUATIC ORGANISMS) (LL/EL50 EXPRESSED AS THE NOMINAL
AMOUNT OF PRODUCT REQUIRED TO PREPARE AQUEOUS TEST EXTRACT).

MOBILITY:
SEMI-SOLID UNDER MOST ENVIRONMENTAL CONDITIONS. FLOATS ON WATER. IF IT
ENTERS SOIL, IT WILL ADSORB TO SOIL PARTICLES AND WILL NOT BE MOBILE.

PERSISTENCE/DEGRADABILITY:
EXPECTED TO BE NOT READILY BIODEGRADABLE. MAJOR CONSTITUENTS ARE EXPECTED
TO BE INHERENTLY BIODEGRADABLE, BUT THE PRODUCT CONTAINS COMPONENTS THAT
MAY PERSIST IN THE ENVIRONMENT.

BIOACCUMULATION: CONTAINS COMPONENTS WITH THE POTENTIAL TO BIOACCUMULATE.

OTHER ADVERSE EFFECTS:
PRODUCT IS A MIXTURE OF NON-VOLATILE COMPONENTS, WHICH ARE NOT EXPECTED TO
BE RELEASED TO AIR IN ANY SIGNIFICANT QUANTITIES. NOT EXPECTED TO HAVE
OZONE DEPLETION POTENTIAL, PHOTOCHEMICAL OZONE CREATION POTENTIAL OR
GLOBAL WARMING POTENTIAL.


13. DISPOSAL CONSIDERATIONS 


MATERIAL DISPOSAL:
RECOVER OR RECYCLE IF POSSIBLE. IT IS THE RESPONSIBILITY OF THE WASTE
GENERATOR TO DETERMINE THE TOXICITY AND PHYSICAL PROPERTIES OF THE
MATERIAL GENERATED TO DETERMINE THE PROPER WASTE CLASSIFICATION AND
DISPOSAL METHODS IN COMPLIANCE WITH APPLICABLE REGULATIONS. DO NOT DISPOSE
INTO THE ENVIRONMENT, IN DRAINS OR IN WATER COURSES.

CONTAINER DISPOSAL:
DISPOSE IN ACCORDANCE WITH PREVAILING REGULATIONS, PREFERABLY TO A
RECOGNISED COLLECTOR OR CONTRACTOR. THE COMPETENCE OF THE COLLECTOR OR
CONTRACTOR SHOULD BE ESTABLISHED BEFOREHAND.

LOCAL LEGISLATION:
DISPOSAL SHOULD BE IN ACCORDANCE WITH APPLICABLE REGIONAL, NATIONAL, AND
LOCAL LAWS AND REGULATIONS.

EU WASTE DISPOSAL CODE (EWC):
12 01 12 SPENT WAXES AND FATS. CLASSIFICATION OF WASTE IS ALWAYS THE
RESPONSIBILITY OF THE END USER.


14. TRANSPORT INFORMATION 


ADR: THIS MATERIAL IS NOT CLASSIFIED AS DANGEROUS UNDER ADR REGULATIONS.

RID: THIS MATERIAL IS NOT CLASSIFIED AS DANGEROUS UNDER RID REGULATIONS.

ADNR: THIS MATERIAL IS NOT CLASSIFIED AS DANGEROUS UNDER ADNR REGULATIONS.

IMDG: THIS MATERIAL IS NOT CLASSIFIED AS DANGEROUS UNDER IMDG REGULATIONS.

IATA (COUNTRY VARIATIONS MAY APPLY):
THIS MATERIAL IS NOT CLASSIFIED AS DANGEROUS UNDER IATA REGULATIONS.


15. REGULATORY INFORMATION 


THE REGULATORY INFORMATION IS NOT INTENDED TO BE COMPREHENSIVE. OTHER
REGULATIONS MAY APPLY TO THIS MATERIAL.

EC CLASSIFICATION: DANGEROUS FOR THE ENVIRONMENT.

EC SYMBOLS: NO HAZARD SYMBOL REQUIRED

EC RISK PHRASES:

R52/53:
HARMFUL TO AQUATIC ORGANISMS, MAY CAUSE LONG-TERM ADVERSE EFFECTS IN THE
AQUATIC ENVIRONMENT.

EC SAFETY PHRASES:

S61:
AVOID RELEASE TO THE ENVIRONMENT. REFER TO SPECIAL INSTRUCTIONS/SAFETY
DATA SHEETS.

CHEMICAL INVENTORY STATUS:

EINECS: ALL COMPONENTS LISTED OR POLYMER EXEMPT.

TSCA: ALL COMPONENTS LISTED.


16. OTHER INFORMATION 


R-PHRASE(S):

R36: IRRITATING TO EYES.

R36/38: IRRITATING TO EYES AND SKIN.

R51/53:
TOXIC TO AQUATIC ORGANISMS, MAY CAUSE LONG-TERM ADVERSE EFFECTS IN THE
AQUATIC ENVIRONMENT.

R52/53:
HARMFUL TO AQUATIC ORGANISMS, MAY CAUSE LONG-TERM ADVERSE EFFECTS IN THE
AQUATIC ENVIRONMENT.

MSDS VERSION NUMBER: 1.0

MSDS EFFECTIVE DATE: 22.12.2010

MSDS REVISIONS:
A VERTICAL BAR (|) IN THE LEFT MARGIN INDICATES AN AMENDMENT FROM THE
PREVIOUS VERSION.

MSDS REGULATION: REGULATION 1907/2006/EC

MSDS DISTRIBUTION:
THE INFORMATION IN THIS DOCUMENT SHOULD BE MADE AVAILABLE TO ALL WHO MAY
HANDLE THE PRODUCT.

DISCLAIMER:
THIS INFORMATION IS BASED ON OUR CURRENT KNOWLEDGE AND IS INTENDED TO
DESCRIBE THE PRODUCT FOR THE PURPOSES OF HEALTH, SAFETY AND ENVIRONMENTAL
REQUIREMENTS ONLY. IT SHOULD NOT THEREFORE BE CONSTRUED AS GUARANTEEING
ANY SPECIFIC PROPERTY OF THE PRODUCT.

PRINT DATE: 24.12.2010

MSDS_FI