Common Name: LITHIUM-ION AND LITHIUM-ION POLYMER BATTERIES (LI-ION BATTERIES)
Manufacturer: VERTEX STANDARD JAPAN
SDS Revision Date: 5/16/2012
SDS Format: No Format Specified
   
Grainger Item Number(s): 18F533
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - PRODUCT AND COMPANY INFORMATION 
SECTION II - COMPOSITION INFORMATION 
SECTION III - HAZARDS IDENTIFICATION 
SECTION IV - FIRST AID MEASURES 
SECTION V - FIREFIGHTING MEASURES 
SECTION VI - ACCIDENTAL RELEASE MEASURES 
SECTION VII - HANDLING AND STORAGE 
SECTION VIII - EXPOSURE CONTROLS / PERSONAL PROTECTION 
SECTION IX - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION X - STABILITY AND REACTIVITY 
SECTION XI - TOXICOLOGICAL INFORMATION 
SECTION XII - ECOLOGICAL INFORMATION 
SECTION XIII - DISPOSAL 
SECTION XIV - TRANSPORT INFORMATION 
SECTION XV - REGULATORY INFORMATION 
SECTION XVI - OTHER INFORMATION 



PRODUCT DATA SHEET

VS

THE PRODUCTS REFERENCED HEREIN ARE "ARTICLES" UNDER 29 CFR 1910.1200(C) AND
ARE NOT SUBJECT TO OSHA'S REQUIREMENTS FOR MATERIAL SAFETY DATA SHEETS
UNDER ITS HAZARD COMMUNICATION STANDARD, 29 CFR 1910.1200. THIS PRODUCT
DATA SHEET IS PROVIDED AS A SERVICE TO OUR CUSTOMERS.


SECTION I - PRODUCT AND COMPANY INFORMATION 


IDENTITY:
LITHIUM-ION AND LITHIUM-ION POLYMER BATTERIES (LI-ION BATTERIES)

MODELS: ALL

EFFECTIVE DATE: MAY 16, 2012

MANUFACTURER:
VERTEX STANDARD CO., LTD.
4-8-8 NAKAMEGURO, MEGURO-KU
TOKYO, 153-8644

PHONE: +81 3 5725 6111


SECTION II - COMPOSITION INFORMATION 


VERTEX STANDARD BATTERY PACKS CONTAIN LI-ION CELLS FROM VARIOUS
MANUFACTURERS. LI-ION CELLS ARE GENERALLY COMPOSED OF THE FOLLOWING MAJOR
INGREDIENTS:

CELL COMPONENT      COMMON CHEMICAL NAME /    CAS NUMBER   CONCENTRATION
                    GENERAL NAME                           RANGE

POSITIVE ELECTRODE  LITHIATED COBALT OXIDES   12190-79-3
                    LITHIATED MANGANESE         48,227-7   20-40%
                    OXIDES
                    PROPRIETARY LITHIATED     N/A
                    NICKEL-MANGANESE-COBALT
                    OXIDES

NEGATIVE ELECTRODE  GRAPHITE                   7782-42-5   10-20%

BINDERS             POLYVINYLIDENE            24937-79-9    0-3%
                    DIFLUORIDE AND/OR          9002-84-0
                    POLYTETRAFLUOROETHYLENE

ELECTROLYTE SALT    LITHIUM SALT (ONE OR MORE  21324-40-3   1-5%
                    OF LITHIUM                 14283-07-9
                    HEXAFLUOROPHOSPHATE AND
                    LITHIUM
                    TETRAFLUOROBORATE)

ELECTROLYTE         ORGANIC SOLVENTS              96-49-1   5-20%
SOLVENT             INCLUDING ONE OR MORE        105-58-8
                    OF THE FOLLOWING:            616-38-6
                    ETHYLENE CARBONATE,          623-53-0
                    DIETHYLCARBONATE,            108-32-7
                    DIMETHYLCARBONATE,
                    ETHYLMETHYLCARBONATE, AND
                    PROPYLENE CARBONATE.

OTHER COMPONENTS    COPPER                      7440-50-8   5-10%
                    ALUMINUM                    7429-90-5   5-40%
                    NICKEL                      7440-02-0   0-5%
                    POLYETHYLENE AND/OR         9002-88-4   1-3%
                    POLYPROPYLENE               9003-07-0

AS MANUFACTURED, LI-ION CELLS DO NOT CONTAIN LITHIUM METAL.


SECTION III - HAZARDS IDENTIFICATION 


POTENTIALLY HAZARDOUS MATERIALS ARE FULLY CONTAINED IN A HERMETICALLY
SEALED CASE DESIGNED TO WITHSTAND NORMAL HANDLING AND USE. EXPOSURE COULD
OCCUR ONLY IF THE BATTERY OR CELLS HAVE BEEN OPENED, DISASSEMBLED, CRUSHED,
BURNED, EXPOSED TO HIGH TEMPERATURES (>60 DEG. C OR 140 DEG. F), OR
SUBJECTED TO OTHER TYPES OF ABUSE. EXPOSURE TO CELL CONTENTS MAY BE HARMFUL
UNDER SOME CIRCUMSTANCES.

FOLLOW INSTRUCTIONS AND PRECAUTIONS FOR SAFE USE OF THE BATTERY PACK.


SECTION IV - FIRST AID MEASURES 


CELL MANUFACTURERS RECOMMEND THAT IN CASE OF EXPOSURE TO CELL CONTENTS,
WASH AFFECTED AREA FOR AT LEAST 15 MINUTES WITH GENEROUS AMOUNTS OF WATER
AND SEEK MEDICAL ATTENTION.


SECTION V - FIREFIGHTING MEASURES 


FIRES INVOLVING THESE TYPES OF BATTERY PACKS SHOULD BE FLOODED WITH WATER
OR USE CO2, FOAM, OR DRY CHEMICAL EXTINGUISHING MEDIA. FIRES INVOLVING
LARGE QUANTITIES OF BATTERIES MAY PRODUCE TOXIC, CORROSIVE, OR IRRITATING
FUMES INCLUDING HF.


SECTION VI - ACCIDENTAL RELEASE MEASURES 


IF BATTERIES ARE SPILLED AND DAMAGED, THEY SHOULD BE DISPOSED OF ACCORDING
TO THE DISPOSAL SECTION.


SECTION VII - HANDLING AND STORAGE 


THE BATTERY PACK AND ENCLOSED CELLS SHOULD NOT BE OPENED, DISASSEMBLED,
CRUSHED, BURNED, OR EXPOSED TO HIGH TEMPERATURES (>60 DEG. C OR 140 DEG.
F).


SECTION VIII - EXPOSURE CONTROLS / PERSONAL PROTECTION 


NO PERSONAL PROTECTION IS REQUIRED DURING NORMAL HANDLING AND USE. EXPOSURE
TO THE INGREDIENTS CONTAINED WITHIN THE CELLS WITHIN THE BATTERY PACK COULD
BE HARMFUL UNDER SOME CIRCUMSTANCES. IN CASE OF EXPOSURE TO CELL CONTENTS,
WASH AFFECTED AREA FOR AT LEAST 15 MINUTES WITH GENEROUS AMOUNTS OF WATER
AND SEEK MEDICAL ATTENTION.


SECTION IX - PHYSICAL AND CHEMICAL PROPERTIES 


THESE BATTERIES ARE SOLID ARTICLES. PROPERTIES SUCH AS ODOR, PH, VAPOR
PRESSURE, SOLUBILITY, ETC. ARE NOT APPLICABLE.


SECTION X - STABILITY AND REACTIVITY 


REACTIVITY: NONE DURING NORMAL HANDLING AND USE

INCOMPATIBILITY: NONE DURING NORMAL HANDLING AND USE

HAZARDOUS DECOMPOSITION PRODUCTS:
NONE DURING NORMAL HANDLING AND USE

CONDITIONS TO AVOID:
THE BATTERY PACK AND ENCLOSED CELLS SHOULD NOT BE OPENED, DISASSEMBLED,
CRUSHED, BURNED, OR EXPOSED TO HIGH TEMPERATURES.


SECTION XI - TOXICOLOGICAL INFORMATION 


THERE ARE NO KNOWN TOXICOLOGICAL PROPERTIES OF THE BATTERIES DURING NORMAL
HANDLING AND USE.


SECTION XII - ECOLOGICAL INFORMATION 


THERE ARE NO KNOWN ECOLOGICAL RISKS OF THE BATTERIES DURING NORMAL HANDLING
AND USE.


SECTION XIII - DISPOSAL 


ALL VERTEX STANDARD LI-ION BATTERIES CONTAIN RECYCLABLE MATERIALS.
RECYCLING OPTIONS AVAILABLE IN YOUR LOCAL AREA SHOULD BE CONSIDERED WHEN
DISPOSING OF THIS PRODUCT. DO NOT DISPOSE OF IN FIRE.


SECTION XIV - TRANSPORT INFORMATION 


UN 3840 - LITHIUM ION BATTERIES

UN 3841 - LITHIUM ION BATTERIES CONTAINED IN EQUIPMENT

UN 3841 - LITHIUM ION BATTERIES PACKED WITH EQUIPMENT

THE WATT-HOUR RATING FOR ALL VERTEX STANDARD, CO. LI-ION BATTERIES IS LESS
THAN 100 WATT-HOURS

WHEN PACKAGED AND SHIPPED BY VERTEX STANDARD, CO., THESE BATTERIES MEET THE
REQUIREMENTS FOR TRANSPORT BY MODE OF SHIPMENT (AIR, SEA OR GROUND) BASED
ON THE APPLICABLE REGULATIONS IN FORCE AT THE TIME OF THAT SHIPMENT.

IT IS THE SHIPPER'S RESPONSIBILITY TO DETERMINE AND ASSURE THAT ANY
SUBSEQUENT SHIPMENTS MEET THE REQUIREMENTS IN PLACE AT THAT TIME.

FOR TRANSPORTATION EMERGENCIES INVOLVING VERTEX STANDARD BATTERY PRODUCTS,
CALL CHEMTREC AT 1-800-424-9300.


SECTION XV - REGULATORY INFORMATION 


THE PRODUCTS REFERENCED HEREIN ARE "ARTICLES" UNDER 29 CFR 1910.1200(C) AND
ARE NOT SUBJECT TO OSHA'S REQUIREMENTS FOR MATERIAL SAFETY DATA SHEETS
UNDER ITS HAZARD COMMUNICATION STANDARD, 29 CFR 1910.1200.


SECTION XVI - OTHER INFORMATION 


NOTICE:
THE INFORMATION AND RECOMMENDATIONS SET FORTH ARE MADE IN GOOD FAITH AND
ARE BELIEVED TO BE ACCURATE AT THE DATE OF PREPARATION. VERTEX STANDARD
MAKES NO WARRANTY EXPRESSED OR IMPLIED WITH RESPECT TO THIS INFORMATION AND
RECOMMENDATIONS AND DISCLAIMS ALL LIABILITY FROM RELIANCE ON IT.
"EQUIVALENT LITHIUM CONTENT" INFORMATION IS AVAILABLE FROM THE
MANUFACTURER.