Common Name: MOBILCUT 102
Manufacturer: EXXON MOBIL CANADA
MSDS Revision Date: 3/22/2010
   
Grainger Item Number(s): 4FVD9
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 3 HAZARDS IDENTIFICATION 
SECTION 4 FIRST AID MEASURES 
SECTION 5 FIRE FIGHTING MEASURES 
SECTION 6 ACCIDENTAL RELEASE MEASURES 
SECTION 7 HANDLING AND STORAGE 
SECTION 8 EXPOSURE CONTROLS / PERSONAL PROTECTION 
SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 STABILITY AND REACTIVITY 
SECTION 11 TOXICOLOGICAL INFORMATION 
SECTION 12 ECOLOGICAL INFORMATION 
SECTION 13 DISPOSAL CONSIDERATIONS 
SECTION 14 TRANSPORT INFORMATION 
SECTION 15 REGULATORY INFORMATION 
SECTION 16 OTHER INFORMATION 



EXXONMOBIL

PRODUCT NAME: MOBILCUT 102

REVISION DATE: 22 MAR 2010

MATERIAL SAFETY DATA SHEET


SECTION 1 PRODUCT AND COMPANY IDENTIFICATION 


PRODUCT:

PRODUCT NAME: MOBILCUT 102

PRODUCT DESCRIPTION: BASE OIL AND ADDITIVES

PRODUCT CODE: 19621

INTENDED USE: WATER-MISCIBLE CUTTING FLUID

COMPANY IDENTIFICATION:

SUPPLIER:
CANADA IMPERIAL OIL LIMITED, AN AFFLIATE OF EXXON MOBIL CORPORATION
P.O. BOX 2480
STATION M
CALGARY, ALBERTA. T2P 3M9
CANADA

24 HOUR HEALTH EMERGENCY: 519-339-2145

TRANSPORTATION EMERGENCY PHONE: 519-339-2145

SUPPLIER GENERAL CONTACT: 1-800-567-3776


SECTION 2 COMPOSITION / INFORMATION ON INGREDIENTS 


REPORTABLE HAZARDOUS SUBSTANCE(S) OR COMPLEX SUBSTANCE(S):

NAME                                       CAS#              CONCENTRATION*

BENZENESULFONIC ACIDS, C15-C30 ALKYL       78330-12-8        1 - 5%
DERIVATIVES, SODIUM SALTS

FATTY ACIDS, TALL-OIL COMPDS. WITH         68132-46-7        1 - 5%
TRIETHANOLAMINE

FATTY ACIDS, TALL-OIL, COMPDS. WITH        68132-47-8        1 - 5%
ETHANOLAMINE

POTASSIUM CARBOXYLIC ACID SOAPS            66072-08-0        1 - 5%

* ALL CONCENTRATIONS ARE PERCENT BY WEIGHT UNLESS MATERIAL IS A GAS.
GAS CONCENTRATIONS ARE IN PERCENT BY VOLUME.


SECTION 3 HAZARDS IDENTIFICATION 


THIS MATERIAL IS NOT CONSIDERED TO BE HAZARDOUS ACCORDING TO REGULATORY
GUIDELINES (SEE (M)SDS SECTION 15).

POTENTIAL HEALTH EFFECTS:
THIS PRODUCT MAY BE USED IN CERTAIN APPLICATIONS WHERE MISTING CAN OCCUR.
EXCESSIVE EXPOSURE TO LIQUIDS AND MISTS MAY CAUSE SKIN AND EYE IRRITATION.
IN ADDITION, EXCESSIVE EXPOSURE TO MISTS MAY CAUSE RESPIRATORY IRRITATION
AND DAMAGE AND AGGRAVATE PRE-EXISTING EMPHYSEMA OR ASTHMA. HIGH-PRESSURE
INJECTION UNDER SKIN MAY CAUSE SERIOUS DAMAGE.

NFPA HAZARD ID:
HEALTH       1
FLAMMABILITY 1
REACTIVITY   0

HMIS HAZARD ID:
HEALTH       1
FLAMMABILITY 1
REACTIVITY   0

NOTE:
THIS MATERIAL SHOULD NOT BE USED FOR ANY OTHER PURPOSE THAN THE INTENDED
USE IN SECTION 1 WITHOUT EXPERT ADVICE. HEALTH STUDIES HAVE SHOWN THAT
CHEMICAL EXPOSURE MAY CAUSE POTENTIAL HUMAN HEALTH RISKS WHICH MAY VARY
FROM PERSON TO PERSON.


SECTION 4 FIRST AID MEASURES 


INHALATION:
REMOVE FROM FURTHER EXPOSURE. FOR THOSE PROVIDING ASSISTANCE, AVOID
EXPOSURE TO YOURSELF OR OTHERS.  USE ADEQUATE RESPIRATORY PROTECTION. IF
RESPIRATORY IRRITATION, DIZZINESS, NAUSEA, OR UNCONSCIOUSNESS OCCURS, SEEK
IMMEDIATE MEDICAL ASSISTANCE. IF BREATHING HAS STOPPED, ASSIST VENTILATION
WITH A MECHANICAL DEVICE OR USE MOUTH-TO-MOUTH RESUSCITATION.

SKIN CONTACT:
WASH CONTACT AREAS WITH SOAP AND WATER. REMOVE CONTAMINATED CLOTHING.
LAUNDER CONTAMINATED CLOTHING BEFORE REUSE. IF PRODUCT IS INJECTED INTO OR
UNDER THE SKIN, OR INTO ANY PART OF THE BODY, REGARDLESS OF THE APPEARANCE
OF THE WOUND OR ITS SIZE, THE INDIVIDUAL SHOULD BE EVALUATED IMMEDIATELY BY
A PHYSICIAN AS A SURGICAL EMERGENCY. EVEN THOUGH INITIAL SYMPTOMS FROM HIGH
PRESSURE INJECTION MAY BE MINIMAL OR ABSENT, EARLY SURGICAL TREATMENT
WITHIN THE FIRST FEW HOURS MAY SIGNIFICANTLY REDUCE THE ULTIMATE EXTENT OF
INJURY.

EYE CONTACT:
FLUSH THOROUGHLY WITH WATER. IF IRRITATION OCCURS, GET MEDICAL ASSISTANCE.

INGESTION:
FIRST AID IS NORMALLY NOT REQUIRED. SEEK MEDICAL ATTENTION IF DISCOMFORT
OCCURS.

NOTE TO PHYSICIAN:
PRE-EXISTING CONDITIONS WHICH MAY BE AGGRAVATED BY EXPOSURE INCLUDE
EMPHYSEMA AND ASTHMA.


SECTION 5 FIRE FIGHTING MEASURES 


EXTINGUISHING MEDIA:

APPROPRIATE EXTINGUISHING MEDIA:
USE WATER FOG, FOAM, DRY CHEMICAL OR CARBON DIOXIDE (CO2) TO EXTINGUISH
FLAMES.

INAPPROPRIATE EXTINGUISHING MEDIA: STRAIGHT STREAMS OF WATER

FIRE FIGHTING:

FIRE FIGHTING INSTRUCTIONS:
EVACUATE AREA. PREVENT RUNOFF FROM FIRE CONTROL OR DILUTION FROM ENTERING
STREAMS, SEWERS, OR DRINKING WATER SUPPLY. FIREFIGHTERS SHOULD USE STANDARD
PROTECTIVE EQUIPMENT AND IN ENCLOSED SPACES, SELF-CONTAINED BREATHING
APPARATUS (SCBA). USE WATER SPRAY TO COOL FIRE EXPOSED SURFACES AND TO
PROTECT PERSONNEL.

UNUSUAL FIRE HAZARDS:
PRESSURIZED MISTS MAY FORM A FLAMMABLE MIXTURE.

HAZARDOUS COMBUSTION PRODUCTS:
SMOKE, FUME, ALDEHYDES, SULFUR OXIDES, INCOMPLETE COMBUSTION PRODUCTS,
OXIDES OF CARBON

FLAMMABILITY PROPERTIES:

FLASH POINT [METHOD]: >179C (354F) [ASTM D-92]

FLAMMABLE LIMITS (APPROXIMATE VOLUME % IN AIR):
LEL: N/D
UEL: N/D

AUTOIGNITION TEMPERATURE: N/D


SECTION 6 ACCIDENTAL RELEASE MEASURES 


NOTIFICATION PROCEDURES:
IN THE EVENT OF A SPILL OR ACCIDENTAL RELEASE, NOTIFY RELEVANT AUTHORITIES
IN ACCORDANCE WITH ALL APPLICABLE REGULATIONS. US REGULATIONS  REQUIRE
REPORTING RELEASES OF THIS MATERIAL TO THE ENVIRONMENT WHICH EXCEED THE
APPLICABLE REPORTABLE QUANTITY OR OIL SPILLS WHICH COULD REACH ANY WATERWAY
INCLUDING INTERMITTENT DRY CREEKS. THE NATIONAL RESPONSE CENTER CAN BE
REACHED AT (800)424-8802.

SPILL MANAGEMENT:

LAND SPILL:
STOP LEAK IF YOU CAN DO IT WITHOUT RISK. RECOVER BY PUMPING OR WITH
SUITABLE ABSORBENT.

WATER SPILL:
STOP LEAK IF YOU CAN DO IT WITHOUT RISK. SEEK ADVICE OF A SPECIALIST THIS
PRODUCT EMULSIFIES, DISPERSES OR IS MISCIBLE IN WATER.

WATER SPILL AND LAND SPILL RECOMMENDATIONS ARE BASED ON THE MOST LIKELY
SPILL SCENARIO FOR THIS MATERIAL; HOWEVER, GEOGRAPHIC CONDITIONS, WIND,
TEMPERATURE, (AND IN THE CASE OF A WATER SPILL) WAVE AND CURRENT DIRECTION
AND SPEED MAY GREATLY INFLUENCE THE APPROPRIATE ACTION TO BE TAKEN.  FOR
THIS REASON, LOCAL EXPERTS SHOULD BE CONSULTED.

NOTE: LOCAL REGULATIONS MAY PRESCRIBE OR LIMIT ACTION TO BE TAKEN.

ENVIRONMENTAL PRECAUTIONS:

LARGE SPILLS:
DIKE FAR AHEAD OF LIQUID SPILL FOR LATER RECOVERY AND DISPOSAL. PREVENT
ENTRY INTO WATERWAYS, SEWERS, BASEMENTS OR CONFINED AREAS.


SECTION 7 HANDLING AND STORAGE 


HANDLING:
AVOID BREATHING MISTS OR VAPORS. AVOID CONTACT WITH SKIN. SMALL METAL
PARTICLES FROM MACHINING MAY CAUSE ABRASION OF THE SKIN AND MAY PREDISPOSE
TO DERMATITIS.  PREVENT SMALL SPILLS AND LEAKAGE TO AVOID SLIP HAZARD.
MATERIAL CAN ACCUMULATE STATIC CHARGES WHICH MAY CAUSE AN ELECTRICAL SPARK
(IGNITION SOURCE).  WHEN THE MATERIAL IS HANDLED IN BULK, AN ELECTRICAL
SPARK COULD IGNITE ANY FLAMMABLE VAPORS FROM LIQUIDS OR RESIDUES THAT MAY
BE PRESENT (E.G., DURING SWITCH-LOADING OPERATIONS). USE PROPER BONDING
AND/OR GROUND PROCEDURES. HOWEVER, BONDING AND GROUNDS MAY NOT ELIMINATE
THE HAZARD FROM STATIC ACCUMULATION. CONSULT LOCAL APPLICABLE STANDARDS FOR
GUIDANCE. ADDITIONAL REFERENCES INCLUDE AMERICAN PETROLEUM INSTITUTE 2003
(PROTECTION AGAINST IGNITIONS ARISING OUT OF STATIC, LIGHTNING AND STRAY
CURRENTS) OR NATIONAL FIRE PROTECTION AGENCY 77 (RECOMMENDED PRACTICE ON
STATIC ELECTRICITY) OR CENELEC CLC/TR 50404 (ELECTROSTATICS - CODE OF
PRACTICE FOR THE AVOIDANCE OF HAZARDS DUE TO STATIC ELECTRICITY).

STATIC ACCUMULATOR: THIS MATERIAL IS A STATIC ACCUMULATOR.

STORAGE:
THE CONTAINER CHOICE, FOR EXAMPLE STORAGE VESSEL, MAY EFFECT STATIC
ACCUMULATION AND DISSIPATION. DO NOT STORE IN OPEN OR UNLABELLED
CONTAINERS. KEEP AWAY FROM INCOMPATIBLE MATERIALS.


SECTION 8 EXPOSURE CONTROLS / PERSONAL PROTECTION 


EXPOSURE LIMIT VALUES:

EXPOSURE LIMITS/STANDARDS FOR MATERIALS THAT CAN BE FORMED WHEN HANDLING
THIS PRODUCT:
WHEN MISTS / AEROSOLS CAN OCCUR, THE FOLLOWING ARE RECOMMENDED:
5 MG/M3 - ACGIH TLV, 10 MG/M3 - ACGIH STEL, 5 MG/M3 - OSHA PEL.

NOTE:
LIMITS/STANDARDS SHOWN FOR GUIDANCE ONLY. FOLLOW APPLICABLE REGULATIONS.

ENGINEERING CONTROLS:
THE LEVEL OF PROTECTION AND TYPES OF CONTROLS NECESSARY WILL VARY DEPENDING
UPON POTENTIAL EXPOSURE CONDITIONS.

CONTROL MEASURES TO CONSIDER:
NO SPECIAL REQUIREMENTS UNDER ORDINARY CONDITIONS OF USE AND WITH ADEQUATE
VENTILATION.

PERSONAL PROTECTION:
PERSONAL PROTECTIVE EQUIPMENT SELECTIONS VARY BASED ON POTENTIAL EXPOSURE
CONDITIONS SUCH AS APPLICATIONS, HANDLING PRACTICES, CONCENTRATION AND
VENTILATION. INFORMATION ON THE SELECTION OF PROTECTIVE EQUIPMENT FOR USE
WITH THIS MATERIAL, AS PROVIDED BELOW, IS BASED UPON INTENDED, NORMAL
USAGE.

RESPIRATORY PROTECTION:
IF ENGINEERING CONTROLS DO NOT MAINTAIN AIRBORNE CONTAMINANT CONCENTRATIONS
AT A LEVEL WHICH IS ADEQUATE TO PROTECT WORKER HEALTH, AN APPROVED
RESPIRATOR MAY BE APPROPRIATE. RESPIRATOR SELECTION, USE, AND MAINTENANCE
MUST BE IN ACCORDANCE WITH REGULATORY REQUIREMENTS, IF APPLICABLE. TYPES OF
RESPIRATORS TO BE CONSIDERED FOR THIS MATERIAL INCLUDE:
PARTICULATE AIR-PURIFYING RESPIRATOR APPROVED FOR DUST / OIL MIST IS
RECOMMENDED.

FOR HIGH AIRBORNE CONCENTRATIONS, USE AN APPROVED SUPPLIED-AIR RESPIRATOR,
OPERATED IN POSITIVE PRESSURE MODE. SUPPLIED AIR RESPIRATORS WITH AN ESCAPE
BOTTLE MAY BE APPROPRIATE WHEN OXYGEN LEVELS ARE INADEQUATE, GAS/VAPOR
WARNING PROPERTIES ARE POOR, OR IF AIR PURIFYING FILTER CAPACITY/RATING MAY
BE EXCEEDED.

HAND PROTECTION:
ANY SPECIFIC GLOVE INFORMATION PROVIDED IS BASED ON PUBLISHED LITERATURE
AND GLOVE MANUFACTURER DATA. GLOVE SUITABILITY AND BREAKTHROUGH TIME WILL
DIFFER DEPENDING ON THE SPECIFIC USE CONDITIONS. CONTACT THE GLOVE
MANUFACTURER FOR SPECIFIC ADVICE ON GLOVE SELECTION AND BREAKTHROUGH TIMES
FOR YOUR USE CONDITIONS. INSPECT AND REPLACE WORN OR DAMAGED GLOVES. THE
TYPES OF GLOVES TO BE CONSIDERED FOR THIS MATERIAL INCLUDE:
IF PROLONGED OR REPEATED CONTACT IS LIKELY, CHEMICAL RESISTANT GLOVES ARE
RECOMMENDED. IF CONTACT WITH FOREARMS IS LIKELY, WEAR GAUNTLET STYLE
GLOVES.

EYE PROTECTION:
IF CONTACT IS LIKELY, SAFETY GLASSES WITH SIDE SHIELDS ARE RECOMMENDED.
CHEMICAL TYPE GOGGLES SHOULD BE WORN DURING MISTING OPERATIONS.

SKIN AND BODY PROTECTION:
ANY SPECIFIC CLOTHING INFORMATION PROVIDED IS BASED ON PUBLISHED LITERATURE
OR MANUFACTURER DATA. THE TYPES OF CLOTHING TO BE CONSIDERED FOR THIS
MATERIAL INCLUDE:
IF PROLONGED OR REPEATED CONTACT IS LIKELY, CHEMICAL, AND OIL RESISTANT
CLOTHING IS RECOMMENDED.

SPECIFIC HYGIENE MEASURES:
ALWAYS OBSERVE GOOD PERSONAL HYGIENE MEASURES, SUCH AS WASHING AFTER
HANDLING THE MATERIAL AND BEFORE EATING, DRINKING, AND/OR SMOKING.
ROUTINELY WASH WORK CLOTHING AND PROTECTIVE EQUIPMENT TO REMOVE
CONTAMINANTS. DISCARD CONTAMINATED CLOTHING AND FOOTWEAR THAT CANNOT BE
CLEANED. PRACTICE GOOD HOUSEKEEPING.

ENVIRONMENTAL CONTROLS: SEE SECTIONS 6, 7, 12, 13.


SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 


TYPICAL PHYSICAL AND CHEMICAL PROPERTIES ARE GIVEN BELOW. CONSULT THE
SUPPLIER IN SECTION 1 FOR ADDITIONAL DATA.

GENERAL INFORMATION:

PHYSICAL STATE: LIQUID

COLOR: YELLOW

ODOR: CHARACTERISTIC

ODOR THRESHOLD: N/D

IMPORTANT HEALTH, SAFETY, AND ENVIRONMENTAL INFORMATION:

RELATIVE DENSITY (AT 15 C): 0.89

FLASH POINT [METHOD]: >179C (354F) [ASTM D-92]

FLAMMABLE LIMITS (APPROXIMATE VOLUME % IN AIR):
LEL: N/D
UEL: N/D

AUTOIGNITION TEMPERATURE: N/D

BOILING POINT / RANGE: 270C (518F) -  500C  (932F)

VAPOR DENSITY (AIR = 1): >2 AT 101 KPA

VAPOR PRESSURE: [N/D AT 20 DEG. C]  | <1 KPA (7.5 MM HG) AT 38C

EVAPORATION RATE (N-BUTYL ACETATE = 1): <1

PH: N/A

LOG POW (N-OCTANOL/WATER PARTITION COEFFICIENT): N/D

SOLUBILITY IN WATER: EMULSIFIES

VISCOSITY: 35 CST  (35 MM2/SEC) AT 40 C

OXIDIZING PROPERTIES: SEE HAZARDS IDENTIFICATION SECTION.

OTHER INFORMATION:

FREEZING POINT: N/D

MELTING POINT: N/A

POUR POINT: -6 DEG. C (-21 DEG. F)

DMSO EXTRACT (MINERAL OIL ONLY), IP-346: <3 %WT


SECTION 10 STABILITY AND REACTIVITY 


STABILITY: MATERIAL IS STABLE UNDER NORMAL CONDITIONS.

CONDITIONS TO AVOID:
HIGH ENERGY SOURCES OF IGNITION.,  HEAT/ FREEZING TEMPERATURES.

MATERIALS TO AVOID: STRONG OXIDIZERS

HAZARDOUS DECOMPOSITION PRODUCTS:
MATERIAL DOES NOT DECOMPOSE AT AMBIENT TEMPERATURES.

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR.


SECTION 11 TOXICOLOGICAL INFORMATION 


ACUTE TOXICITY:

ROUTE OF EXPOSURE             CONCLUSION / REMARKS

INHALATION:

TOXICITY (RAT):               MINIMALLY TOXIC. BASED ON ASSESSMENT OF THE
LC50: >5000 MG/M3             COMPONENTS.

IRRITATION:                   ELEVATED TEMPERATURES OR MECHANICAL ACTION
NO END POINT DATA.            MAY FORM VAPORS, MIST, OR FUMES WHICH MAY BE
                              IRRITATING TO THE EYES, NOSE, THROAT, OR
                              LUNGS. BASED ON ASSESSMENT OF THE COMPONENTS.

INGESTION:

TOXICITY (RAT):               MINIMALLY TOXIC. BASED ON TEST DATA FOR
LD50: >2000 MG/KG             STRUCTURALLY SIMILAR MATERIALS.

SKIN:

TOXICITY (RABBIT):            MINIMALLY TOXIC. BASED ON TEST DATA FOR
LD50: >2000 MG/KG             STRUCTURALLY SIMILAR MATERIALS.

IRRITATION (RABBIT):          IRRITATING TO THE SKIN. BASED ON ASSESSMENT
DATA AVAILABLE.               OF THE COMPONENTS.

EYE:

IRRITATION (RABBIT):          IRRITATING AND WILL INJURE EYE TISSUE. BASED
DATA AVAILABLE.               ON ASSESSMENT OF THE COMPONENTS.

CHRONIC/OTHER EFFECTS:

FOR THE PRODUCT ITSELF:
OIL MIST (HIGHLY REFINED OILS):
ANIMALS EXPOSED TO HIGH CONCENTRATIONS OF MIST DEVELOPED OIL RETENTION,
INFLAMMATION, AND OIL GRANULOMAS IN THE RESPIRATORY TRACT. OILS EXPOSED
TO HIGH TEMPERATURES, CRACKING CONDITIONS, OR MIXING WITH TRAMP / USED
OILS MAY INTRODUCE POLYCYCLIC AROMATIC COMPOUNDS OR MICROBIAL CONTAMINANTS
THAT COULD RESULT IN CANCER OR SEVERE RESPIRATORY HAZARDS.

CONTAINS:
BASE OIL SEVERELY REFINED:
NOT CARCINOGENIC IN ANIMAL STUDIES. REPRESENTATIVE MATERIAL PASSES IP-346,
MODIFIED AMES TEST, AND/OR OTHER SCREENING TESTS. DERMAL AND INHALATION
STUDIES SHOWED MINIMAL EFFECTS; LUNG NON-SPECIFIC INFILTRATION OF IMMUNE
CELLS, OIL DEPOSITION AND MINIMAL GRANULOMA FORMATION. NOT SENSITIZING IN
TEST ANIMALS.

ADDITIONAL INFORMATION IS AVAILABLE BY REQUEST.

THE FOLLOWING INGREDIENTS ARE CITED ON THE LISTS BELOW: NONE.

REGULATORY LISTS SEARCHED:
1 = NTP CARC
2 = NTP SUS
3 = IARC 1
4 = IARC 2A
5 = IARC 2B
6 = OSHA CARC


SECTION 12 ECOLOGICAL INFORMATION 


THE INFORMATION GIVEN IS BASED ON DATA AVAILABLE FOR THE MATERIAL, THE
COMPONENTS OF THE MATERIAL, AND SIMILAR MATERIALS.

ECOTOXICITY:
MATERIAL: NOT EXPECTED TO BE HARMFUL TO AQUATIC ORGANISMS.

PERSISTENCE AND DEGRADABILITY:
BIODEGRADATION:
BASE OIL COMPONENT --  EXPECTED TO BE INHERENTLY BIODEGRADABLE


SECTION 13 DISPOSAL CONSIDERATIONS 


DISPOSAL RECOMMENDATIONS BASED ON MATERIAL AS SUPPLIED.  DISPOSAL MUST BE
IN ACCORDANCE WITH CURRENT APPLICABLE LAWS AND REGULATIONS, AND MATERIAL
CHARACTERISTICS AT TIME OF DISPOSAL.

REGULATORY DISPOSAL INFORMATION:
RCRA INFORMATION:
THE UNUSED PRODUCT, IN OUR OPINION, IS NOT SPECIFICALLY LISTED BY THE EPA
AS A HAZARDOUS WASTE (40 CFR, PART 261D), NOR IS IT FORMULATED TO CONTAIN
MATERIALS WHICH ARE LISTED AS HAZARDOUS WASTES.  IT DOES NOT EXHIBIT THE
HAZARDOUS CHARACTERISTICS OF IGNITABILITY, CORROSITIVITY OR REACTIVITY AND
IS NOT FORMULATED WITH CONTAMINANTS AS DETERMINED BY THE TOXICITY
CHARACTERISTIC LEACHING PROCEDURE (TCLP).  HOWEVER, USED PRODUCT MAY BE
REGULATED.

EMPTY CONTAINER WARNING:
EMPTY CONTAINER WARNING (WHERE APPLICABLE):
EMPTY CONTAINERS MAY CONTAIN RESIDUE AND CAN BE DANGEROUS. DO NOT ATTEMPT
TO REFILL OR CLEAN CONTAINERS WITHOUT PROPER INSTRUCTIONS.  EMPTY DRUMS
SHOULD BE COMPLETELY DRAINED AND SAFELY STORED UNTIL APPROPRIATELY
RECONDITIONED OR DISPOSED. EMPTY CONTAINERS SHOULD BE TAKEN FOR RECYCLING,
RECOVERY, OR DISPOSAL THROUGH SUITABLY QUALIFIED OR LICENSED CONTRACTOR AND
IN ACCORDANCE WITH GOVERNMENTAL REGULATIONS.  DO NOT PRESSURISE, CUT, WELD,
BRAZE, SOLDER, DRILL, GRIND, OR EXPOSE SUCH CONTAINERS TO HEAT, FLAME,
SPARKS, STATIC ELECTRICITY, OR OTHER SOURCES OF IGNITION.  THEY MAY EXPLODE
AND CAUSE INJURY OR DEATH.


SECTION 14 TRANSPORT INFORMATION 


LAND (DOT): NOT REGULATED FOR LAND TRANSPORT

LAND (TDG): NOT REGULATED FOR LAND TRANSPORT

SEA (IMDG): NOT REGULATED FOR SEA TRANSPORT ACCORDING TO IMDG-CODE

AIR (IATA): NOT REGULATED FOR AIR TRANSPORT


SECTION 15 REGULATORY INFORMATION 


OSHA HAZARD COMMUNICATION STANDARD:
WHEN USED FOR ITS INTENDED PURPOSES, THIS MATERIAL IS NOT CLASSIFIED AS
HAZARDOUS IN ACCORDANCE WITH OSHA 29 CFR 1910.1200.

NATIONAL CHEMICAL INVENTORY LISTING: AICS, IECSC, DSL, KECI, TSCA

EPCRA: THIS MATERIAL CONTAINS NO EXTREMELY HAZARDOUS SUBSTANCES.

SARA (311/312) REPORTABLE HAZARD CATEGORIES: NONE.

SARA (313) TOXIC RELEASE INVENTORY:
THIS MATERIAL CONTAINS NO CHEMICALS SUBJECT TO THE SUPPLIER NOTIFICATION
REQUIREMENTS OF THE SARA 313 TOXIC RELEASE PROGRAM.

REGULATORY LISTS SEARCHED:
1 = ACGIH ALL
2 = ACGIH A1
3 = ACGIH A2
4 = OSHA Z
5 = TSCA 4
6 = TSCA 5A2
7 = TSCA 5E
8 = TSCA 6
9 = TSCA 12B
10 = CA P65 CARC
11 = CA P65 REPRO
12 = CA RTK
13 = IL RTK
14 = LA RTK
15 = MI 293
16 = MN RTK
17 = NJ RTK
18 = PA RTK
19 = RI RTK

CODE KEY:
CARC=CARCINOGEN
REPRO=REPRODUCTIVE


SECTION 16 OTHER INFORMATION 


N/D = NOT DETERMINED
N/A = NOT APPLICABLE

THIS SAFETY DATA SHEET CONTAINS THE FOLLOWING REVISIONS:

REVISION CHANGES:

SECTION 04: FIRST AID EYE WAS MODIFIED.

SECTION 05: FIRE FIGHTING MEASURES - UNUSUAL FIRE HAZARDS WAS MODIFIED.

SECTION 06: NOTIFICATION PROCEDURES - HEADER WAS MODIFIED.

SECTION 11: EYE IRRITATION CONCLUSION WAS MODIFIED.

SECTION 11: SKIN IRRITATION CONCLUSION WAS MODIFIED.

SECTION 09: COLOR WAS MODIFIED.

SECTION 09: POUR POINT C(F) WAS MODIFIED.

SECTION 09: EVAPORATION RATE - HEADER WAS MODIFIED.

SECTION 08: PERSONAL PROTECTION - HEADER WAS MODIFIED.

SECTION 07: HANDLING AND STORAGE - HANDLING WAS MODIFIED.

SECTION 07: HANDLING AND STORAGE - STORAGE PHRASES WAS MODIFIED.

HAZARD IDENTIFICATION: HEALTH HAZARDS WAS MODIFIED.

HAZARD IDENTIFICATION: NFPA HEALTH WAS MODIFIED.

HAZARD IDENTIFICATION: HMIS HEALTH WAS MODIFIED.

SECTION 11: INHALATION LETHALITY TEST DATA WAS MODIFIED.

SECTION 11: DERMAL IRRITATION TEST COMMENT WAS MODIFIED.

SECTION 11: EYE IRRITATION TEST COMMENT WAS MODIFIED.

SECTION 05: HAZARDOUS COMBUSTION PRODUCTS WAS MODIFIED.

SECTION 09: VISCOSITY WAS MODIFIED.

SECTION 08: HAND PROTECTION WAS MODIFIED.

SECTION 08: EYE PROTECTION WAS MODIFIED.

SECTION 08: SKIN AND BODY PROTECTION WAS MODIFIED.

SECTION 14: SEA (IMDG) - HEADER WAS MODIFIED.

SECTION 14: AIR (IATA) - HEADER WAS MODIFIED.

SECTION 14: LAND (TDG) - HEADER WAS MODIFIED.

SECTION 14: LAND (DOT) - HEADER WAS MODIFIED.

COMPOSITION: COMPONENT TABLE WAS MODIFIED.

SECTION 14: LAND (DOT) - DEFAULT WAS MODIFIED.

SECTION 14: LAND (TDG) DEFAULT WAS MODIFIED.

SECTION 14: SEA (IMDG) - DEFAULT WAS MODIFIED.

SECTION 14: AIR (IATA) - DEFAULT WAS MODIFIED.

SECTION 15: SARA (311/312) REPORTABLE HAZARD CATEGORIES WAS MODIFIED.

SECTION 16: CODE TO MHCS WAS MODIFIED.

SECTION 16: MSN, MAT ID WAS MODIFIED.

SECTION 15: OSHA HAZARD COMMUNICATION STANDARD WAS MODIFIED.

HAZARD IDENTIFICATION: OSHA - MAY BE HAZARDOUS STATEMENT WAS ADDED.

SECTION 16: OSHA MAYBE CLASSIFIED LABEL WAS ADDED.

SECTION 06: PROTECTIVE MEASURES WAS DELETED.

SECTION 06: ACCIDENTAL RELEASE - PROTECTIVE MEASURES - HEADER WAS DELETED.

HAZARD IDENTIFICATION: HEALTH HAZARDS WAS DELETED.

SECTION 16: SIGNAL WORD WAS DELETED.

SECTION 16: HEALTH HAZARDS WAS DELETED.

SECTION 16: HEALTH HAZARDS - HEADER WAS DELETED.

SECTION 16: PRECAUTIONS WAS DELETED.

SECTION 16: PRECAUTIONS - HEADER WAS DELETED.

SECTION 16: FIRST AID - HEADER WAS DELETED.

SECTION 16: FIRST AID EYE - HEADER WAS DELETED.

SECTION 16: FIRST AID EYE WAS DELETED.

SECTION 16: FIRST AID SKIN WAS DELETED.

SECTION 16: FIRST AID SKIN - HEADER WAS DELETED.

SECTION 16: FIRE FIGHTING MEDIA - HEADER WAS DELETED.

SECTION 16: FIRE FIGHTING MEDIA - HEADER WAS DELETED.

SECTION 16: SPILL - HEADER WAS DELETED.

SECTION 16: WATER SPILL - HEADER WAS DELETED.

SECTION 16: WATER SPILL WAS DELETED.

SECTION 16: LAND SPILL WAS DELETED.

SECTION 16: LAND SPILL - HEADER WAS DELETED.

SECTION 16: LABELING USE WAS DELETED.

SECTION 16: LABELING USE - HEADER WAS DELETED.

SECTION 08: EXPOSURE LIMIT VALUES - HEADER WAS DELETED.

HAZARD IDENTIFICATION: OSHA - HAZARDS STATEMENT WAS DELETED.

PRECAUTIONARY LABEL TEXT:

CAUTION!

EXCESSIVE EXPOSURE TO MIST MAY CAUSE SKIN AND EYE IRRITATION. IN ADDITION,
EXCESSIVE EXPOSURE TO MIST MAY CAUSE RESPIRATORY IRRITATION AND DAMAGE, AND
AGGRAVATE PRE-EXISTING EMPHYSEMA AND ASTHMA.  USE WITH ADEQUATE
VENTILATION. IF INHALED AND SYMPTOMS DEVELOP, REMOVE TO FRESH AIR AND GET
MEDICAL ATTENTION.

THE INFORMATION AND RECOMMENDATIONS CONTAINED HEREIN ARE, TO THE BEST OF
EXXONMOBIL'S KNOWLEDGE AND BELIEF, ACCURATE AND RELIABLE AS OF THE DATE
ISSUED. YOU CAN CONTACT EXXONMOBIL TO INSURE THAT THIS DOCUMENT IS THE MOST
CURRENT AVAILABLE FROM EXXONMOBIL. THE INFORMATION AND RECOMMENDATIONS ARE
OFFERED FOR THE USER'S CONSIDERATION AND EXAMINATION.  IT IS THE USER'S
RESPONSIBILITY TO SATISFY ITSELF THAT THE PRODUCT IS SUITABLE FOR THE
INTENDED USE. IF BUYER REPACKAGES THIS PRODUCT, IT IS THE USER'S
RESPONSIBILITY TO INSURE PROPER HEALTH, SAFETY AND OTHER NECESSARY
INFORMATION IS INCLUDED WITH AND/OR ON THE CONTAINER.  APPROPRIATE WARNINGS
AND SAFE-HANDLING PROCEDURES SHOULD BE PROVIDED TO HANDLERS AND USERS.
ALTERATION OF THIS DOCUMENT IS STRICTLY PROHIBITED.  EXCEPT TO THE EXTENT
REQUIRED BY LAW, RE-PUBLICATION OR RETRANSMISSION OF THIS DOCUMENT, IN
WHOLE OR IN PART, IS NOT PERMITTED.  THE TERM, "EXXONMOBIL" IS USED FOR
CONVENIENCE, AND MAY INCLUDE ANY ONE OR MORE OF EXXONMOBIL CHEMICAL
COMPANY, EXXON MOBIL CORPORATION, OR ANY AFFILIATES IN WHICH THEY DIRECTLY
OR INDIRECTLY HOLD ANY INTEREST.

INTERNAL USE ONLY

MHC: 0, 0, 0, 0, 2, 1
PPEC: D

DGN: 7087019 (1012434)

COPYRIGHT 2002 EXXON MOBIL CORPORATION, ALL RIGHTS RESERVED