Common Name: ETERNAPRIME
Manufacturer: ETERNABOND
MSDS Revision Date: 9/1/2009
MSDS Format: No Format Specified
   
Grainger Item Number(s): 3GYF1, 3GYF2
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION I - PRODUCT IDENTIFICATION 
SECTION II - HAZARDOUS COMPONENTS 
SECTION III - PHYSICAL DATA 
SECTION IV - FIRE AND EXPLOSION HAZARD DATA 
SECTION V - HEALTH HAZARD DATA 
SECTION VI - REACTIVITY DATA 
SECTION VII - SPILL OR LEAK PROCEDURES 
SECTION VIII - SPECIAL PROTECTION INFORMATION 
SECTION IX - SPECIAL PRECAUTIONS 
SECTION X - NOTES 



ETERNABOND, INC.

MATERIAL SAFETY DATA SHEET

PROVIDED BY:
ETERNABOND, INC.
75 E. DIVISION ST.
MUNDELEIN, IL 60060
847-837-9400

THIS FORM IS DESIGNED TO MEET THE REQUIREMENTS OF THE U.S. LABOR DEPARTMENT
OSHA FORM NO 174.


SECTION I - PRODUCT IDENTIFICATION 


PRODUCT: ETERNABOND ETERNAPRIME

24 HOUR EMERGENCY ASSISTANCE - INFOTRAC: (800)-535-5053

CHEMICAL NAME: MIXTURE

CHEMICAL FAMILY: MIXTURE

HMIS/NFPA HAZARD RATINGS:
HEALTH HAZARD       1
FLAMMABILITY HAZARD 3
REACTIVITY HAZARD   0


SECTION II - HAZARDOUS COMPONENTS 


NAME                          C.A.S. #       EXPOSURE LIMITS      % BY
WEIGHT

THERMOPLASTIC RUBBER          66070-58-4     OSHA PEL: NA           3-7
                                             ACGIH TLV: NA

HYDROCARBON RESIN             69430-35-9     OSHA PEL: NA           5-11
                                             ACGHI TLV: NA

*HEXANE                         110-54-3     OSHA TWA:             70-95
                                             50 PPM (SKIN)
                                             50 PPM (SKIN)

TETRAKIS(METHYLENE             6683-19-8     OSHA TWA: NE         .01-.05
(3,5,-DI-(TERT)-BUTYL-4-                     ACGIH TWA: NE
HYDROXYHYDROCINNIAMATE))
METHANE

# DENOTES CONSTITUENT OF ABOVE LISTED INGREDIENT. % CONCENTRATION IS OF
PRODUCT MASS.

* IDENTIFIED AS SARA SECTION 313 REPORTABLE.


SECTION III - PHYSICAL DATA 


BOILING POINT: 69 DEG. C

SPECIFIC GRAVITY: .75

FLASH POINT (SETA): -23 DEG. C (-9 DEG. F)

VAPOR DENSITY: 3.0

EVAPORATION RATE (BUTYL ACETATE = 1.0): 8.1

SOLUBILITY: NEG

APPEARANCE AND ODOR: CLEAR LIQUID WITH A HYDROCARBON ODOR.


SECTION IV - FIRE AND EXPLOSION HAZARD DATA 


EXTINGUISHING MEDIA:
CLASS "B" DRY CHEMICAL, CARBON DIOXIDE, OR OTHER SUITABLE EXTINGUISHING
MATERIAL SUCH AS DRY SAND. DO NOT USE HALOGENATED AGENTS. WHEN FLAMES HAVE
BEEN ELIMINATED, COVER RESIDUE WITH DRY EXTINGUISHING AGENT OR DRY SAND AND
ALLOW IT TO REMAIN UNDISTURBED UNTIL IT HAS COOLED. IF FIRE APPEARS TO
INCREASE IN INTENSITY, STOP USING THESE AGENTS. APPLY CLASS "D"
EXTINGUISHING
AGENT OR MORE DRY, INERT, GRANULAR MATERIAL. RING FIRE WITH EXTINGUISHING
MATERIAL AND ALLOW THE FIRE TO BURN OUT.

SPECIAL FIRE FIGHTING PROCEDURES:
IF THE FIRE DOES NOT RESPOND TO ABOVE AGENTS OR THEY ARE NOT AVAILABLE, USE
FOAM OR WATER FOG AS A LAST RESORT. WATER MAY ALSO BE USED TO COOL EXPOSED,
BUT NOT BURNING, CONTAINERS. THESE PRODUCTS MAY FLOAT AND BE RE-IGNITED ON
TOP OF WATER. PERSONNEL FIGHTING FIRE SHOULD USE A SELF CONTAINED BREATHING
APPARATUS.

UNUSUAL FIRE AND/OR EXPLOSION HAZARDS:
CLOSED CONTAINERS MAY EXPLODE IN A FIRE. KEEP CONTAINERS COOL AND REMOVE TO
A
SAFE LOCATION.


SECTION V - HEALTH HAZARD DATA 


EYE CONTACT:
THESE PRODUCTS ARE MILDLY IRRITATING TO THE EYES. THE EFFECT OF PROLONGED
EYE
CONTACT IS NOT KNOWN. FLUSH WITH WATER IMMEDIATELY FOR AT LEAST 15 MINUTES.
SEEK MEDICAL ATTENTION IMMEDIATELY.

SKIN CONTACT:
PROLONGED OR REPEATED CONTACT CAN CAUSE DERMATITIS. WASH SKIN WITH WATERLESS
HAND CLEANER FOLLOWED BY SOAP AND WATER. IF REDNESS APPEARS TREAT IT AS A
SUNBURN, IF REDNESS PERSISTS OR RASH APPEARS SEEK MEDICAL ATTENTION
IMMEDIATELY.

INHALATION:
UPPER RESPIRATORY TRACT IRRITATION. MAY CAUSE NAUSEA OR DIZZINESS. HIGH
VAPOR
CONCENTRATIONS CAN CAUSE CENTRAL NERVOUS SYSTEM DEPRESSION, LIVER, AND
KIDNEY
DAMAGE. REMOVE INDIVIDUAL TO FRESH AIR, UPWIND FROM FUME SOURCE. IF
IRRITATION
PERSISTS SEEK MEDICAL ATTENTION IMMEDIATELY.

INGESTION:
ACUTE GASTROINTESTINAL TRACT IRRITATION. DO NOT INDUCE VOMITING. PREVENT
ASPIRATION INTO LUNGS. ASPIRATION OF EVEN SMALL AMOUNTS INTO LUNGS MAY
RESULT
IN ASPIRATION PNEUMONITIS. SEEK MEDICAL ATTENTION IMMEDIATELY.

PRE-EXISTING EYE, SKIN, AND RESPIRATORY DISORDERS MAY BE AGGRAVATED BY
EXPOSURE TO THESE PRODUCTS. EXPOSURE TO HIGH CONCENTRATIONS OF FUMES MAY
HAVE
AN ANESTHETIC EFFECT.


SECTION VI - REACTIVITY DATA 


STABILITY: STABLE

HAZARDOUS POLYMERIZATION: WILL NOT OCCUR

INCOMPATABILITY: STRONG OXIDIZERS

HAZARDOUS DECOMPOSITION PRODUCTS:
OXIDES OF CARBON, VARIOUS HYDROCARBON FRAGMENTS


SECTION VII - SPILL OR LEAK PROCEDURES 


PRECAUTIONS IN CASE OF SPILL:
CONTAIN SPILL AS QUICKLY AS POSSIBLE. KEEP FLOWING MATERIAL AWAY FROM HEAT,
SPARKS, OR OPEN FLAMES. DO NOT SMOKE NEAR A SPILL. USE CLAY (OIL DRY(TM)),
SAND, EARTH, ETC. TO ABSORB THE SPILL. PUT MATERIAL INTO A SUITABLE STEEL
DRUM
WHICH CAN BE CLOSED SECURELY.

WASTE DISPOSAL:
BURY IN AN APPROVED LANDFILL ACCORDING TO FEDERAL, STATE, AND LOCAL
REGULATIONS. EMPTY CONTAINERS THAT HAVE BEEN COMPLETELY EMPTIED AND THE
RESIDUE ALLOWED TO DRY ARE NOT CONSIDERED HAZARDOUS WASTE.

HANDLING & STORAGE PRECAUTIONS:
STORE AWAY FROM HEAT, SPARKS, AND OPEN FLAMES. SOLVENT VAPORS ARE HEAVIER
THAN
AIR AND MAY BE MOVED FROM THE SOURCE LOCATION BY VENTILATION SYSTEMS TO
POINTS
FAR AWAY. DO NOT STORE NEAR OXIDIZERS.

OTHER PRECAUTIONS:
KEEP CONTAINER CLOSED WHEN NOT IN USE. STORE IN A DRY VENTILATED AREA.
MAINTAIN PACKAGE LABELING DURING STORAGE.


SECTION VIII - SPECIAL PROTECTION INFORMATION 


VENTILATION:
USE NATURAL CROSS VENTILATION, LOCAL (MECHANICAL) PICK-UP, AND/OR GENERAL
AREA MECHANICAL CROSS VENTILATION. VENTILATION PATTERN SHOULD BE DESIGNED TO
PREVENT ACCUMULATION OF HEAVIER THAN AIR SOLVENT VAPORS. VENTILATION MUST BE
SUFFICIENT TO MAINTAIN SOLVENT VAPOR CONCENTRATIONS BELOW THE TLV.

RESPIRATORY PROTECTION:
AS REQUIRED IF AIRBORNE CONCENTRATIONS ARE ABOVE THE TLV. IF RESPIRATORS
BECOME NECESSARY USE NIOSH APPROVED UNIT FOR ORGANIC VAPOR AND DUSTS.

PROTECTIVE CLOTHING: AS NECESSARY TO PREVENT WETTING OF THE SKIN.

EYE PROTECTION: AS NECESSARY IN ACCORDANCE WITH 29 CFR 1910.113

OTHER PRECAUTIONS:
WITH GOOD INDUSTRIAL HYGIENE NO OTHER PRECAUTIONS SHOULD BE NECESSARY. THESE
PRODUCTS ARE INTENDED FOR PROFESSIONAL USE. USE ONLY AFTER THE APPROPRIATE
PRODUCT DATA BULLETIN HAS BEEN READ AND UNDERSTOOD.


SECTION IX - SPECIAL PRECAUTIONS 


PRECAUTIONS TO BE TAKEN IN HANDLING AND STORING:
FOR INDUSTRIAL USE ONLY. KEEP OUT OF REACH OF CHILDREN. KEEP CONTAINER
CLOSED.
AVOID PROLONGED OR REPEATED CONTACT WITH SKIN. AVOID BREATHING VAPORS. DO
NOT
TAKE INTERNALLY. STORE IN A COOL PLACE. STORE IN TIGHTLY CLOSED CONTAINERS
IN
A VENTILATED FIRE RESISTANT AREA AWAY FROM HEAT, OPEN FLAME, SPARKS OR
STRONG
OXIDIZING AGENTS. GROUND ALL EQUIPMENT. USE ONLY IN A WELL VENTILATED AREA.
USE ONLY NON-SPARKING TOOLS. VAPORS ARE HEAVIER THAN AIR AND WILL COLLECT IN
LOW AREAS SUCH AS PITS. CHRONIC OVEREXPOSURE MAY CREATE HEALTH RISKS. WASH
THOROUGHLY AFTER HANDLING OR CONTACT. DO NOT EAT, DRINK OR SMOKE IN AREAS
WHERE THIS PRODUCT IS USED. DO NOT APPLY AIR PRESSURE, PUNCTURE OR WELD ON
OR NEAR CONTAINERS. DO NOT REUSE CONTAINERS.


SECTION X - NOTES 


DOT INFORMATION:
ETERNAPRIME IS REGULATED AS FLAMMABLE LIQUIDS PER CFR 172.504. ALL BULK
SHIPMENTS IN CONTAINERS WITH A CAPACITY OF 119 GALLONS OR MORE AND ALL OTHER
SHIPMENTS OVER 1000 LBS. MUST DISPLAY FLAMMABLE PLACARDS AND BE FULLY
SECURED
BEFORE AND DURING TRANSIT. THEY MUST BE PLACED ON ALL FOUR SIDES OF THE
VEHICLE.

UN#: 1133

CLASS: 3

PACKING GROUP: II

NA

NOTE:
NA = NOT APPLICABLE
NE = NOT ESTABLISHED

ISSUE DATE: MAY 1, 2006

ISSUED BY: R. BARRY

REVISION DATE: SEPTEMBER 1, 2009

INFORMATION HEREIN IS GIVEN IN GOOD FAITH AND IS, TO THE BEST OF OUR
KNOWLEDGE
AND BELIEF, ACCURATE AND RELIABLE. HOWEVER, SINCE INFORMATION HEREIN WAS
OBTAINED, IN PART, FROM INDEPENDENT SUPPLIERS NOT UNDER THE DIRECTION AND
SUPERVISION OF ETERNABOND, INC., ETERNABOND, INC. MAKES NO WARRANTY OR
REPRESENTATION, EXPRESS OR IMPLIED, THAT THE INFORMATION IS ACCURATE,
RELIABLE, COMPLETE OR REPRESENTATIVE. ETERNABOND, INC., WARRANTS ONLY THAT
IT
HAS MADE NO EFFORT TO CENSOR OTHER THAN TRADE SECRET INFORMATION OR TO
CONCEAL
DELETERIOUS ASPECTS OF ITS PRODUCTS. THE DATA SHOWN ABOVE IN NO WAY
MODIFIES,
AMENDS, OR ENLARGES ANY SPECIFICATION OR WARRANTY.