Common Name: ALPET D2
Manufacturer: BEST SANITIZERS
MSDS Revision Date: 8/29/2012
   
Grainger Item Number(s): 19RC79, 19RC83, 36P184, 36P185, 36P186, 36P191, 36P192
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1. CHEMICAL PRODUCT & COMPANY IDENTIFICATION 
SECTION 2. COMPOSITION/INFORMATION ON INGREDIENTS 
SECTION 3. HAZARDS INFORMATION 
SECTION 4. EMERGENCY & FIRST AID PROCEDURES 
SECTION 5. FIRE FIGHTING MEASURES 
SECTION 6. ACCIDENTAL RELEASE MEASURES 
SECTION 7. HANDLING & STORAGE REQUIREMENTS 
SECTION 8. EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9. PHYSICAL & CHEMICAL PROPERTIES 
SECTION 10. STABILITY & REACTIVITY 
SECTION 11. TOXICOLOGICAL INFORMATION 
SECTION 12. ECOLOGICAL INFORMATION 
SECTION 13. DISPOSAL CONSIDERATION 
SECTION 14. TRANSPORT INFORMATION 
SECTION 15. REGULATORY INFORMATION 
SECTION 16. OTHER INFORMATION 



ALPET D2

MATERIAL SAFETY DATA SHEET


SECTION 1. CHEMICAL PRODUCT & COMPANY IDENTIFICATION 


DISTRIBUTOR'S NAME: BEST SANITIZERS, INC.

ADDRESS:
154 MULLEN DRIVE WALTON
KY 41094

REGULAR TELEPHONE: 888-225-3267

EMERGENCY TELEPHONE:
CHEMTREC: (800) 424-9300

TRADE NAME: ALPET D2

SYNONYMS: SANITIZER-DISINFECTANT


SECTION 2. COMPOSITION/INFORMATION ON INGREDIENTS 


MATERIAL/COMPONENT                CAS #      %              HAZARD DATA

ISOPROPANOL (ISOPROPYL ALCOHOL)   67-63-0    55 - 75%       TLV: 1000 PPM


SECTION 3. HAZARDS INFORMATION 


EMERGENCY OVERVIEW DESCRIPTION:
A CLEAR ALCOHOL BASED SANITIZER WITH A STRONG ALCOHOL ODOR.

NOTE:
WARNINGS BELOW ARE FOR EXPOSURE TO LARGE QUANTITIES OF THE PRODUCT.
NORMAL USAGE SHOULD NOT CREATE HAZARDOUS CONDITIONS.

POTENTIAL HEALTH EFFECTS:

ISOPROPYL ALCOHOL:
ACUTE ORAL LD50: >5000 MG/KG (RAT)
ACUTE DERMAL LD50: >2000 MG/KG (RABBIT)
INHALATION LC50: 5000 PPM/1 HR. (RAT)

ROUTES OF EXPOSURE:

INHALATION:
NONE EXPECTED UNDER FORESEEABLE CONDITIONS. EXPOSURE TO HIGH LEVELS OF
ISOPROPANOL CAN CAUSE IRRITATION TO NOSE & THROAT AND NARCOTIC EFFECTS
AS LISTED UNDER INGESTION.

SKIN CONTACT:
NONE ANTICIPATED UNDER FORESEEABLE USE CONDITIONS. MAY CAUSE OPEN CUTS TO
BURN OR STING.

SKIN ABSORPTION:
SEE SKIN CONTACT. EXCESSIVE CONTACT TIME NOT ANTICIPATED WITH NORMAL USE.

EYE CONTACT: VAPORS MAY IRRITATE THE EYES.

INGESTION:
MAY CAUSE NAUSEA AND VOMITING. INGESTION OF LARGE AMOUNTS CAN CAUSE
DROWSINESS, UNCONSCIOUSNESS, CRAMPS AND EVEN DEATH

EFFECTS OF OVEREXPOSURE:

ACUTE OVEREXPOSURE:
IRRITATION OF SKIN, EYES AND MUCOUS MEMBRANES. (SEE ALSO SKIN INGESTION.)

CHRONIC OVEREXPOSURE:
PERSONS WITH EXISTING SKIN PROBLEMS SHOULD CONSULT A PHYSICIAN BEFORE
CONSISTENT USE OF THIS PRODUCT.


SECTION 4. EMERGENCY & FIRST AID PROCEDURES 


EYES:
IMMEDIATELY FLUSH EYES WITH LARGE AMOUNTS OF WATER FOR AT LEAST 15 MINUTES.
HOLD EYELIDS APART WHILE FLUSHING. GET MEDICAL ATTENTION IMMEDIATELY.

SKIN:
FOR ACCIDENTAL EXPOSURE TO LARGE QUANTITIES, NOT NORMAL USAGE. IMMEDIATELY
FLUSH WITH WATER. WASH WITH SOAP AND WATER.

INHALATION:
FOR ACCIDENTAL EXPOSURE TO LARGE QUANTITIES, NOT NORMAL USAGE. MOVE PERSON
TO FRESH AIR. IF BREATHING STOPS, GIVE ARTIFICIAL RESPIRATION, GET MEDICAL
ATTENTION IMMEDIATELY.

INGESTION:
NEVER GIVE ANYTHING BY MOUTH TO AN UNCONSCIOUS PERSON. GIVE 250 ML (8OZ) OF
WATER DO NOT INDUCE VOMITING. IF VOMITING OCCURS SPONTANEOUSLY, KEEP AIRWAY
CLEAR. GET MEDICAL ATTENTION IMMEDIATELY.

OBJECT IS TO SEEK MEDICAL ATTENTION IMMEDIATELY:


SECTION 5. FIRE FIGHTING MEASURES 


FLASH POINT (PENSKY-MARTIN CLOSED CUP): 70.68 DEG. F (21.49 DEG. C)

FLAMMABLE LIMITS IN AIR, % BY VOLUME: ISOPROPANOL
LOWER: 2.0
HIGHER: 12.7

EXTINGUISHING MEDIA:
USE CARBON DIOXIDE (CO2), DRY CHEMICALS, WATER FOG OR FOAM WHERE THIS
PRODUCT IS STORED.

SPEC. FIRE FIGHT PROCEDURES:
CAUTION:
FLAMMABLE. DO NOT ENTER CONFINED FIRE SPACE WITHOUT FULL BUNKER GEAR
(HELMET WITH FACE SHIELD, BUNKER COATS, GLOVES AND RUBBER BOOTS, INCLUDING
A POSITIVE PRESSURE NIOSH BREATHING APPARATUS). COOL FIRE EXPOSED
CONTAINERS WITH WATER SPRAY.

UNUSUAL FIRE & EXPOSURE HAZARD:
CONTAINERS EXPOSED TO HEAT FROM FIRES SHOULD BE COOLED WITH WATER SPRAY TO
PREVENT PRESSURE BUILD UP WHICH COULD RUPTURE CONTAINER, CONTAINERS EXPOSED
TO DIRECT FLAME SHOULD BE COOLED WITH LARGE QUANTITIES OF WATER.


SECTION 6. ACCIDENTAL RELEASE MEASURES 


STEPS TO BE TAKEN IF MATERIAL IS RELEASED OR SPILLED:
STOP SPILL. CONTAIN SPILL. ABSORB ON INERT MATERIAL SUCH AS SAND, CLAY,
ETC. SHOVEL INTO APPROVED CONTAINERS, CLOSE, LABEL AND SEND TO APPROVED
HAZARDOUS CHEMICAL DUMP. NEUTRALIZE REMAINING TRACES. FLUSH AREA WITH
WATER.

NEUTRALIZING CHEMICALS: NA

WASTE DISPOSAL METHOD:
THE MATERIALS RESULTING FROM CLEAN-UP OPERATIONS MAY BE HAZARDOUS WASTES
AND THEREFORE SUBJECT TO SPECIFIC REGULATIONS. PACKAGE, STORE, TRANSPORT
AND DISPOSE OF ALL CLEAN-UP MATERIALS IN ACCORDANCE WITH ALL APPLICABLE
FEDERAL, STATE AND LOCAL HEALTH AND EPA REGULATIONS.


SECTION 7. HANDLING & STORAGE REQUIREMENTS 


STORE IN A COOL, DRY PLACE, KEEP AWAY FROM HEAT. KEEP AWAY FROM
HYPOCHLORITE AND STRONG OXIDIZERS.

KEEP LIQUID AND VAPOR AWAY FROM HEAT, SPARKS AND FLAME. SURFACES THAT ARE
SUFFICIENTLY HOT MAY IGNITE EVEN LIQUID PRODUCTS IN THE ABSENCE OF SPARKS
OR FLAME. EXTINGUISH PILOT LIGHTS, CIGARETTES AND TURNS OFF OTHER SOURCES
OF IGNITION PRIOR TO USE AND UNTIL ALL VAPORS ARE GONE. VAPORS MAY
ACCUMULATE AND TRAVEL TO IGNITION SOURCES DISTANT FROM THE HANDLING SITE;
FLASH-FIRE CAN RESULT. KEEP CONTAINERS CLOSED WHEN NOT IN USE. USE WITH
ADEQUATE VENTILATION. CONTAINERS, EVEN THOSE THAT HAVE BEEN EMPTIED, CAN
CONTAIN EXPLOSIVE VAPORS. DO NOT CUT, DRILL, GRIND, WELD OR PERFORM SIMILAR
OPERATIONS ON OR NEAR CONTAINERS.

STATIC ELECTRICITY MAY ACCUMULATE AND CREATE A FIRE HAZARD. GROUND FIXED
EQUIPMENT. BOND AND GROUND TRANSFER CONTAINERS AND EQUIPMENT.


SECTION 8. EXPOSURE CONTROLS/PERSONAL PROTECTION 


VENTILATION REQUIREMENTS:
USE EXHAUST VENTILATION TO KEEP AIRBORNE CONCENTRATIONS BELOW EXPOSURE
LIMITS. SPECIAL VENTILATION NOT USUALLY REQUIRED. (ETHANOL: TLV 1000 PPM)

PERSONAL PROTECTIVE EQUIPMENT:
SHOULD ONLY BE NEEDED IF HANDLING LARGE QUANTITIES NOT FOR NORMAL USAGE

RESPIRATORY:
AVOID BREATHING MISTS OR VAPORS. USE OF NIOSH/MSHA APPROVED RESPIRATOR
PROTECTION IS REQUIRED WHEN TLV VALUES FOR AIRBORNE MATERIALS ARE MET OR
EXCEEDED. RESPIRATORY PROTECTION MUST BE IN COMPLIANCE WITH 29 CFR 1910.134
& OTHER APPLICABLE REGULATION.

EYE:
OSHA APPROVED CHEMICAL SPLASH GOGGLES. NEVER WEAR CONTACT LENSES. EYE
PROTECTION MUST CONFORM TO ANSI Z87.1 - 1989.

GLOVES:
ALWAYS WEAR PERMEATION RESISTANT GLOVES (NEOPRENE, BUTYL & OTHER RUBBERS).
CONSULT WITH GLOVE MANUFACTURER FOR MOST RESISTANT GLOVE TO MATERIAL
HANDLED.

OTHER CLOTHING EQUIPMENT:
IMPERVIOUS PROTECTIVE CLOTHING SUCH AS RAIN SUITS AND RUBBER BOOTS. AN
EMERGENCY EYE WASH AND SHOWER SHOULD BE IN THE CHEMICAL STORAGE AREA PLUS
IN ANY AREA WHERE CHEMICALS ARE MIXED.


SECTION 9. PHYSICAL & CHEMICAL PROPERTIES 


BOILING POINT: 180 DEG. F

MELTING POINT: NA

FREEZING POINT: NA

SPECIFIC GRAVITY (H2O=1): 0.89

VAPOR PRESSURE: 30 MMHg AT 20 DEG. C

VAPOR DENSITY (AIR=1): NA

SOLUBILITY IN H2O, % BY WT: SOLUBLE

% VOLATILE BY VOLUME: <60%

EVAPORATION RATE: NA

APPEARANCE & ODOR: CLEAR SOLUTION WITH A STRONG ALCOHOL ODOR

PH: NA


SECTION 10. STABILITY & REACTIVITY 


CONDITIONS CONTRIBUTING TO INSTABILITY:
UNDER NORMAL CONDITIONS THIS PRODUCT IS STABLE.

INCOMPATIBILITY:
DO NOT MIX WITH STRONG OXIDIZING AGENTS. KEEP AWAY FROM IGNITION SOURCES.

HAZARDOUS DECOMPOSITION PRODUCTS: OXIDES OF CARBON.

CONDITIONS CONTRIBUTING TO HAZ. POLYMERIZATION: NONE


SECTION 11. TOXICOLOGICAL INFORMATION 


CONSULT SECTION 3. IF MORE DETAILED INFORMATION IS REQUIRED, WRITE TO THE
ADDRESS LISTED IN SECTION 1, ATTENTION: TECHNICAL DEPARTMENT.


SECTION 12. ECOLOGICAL INFORMATION 


THIS PRODUCT DOES NOT CONTAIN PHOSPHATES.


SECTION 13. DISPOSAL CONSIDERATION 


THE MATERIALS RESULTING FROM CLEAN-UP OPERATIONS MAY BE HAZARDOUS WASTES
AND THEREFORE SUBJECT TO SPECIFIC REGULATIONS. PACKAGE, STORE, TRANSPORT
AND DISPOSE OF ALL CLEAN-UP MATERIALS IN ACCORDANCE WITH ALL APPLICABLE
FEDERAL, STATE AND LOCAL HEALTH & EPA REGULATIONS.


SECTION 14. TRANSPORT INFORMATION 


REGULATORY      UN NUMBER  PROPER         CLASS  PACKING  OTHER INFORMATION
INFORMATION                SHIPPING NAME         GROUP

DOT             UN 1219    ISOPROPANOL    3      II       ORM-D FOR
CLASSIFICATION                                            PACKAGES UNDER 1
                                                          LITERS
                                                          EXEMPT DOT-SP
                                                          9275 FOR PACKAGES
                                                          UNDER 1 GALLON


SECTION 15. REGULATORY INFORMATION 


HCS CLASSIFICATION: FLAMMABLE LIQUID, IRRITATING MATERIAL

U. S. FEDERAL REGULATIONS:
SARA 302/304/311/312 EXTREMELY HAZARDOUS SUBSTANCES: NO PRODUCTS FOUND
SARA 302/304 EMERGENCY PLANNING AND NOTIFICATION: NO PRODUCTS FOUND

TSCA 8(B) INVENTORY: ALL MATERIALS LISTED OR EXEMPT

CALIFORNIA PROP 65: NOT LISTED


SECTION 16. OTHER INFORMATION 


HMIS RATING:
HEALTH           2
FLAMMABILITY     3
PHYSICAL HAZARDS 0

NFPA RATING:
HEALTH      2
FIRE        3
INSTABILITY 0

DOES NOT APPLY TO EXPOSURE HAZARDS OTHER THAN DURING A FIRE:

ALL INFORMATION, RECOMMENDATIONS AND SUGGESTIONS APPEARING HEREIN
CONCERNING OUR PRODUCT ARE BASED UPON TESTS AND DATA BELIEVED TO BE
RELIABLE; HOWEVER, IT IS THE USER'S RESPONSIBILITY TO DETERMINE THE SAFETY,
TOXICITY AND SUITABILITY FOR HIS OWN USE OF THE PRODUCT DESCRIBED HEREIN.
SINCE THE ACTUAL USE BY OTHERS IS BEYOND OUR CONTROL, NO GUARANTEE
EXPRESSED OR IMPLIED, IS MADE BY BEST SANITIZERS, INC.. AS TO THE EFFECT OF
SUCH USE, THE RESULTS TO BE OBTAINED, OR THE SAFETY AND TOXICITY OF THE
PRODUCT NOR DOES BEST SANITIZERS, INC. ASSUME LIABILITY ARISING OUT OF USE
BY OTHERS, OF THE PRODUCT REFERRED TO HEREIN. NOR IS THE INFORMATION HEREIN
TO BE CONSTRUED AS ABSOLUTELY COMPLETE SINCE ADDITIONAL INFORMATION MAY BE
NECESSARY OR DESIRABLE WHEN PARTICULAR OR EXCEPTIONAL CONDITIONS EXIST
BECAUSE OF APPLICABLE LAWS OR GOVERNMENT REGULATIONS.

PREPARED BY: DUNCAN C. BADERTSCHER

DATE: 29 AUGUST 2012

LS-104-037-00

REV.: 005