Common Name: NICKEL-CADMIUM BATTERY
Manufacturer: LENMAR
SDS Revision Date: 11/1/2010
SDS Format: No Format Specified
   
Item Number(s): 12A605, 12C394, 12C395, 12D091, 12D097, 12Z669, 12Z671, 12Z672, 12Z673, 12Z678, 12Z680, 12Z683, 12Z686, 12Z687, 12Z688, 12Z690, 12Z696, 12Z697, 12Z698, 12Z699, 12Z702, 36N235, 36N305
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION I - MANUFACTURER INFORMATION 
SECTION II - HAZARDOUS INGREDIENTS 
SECTION III - FIRE AND EXPLOSION HAZARD DATA 
SECTION IV - HEALTH HAZARD DATA 
SECTION V - PRECAUTIONS FOR SAFE HANDLING AND USE 
SECTION VI - SPECIAL PROTECTION INFORMATION 
SECTION VII - REGULATORY INFORMATION 



LENMAR(R*)
BATTERY SOLUTIONS

MATERIAL SAFETY DATA SHEET

NICKEL-CADMIUM BATTERY

EFFECTIVE DATE: NOV 1, 2010

NICKEL-CADMIUM BATTERY

MATERIAL SAFETY DATA SHEET (MSDS)


SECTION I - MANUFACTURER INFORMATION 


MANUFACTURED FOR:
LENMAR ENTERPRISES, INC.
4035 VIA PESCASDOR
CAMARILLO, CA 93012

CONTACT INFORMATION:
805.384.9600
800.424.2703 (US)
LENMAR.COM


SECTION II - HAZARDOUS INGREDIENTS 


MATERIAL OR INGREDIENT     PEL (OSHA)        TLV (ACGIH)            %/WT.

CADMIUM AS CADMIUM METAL   5 (MICRO)G/M3     0.01 MG/M3              13-22
(CAS# 7440-43-9)           TWA (AS Cd)       TWA (AS Cd)
AS CADMIUM OXIDE                             0.002 MG/M3
(CAS# 1306-19-0)                             TWA (AS Cd
AS CADMIUM HYDROXIDE                         RESPIRABLE FRACTION)
(CAS# 21041-95-2)

COBALT AS COBALT METAL     0.1 MG/M3         0.02 MG/M3 TWA         0.5-2
(CAS# 7440-48-4)           TWA (AS Co)       (AS Co)
AS COBALT OXIDE
(CAS# 1307-96-6)
AS COBALT HYDROXIDE
(CAS# 21041-93-0)

LITHIUM HYDROXIDE          NONE ESTABLISHED  NONE ESTABLISHED         0-4
(CAS# 1310-65-2)

NICKEL AS NICKEL METAL     1 MG/M3 TWA       1.5 MG/M3 TWA (AS       20-32
(CAS# 7440-02-0)           (AS Ni)           INHALABLE Ni)
AS NICKEL OXIDE                              0.2 MG/M3 TWA (AS
(CAS# 1313-99-1)                             INHALABLE Ni,
AS NICKEL HYDROXIDE                          INSOLUBLE COMPOUNDS)
(CAS# 12054-48-7)

POTASSIUM HYDROXIDE        NONE ESTABLISHED  2 MG/M3 CEILING          0-4
(CAS# 1310-58-3)

SODIUM HYDROXIDE           2 MG/M3 TWA       2 MG/M3 CEILING          0-4
(CAS# 1310-73-2)

IMPORTANT NOTE:
THE BATTERY SHOULD NOT BE OPENED OR INCINERATED. EXPOSURE TO THE
INGREDIENTS CONTAINED WITHIN OR THEIR COMBUSTION PRODUCTS COULD BE HARMFUL.


SECTION III - FIRE AND EXPLOSION HAZARD DATA 


IF FIRE OR EXPLOSION OCCURS WHEN BATTERIES ARE ON CHARGE, SHUT OFF POWER TO
CHARGER.

IN CASE OF FIRE, IT IS PERMISSIBLE TO USE ANY CLASS OF EXTINGUISHING MEDIUM
ON THESE BATTERIES OR THEIR PACKAGING MATERIALS. COOL THE EXTERIOR OF THE
BATTERIES IF EXPOSED TO FIRE TO PREVENT RUPTURE.

FIRE FIGHTERS SHOULD WEAR SELF-CONTAINED BREATHING APPARATUS.
NICKEL-CADMIUM BATTERIES INVOLVED IN A FIRE CAN VENT AND PRODUCE TOXIC
FUMES INCLUDING NICKEL, NICKEL OXIDES, CADMIUM, CADMIUM OXIDES, AND COBALT
OXIDES.


SECTION IV - HEALTH HAZARD DATA 


UNDER NORMAL CONDITIONS OF USE, THE BATTERY IS HERMETICALLY SEALED.

INGESTION: SWALLOWING A BATTERY MAY BE HARMFUL.

CONTENTS OF AN OPEN BATTERY CAN CAUSE SERIOUS CHEMICAL BURNS OF MOUTH,
ESOPHAGUS, AND GASTROINTESTINAL TRACT. CONTENTS INCLUDE TOXIC CADMIUM AND
CADMIUM COMPOUNDS WHICH CAN CAUSE EXCESSIVE SALIVATION, CHOKING, NAUSEA,
PERSISTENT VOMITING, DIARRHEA, ABDOMINAL PAIN, DIZZINESS, FAINTNESS,
UNCONSCIOUSNESS, AND POSSIBLE LIVER AND KIDNEY INJURY.

IF BATTERY OR CONTENTS OF THE BATTERY ARE INGESTED, DO NOT INDUCE VOMITING
OR GIVE FOOD OR DRINK. SEEK MEDICAL ATTENTION IMMEDIATELY AND CALL THE
NATIONAL BATTERY INGESTION HOTLINE (202-625-3333) FOR TREATMENT
INFORMATION.

INHALATION:
CONTENTS OF AN OPEN BATTERY CAN CAUSE RESPIRATORY IRRITATION. CADMIUM OXIDE
FUMES CAN CAUSE METAL FUME FEVER. HYPERSENSITIVITY TO NICKEL CAN CAUSE
ALLERGIC PULMONARY ASTHMA. PROVIDE FRESH AIR AND SEEK MEDICAL ATTENTION.

SKIN CONTACT:
CONTENTS OF AN OPEN BATTERY CAN CAUSE SKIN IRRITATION AND/OR CHEMICAL
BURNS. COBALT, COBALT COMPOUNDS, NICKEL, AND NICKEL COMPOUNDS CAN CAUSE
SKIN SENSITIZATION AND AN ALLERGIC CONTACT DERMATITIS. REMOVE CONTAMINATED
CLOTHING AND WASH SKIN WITH SOAP AND WATER. IF A CHEMICAL BURN OCCURS OR IF
IRRITATION PERSISTS, SEEK MEDICAL ATTENTION.

EYE CONTACT:
CONTENTS OF AN OPEN BATTERY CAN CAUSE SEVERE IRRITATION AND CHEMICAL BURNS.
IMMEDIATELY FLUSH EYES THOROUGHLY WITH WATER FOR AT LEAST 15 MINUTES,
LIFTING UPPER AND LOWER LIDS, UNTIL NO EVIDENCE OF THE CHEMICAL REMAINS.
SEEK MEDICAL ATTENTION.

NOTE:
NICKEL, NICKEL COMPOUNDS, CADMIUM, CADMIUM COMPOUNDS, COBALT, AND COBALT
COMPOUNDS ARE LISTED AS POSSIBLE CARCINOGENS BY INTERNATIONAL AGENCY FOR
RESEARCH ON CANCER (IARC) OR NATIONAL TOXICOLOGY PROGRAM (NTP).


SECTION V - PRECAUTIONS FOR SAFE HANDLING AND USE 


STORAGE:
STORE IN A COOL, WELL VENTILATED AREA. ELEVATED TEMPERATURES CAN RESULT IN
SHORTENED BATTERY LIFE.

MECHANICAL CONTAINMENT:
POTTING OR SEALING THE BATTERY IN AN AIRTIGHT OR WATERTIGHT CONTAINER IS
NOT RECOMMENDED. BATTERIES NORMALLY EVOLVE HYDROGEN WHICH, WHEN COMBINED
WITH OXYGEN FROM THE AIR, CAN PRODUCE A COMBUSTIBLE OR EXPLOSIVE MIXTURE
UNLESS VENTED. IF SUCH A MIXTURE IS PRESENT, SHORT CIRCUITS, HIGH
TEMPERATURE, OR STATIC SPARKS CAN CAUSE AN IGNITION.

DO NOT OBSTRUCT SAFETY RELEASE VENTS ON BATTERIES. ENCAPSULATION (POTTING)
OF BATTERIES WILL NOT ALLOW CELL VENTING AND CAN CAUSE HIGH PRESSURE
RUPTURE.

HANDLING:
ACCIDENTAL SHORT CIRCUIT FOR A FEW SECONDS WILL NOT SERIOUSLY AFFECT THE
BATTERY. HOWEVER, THIS BATTERY IS CAPABLE OF DELIVERING VERY HIGH SHORT
CIRCUIT CURRENTS. PROLONGED SHORT CIRCUITS WILL CAUSE HIGH CELL
TEMPERATURES WHICH CAN CAUSE SKIN BURNS. SOURCES OF SHORT CIRCUITS INCLUDE
JUMBLED BATTERIES IN BULK CONTAINERS, METAL JEWELRY, AND METAL COVERED
TABLES OR METAL BELTS USED FOR ASSEMBLY OF BATTERIES INTO DEVICES.

IF SOLDERING OR WELDING TO THE BATTERY IS REQUIRED, USE OF TABBED BATTERIES
IS RECOMMENDED. SOLDERING DIRECTLY TO THE CELL CAN DAMAGE THE BATTERY
SAFETY SEAL, CAUSE INTERNAL DAMAGE OR SHORT CIRCUIT THE CELL.

DO NOT OPEN BATTERY. THE NEGATIVE ELECTRODE MATERIAL MAY BE PYROPHORIC.
SHOULD AN INDIVIDUAL CELL FROM A BATTERY BECOME DISASSEMBLED, SPONTANEOUS
COMBUSTION OF THE NEGATIVE ELECTRODE IS POSSIBLE. THIS IS MUCH MORE LIKELY
TO HAPPEN IF THE ELECTRODE IS REMOVED FROM ITS METAL CONTAINER. THERE CAN
BE A DELAY BETWEEN EXPOSURE TO AIR AND SPONTANEOUS COMBUSTION.

CHARGING:
THIS BATTERY IS MADE TO BE CHARGED MANY TIMES. BECAUSE IT GRADUALLY LOSES
ITS CHARGE OVER A FEW MONTHS, IT IS GOOD PRACTICE TO CHARGE BATTERY BEFORE
USE. USE RECOMMENDED CHARGER. IMPROPER CHARGING CAN CAUSE HEAT DAMAGE OR
EVEN HIGH PRESSURE RUPTURE. OBSERVE PROPER CHARGING POLARITY.

LABELING:

IF THE LABEL OR PACKAGE WARNINGS ARE NOT VISIBLE, IT IS IMPORTANT TO
PROVIDE A PACKAGE AND/OR DEVICE LABEL STATING:

NICKEL CADMIUM CONSUMER ROUND CELLS AA AND LARGER:

WARNING:
CHARGE ONLY WITH STANDARD HOUSEHOLD NICKEL CADMIUM BATTERY CHARGERS. DO NOT
OPEN BATTERY, DISPOSE OF IN FIRE, PUT IN BACKWARDS, MIX WITH OTHER BATTERY
TYPES OR SHORT CIRCUIT - MAY EXPLODE, LEAK OR GET HOT CAUSING PERSONAL
INJURY.

AAA AND SMALLER:

WARNING:
(1) KEEP AWAY FROM SMALL CHILDREN. IF SWALLOWED, PROMPTLY SEE DOCTOR; HAVE
DOCTOR PHONE (202) 625-3333 COLLECT.

(2) CHARGE ONLY WITH STANDARD HOUSEHOLD NICKEL CADMIUM BATTERY CHARGERS.
DO NOT OPEN BATTERY, DISPOSE OF IN FIRE, PUT IN BACKWARDS, MIX WITH OTHER
BATTERY TYPES OR SHORT CIRCUIT - MAY EXPLODE, LEAK OR GET HOT CAUSING
PERSONAL INJURY.

ALL NICKEL CADMIUM PACKS (OEM AND BRANDED) AND NICKEL CADMIUM OEM ROUND
CELLS:

WARNING:
USE ONLY WITH SPECIFIED CHARGERS ACCORDING TO CHARGER MANUFACTURER'S
INSTRUCTIONS. DO NOT OPEN BATTERY, DISPOSE OF IN FIRE OR SHORT CIRCUIT -
MAY EXPLODE, LEAK OR GET HOT CAUSING PERSONAL INJURY.

DISPOSAL:
DISPOSE IN ACCORDANCE WITH ALL APPLICABLE FEDERAL, STATE, AND LOCAL
REGULATIONS.

WHEN GENERATED AS A WASTE, THESE BATTERIES MAY BE REGULATED BY THE RESOURCE
CONSERVATION AND RECOVERY ACT (RCRA) AS A D006 (CADMIUM) HAZARDOUS WASTE.

NOTE:
RECYCLING OF THIS PRODUCT MAY BE AVAILABLE. CONTACT YOUR LOCAL RECYCLING
OFFICE OR CALL TOLL FREE AT 1-800-8-BATTERY FOR INFORMATION ABOUT HOW AND
WHERE YOU CAN RECYCLE USED NICKEL CADMIUM BATTERIES.

THE FEDERAL UNIVERSAL WASTE RULE CITED AT 40 CFR PART 273 GOVERNS NICKEL
CADMIUM BATTERY RECYCLING AND MAY BE APPLICABLE IN YOUR STATE.


SECTION VI - SPECIAL PROTECTION INFORMATION 


VENTILATION REQUIREMENTS: NOT NECESSARY UNDER NORMAL CONDITIONS.

RESPIRATORY PROTECTION: NOT NECESSARY UNDER NORMAL CONDITIONS.

EYE PROTECTION:
NOT NECESSARY UNDER NORMAL CONDITIONS. WEAR SAFETY GLASSES WITH SIDE
SHIELDS IF HANDLING AN OPEN OR LEAKING BATTERY.

GLOVES:
NOT NECESSARY UNDER NORMAL CONDITIONS. USE NEOPRENE OR NATURAL RUBBER
GLOVES IF HANDLING AN OPEN OR LEAKING BATTERY.

OPEN BATTERY STORAGE:
BATTERY SHOULD NOT BE OPENED. SHOULD A CELL BECOME DISASSEMBLED, THE
ELECTRODE SHOULD BE STORED IN A FIREPROOF CABINET, AWAY FROM COMBUSTIBLES.


SECTION VII - REGULATORY INFORMATION 


THE TRANSPORTATION OF THE DRY CELL BATTERIES DESCRIBED IN THIS DOCUMENT IS
NOT REGULATED BY THE U.S. DEPARTMENT OF TRANSPORTATION OR THE MAJOR
INTERNATIONAL REGULATORY BODIES.

SARA/TITLE III:
AS AN ARTICLE, THIS BATTERY AND ITS CONTENTS ARE NOT SUBJECT TO THE
REQUIREMENTS OF THE EMERGENCY PLANNING AND COMMUNITY RIGHT-TO-KNOW ACT.

THIS MATERIAL SAFETY DATA SHEET IS APPLICABLE FOR THE FOLLOWING PRODUCT
NUMBERS:
CB0301, CB0302, CB0314, CB0323, CB0325, CB0331, CB0334, CB0343, CB0367,
CB0412, CB0455, CB0610, CB718, CBB212, CBB310, CBB346, CBB392, CBB688,
CBC310, CBC348, CBD366, CBD446, CBE22, CBE388, CBF222, CBG311, CBZ319S,
GP300SU, GP301AD, HBC520, HBV522, JBC962S, LBTX4000, NMG77, NMG98D, OBC84S,
PTB038, PTB048, PTBD130, PTBD140, PTBD145, PTBD18FS, PTC078, PTC090,
PTC151, PTC310, PTC943, PTD9050, PTM0100, PTM1014, PTM1210, PTM6043,
PTM9100, PTMW080, PTMW140, PTR1815, PTR1817, PTR652, PTR669, PTR671,
RBM7143C, RBZ300U, RBZ307MI, SPJ2000, WS-259601-C, WS-30000F-C,
WS-503002-C, WS-790001-C, WS-861000-C, WS-881000-C

THE INFORMATION CONTAINED IN THIS DOCUMENT IS PROVIDED FOR INFORMATION
ONLY. THE BATTERIES DESCRIBED IN THIS DOCUMENT ARE ARTICLES PURSUANT TO
29 CFR 1910.1200 AND, AS SUCH, ARE NOT SUBJECT TO THE OSHA HAZARD
COMMUNICATION STANDARD REQUIREMENT FOR PREPARATION OF A MATERIAL SAFETY
DATA SHEET. THE INFORMATION AND RECOMMENDATIONS IN THIS DOCUMENT ARE MADE
IN GOOD FAITH AND ARE BELIEVED TO BE ACCURATE AS OF THE DATE OF
PREPARATION. HOWEVER, LENMAR ENTERPRISES, INC., MAKES NO WARRANTY, EITHER
EXPRESS OR IMPLIED, WITH RESPECT TO THIS INFORMATION AND DISCLAIMS ALL
LIABILITY FROM RELIANCE ON IT.

COPYRIGHT 2006 LENMAR ENTERPRISES - SPECIFICATIONS SUBJECT TO CHANGE
WITHOUT NOTICE