Common Name: INCANDESCENT LAMPS (WITH LEAD-FREE SOLDER)
Manufacturer: WESTINGHOUSE LIGHTING
SDS Revision Date: 2/16/2009
SDS Format: No Format Specified
   
Item Number(s): 2CUW6, 2CUW7, 2CUW8, 2CUW9, 2CUX1, 2CUX2, 2CUX3, 2CUX4, 2CUX5, 2CUX6, 2CUX7, 2CUX8, 2CUX9, 2CUY1, 2CUY2, 2CUY3, 2CUY4, 2CUY5, 2CUY6, 2CUY7, 2CUY8, 2CUY9, 2CUZ1, 2CUZ2, 2CUZ3, 2PGX9, 2PGY1, 4TAA2
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
PRODUCT AND COMPANY IDENTIFICATION 
HAZARDOUS INGREDIENTS 
CHEMICAL/PHYSICAL DATA 
FIRE AND EXPLOSION DATA 
REACTIVITY DATA 
EMERGENCY FIRST AID 
PRECAUTIONS FOR SAFE HANDLING AND USE 
CONTROL MEASURES 



W
WESTINGHOUSE

INCANDESCENT LAMP (WITH LEAD-FREE SOLDER)

MATERIAL SAFETY DATA SHEET

(MSDS)

INCANDESCENT LAMPS (WITH LEAD-FREE SOLDER)

INFORMATION AND APPLICABILITY:
WESTINGHOUSE LIGHTING CORPORATION BELIEVES THAT UNDER THE OCCUPATIONAL
SAFETY AND HEALTH ADMINISTRATION (OSHA) HAZARDS COMMUNICATIONS STANDARD,
A LAMP (LIGHT BULB) IS EXEMPTED AS AN "ARTICLE" SO IT DOES NOT REQUIRE AN
MSDS. THE ORIGINAL OSHA STANDARD DEFINED AN ARTICLE AS SOMETHING THAT:
1) IS FORMED TO A SPECIFIC SHAPE AND DESIGN, 2) HAS END USE FUNCTIONS
DEPENDENT UPON ITS SHAPE AND DESIGN, AND 3) DOES NOT RELEASE OR OTHERWISE
RESULT IN AN EXPOSURE TO A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF
USE.

IN FEBRUARY, 1994, OSHA AMENDED THE HAZARD COMMUNICATION STANDARD AND
MODIFIED PART 3 OF THE ABOVE TO READ: 3) DOES NOT RELEASE MORE THAN VERY
SMALL QUANTITIES OF A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF USE.
STATE AND LOCAL REGULATIONS ALSO CONTAIN SIMILAR EXEMPTIONS FOR SUCH
ARTICLES.

HAZARDOUS MATERIALS ARE NOT RELEASED DURING NORMAL USE AND OPERATION OF
THESE LAMPS.


PRODUCT AND COMPANY IDENTIFICATION 


MANUFACTURER:
WESTINGHOUSE LIGHTING CORPORATION
12401 MCNULTY ROAD
PHILADELPHIA, PA 19154
1-800-248-6900


HAZARDOUS INGREDIENTS 


THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE INTACT.
IF LAMP IS BROKEN, SOME OF THE FOLLOWING MATERIALS MAY BE RELEASED:

CHEMICAL NAME        CAS NUMBER   HAZARD         EXPOSURE LIMITS IN AIR
                                                 (MG/CUBIC M)
                                                 ACGIH (TLV)    OSHA (PEL)

GLASS (SODA LIME)                 RESPIRATORY    10.0 (2)       15.0 (2)
                                  IRRITANT

SOLDER (Sb/Sn)

ANTIMONY (Sb)        7440-36-0    TOXIC          0.5            0.5

TIN (Sb)             7440-31-5    RESPIRATORY    2.0            2.0
                                  IRRITANT

(1.3) LEAD GLASS     7439-92-1    TOXIC          0.15           0.05
(AS Pb)

ALUMINUM             7429-90-5    RESPIRATORY    10.0           10.0
                                  IRRITANT

COPPER (AS DUST)     7440-50-8    RESPIRATORY    1.0            1.0
                                  IRRITANT

PHENOLIC RESIN                    PHYSICAL
                                  IRRITANT

(1) THESE CHEMICALS ARE SUBJECT TO THE REPORTING REQUIREMENTS OF SECTION
313 OF TITLE III OF THE SUPERFUND AMENDMENTS AND REAUTHORIZATION ACT OF
1986 AND 40 CFR PART 372.

(2) LIMITS AS NUISANCE PARTICULATE.

(3) THE LEAD IN THIS PRODUCT IS ONE OF THE SUBSTANCES KNOWN TO THE STATE
OF CALIFORNIA TO CAUSE REPRODUCTIVE TOXICITY IF INGESTED. CALIFORNIA SAFE
DRINKING WATER AND TOXIC ENFORCEMENT ACT OF 1986)


CHEMICAL/PHYSICAL DATA 


NOT APPLICABLE TO INTACT LAMP.


FIRE AND EXPLOSION DATA 


FLAMMABILITY: NON-COMBUSTIBLE

FIRE EXTINGUISHING MATERIALS:
USE EXTINGUISHING AGENTS SUITABLE FOR SURROUNDING FIRE.

SPECIAL FIREFIGHTING PROCEDURE:
USE A SELF-CONTAINED BREATHING APPARATUS TO PREVENT INHALATION OF DUST
AND/OR FUMES THAT MAY BE GENERATED FROM BROKEN LAMPS DURING FIREFIGHTING
ACTIVITIES.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
WHEN EXPOSED TO HIGH TEMPERATURE, TOXIC FUMES MAY BE RELEASED FROM BROKEN
LAMPS.


REACTIVITY DATA 


STABILITY: LAMP IS STABLE.

CONDITIONS TO AVOID: NONE FOR INTACT LAMPS

INCOMPATIBILITY (MATERIALS TO AVOID): NONE FOR INTACT LAMPS

HAZARDOUS DECOMPOSITION PRODUCTS: NONE FOR INTACT LAMPS

HAZARDOUS POLYMERIZATION PRODUCTS: WILL NOT OCCUR.

HEALTH CONCERNS:
THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE INTACT.
NO ADVERSE EFFECTS ARE EXPECTED FROM OCCASIONAL EXPOSURE TO BROKEN LAMPS.
AS A MATTER OF GOOD PRACTICE, AVOID PROLONGED OR FREQUENT EXPOSURE TO
BROKEN LAMPS UNLESS THERE IS ADEQUATE VENTILATION. THE MAJOR HAZARD FROM
BROKEN LAMPS IS THE POSSIBILITY OF BEING CUT BY THE BROKEN GLASS.

EFFECTS OF OVEREXPOSURE TO BROKEN LAMPS BY INHALATION, INGESTION, OR
CONTACT (SKIN OR EYE):

LEAD:
INGESTION AND INHALATION OF LEAD DUST OR FUME MUST BE AVOIDED. IRRITATION
OF THE EYES AND RESPIRATORY TRACT MAY OCCUR. EXCESSIVE LEAD ABSORPTION IS
TOXIC AND MAY INCLUDE SYMPTOMS SUCH AS ANEMIA, WEAKNESS, ABDOMINAL PAIN,
AND KIDNEY DISEASE.

ALL OTHER COMPONENTS OF THIS PRODUCT DO NOT POSE A SIGNIFICANT RUSH OF
RESPIRATORY AND PHYSICAL EFFECTS.


EMERGENCY FIRST AID 


GLASS CUTS:
PERFORM NORMAL FIRST AID PROCEDURES. SEEK MEDICAL ATTENTION AS REQUIRED.

INHALATION:
IF DISCOMFORT, IRRITATION OR SYMPTOMS OF PULMONARY INVOLVEMENT DEVELOP,
REMOVE FROM EXPOSURE AND SEEK MEDICAL ATTENTION.

INGESTION:
IN THE UNLIKELY EVENT OF INGESTING A LARGE QUANTITY OF MATERIAL, SEEK
MEDICAL ATTENTION IMMEDIATELY.

CONTACT SKIN:
THOROUGHLY WASH AFFECTED AREA WITH MILD SOAP OR DETERGENT AND WATER AND
PREVENT FURTHER CONTACT. SEEK MEDICAL ATTENTION AS NEEDED.

CONTACT EYE:
WASH EYES, INCLUDING UNDER EYELIDS, IMMEDIATELY WITH COPIOUS AMOUNT OF
WATER FOR 15 MINUTES. SEEK MEDICAL ATTENTION.

CARCINOGENIC ASSESSMENT (NTP ANNUAL REPORT. IARC MONOGRAPHS, OTHER): NONE


PRECAUTIONS FOR SAFE HANDLING AND USE 


IF LAMPS ARE BROKEN, VENTILATE AREA WHERE BREAKAGE OCCURRED. CLEAN-UP BY
VACUUMING OR OTHER METHOD THAT AVOIDS DUST GENERATION. TAKE USUAL
PRECAUTIONS FOR COLLECTION OF BROKEN GLASS. PLACE MATERIALS IN CLOSED
CONTAINERS TO AVOID GENERATING DUST.

IT IS THE RESPONSIBILITY OF THE WASTE GENERATOR TO ENSURE PROPER
CLASSIFICATION OF WASTE PRODUCTS. TO THAT END, TCLP TESTS SHOULD BE
CONDUCTED ON ALL WASTE PRODUCTS, INCLUDING THIS ONE, TO DETERMINE THE
ULTIMATE DISPOSITION IN ACCORDANCE WITH APPLICABLE FEDERAL, STATE AND LOCAL
REGULATIONS.


CONTROL MEASURES 


VENTILATION:
USE ADEQUATE GENERAL AND LOCAL EXHAUST VENTILATION TO MAINTAIN EXPOSURE
LEVELS BELOW THE PEL OR TLV LIMITS. IF SUCH VENTILATION IS UNAVAILABLE,
USE RESPIRATORS AS SPECIFIED BELOW.

RESPIRATORY PROTECTION:
USE APPROPRIATE NIOSH APPROVED RESPIRATOR IF AIRBORNE DUST CONCENTRATIONS
EXCEED THE PERTINENT PEL OR TLV LIMITS. ALL APPROPRIATE REQUIREMENTS SET
FORTH IN 29 CFR 1910.134 SHOULD BE MET.

EYE PROTECTION:
OSHA SPECIFIED SAFETY GLASSES, GOGGLES OR FACE SHIELD ARE RECOMMENDED FOR
DEALING WITH BROKEN LAMPS.

PROTECTIVE CLOTHING:
OSHA SPECIFIED GLOVES ARE RECOMMENDED FOR DEALING WITH BROKEN LAMPS.

HYGIENIC PRACTICES:
AFTER HANDLING BROKEN LAMPS, WASH THOROUGHLY BEFORE EATING, SMOKING OR
USING TOILET FACILITIES.

ISSUE DATE: FEBRUARY 16, 2009

CALL 1-800-999-2226 OR VISIT WWW.WESTINGHOUSELIGHTING.COM

WESTINGHOUSE LIGHTING CORPORATION
PHILADELPHIA, PA 19154-1029
U.S.A.

WESTINGHOUSE LIGHTING CORPORATION, A WESTINGHOUSE ELECTRIC CORPORATION
LICENSEE

W
"WESTINGHOUSE" AND "YOU CAN BE SURE...IF IT'S WESTINGHOUSE" ARE ALL
REGISTERED TRADEMARKS OF WESTINGHOUSE ELECTRIC CORPORATION

YOU CAN BE SURE...IF IT'S WESTINGHOUSE
W

(C) 2012 WESTINGHOUSE LIGHTING CORPORATION/WLC/1012/102342