Common Name: COMPACT FLUORESCENT LAMPS - TWISTS, FLOODS, GLOBES, A-BULBS, TORPEDO AND PIN-BAS
Manufacturer: WESTINGHOUSE LIGHTING
SDS Revision Date: 2/16/2009
SDS Format: No Format Specified
   
Grainger Item Number(s): 2CEK1, 2CEK2, 2CEK3, 2CEK4, 2CEK5, 2CEK6, 2CEK7, 2CEK8, 2CEK9, 2CEL1, 2CEL2, 2CEL3, 2CEL4, 2CEL5, 2CEL6, 2CEL7, 2CEL8, 2CEL9, 2CEN1, 2CEN2, 2CUR9, 2CUT1, 2CUT2, 2CUT3, 2CUT4, 2CUT5, 2CUT6, 2CUT7, 2CUT8, 2CUT9, 2CUU1, 2CUU2, 2CUU3, 2CUU4, 2CUU5, 2CUU6, 2CUU7, 2CUU8, 2CUU9, 2CUV1, 2CUV2, 2CUV3, 2CUV4, 2CUV5, 2CUV6, 2CUV7, 2CUV8, 2CUV9, 2CUW1, 2CUW2, 2CUW3, 2CUW4, 2CUW5, 3EMT8, 3EMT9, 3EMU1, 3EMU2, 3EMU3, 3EMU4, 3EMU5, 3EMU6, 3EMU7, 3EMU8, 3EMU9, 3EMV1, 3EMV2, 3EMV3, 3EMV4, 3EMV5, 3EMV6, 3EMV7, 3EMV8, 3EMV9, 3EMW1, 3EMW2, 3EMW3, 3EMW4, 3EMW5, 3EMW6, 3EMW7, 3EMW8, 3EMW9, 3EMX1, 3EMX2, 3EMX3, 3EMX4, 3EMX5, 3EMX6, 3EMX7, 3EMX8, 3EMX9, 3EMY1, 3EMY2, 3EMY3, 3EMY4, 3EMY5, 3TFP5, 3TFP6, 3TFP7, 3TFP8, 3TFP9, 3TFR1, 3TFR2, 3TFR3, 3TFR4, 5MRK6, 5MRK7, 5MRK8, 5MRK9, 5MRL0
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
PRODUCT AND COMPANY IDENTIFICATION 
COMPOSITION/INFORMATION ON INGREDIENTS 
PHYSICAL PROPERTIES 
EXPLOSION HAZARDS 
PROCEDURE FOR DISPOSAL OF LAMPS 



W
WESTINGNOUSE

COMPACT FLUORESCENT LAMP

MATERIAL SAFETY DATA SHEET

(MSDS)

COMPACT FLUORESCENT LAMPS - TWISTS, FLOODS, GLOBES, A-BULBS, TORPEDO AND
PIN-BASED LAMPS

INFORMATION AND APPLICABILITY:
WESTINGHOUSE LIGHTING CORPORATION BELIEVES THAT UNDER THE OCCUPATIONAL
SAFETY AND HEALTH ADMINISTRATION (OSHA) HAZARDS COMMUNICATIONS STANDARD,
A LAMP (LIGHT BULB) IS EXEMPTED AS AN "ARTICLE" SO IT DOES NOT REQUIRE AN
MSDS. THE ORIGINAL OSHA STANDARD DEFINED AN ARTICLE AS SOMETHING THAT:
1) IS FORMED TO A SPECIFIC SHAPE AND DESIGN, 2) HAS END USE FUNCTIONS
DEPENDENT UPON ITS SHAPE AND DESIGN, AND 3) DOES NOT RELEASE OR OTHERWISE
RESULT IN AN EXPOSURE TO A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF
USE.

IN FEBRUARY, 1994, OSHA AMENDED THE HAZARD COMMUNICATION STANDARD AND
MODIFIED PART 3 OF THE ABOVE TO READ: 3) DOES NOT RELEASE MORE THAN VERY
SMALL QUANTITIES OF A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF USE.
STATE AND LOCAL REGULATIONS ALSO CONTAIN SIMILAR EXEMPTIONS FOR SUCH
ARTICLES.

HAZARDOUS MATERIALS ARE NOT RELEASED DURING NORMAL USE AND OPERATION OF
THESE LAMPS.


PRODUCT AND COMPANY IDENTIFICATION 


TRADE NAMES INCLUDE:
MINI-TWIST(TM), MINI-SPIRAL, TWIST(R*), SPIRAL, TRIPLE(TM), GLOBE,
REFLECTOR, 3-WAY. THESE LAMPS ARE FOR USE IN GENERAL LIGHTING APPLICATIONS.
THESE CFLS CAN CONSIST OF LAMP BALLAST/ADAPTER AS A SINGLE UNIT, OR LAMP
ALONE WITH NO BALLAST/ADAPTER.

MANUFACTURER:
WESTINGHOUSE LIGHTING CORPORATION
12401 MCNULTY ROAD
PHILADELPHIA, PA 19154
1-800-999-2226


COMPOSITION/INFORMATION ON INGREDIENTS 


THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS WHICH ARE NOT
BROKEN OR DAMAGED IN ANY WAY.

LAMP ASSEMBLY - GLASS AND METAL:
THE GLASS IS MADE FROM SODA LIME, A SIMILAR TYPE OF GLASS THAT IS USED
THROUGHOUT THE GLASS INDUSTRY FOR OTHER CONSUMER ITEMS. THE METALS FOR END
CAPS AND FILAMENTS ARE GENERALLY MADE FROM VARIOUS AMOUNTS OF ALUMINUM,
TIN, LEAD, COPPER, ZINC AND NICKEL. IF THE LAMP BROKE, NONE OF THESE
MATERIALS WOULD PRESENT A POTENTIAL HAZARD, ASIDE FROM POSSIBLE INJURY DUE
TO BROKEN GLASS.

MERCURY:
SMALL AMOUNTS OF MERCURY ARE USED IN ALL FLUORESCENT LAMPS (GENERALLY
AROUND 0.025% BY WEIGHT). THE AMOUNT OF MERCURY IN ANY GIVEN LAMP VARIES
DEPENDING ON BOTH THE SIZE OF THE LAMP AND ON THE EQUIPMENT THAT WAS USED
IN ITS PRODUCTION. WESTINGHOUSE LIGHTING CONTINUES TO REDUCE THE AMOUNTS
OF MERCURY USED IN FLUORESCENT PRODUCTS.

PHOSPHOR:
(NUISANCE DUST) PHOSPHATE MIX USING MANGANESE, RARE EARTH ELEMENTS SUCH AS
LANTHANUM, AND YTTRIUM AS EITHER AN OXIDE OR AS A PHOSPHATE, ALONG WITH A
BARIUM/ALUMINUM OXIDE ARE ALL TIGHTLY BOUND IN THE PHOSPHOR MATRIX.
THE PHOSPHORS PRODUCE BETTER LAMP EFFICIENCY AND COLOR RENDITION. THE
PHOSPHOR COMPONENTS MAY VARY SLIGHTLY DEPENDING ON THE COLOR OF THE LAMP.
SOME LAMPS MAY CONTAIN A THIN COATING OF TIN OXIDE INSIDE THE GLASS.


PHYSICAL PROPERTIES 


NOT APPLICABLE TO A LAMP NOT BROKEN OR DAMAGED.


EXPLOSION HAZARDS 


WHEN EXPOSED TO HIGH TEMPERATURES, TOXIC FUMES MAY BE EMITTED FROM BROKEN
LAMPS.

HEALTH CONCERNS:
THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE NOT
BROKEN OR DAMAGED. NO ADVERSE EFFECTS ARE EXPECTED FROM OCCASIONAL EXPOSURE
TO BROKEN LAMPS. AS A MATTER OF GOOD PRACTICE, AVOID PROLONGED OR FREQUENT
EXPOSURE TO BROKEN LAMPS UNLESS THERE IS ADEQUATE VENTILATION. THE MAJOR
HAZARD FROM BROKEN LAMPS IS THE POSSIBILITY OF BEING CUT BY THE BROKEN
GLASS.

MERCURY:
THE IN THE AIR AS A RESULT OF BREAKING ONE OR A SMALL NUMBER OF FLUORESCENT
LAMPS SHOULD NOT RESULT IN SIGNIFICANT DAMAGE. HOWEVER, WHEN MERCURY
BREAKING A LARGE NUMBER OF LAMPS FOR DISPOSAL, APPROPRIATE INDUSTRIAL
HYGIENE MONITORING AND CONTROLS SHOULD BE IMPLEMENTED TO MINIMIZE AIRBORNE
LEVELS OF MERCURY OR SURFACE CONTAMINATION. WE RECOMMEND A WELL-VENTILATED
AREA, AND LOCAL EXHAUST VENTILATION OR PERSONAL PROTECTIVE EQUIPMENT.

PHOSPHOR:
THERE HAVE BEEN NO SIGNIFICANT ADVERSE EFFECTS ON HUMANS BY INGESTION,
INHALATION, SKIN CONTACT OR EYE CONTACT. ANTIMONY, MANGANESE, YTTRIUM AND
TIN COMPOUNDS ARE CHARACTERIZED BY OSHA AS HAZARDOUS CHEMICALS, HOWEVER,
DUE TO THEIR INSOLUBILITY AS WELL AS THEIR RELATIVELY LOW TOXICITY AND
SMALL AMOUNT PRESENT IN THE PHOSPHOR AND LAMP, THESE MATERIALS DO NOT
PRESENT A SIGNIFICANT HAZARD IN THE EVENT OF THE LAMP BEING BROKEN.

GLASS:
GLASS DUST IS CONSIDERED TO BE PHYSIOLOGICALLY INERT SO IT HAS AN OSHA
EXPOSURE LIMIT OF 15-MG/CUBIC METER FOR TOTAL DUST, AND 5-MG/CUBIC METER
FOR RESPIRABLE DUST. IF GLASS DUST IS INHALED OR INGESTED, PERFORM NORMAL
FIRST AID PROCEDURES AND SEEK MEDICAL ATTENTION IF NEEDED.

INHALATION:
IF DISCOMFORT, IRRITATION OR SYMPTOMS OF PULMONARY DISTRESS DEVELOP, LEAVE
THE SITE OF EXPOSURE AND SEEK MEDICAL ATTENTION.

INGESTION: IN THE UNLIKELY EVENT OF INGESTION, SEEK MEDICAL ATTENTION.

CONTACT EYE/SKIN:
WASH SKIN OR FLUSH EYES, INCLUDING UNDER EYELIDS, IMMEDIATELY AND SEEK
MEDICAL ATTENTION.


PROCEDURE FOR DISPOSAL OF LAMPS 


TAKE THE USUAL PRECAUTIONS FOR GETTING RID OF BROKEN GLASS. PLACE MATERIALS
IN CLOSED CONTAINERS TO AVOID GENERATING DUST. A TOXICITY CHARACTERISTIC
LEACHING PROCEDURE (TCLP) WAS CONDUCTED ON THESE PRODUCTS SHOWING THE
MERCURY CONTENT IN THESE LAMPS IS NOT CONSIDERED HAZARDOUS WASTE. FOR FIELD
DISPOSAL, THE LEAD IN THE SOLDERING IS CONSIDERED HAZARDOUS WASTE AND MUST
BE DISPOSED OF BY APPLICABLE FEDERAL, STATE AND LOCAL REGULATIONS.

ALTHOUGH WESTINGHOUSE LIGHTING ATTEMPTS TO PROVIDE CURRENT AND ACCURATE
INFORMATION, IT MAKES NO REPRESENTATION REGARDING THE ACCURACY OF
COMPLETENESS OF THE INFORMATION AND ASSUMES NO LIABILITY FOR ANY LOSS,
DAMAGE OR INJURY OF ANY KIND WHICH MAY RESULT FROM OR ARISE OUT OF THE USE
OF/OR RELIANCE ON THIS INFORMATION.

ISSUE DATE: FEBRUARY 16, 2009

CALL:
1-800-999-2226 EST/CST, 1-800-421-3433 PST/MST OR LOG ON AT
WWW.WESTINGHOUSELIGHTBULBS.COM

WESTINGHOUSE LIGHTING CORPORATION
PHILADELPHIA, PA 19154-1029
U.S.A.

WESTINGHOUSE LIGHTING CORPORATION, A WESTINGHOUSE ELECTRIC CORPORATION
LICENSEE

W
"WESTINGHOUSE" AND "YOU CAN BE SURE. IF IT'S WESTINGHOUSE" ARE ALL
REGISTERED TRADEMARKS OF WESTINGHOUSE ELECTRIC CORPORATION (C)2009
WESTINGHOUSE LIGHTING CORPORATION / 0209

YOU CAN BE SURE...IF IT'S WESTINGHOUSE
W