Common Name: LED REPLACEMENT LAMPS - GENERAL PURPOSE AND PROFESSIONAL SERIES LAMPS
Manufacturer: WESTINGHOUSE LIGHTING
SDS Revision Date: 11/21/2012
SDS Format: No Format Specified
   
Grainger Item Number(s): 6GEM2, 6GEM3, 6GEM4, 6GEM5, 6GEM6, 6GEM7, 6GEM8, 6GEM9
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
PRODUCT AND COMPANY IDENTIFICATION 
LAMP MATERIALS AND HAZARDOUS INGREDIENTS 
PROCEDURE FOR DISPOSAL OF LAMPS 



W
WESTINGHOUSE

LED REPLACEMENT LAMP

MATERIAL SAFETY DATA SHEET

(MSDS)

LED REPLACEMENT LAMPS - GENERAL PURPOSE(TM) AND PROFESSIONAL SERIES LAMPS

INFORMATION AND APPLICABILITY:
WESTINGHOUSE LIGHTING CORPORATION BELIEVES THAT UNDER THE OCCUPATIONAL
SAFETY AND HEALTH ADMINISTRATION (OSHA) HAZARDS COMMUNICATIONS STANDARD, A
LAMP (LIGHT BULB) IS EXEMPTED AS AN "ARTICLE" SO IT DOES NOT REQUIRE AN
MSDS. THE ORIGINAL OSHA STANDARD DEFINED AN ARTICLE AS SOMETHING THAT:
1) IS FORMED TO A SPECIFIC SHAPE AND DESIGN, 2) HAS END USE FUNCTIONS
DEPENDENT UPON ITS SHAPE AND DESIGN, AND 3) DOES NOT RELEASE OR OTHERWISE
RESULT IN AN EXPOSURE TO A HAZARDOUS CHEMICAL UNDER NORMAL CONDITIONS OF
USE.

IN FEBRUARY, 1994, OSHA AMENDED THE HAZARD COMMUNICATION STANDARD AND
MODIFIED PART 3 OF THE ABOVE TO READ:
3) DOES NOT RELEASE MORE THAN VERY SMALL QUANTITIES OF A HAZARDOUS CHEMICAL
UNDER NORMAL CONDITIONS OF USE. STATE AND LOCAL REGULATIONS ALSO CONTAIN
SIMILAR EXEMPTIONS FOR SUCH ARTICLES.

HAZARDOUS MATERIALS ARE NOT RELEASED DURING NORMAL USE AND OPERATION OF
THESE LAMPS.


PRODUCT AND COMPANY IDENTIFICATION 


GENERAL PURPOSE LED LAMPS ARE PERFECT FOR EVERYDAY APPLICATIONS. IDEAL FOR
GENERAL ILLUMINATION AND OFFER EXCELLANT COLOR QUALITY WHILE CONSERVING
ENERGY. PROFESSIONAL SERIES LED LAMPS ARE DESIGNED FOR MORE DEMANDING
DIRECTIONAL APPLICATIONS THAT REQUIRE HIGHER LUMENS AND MORE NARROW BEAM
SPREADS.

MANUFACTURER: WESTINGHOUSE LIGHTING CORPORATION

12401 MCNULTY ROAD
PHILADELPHIA, PA 19154
1-800-999-2226.


LAMP MATERIALS AND HAZARDOUS INGREDIENTS 


THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LED LAMPS THAT ARE
INTACT.

LAMP ASSEMBLY - GLASS AND METAL:
THE GLASS GLOBE USED IN SOME OF THE LED LAMP IS MANUFACTURED FROM SODA LIME
GLASS AND IS ESSENTIALLY SIMILAR BUT NOT IDENTICAL TO THAT USED THROUGHOUT
THE GLASS INDUSTRY FOR INCANDESCENT LAMPS, BOTTLES AND OTHER COMMON
CONSUMER ITEMS. SOME OF THE GLASS GLOBES MAY CONTAIN A THIN COATING OF CLAY
AND SILICA INSIDE THE SURFACE OF THE GLASS. THE LAMP BASES ARE GENERALLY
NICKEL PLATED BRASS. NONE OF THESE MATERIALS WOULD PRESENT A HAZARD IN THE
EVENT OF BREAKAGE OF THE LAMP, ASIDE FROM THE OBVIOUS ONES DUE TO BROKEN
GLASS.

LED:
REPLACEMENT LAMPS USE LEDS THAT EMIT WHITE LIGHT. THE LED'S COMPOSITION
CONSISTS OF METALS, PHOSPHOR, PLASTICS AND INGAN (INDIUM GALLIUM NITRIDE)
SEMICONDUCTOR CHIP. DUE TO THEIR INSOLUBILITY AND INERTNESS, THESE
MATERIALS DO NOT PRESENT A SIGNIFICANT HAZARD.

ELECTRONIC LED DRIVER:
THE ELECTRONIC LED DRIVER IS BUILT INTO THE LAMP HOUSING. THE DRIVER
CONSISTS OF PARTS THAT ARE ESSENTIALLY SIMILAR, BUT NOT IDENTICAL, TO THOSE
USED THROUGHOUT THE ELECTRONICS INDUSTRY FOR OTHER COMMON CONSUMER
ELECTRONIC EQUIPMENT.

PLASTIC MATERIAL:
THE PLASTIC HOUSING IS TYPICALLY MADE OF PBT (POLYBUTYLENE TEREPHTHALATE)
OR PC (POLYCARBONATE) FIRE RETARDED PLASTIC WITH A BROMINE CONTAINING
POLYMER AND ANTIMONY OXIDE. THE PLASTIC HOUSING IS GLASS FIBER FILLED. THIS
PRODUCT CONSISTS PRIMARILY OF HIGH MOLECULAR WEIGHT POLYMERS THAT ARE NOT
HAZARDOUS.

HEALTH CONCERNS:
THERE ARE NO KNOWN HEALTH HAZARDS FROM EXPOSURE TO LAMPS THAT ARE INTACT.
NO ADVERSE EFFECTS ARE EXPECTED FROM OCCASIONAL EXPOSURE TO BROKEN LAMPS.
IF THE LAMP IS BROKEN AND THE LEDS ARE EXPOSED, DO NOT LOOK DIRECTLY INTO
THE LEDS. AS A MATTER OF GOOD PRACTICE, AVOID PROLONG OR FREQUENT EXPOSURE
TO BROKEN LAMPS. THE MAJOR HAZARD FROM BROKEN LAMPS IS THE POSSIBILITY OF
SUSTAINING CUTS FROM THE GLASS AND EYE INJURY IF YOU LOOK DIRECTLY INTO
EXPOSED LEDS WHEN EMITTING LIGHT.

UV:
THE ULTRAVIOLET ENERGY EMITTED BY LED LAMPS COMPLIES WITH THE
PHOTOBIOLOGICAL SAFETY OF LAMPS IEC 62471.


PROCEDURE FOR DISPOSAL OF LAMPS 


DISPOSE IN ACCORDANCE WITH LOCAL REGULATIONS; RECYCLING IS RECOMMENDED FOR
LARGE QUANTITY DISPOSAL. ALL LAMPS SOLD MEET THE EC DIRECTIVE 2011/65/EU
FOR ROHS (RESTRICTION OF HAZARDOUS SUBSTANCES) AND EC DIRECTIVE
2006/1907/EC REACH (REGISTRATION, EVALUATION, AUTHORIZATION AND RESTRICTION
OF CHEMICALS).

ALTHOUGH WESTINGHOUSE LIGHTING ATTEMPTS TO PROVIDE CURRENT AND ACCURATE
INFORMATION, IT MAKES NO REPRESENTATION REGARDING THE ACCURACY OF
COMPLETENESS OF THE INFORMATION AND ASSUMES NO LIABILITY FOR ANY LOSS,
DAMAGE OR INJURY OF ANY KIND WHICH MAY RESULT FROM OR ARISE OUT OF THE USE
OF/OR RELIANCE ON THIS INFORMATION.

ISSUE DATE: NOVEMBER 21, 2012

CALL: 1-800-999-2226 OR VISIT WWW.WESTINGHOUSELIGHTING.COM

WESTINGHOUSE LIGHTING CORPORATION
PHILADELPHIA, PA 19154-1029
U.S.A.

WESTINGHOUSE LIGHTING CORPORATION, A WESTINGHOUSE ELECTRIC CORPORATION
LICENSEE

W
"WESTINGHOUSE" AND "YOU CAN BE SURE...IF IT'S WESTINGHOUSE" ARE ALL
REGISTERED TRADEMARKS OF WESTINGHOUSE ELECTRIC CORPORATION

YOU CAN BE SURE...IF IT'S WESTINGHOUSE
W

(C)2012 WESTINGHOUSE LIGHTING CORPORATION/WLC/1012/102342