Common Name: 1C HUMIDIFIER CLEANER
Manufacturer: RPS PRODUCTS
SDS Revision Date: 11/1/2005
SDS Format: No Format Specified
   
Grainger Item Number(s): 21EX24
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
A. IDENTIFICATION AND EMERGENCY INFORMATION 
B. COMPONENTS AND HAZARD INFORMATION 
C. EMERGENCY AND FIRST AID PROCEDURES 
D. FIRE AND EXPLOSION HAZARD INFORMATION 
E. HEALTH AND HAZARD INFORMATION 
F. PHYSICAL DATA 
G. REACTIVITY 
H. SPILL OR LEAK PROCEDURES 
I. PROTECTION AND PRECAUTIONS 
J. TRANSPORTATION INFORMATION 



1C HUMIDIFIER CLEANER

RPS PRODUCTS, INC.
281 KEYES AVENUE
HAMPSHIRE, IL 60140
(847-683-3400)

MATERIAL SAFETY DATA SHEET


A. IDENTIFICATION AND EMERGENCY INFORMATION 


PRODUCT IDENTITY: 1C HUMIDIFIER CLEANER

EMERGENCY TELEPHONE NUMBERS:
R.P.S. PRODUCTS: 847-683-3400
CHEMTREC: 800-424-9300


B. COMPONENTS AND HAZARD INFORMATION 


HAZARDOUS COMPONENTS (SPECIFIC CHEMICAL IDENTITY):

(COMMON NAME(S))             CAS NUMBER   OSHA PEL  ACGIH TLV  % PERCENT

HYDROCHLORIC/MURIATIC ACID   7647-01-0    5 PPM     5 PPM      11 (302,311,
                                                               312, 313)

HMIS (HAZARDOUS MATERIALS IDENTIFICATION SYSTEM):
HEALTH       3
FLAMMABILITY 0
REACTIVITY   0


C. EMERGENCY AND FIRST AID PROCEDURES 


EYE CONTACT:
IMMEDIATELY FLUSH EYES WITH PLENTY OF FLOWING WATER FOR 30 MINUTES LIFTING
UPPER AND LOWER LIDS. REMOVE CONTACT LENSES IF APPLICABLE. SEEK MEDICAL
ATTENTION IMMEDIATELY.

SKIN CONTACT:
IMMEDIATELY FLUSH WITH PLENTY OF SOAP AND WATER FOR AT LEAST 30 MINUTES.
IF IRRITATION DEVELOPS, SEEK MEDICAL ATTENTION.

INHALATION:
REMOVE PERSON TO FRESH AIR. IF BREATHING IS DIFFICULT, GIVE OXYGEN.
IF BREATHING HAS STOPPED, RESUSCITATE AND SEEK MEDICAL ATTENTION.

INGESTION:
IF INGESTED, DO NOT INDUCE VOMITING. HAVE PATIENT LIE DOWN AND KEEP WARM.
VOMITING MAY LEAD TO SEVERE DAMAGE TO ESOPHAGUS, WHICH MAY BE FATAL. GIVE
LARGE AMOUNTS OF WATER. GIVE AT LEAST ONE OUNCE OF MILK OF MAGNESIA OR
ALUMINUM HYDROXIDE GEL IN AN EQUAL AMOUNT OF WATER, IF UNAVAILABLE GIVE THE
WHITE OF TWO OR THREE EGGS. NEVER GIVE ANYTHING BY MOUTH TO AN UNCONSCIOUS
PERSON.


D. FIRE AND EXPLOSION HAZARD INFORMATION 


FLASH POINT: N/A
METHOD USED: N/A

FLAMMABILITY CLASSIFICATION: NON-COMBUSTIBLE

FIRE AND EXPLOSION HAZARDS:
REACTS WITH MOST METALS PRODUCING HYDROGEN, WHICH IS EXTREMELY FLAMMABLE
AND MAY EXPLODE.

(NFPA) NATIONAL FIRE PROTECTION ASSOCIATION - HAZARD INFORMATION:
HEALTH       3
FLAMMABILITY 0
REACTIVITY   0

HANDLING PRECAUTIONS:
USE ONLY WITH ADEQUATE VENTILATION. DO NOT STORE ABOVE 49C/120F.


E. HEALTH AND HAZARD INFORMATION 


EFFECTS OF OVEREXPOSURE (SIGNS AND SYMPTOMS OF EXPOSURE):

POISON-CALL PHYSICIAN IMMEDIATELY!

EYE CONTACT:
PRODUCT CONTACTING THE EYES MAY CAUSE REDNESS, TEARING AND SEVERE BURNS.
RINSE EYES THOROUGHLY FOR 30 MINUTES. SEEK MEDICAL ATTENTION.

SKIN CONTACT:
CONTACT WITH SKIN MAY CAUSE SEVERE BURNS TO THE SKIN, DEFATTING, AND
DERMATITIS IF NOT WASHED IMMEDIATELY.

INHALATION:
AFTER HIGH VAPOR EXPOSURE, REMOVE TO FRESH AIR. IF BREATHING IF DIFFICULT,
GIVE OXYGEN. IF BREATHING HAS STOPPED GIVE ARTIFICIAL RESPIRATION.

INGESTION:
IF SWALLOWED, DO NOT INDUCE VOMITING!

MOUTH MAY BE RINSED WITH WATER. IF SWALLOWED, GIVE LARGE QUANTITIES OF
WATER. NEVER GIVE ANYTHING BY MOUTH TO AN UNCONSCIOUS PERSON. SEEK MEDICAL
ATTENTION IMMEDIATELY.

CANCER HAZARD:
THIS PRODUCT HAS NO CARCINOGENS LISTED BY IARC, NTP, NIOSH, OSHA, OR ACGIH
AS OF THIS DATE, GREATER OR EQUAL TO 0.1%.


F. PHYSICAL DATA 


THE FOLLOWING DATA ARE APPROXIMATE OR TYPICAL VALUES AND SHOULD BE USED FOR
PRECISE DESIGN PURPOSES.

BOILING RANGE: 81 97 100*DEG. C/178 206 212*DEG. F (*=END POINT)

API GRAVITY: 4.6

SPECIFIC GRAVITY (WATER=1): 1.039

POUNDS/GALLON: 8.658

VAPOR PRESSURE (MM OF HG) @ 20 C: 16.5

VAPOR DENSITY (AIR=1): 0.8

WATER ABSORPTION: COMPLETE

ACID ABSORPTION (85% H2SO4): COMPLETE

DRY TIME (ETHER=1): LONG

% VOLATILE BY VOL: 98.0

APPEARANCE: CLEAR, LIGHT BLUE

ODOR: MILD

REACTIVE INDEX: 1.325


G. REACTIVITY 


STABLE, BUT REACTS WITH MOST METALS PRODUCING HYDROGEN, WHICH IS EXTREMELY
FLAMMABLE AND MAY EXPLODE.

CONDITIONS TO AVOID: ISOLATE FROM OXIDIZERS, HEAT, AND OPEN FLAME.

MATERIALS TO AVOID:
ISOLATE FROM ALKALIES, AMINES, AND NON-RESISTANT METALS.

HAZARDOUS: CARBON MONOXIDE, CARBON DIOXIDE.

DECOMPOSITION: HYDROGEN CHLORIDE, PHOSGENE FROM HEATING.


H. SPILL OR LEAK PROCEDURES 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
AVOID PERSONAL CONTACT. STOP SPILL AT SOURCE. DIKE AREA AND CONTAIN.
NEUTRALIZE WITH SODA ASH AND DILUTE WITH PLENTY OF WATER. PUMP LIQUID TO
SALVAGE TANK. REMAINING RESIDUE MAY BE TAKEN UP ON ABSORBENT MATERIAL AND
SHOVELED INTO CONTAINERS. DISPOSE OF IN ACCORDANCE WITH ALL LOCAL, STATE
AND FEDERAL REGULATIONS.


I. PROTECTION AND PRECAUTIONS 


VENTILATION:
USE LOCAL EXHAUST TO CAPTURE EXCESSIVE VAPOR, MISTS OR FUMES.

RESPIRATORY PROTECTION:
USE SUPPLIED-AIR RESPIRATORY PROTECTION IN CONFINED OR ENCLOSED SPACES.

MECHANICAL (GENERAL): OSHA ACCEPTABLE

PROTECTIVE GLOVES:
USE CHEMICAL-RESISTANT GLOVES, IF NEEDED, TO AVOID PROLONGED OR REPEATED
SKIN CONTACT.

EYE PROTECTION:
USE SPLASH GOGGLES OR FACE SHIELD WHEN EYE CONTACT MAY OCCUR.

OTHER PROTECTIVE EQUIPMENT:
USE CHEMICAL RESISTANT APRON OR OTHER IMPERVIOUS CLOTHING AT ALL TIMES WHEN
USING OR TRANSPORTING THIS PRODUCT TO AVOID CONTACT.

WORK PRACTICES/ENGINEERING CONTROLS:
KEEP CONTAINER TIGHTLY CLOSED AND UPRIGHT WHEN NOT IN USE TO PREVENT
LEAKAGE. KEEP OUT OF REACH OF CHILDREN.

PERSONAL HYGIENE:
CLEANSE SKIN THOROUGHLY AFTER CONTACT, BEFORE BREAKS AND MEALS, AND AT END
OF WORK PERIOD. REMOVE AND WASH CONTAMINATED CLOTHING BEFORE REUSE.
(DISCARD CONTAMINATED SHOES) MAINTAIN GOOD PERSONAL HYGIENE.

ADDITIONAL INFORMATION:
PERSONS WITH SEVERE SKIN, LIVER OR KIDNEY PROBLEMS SHOULD AVOID USE.


J. TRANSPORTATION INFORMATION 


FOR FURTHER INFORMATION RELATIVE TO SPILLS RESULTING FROM TRANSPORTATION
INCIDENTS, REFER TO LATEST DEPARTMENT OF TRANSPORTATION EMERGENCY RESPONSE
GUIDEBOOK FOR HAZARDOUS MATERIALS INCIDENTS.

LOWEST KNOWN LD50 (ORAL): 0 3000MG/KG (RATS)

ATTENTION:
THIS CONTAINER HAZARDOUS WHEN EMPTIED SINCE EMPTIED CONTAINERS RETAIN VAPOR
OR LIQUID RESIDUES, ALL HAZARD PRECAUTIONS MUST BE OBSERVED.

LEGAL RESPONSIBILITY IS ASSUMED ONLY FOR THE FACT THAT ALL STUDIES REPORTED
ARE THOSE OF QUALIFIED EXPERTS. BUYER ASSUMES ALL RISK AND LIABILITY. HE
ACCEPTS AND USES THIS MATERIAL ON THESE CONDITIONS. HE MUST KEEP A COPY OF
THIS MSDS WHERE MATERIAL IS HANDLED

N. A.: (NOT APPLICABLE)
N. D.: (NOT DETERMINED)
N. K.: (NOT KNOWN)

REVISED DATE: 11/01/05

RPS PRODUCTS (HEREIN CALLED RPS) HAS BEEN ASKED TO SUPPLY THE ATTACHED
MATERIAL SAFETY DATA SHEET ("MSDS") DESPITE THE FACT THAT SOME OF THE DATA
CONTAINED THEREIN IS BASED ON INFORMATION SUPPLIED TO RPS BY THIRD PARTIES
AND THE FACT THAT RPS CANNOT ANTICIPATE ALL OF THE CONDITIONS OF USE AND
APPLICATION WITH THE RESPECT TO THE PRODUCT DESCRIBED IN THE MSDS. ALTHOUGH
RPS HAS MADE A GOOD FAITH EFFORT IN FILLING OUT THE MSDS AND BELIEVES THE
INFORMATION, DATA AND SUGGESTIONS CONTAINED THEREIN TO BE RELIABLE, RPS
DOES NOT WARRANT OR GUARANTEE THE COMPLETENESS OR THE ACCURACY OF THE DATA
CONTAINED IN THE MSDS. RPS DISCLAIMS ANY AND ALL RESPONSIBILITY FOR ANY USE
OF OR RELIANCE ON SUCH DATA.