Common Name: LITHIUM RECHARGEABLE BATTERIES
Manufacturer: CHAM BATTERY TECHNOLOGY CHINA
SDS Revision Date: 12/30/2012
SDS Format: No Format Specified
   
Item Number(s): 24JZ59, 24JZ63
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - INFORMATION OF MANUFACTURER 
SECTION 2 - HAZARDOUS INGREDIENTS / IDENTITY INFORMATION 
SECTION 3 - PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION 4 - HAZARD CLASSIFICATION 
SECTION 5 - FIRST AID MEASURES 
SECTION 6 - PRECAUTIONS FOR INCIDENTAL LEAKAGE 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - FIRE AND EXPLOSION HAZARD DATA 
SECTION 9 - ACCIDENTAL RELEASE OR SPILLAGE 
SECTION 10 - STABILITY AND DISINTEGRANT 
SECTION 11 - EXPOSURE CONTROLS/PERSON PROTECTION 
SECTION 12 - ECO INFORMATION 
SECTION 13 - DISPOSAL PRECAUTIONS 
SECTION 14 - TRANSPORT INFORMATION 
SECTION 15 - ADJUSTED INFORMATION 
SECTION 16 - OTHER INFORMATION 



CHAM BATTERY TECHNOLOGY CO., LTD

MATERIAL SAFETY DATA SHEET


SECTION 1 - INFORMATION OF MANUFACTURER 


CHAM BATTERY TECHNOLOGY CO., LTD.
B3 BUILDING, GAOXINJIAN INDUSTRIAL PARK, HEPING
FU YONG TOWN, BAO'AN DISTRICT, SHENZHEN 518103
CHINA

TEL: +86-755-33937988

FAX: +86-755-33939766

PRODUCT NAME: LITHIUM RECHARGEABLE BATTERIES


SECTION 2 - HAZARDOUS INGREDIENTS / IDENTITY INFORMATION 


INGREDIENT                              CONTENT  CAS NO

LITHIUM COBALT NICKEL MANGENESE OXYGEN  35.76%   182442-95-1

POLYVINGLIDENE FLUORIDE                  1.01%    24937-79-9

CARBON                                  23.49%     7440-44-0

ALUMINUM FOIL                            8.55%     7429-90-5

COPPER FOIL                             14.76%     7460-50-8

POLYPROPYLENE                            1.36%     9003-07-0

LITHIUM HEXAFLUOROPHOSPHATE              2.57%    21324-40-3

ETHYLENE CARBONATE                       5.32%       96-49-1

DIMETHYL CARBONATE                       6.61%      616-38-6

RANEY NICKEL                             0.57%     7440-02-0


SECTION 3 - PHYSICAL/CHEMICAL CHARACTERISTICS 


BOILING POINT: N.A.

SPECIFIC GRAVITY (H2O=1): N.A.

VAPOR PRESSURE (MM.Hg): N.A.

MELTING POINT: N.A.

VAPOR DENSITY (AIR=1): N.A.

EVAPORATION RATE(BUTYL ACETATE): N.A.

SOLUBILITY IN WATER: N.A.

APPEARANCE AND ODOR: PRISMATIC SHAPE, ODORLESS


SECTION 4 - HAZARD CLASSIFICATION 


CLASSIFICATION: N.A.


SECTION 5 - FIRST AID MEASURES 


FIRST AID PROCEDURES:

IF ELECTROLYTE LEAKAGE OCCURS AND MAKES CONTACT WITH SKIN, WASH WITH PLENTY
OF WATER IMMEDIATELY.

IF ELECTROLYTE COMES INTO CONTACT WITH EYES, WASH WITH COPIOUS AMOUNTS OF
WATER FOR FIFTEEN MINUTES, AND CONTACT A PHYSICIAN.

IF ELECTROLYTE VAPORS ARE INHALED, PROVIDE FRESH AIR AND SEEK MEDICAL
ATTENTION IF RESPIRATORY IRRITATION DEVELOPS, VENTILATE THE CONTAMINATED
AREA.


SECTION 6 - PRECAUTIONS FOR INCIDENTAL LEAKAGE 


INCIDENTAL LEAKAGE:
TO BREATH STEAM AND TOUCH THE LIQUID EMPTY-HANDED ARE AVOIDED. (SEE PART 4)

DISPOSAL METHOD:
TO SEP UP SPECIAL DISPOSAL AREA AND ARRANGE THE SPECIALLY TRAINED PERSONS
TO PREVENT THE LEAKAGE WITH BARILLA OR CALCES IS RECOMMENDED. THE VEIL
FILTERED BY NIOSH CERTIFIED ACID GAS OR AUTOMATIC OXYGEN FEEDER MUST BE
WORN. THE LEAKED BATTERY, BARILLA AND BAKING SODA MUST BE DISPOSED AS
DANGEROUS SUBSTANCE.

OTHER:
TAKE REFERENCE FOR THE MANAGEMENT REGULATION OF REACTION TO EMERGENCY ITEM
138, WHICH IS CONCERNED ABOUT THE BATTERY EJECTABLE EXPLOSIONS.


SECTION 7 - HANDLING AND STORAGE 


SAFE HANDLING AND STORAGE ADVICE:

BATTERIES SHOULD BE HANDLED AND STORED CAREFULLY TO AVOID SHORT CIRCUITS.

DO NOT STORE IN DISORDERLY FASHION, OR ALLOW METAL OBJECTS TO BE MIXED WITH
STORED BATTERIES.

NEVER DISASSEMBLE A BATTERY.

DO NOT BREATHE CELL VAPORS OR TOUCH INTERNAL MATERIAL WITH BARE HANDS.

KEEP BATTERIES BETWEEN -30 CENTIGRADE AND 35 CENTIGRADE FOR PROLONG
STORAGE.


SECTION 8 - FIRE AND EXPLOSION HAZARD DATA 


FLASHPOINT (METHOD USED): N.A.

IGNITION TEMP.: N.A.

FLAMMABLE LIMITS: N.A.

LEL: N.A.

EXTINGUISHING MEDIA: CARBON DIOXIDE, DRY CHEMICAL OR FOAM EXTINGUISHERS

SPECIAL FIRE FIGHTING PROCEDURES: N.A.

UNUSUAL FIRE AND EXPLOSION HAZARDS:
DO NOT DISPOSE OF BATTERY IN FIRE - MAY EXPLODE.
DO NOT SHORT-CIRCUIT BATTERY-MAY CAUSE BURNS.


SECTION 9 - ACCIDENTAL RELEASE OR SPILLAGE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:

BATTERIES THAT ARE LEAKAGE SHOULD BE HANDLED WITH RUBBER GLOVES.

AVOID DIRECT CONTACT WITH ELECTROLYTE.

WEAR PROTECTIVE CLOTHING AND A POSITIVE PRESSURE SELF-CONTAINED BREATHING
APPARATUS (SCBA).


SECTION 10 - STABILITY AND DISINTEGRANT 


STABILITY: STABLE UNDER CONDITIONS DESCRIBED IN SECTION 7

TO BE AVOIDED:
HIGHER THAN 150 DEG. C, LONG TIME ON THE HIGH HUMIDITY ENVIRONMENT.

INCOMPATIBILITY: N/A

DANGEROUS DISINTEGRANT: CARBON DIOXIDE, HYDROGEN FLUORIDE

DANGER OF POLYMER: NOT EXIST

OTHER: N/A


SECTION 11 - EXPOSURE CONTROLS/PERSON PROTECTION 


OCCUPATION EXPOSURE LIMITS:
LTEP: N.A.
STEP: N.A.

RESPIRATORY PROTECTION (SPECIFY TYPE): N.A.

VENTILATION:
LOCAL EXHAUSTS: N.A.
SPECIAL: N.A.
MECHANICAL (GENERAL): N.A.
OTHER: N.A.

PROTECTIVE GLOVES: N.A.

EYE PROTECTION: N.A.

OTHER PROTECTIVE CLOTHING OR EQUIPMENT: N.A.

WORK/HYGIENIC PRACTICES: N.A.


SECTION 12 - ECO INFORMATION 


N.A.


SECTION 13 - DISPOSAL PRECAUTIONS 


DISPOSE OF BATTERIES ACCORDING TO GOVERNMENT REGULATIONS.


SECTION 14 - TRANSPORT INFORMATION 


THE RECHARGEABLE LITHIUM-ION BATTERY PACK AS STATED IN APPENDIX ARE MADE IN
COMPLIANCE TO THE REQUIREMENTS STATED IN THE LATEST EDITION OF THE IATA
DANGEROUS GOODS REGULATIONS PACKING INSTRUCTION 965 SECTION II SUCH THAT
THEY CAN BE TRANSPORTED AS A NOT RESTRICTED (NON-HAZARDOUS/NON-DANGEROUS)
GOODS. HOWEVER, IF THOSE LITHIUM-ION BATTERY PACKS ARE PACK WITH CONTAINED
IN AN EQUIPMENT, THEN IT IS THE RESPONSIBILITY OF THE SHIPPER TO ENSURE
THAT THE CONSIGNMENT ARE PACKED IN COMPLIANCE TO THE LATEST EDITION OF THE
IATA DANGEROUS GOODS REGULATIONS SECTION II OF EITHER PACKING INSTRUCTION
966 OR 967 IN ORDER FOR THAT CONSIGNMENT TO BE DECLARED AS NOT RESTRICTED
(NON-HAZARDOUS/NON-DANGEROUS).

WITH REGARD TO TRANSPORT, THE FOLLOWING REGULATIONS ARE CITED AND
CONSIDERED:

THE INTERNATIONAL CIVIL AVIATION ORGANIZATION (ICAO) TECHNICAL INSTRUCTIONS
(2009-2010 EDITION),

THE INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) DANGEROUS GOODS
REGULATIONS (52ND EDITION, 2011)

THE INTERNATIONAL MARITIME DANGEROUS GOODS (IMDG) CODE (2008 EDITION).

US HAZARDOUS MATERIALS REGULATIONS 49 CFR (CODE OF FEDERAL REGULATIONS)
SECTIONS 173-185 LITHIUM BATTERIES AND CELLS

THE UN RECOMMENDATIONS ON THE TRANSPORT OF DANGEROUS GOODS, MANUAL OF TESTS
AND CRITERIA 38.3 LITHIUM BATTERIES, 4TH REVISED EDITION (UN3480)

OUR PRODUCTS ARE PROPERLY CLASSIFIED, DESCRIBED, PACKAGED, MARKED, AND
LABELED, AND ARE IN PROPER CONDITION FOR TRANSPORTATION ACCORDING TO ALL
THE APPLICABLE INTERNATIONAL AND NATIONAL GOVERNMENTAL REGULATIONS, NOT
LIMITED TO THE ABOVE MENTIONED.


SECTION 15 - ADJUSTED INFORMATION 


SPECIAL REQUIREMENT BE ACCORDING TO THE LOCAL REGULATORIES.


SECTION 16 - OTHER INFORMATION 


THE DATA IN THIS MATERIAL SAFETY DATA SHEET RELATES ONLY TO THE SPECIFIC
MATERIAL DESIGNATE HEREIN.

THE VALID TIME: 2012-12-30