Common Name: NICKEL CADMIUM RECHARGEABLE BATTERY, NI-CD AA 2.4V 300MAH
Manufacturer: SHENZHEN KUNTENG CHINA
SDS Revision Date: 1/29/2013
SDS Format: No Format Specified
   
Grainger Item Number(s): 48H468
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - IDENTIFICATION OF THE SUBSTANCE AND OF THE COMPANY 
SECTION 2 - COMPOSITION AND INFORMATION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRE-FIGHTING MEASURES 
SECTION 6 - EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 7 - ACCIDENTAL RELEASE OR SPILLAGE 
SECTION 8 - HANDLING AND STORAGE 
SECTION 9 - PHYSICAL/CHEMICAL CHARACTERISTICS 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL INFORMATION 
SECTION 12 - ECOLOGICAL INFORMATION 
SECTION 13 - DISPOSAL CONSIDERATION 
SECTION 14 - TRANSPORT INFORMATION 
SECTION 15 - REGULATORY INFORMATION 
SECTION 16 - OTHER INFORMATION 



REPORT NO: 1007162-010

DATE: 01.29.2013

TINKO

MATERIAL SAFETY DATA SHEET


SECTION 1 - IDENTIFICATION OF THE SUBSTANCE AND OF THE COMPANY 


MANUFACTURER: SHENZHEN KUNTENG CO., LTD

ADDRESS:
NO.1 FACTORY
ORIENTAL HITECH PARK
QIAOXIANG RD
SHENZHEN
CHINA

POST CODE: 518053

TEL: 0755-26756070

FAX: 0755-26755329

E-MAIL: INFO@TINKO.COM.CN

IDENTIFICATION OF THE PRODUCT: NICKEL CADMIUM RECHARGEABLE BATTERY

MODEL: NI-CD AA 2.4V 300MAH

EVEN CLASSIFIED AS PRIMARY LITHIUM BATTERIES (UN3091, 3090), 2010 IATA
DANGEROUS GOODS REGULATION 51TH EDITION PACKING INSTRUCTION 968-970 PART I
IS APPLIED. THE PRODUCT IS HANDLED AS NON-DANGEROUS GOODS BY MEETING THE
FOLLOWING REQUIREMENTS.

1 FOR CELLS, THE LITHIUM SHOULD NOT BE MORE THAN 1G.

2 FOR THOSE LITHIUM METAL CELLS CONTAINED IN EQUIPMENT, THE EQUIPMENT MUST
BE EQUIPPED WITH AN EFFECTIVE MEANS OF PREVENTING ACCIDENTAL ACTIVATION.

3 EACH CELL IS OF THE TYPE PROVEN TO MEET THE REQUIREMENTS OF EACH TEST IN
THE UN MANUAL OF TESTS AND CRITERIA PART III SUBSECTION 38.3.


SECTION 2 - COMPOSITION AND INFORMATION ON INGREDIENTS 


CHEMICAL NAME           CAS NO.        %(1)     PEL            TLV

CADMIUM                  7440-43-9     10-25    0.005 TWA(2)   0.05 TWA

CADMIUM HYDROXIDE       21041-95-2     10-25    0.005 TWA      0.05 TWA

NICKEL (POWDER)          7440-02-0      5-7     1 TWA          1 TWA

NICKEL HYDROXIDE        12054-48-7     10-16    1 TWA          1 TWA

POTASSIUM HYDROXIDE      1310-58-3     <4       2 CEILING      2 CEILING

NYLON                   N/A            <5       N/A            N/A

STEEL                   N/A            16-17    N/A            N/A

OTHER                   N/A            <1       N/A            N/A

TOTAL                                  100

NOMINAL VOLTAGE: 2. 4V


SECTION 3 - HAZARDS IDENTIFICATION 


CAUTION: CONNECT PROPERLY, DO NOT RECHARGE, SHORT OR DISPOSE OF IN FIRE.

HEALTH: NO HAZARD TO HEALTH


SECTION 4 - FIRST AID MEASURES 


FIRST AID PROCEDURES:
1. IF ELECTROLYTE LEAKAGE OCCURS AND MAKES CONTACT WITH SKIN, WASH WITH
PLENTY OF WATER IMMEDIATELY.

2. IF ELECTROLYTE COMES INTO CONTACT WITH EYES, WASH WITH COPIOUS AMOUNTS
OF WATER FOR FIFTEEN (15)MINUTES, AND CONTACT A PHYSICIAN.

3. IF ELECTROLYTE VAPORS ARE INHALED, PROVIDE FRESH AIR AND SEEK MEDICAL
ATTENTION.

4. IF RESPIRATORY IRRITATION DEVELOPS, VENTILATE THE CONTAMINATED AREA.


SECTION 5 - FIRE-FIGHTING MEASURES 


DO NOT DISPOSE OF BATTERY IN FIRE-MAY CAUSE EXPLOSION.
DO NOT SHORT-CIRCUIT BATTERY - MAY CAUSE BURNS.


SECTION 6 - EXPOSURE CONTROLS/PERSONAL PROTECTION 


IT IS SUGGESTED TO HANDLE THE BATTERIES IN A VENTILATED PLACE, TO DON'T
SMOKE, EAT OR DRINK DURING THE ASSEMBLING.


SECTION 7 - ACCIDENTAL RELEASE OR SPILLAGE 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
BATTERIES THAT ARE LEAKAGE SHOULD BE HANDLED WITH RUBBER GLOVES.

AVOID DIRECT CONTACT WITH ELECTROLYTE.

WEAR PROTECTIVE CLOTHING AND A POSITIVE PRESSURE SELF-CONTAINED BREATHING
APPARATUS (SCBA).


SECTION 8 - HANDLING AND STORAGE 


SAFE HANDLING AND STORAGE ADVICE

BATTERIES SHOULD BE HANDLED AND STORED CAREFULLY TO AVOID SHORT CIRCUITS.

DO NOT STORE IN DISORDERLY FASHION, OR ALLOW METAL OBJECTS TO BE MIXED WITH
STORED BATTERIES.

NEVER DISASSEMBLE A BATTERY.

DO NOT BREATHE CELL VAPORS OR TOUCH INTERNAL MATERIAL WITH BARE HANDS.

KEEP BATTERIES BETWEEN 5 DEG. C AND 25 DEG. C FOR PROLONG STORAGE.


SECTION 9 - PHYSICAL/CHEMICAL CHARACTERISTICS 


BOILING POINT: N.A.

SPECIFIC GRAVITY(H2O=1): N.A.

VAPOR PRESSURE(MMHg): N.A.

MELTING POINT: N.A.

VAPOR DENSITY(AIR=1): N.A.

EVAPORATION RATE(BUTYL ACETATE): N.A.

SOLUBILITY IN WATER: N.A.

APPEARANCE AND ODOR: CYLINDRICAL SHAPE, ODORLESS


SECTION 10 - STABILITY AND REACTIVITY 


STABILITY:
UNSTABLE ( )
STABLE   (X)

CONDITIONS TO AVOID:

INCOMPATIBILITY (MATERIALS TO AVOID):

HAZARDOUS DECOMPOSITION OR BYPRODUCTS:

HAZARDOUS POLYMERIZATION:
MAY OCCUR      ( )
WILL NOT OCCUR (X)

CONDITIONS TO AVOID:


SECTION 11 - TOXICOLOGICAL INFORMATION 


ROUTE(S) OF ENTRY:
INHALATION?: N.A.
SKIN?: N.A.
INGESTION?: N.A.

HEALTH HAZARD (ACUTE AND CHRONIC) / TOXICOLOGICAL INFORMATION:
IN CASE OF ELECTROLYTE LEAKAGE, SKIN WILL BE ITCHY WHEN CONTAMINATED WITH
ELECTROLYTE.

NOTE: N.A. MEANS NOT APPLICABLE.


SECTION 12 - ECOLOGICAL INFORMATION 


LITHIUM-MANGANESE DIOXIDE BATTERY IS A KIND OF NEW-GENERATION CHEMICAL
BATTERY, IT IS ENVIRONMENT-FRIENDLY AND THE PRODUCTS ARE IN COMPLIANCE WITH
BATTERY DIRECTIVE. IT IS NOT DANGEROUS TO HUMAN OR ENVIRONMENT. CADMIUM,
LEAD, AND MERCURY OR OTHER DANGEROUS CHEMICALS ARE NOT INCLUDED IN THE
BATTERY.


SECTION 13 - DISPOSAL CONSIDERATION 


DISPOSE OF THE BATTERIES ACCORDING TO THE GOVERNMENT REGULATIONS.


SECTION 14 - TRANSPORT INFORMATION 


14.1 INTERNATIONAL CONVENTIONS:

AIR:
IATA: YES

SEA LAND:
IMDG: YES
ADR(ROAD): YES
RID(RAIL): YES

IN GENERAL, THE TRANSPORTATION OF PRIMARY LITHIUM CELLS AND BATTERIES IS
REGULATED BY THE INTERNATIONAL CIVIL AVIATION ORGANIZATION, INTERNATIONAL
AIR TRANSPORT ASSOCIATION, INTERNATIONAL MARITIME DANGEROUS GOODS CODE AND
THE US DEPARTMENT OF TRANSPORTATION. THE BATTERIES MUST MEET THE FOLLOWING
CRITERIA FOR SHIPMENT:

PRIMARY LITHIUM CELLS TESTED AND FOUND IN COMPLIANCE WITH UN CHAPTER 38.3
REQUIREMENTS CAN BE SHIPPED WITHOUT DESIGNATION AS "CLASS 9" HAZARDOUS
MATERIAL, IF ALL OTHER MARKING, LABELING, PACKING, AND UNIT VOLUMES ARE
MET.

FOR AIR SHIPMENTS, MEET THE REQUIREMENTS LISTED IN SPECIAL PROVISION A51 OF
THE INTERNATIONAL AIR TRANSPORT ASSOCIATION DANGEROUS GOODS REGULATIONS.
PACKING GROUP EXPLANATION 968-970

INDICATE MESSAGE:
"HANDLE WITH CARE, FLAMMABILITY HAZARD EXISTS IF THE PACKAGED IS DAMAGED."

INDICATE WHICH SPECIAL PROCEDURE SHOULD BE FOLLOWED IN THE EVENT THE
PACKAGE IS DAMAGED, TO INCLUDE INSPECTION AND REPACKING IF NECESSARY"

PROVIDE THE TELEPHONE NUMBER FOR ADDITIONAL INFORMATION.

THE PACKING MUST MEET THE REQUIREMENTS OF SPECIAL PROVISION 188.

LITHIUM BATTERIES MANUFACTURED, PACKED AND SHIPPED BY LIBA MEET THE
REQUIREMENTS SPECIFIED ABOVE. ANY LITHIUM BATTERIES SUBSEQUENTLY REPACKAGED
OR RESHIPPED ARE REQUIRED TO MEET ALL OF THE REQUIREMENTS, LITHIUM
BATTERIES MANUFACTURED, PACKED AND SHIPPED BY LIBA MEET THE REQUIREMENTS OF
GOVERNMENT REGULATIONS.

FOR SPECIFIC DETAILS, PLEASE VISIT:
HTTP://WWW.RAYOVAC.COM/ABOUT/ENVIRONMENTAL/EFAQ6.SHTML.

FOR MORE INFORMATION, VISIT: HTTP://WWW.NEMA.ORG/INDEX_NEMA.CFM/666


SECTION 15 - REGULATORY INFORMATION 


SPECIAL REQUIREMENT BE ACCORDING TO THE LOCAL REGULATIONS.


SECTION 16 - OTHER INFORMATION 


THEY MUST BE KEPT OUT OF REACH FROM CHILDREN.

THEY MUST BE USED FOLLOWING THE TECHNICAL SPECIFICATIONS, WITHOUT EXCEED
THE VALUES DEFINED.

THE INFORMATION CONTAINED IN THIS SHEET IS BASED ON THE PRESENT KNOWLEDGE
AND THE CONDITIONS OF USE.

FOR EVERY USE NOT IN CONFORMITY TO THE SAFETY SHEET OR FOR THE USE IN
COMBINATION WITH ANY OTHER MATERIAL OR IN ANY OTHER PROCESS THE USER IS THE
RESPONSIBLE.

APPROVED BY: