Common Name: CR123A BATTERIES
Manufacturer: ARMAMENT SYSTEMS AND PROCEDURES
SDS Revision Date: 1/24/2013
SDS Format: No Format Specified
   
Grainger Item Number(s): 25VF10, 25VF15, 25VG23
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. PRODUCT & COMPANY IDENTIFICATION 
2. HAZARDS IDENTIFICATION 
3. COMPOSITION/INFORMATION ON INGREDIENTS 
4. FIRST AID MEASURES 
5. FIRE FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROLS, PERSONAL PROTECTION 
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
16. ADDITIONAL INFORMATION 



ASP
BOX 1794
APPLETON, WI 54912
(920) 735-6242

FAX: (920) 735-6245

ASP-USA.COM

MSDS

MATERIAL SAFETY DATA SHEET

CR123A BATTERIES


1. PRODUCT & COMPANY IDENTIFICATION 


MANUFACTURER NAME: ARMAMENT SYSTEMS AND PROCEDURES, INC

ADDRESS:
2511 E CAPITOL DRIVE
APPLETON, WI 54911

TELEPHONE NO: (920) 735-6242

DATE: 24 JANUARY 2013

MODEL: CR123A

CHEMICAL SYSTEM: LITHIUM METAL BATTERY


2. HAZARDS IDENTIFICATION 


INVASION ROUTE:

SKIN CONTACT:
CONTACT WITH BATTERY ELECTROLYTE MAY CAUSE BURNS AND SKIN IRRITATION.

EYE CONTACT:
CONTACT WITH BATTERY ELECTROLYTE MAY CAUSE BURNS. EYE DAMAGE IS POSSIBLE.

INHALATION:
INHALATION OF VAPORS OR FUMES RELEASED DUE TO HEAT OR A LARGE NUMBER OF
LEAKING BATTERIES MAY CAUSE RESPIRATORY AND EYE IRRITATION.

INGESTION:
INGESTION OF BATTERY CONTENTS MAY CAUSE MOUTH, THROAT AND INTESTINAL BURNS
AND DAMAGE.

HEALTH HAZARDS:
THE CHEMICAL IS CONTAINED IN A SEALED CAN. RISK OF EXPOSURE OCCURS ONLY IF
THE BATTERY IS MECHANICALLY OR ELECTRICALLY ABUSED.

ENVIRONMENT HAZARDS: DO NOT DISPOSE OF THE BATTERY INTO THE ENVIRONMENT.

BURN AND BURST DANGER:
DO NOT DISPOSE OF BATTERY IN FIRE OR RECHARGE BATTERY; IT MAY EXPLODE.
DO NOT SHORT-CIRCUIT THE BATTERY OR IT MAY CAUSE BURNS.


3. COMPOSITION/INFORMATION ON INGREDIENTS 


CHEMICAL NAME              MOLECULAR        CAS NO*         WEIGHT (%)
                           FORMULA

LITHIUM                    Li               7239-93-2        3.0-4.0

CARBON                     C                7782-42-5        2.0-3.0

MANGANESE DIOXIDE          MnO2             1313-13-9       35.0-45.0

ALUMINUM                   Al               7429-90-5        2.0

1,2-DIMETHOXYETHANE        C4H10O2           110-714-4       7.0

PROPYLENE CARBONATE        C4H6O3            108-32-7        7.0

LITHIUM PERCHLORATE        LiClO4           7791-03-9        1.0-1.5

POLYPROPYLENE              (C3H6)n          9003-07-0        3.0

POLYTETRAFLUOROETHENE      (C2F4)n          9002-84-0        5.0

FERRUM                     Fe               7429-90-5        2.0

NICKEL                     Ni               7440-02-0        1.0

*CHEMICAL ABSTRACT SERVICE REGISTRY NUMBER


4. FIRST AID MEASURES 


EYE:
IF THE BATTERY IS LEAKING AND THE CONTAINED MATERIAL CONTACTS THE EYES,
FLUSH THE EYES WITH PLENTY OF WATER OR SALINE WATER AT LEAST 15 MINUTES.
SEEK MEDICAL ATTENTION RIGHT AWAY.

SKIN:
IF THE BATTERY IS LEAKING AND THE CONTAINED MATERIAL CONTACTS THE SKIN,
REMOVE CONTAMINATED CLOTHES QUICKLY AND RINSE THE SKIN WITH PLENTY OF WATER
AT LEAST 15 MINUTES. IF IRRITATION OR PAIN PERSISTS. SEEK MEDICAL ATTENTION
RIGHT AWAY.

INHALATION:
IF THE BATTERY IS LEAKING, REMOVE TO FRESH AIR IMMEDIATELY. KEEP THE
RESPIRATORY TRACT SMOOTH. USE OXYGEN IF AVAILABLE. SEEK MEDICAL ATTENTION.

INGESTION:
IF THE BATTERY IS LEAKING AND THE CONTAINED MATERIAL IS INGESTED, RINSE
MOUTH AND SURROUNDING AREA WITH CLEAR WATER. SEEK MEDICAL ATTENTION RIGHT
AWAY.


5. FIRE FIGHTING MEASURES 


DANGER CHARACTERISTIC:
EXPOSURE TO EXCESSIVE HEAT CAN CAUSE VENTING OF THE LIQUID ELECTROLYTE.
BATTERY MAY BURST AND RELEASE HAZARDOUS DECOMPOSITION PRODUCTS WHEN EXPOSED
TO A FIRE SITUATION.

HAZARDOUS COMBUSTION PRODUCTS: CO, CO2, METAL OXIDES, IRRITATING FUMES

FIRE FIGHTING METHOD:
THE PERSON MUST BE EQUIPPED WITH A FILTERMASK (FULL MASK) OR ISOLATED
BREATHING APPARATUS. THE PERSON MUST WEAR THE CLOTHES WHICH CAN DEFEND THE
FIRE IN AN UPWIND DIRECTION. REMOVE THE CONTAINER TO THE OPEN SPACE AS SOON
AS POSSIBLE. SPRAY WATER ON THE CONTAINERS IN THE FIRE PLACE TO KEEP THEM
COOL UNTIL FIRE EXTINGUISHMENT.

EXTINGUISHING MEDIA: HAZY WATER, FOAM POWER, CO2, SANDY CLAY


6. ACCIDENTAL RELEASE MEASURES 


EMERGENCY TREATMENT:
IF THE BATTERY MATERIAL IS RELEASED, REMOVE PERSONNEL FROM AREA UNTIL FUMES
DISSIPATE. PROVIDE MAXIMUM VENTILATION TO CLEAR OUT HAZARDOUS GASSES. THE
PREFERRED RESPONSE IS TO LEAVE THE AREA AND ALLOW THE BATTERIES TO COOL AND
VAPORS TO DISSIPATE. AVOID SKIN AND EYE CONTACT OR INHALATION OF VAPORS.
REMOVE SPILLED LIQUID WITH ABSORBENT AND INCINERATE WASTE.


7. HANDLING AND STORAGE 


HANDLING:
1. DO NOT ALLOW BATTERY TERMINALS TO CONTACT EACH OTHER OR CONTACT OTHER
METALS.

2. PACK BATTERIES SEPARATELY SO THAT SINGLE BATTERIES ARE NOT MIXED
TOGETHER.

3. DO NOT EXPOSE BATTERY TO EXCESSIVE PHYSICAL SHOCK OR VIBRATION.

4. DO NOT IMMERSE A BATTERY IN WATER.

5. SHORT-CIRCUITING SHOULD BE AVOIDED. SHORT-CIRCUIT WILL REDUCE THE LIFE
OF THE BATTERY AND CAN LEAD TO IGNITION OF SURROUNDING MATERIALS. PHYSICAL
CONTACT WITH TWO SHORT-CIRCUITED BATTERIES CAN CAUSE SKIN BURN.

6. THE BATTERIES SHOULD NOT BE OPENED, DESTROYED OR INCINERATED. THE
INGREDIENTS CONTAINED IN THE HERMETICALLY SEALED CONTAINER MAY LEAK OR
RUPTURE AND RELEASE INTO THE ENVIRONMENT.

7. PLACE THE CELL BEYOND THE CHILD PACKING AND CONTAINER.

8. NEVER KEEP BATTERY IN AN AIRTIGHT COMPARTMENT OR SEALED CONTAINER.

9. DO NOT MIX OLD AND NEW BATTERIES TOGETHER. DO NOT MIX WITH NI-CD, DRY
BATTERIES OR ANOTHER MANUFACTURER'S BATTERIES OR PRODUCT.

STORAGE:
1. BATTERIES SHOULD BE SEPARATED FROM OTHER MATERIALS AND STORED IN A
NONCOMBUSTIBLE, WELL VENTILATED, SPRINKLER-PROTECTED STRUCTURE WITH
SUFFICIENT CLEARANCE BETWEEN WALLS AND BATTERY STACKS.

2. KEEP THE BATTERY IN A COOL, DRY AND WELL VENTILATED PLACE. DO NOT EXPOSE
TO DIRECT SUNLIGHT FOR LONG PERIODS. KEEP AWAY FROM FIRE AND HEAT SOURCES.
DO NOT KEEP THE BATTERY WITH OXIDIZER AND ACID.

3. KEEP BATTERIES IN ORIGINAL PACKAGE UNTIL USE AND DO NOT COMBINE THEM.

4. EQUIP WITH RELEVANT TYPES AND QUANTITIES OF THE EXTINGUISHMENT
INSTRUCTIONS. THE STORAGE PLACE SHOULD BE EQUIPPED WITH SUITABLE SHELTER
MATERIALS FOR DIVULGENCE HANDLING.


8. EXPOSURE CONTROLS, PERSONAL PROTECTION 


ENGINEERING CONTROL:
KEEP AWAY FROM HEAT AND OPEN FLAME. SUPPLY WITH SUFFICIENT PARTIAL AIR
EXHAUST. STORE IN A COOL, DRY PLACE.

RESPIRATORY PROTECTION:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE. WEAR SELF CONTAINED BREATHING
FILTER MASK IF THE DENSITY EXCEEDS IN THE AIR. WEAR BREATHING APPARATUS
UNDER THE CONDITION OF EMERGENCY RESCUE OR EVACUATION.

EYES PROTECTION:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE. WEAR PROTECTIVE GLASSES IF
HANDLING A LEAKING OR RUPTURED BATTERY.

BODY PROTECTION:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE. WEAR FIREPROOFING, GAS
DEFENSE CLOTHES IN CASE OF HANDLING A LEAKING OR RUPTURED BATTERY.

HANDS PROTECTION:
NOT NECESSARY UNDER CONDITIONS OF NORMAL USE. WEAR CHEMICAL RESISTANT
RUBBER GLOVES IN CASE OF HANDLING A LEAKING OR RUPTURED BATTERY.

OTHER PROTECTIONS:
NO SMOKING, DINING OR DRINKING WATER IN THE WORKPLACE. KEEP GOOD HABIT OF
HYGIENE.


9. PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: CYLINDER

ODOR: ODORLESS

SOLUBILITY: INSOLUBLE IN WATER


10. STABILITY AND REACTIVITY 


STABILITY: STABLE UNDER NORMAL TEMPERATURE AND PRESSURE.

DISTRIBUTION OF BAN: STRONG OXIDIZER, STRONG ACID AND CORROSIVES

CONDITIONS TO AVOID:
FIRE SOURCE, HEATING SOURCE, DISASSEMBLY, SHORT-CIRCUIT OR IMMERSION IN
WATER.

HAZARDOUS DECOMPOSITION PRODUCTS:
THE BATTERY MAY RELEASE IRRITATIVE GAS IF THE ELECTROLYTE LEAKS.


11. TOXICOLOGICAL INFORMATION 


IRRITATION:
THE LIQUID IN THE BATTERY MAY IRRITATE EYES AND SKIN WITH ANY CONTACT.

SENSITIZATION:
THE LIQUID IN THE BATTERY MAY CAUSE SENSITIZATION TO SOME PEOPLE.

OTHERS:
SINCE THE MATERIALS IN THIS BATTERY ARE SEALED IN THE CAN, THE POTENTIAL
FOR EXPOSURE TO THE COMPONENTS OF THE BATTERY IS NEGLIGIBLE WHEN THE
BATTERY IS USED AS DIRECTED. HOWEVER TECHNICAL OR ELECTRICAL ABUSE OF THE
BATTERY MAY RESULT IN THE RELEASE OF BATTERY CONTENTS.


12. ECOLOGICAL INFORMATION 


DO NOT DISPOSE OF THE BATTERY INTO THE ENVIRONMENT. IT MAY CAUSE WATER OR
SOIL POLLUTION.


13. DISPOSAL CONSIDERATIONS 


REFER TO NATIONAL OR LOCAL REGULATIONS BEFORE HANDLING. DISPOSAL OF THE
BATTERY SHOULD BE PERFORMED BY PERMITTED, PROFESSIONAL DISPOSAL FIRMS
KNOWLEDGEABLE IN NATIONAL OR LOCAL REGULATIONS OF HAZARDOUS WASTE TREATMENT
AND HAZARDOUS WASTE TRANSPORTATION. THE BATTERY SHOULD BE COMPLETELY
DISCHARGED PRIOR TO DISPOSAL IN ORDER TO PREVENT SHORT-CIRCUIT. THE BATTERY
CONTAINS RECYCLABLE MATERIALS. IT IS SUGGESTED TO RECYCLE.


14. TRANSPORT INFORMATION 


ACCORDING TO PACKING INSTRUCTION 968-970 OF IATA DGR 54TH EDITION FOR
TRANSPORTATION, THE SPECIAL PROVISION 188 OF IMDG (INC AMDT 35-10), THE
BATTERIES SHOULD BE SECURELY PACKED AND PROTECTED AGAINST SHORT-CIRCUITS.
EXAMINE WHETHER THE PACKAGE OF THE CONTAINERS ARE INTEGRATE AND TIGHTLY
CLOSED BEFORE TRANSPORT. TAKE CARE WITH CARGO; DO NOT FALL, DROP OR BREAK.
PREVENT COLLAPSING OF CARGO PILES AND BECOMING WET BY RAIN. THE TRANSPORT
VEHICLE AND SHIP MUST BE CLEANED AND STERILIZED OTHERWISE IT IS NOT ALLOWED
TO ASSEMBLE ARTICLES. DURING TRANSPORT, THE VEHICLE SHOULD AVOID EXPOSURE,
RAIN AND HIGH TEMPERATURES. FOR STOPOVERS, THE VEHICLE SHOULD BE AWAY FROM
FIRE AND HEAT SOURCES. WHEN TRANSPORTED BY SEA, THE ASSEMBLE PLACE SHOULD
KEEP AWAY FROM BEDROOM, KITCHEN AND ISOLATED FROM THE ENGINE ROOM, POWER
AND FIRE SOURCE. UNDER THE CONDITION OF ROAD TRANSPORTATION, THE DRIVER
SHOULD DRIVE IN ACCORDANCE WITH REGULATED ROUTE, DO NOT STOP IN A
RESIDENTIAL AREA OR CONGESTED AREA.


15. REGULATORY INFORMATION 


ISO 11014-2009:
SAFETY DATA SHEET FOR CHEMICAL PRODUCTS - CONTENT AND ORDER OF SECTIONS.

REGULATION (EC) NO 1272/2008:
CLASSIFICATION, LABELING AND PACKAGING OF SUBSTANCES AND MIXTURES

INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) DANGEROUS GOODS
REGULATIONS, 54TH EDITION

THE INTERNATIONAL MARITIME DANGEROUS GOODS (IMDG) CODE (INC AMDT 35-10)


16. ADDITIONAL INFORMATION 


TO THE BEST OF OUR KNOWLEDGE, THE INFORMATION CONTAINED HEREIN IS ACCURATE.
HOWEVER, NEITHER THE ABOVE NAMED SUPPLIER, NOR ANY OF ITS SUBSIDIARIES,
ASSUMES ANY LIABILITY WHATSOEVER FOR THE ACCURACY OR COMPLETENESS OF THE
INFORMATION CONTAINED HEREIN.

FINAL DETERMINATION OF SUITABILITY OF ANY MATERIAL IS THE SOLE
RESPONSIBILITY OF THE USER. ALL MATERIALS MAY PRESENT UNKNOWN HAZARDS AND
SHOULD BE USED WITH CAUTION. ALTHOUGH CERTAIN HAZARDS ARE DESCRIBED HEREIN,
WE CANNOT GUARANTEE THAT THESE ARE THE ONLY HAZARDS THAT EXIST.