Common Name: VITRIFIED BOND WHEELS
Manufacturer: NORTON
SDS Revision Date: 11/25/2013
SDS Format: No Format Specified
   
Item Number(s): 6NW94, 6NW95, 6NW96, 6NW97, 6NW98, 6NW99, 6NX01, 6NX02, 6NX03, 6NX04, 6NX05, 6NX06, 6NX07, 6NX08, 6NX09, 6NX10, 6NX11, 6NX12, 6NX13, 6NX14, 6NX15, 6NX16, 6NX17, 6NX18, 6NX19, 6NX20, 6NX21, 6NX22, 6NX23, 6NX24, 6NX25, 6NX26, 6NX27, 6NX28, 6NX29, 6NX30, 6NX31, 6NX32, 6NX33, 6NX34, 6NX35, 6NX36, 6NX37, 6NX38, 6NX39, 6NX40, 6NX41, 6NX42, 6NX43, 6NX44, 6NX45, 6NX46, 6NX47, 6NX48, 6NX49, 6NX50, 6NX51, 6NX52, 6NX53, 6NX54, 6NX55, 6NX56, 6NX57, 6NX58, 6NX59, 6NX60, 6NX61, 6NX62, 6NX63, 6NX64, 6NX65, 6NX66, 6NX67, 6NX68, 6NX69, 6NX70, 6NX71, 6NX72, 6NX73, 6NX74, 6NX75, 6NX76, 6NX77, 6NX78, 6NX79, 6NX80, 6NX81, 6NX82, 6NX83, 6NX84, 6NX85, 6NX86, 6NX87, 6NX88, 6NX89, 6NX90, 6NX91, 6NX92, 6NX93, 6NX94, 6NX95, 6NX96, 6NX97, 6NX98, 6NX99, 6NZ01, 6NZ02, 6NZ03, 6NZ04, 6NZ05, 6NZ06, 6NZ07, 6NZ08
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
1. PRODUCT IDENTIFICATION: VITRIFIED BOND WHEELS. 
2. COMPOSITION / INFORMATION ON INGREDIENTS 
3. HAZARDS IDENTIFICATION 
4. FIRST AID MEASURES 
5. FIRE FIGHTING MEASURES 
6. ACCIDENTAL RELEASE MEASURES 
7. HANDLING AND STORAGE 
8. EXPOSURE CONTROL/PERSONAL PROTECTION 
9. PHYSICAL AND CHEMICAL PROPERTIES 
10. STABILITY AND REACTIVITY 
11. TOXICOLOGICAL INFORMATION 
12. ECOLOGICAL INFORMATION 
13. DISPOSAL CONSIDERATIONS 
14. TRANSPORT 
15. REGULATORY INFORMATIONS 
16. OTHER INFORMATION 



25.11.13

MATERIAL SAFETY DATA SHEET

SKU # 6NX30

IMPORTANT NOTICE:
THE BONDED ABRASIVES ARE INERT PRODUCTS, WHICH DO NOT CREATE ANY RISK WHEN
HANDLED OR STORES. WHEN USED ON GRINDING OPERATION 90% OR MORE OF THE
PARTICULATE OF THE DUST COME FROM THE MATERIAL BEING GROUND AND FOR WET
GRINDING, FROM AEROSOL GENERATED BY THE GRINDING FLUID. SPECIFIC ATTENTION,
MUST THEREFORE BE GIVEN TO THE NATURE OF THE PART AND OF THE FLUID AND THE
APPROPRIATE EQUIPMENT TO EXTRACT THESE GENERATED MATERIALS MUST BE
INSTALLED.


1. PRODUCT IDENTIFICATION: VITRIFIED BOND WHEELS. 


MANUFACTURER: NORTON


2. COMPOSITION / INFORMATION ON INGREDIENTS 


S.NO.                   COMPOSITION

2.1. ABRASIVE           ALUMINIUM OXIDE AND SILICON CARBIDE

2.2. BOND               VITRIFIED

2.3. BOND FILLERS

2.4. REINFORCEMENTS


3. HAZARDS IDENTIFICATION 


NOT APPLICABLE:
BONDED ABRASIVES ARE NOT DANGEROUS PRODUCTS. DEFINED IN EC DIRECTIVE
N.88/379


4. FIRST AID MEASURES 


NOT APPLICABLE. WHEN NOT IN USE.

WHEN ON MACHINES. FOLLOWING RECOMMENDATIONS ARE BASIC RULES.

DURING A GRINDING OPERATION FOLLOW THE INFORMATION APPEARING IN THE SAFETY
DATA SHEETS OF THE MATERIAL GROUND AND OF THE GRINDING FLUID.

DUST INHALATION:
REMOVE FROM EXPOSURE, SEEK MEDICAL SERVICE IF SYMPTOMS PERSIST.

EYE:
REMOVE FROM EXPOSURE AND FLUSH WITH CLEAN WATER. IF SYMPTOMS PERSIST SEEK,
MEDICAL SERVICE.

SKIN: NO HAZARDOUS EFFECT KNOWN.

INGESTION: NO HAZARDOUS EFFECT KNOWN.


5. FIRE FIGHTING MEASURES 


NONE SPECIFIC - WATER, POWDER, FOAM, SAND, CO2... CAN BE USED IF COMPATIBLE
WITH OPERATING CONDITIONS.


6. ACCIDENTAL RELEASE MEASURES 


NOT APPLICABLE


7. HANDLING AND STORAGE 


THE FOLLOWING RECOMMENDATIONS SHOULD BE FOLLOWED TO PREVENT DAMAGE TO
BONDED ABRASIVES WHICH MAY CREATE A RISK OF RUPTURE WHEN IN USE

FRAGILE PRODUCTS: HANDLE AND STORE WITH CARE.

STORE AT MODERATE TEMPERATURE AND HUMIDITY. EXCESSIVE HEAT, HUMIDITY OR
THERMAL SHOCKS MAY MECHANICALLY WEAKEN THE PRODUCTS AND CREATE SAFETY
HAZARDS WHEN USED ON MACHINE.

FOR DETAILED RECOMMENDATIONS REFER TO THE FEPA SAFETY CODE AND TO THE
SAFETY LEAFLETS - GENERAL AND PORTABLE.


8. EXPOSURE CONTROL/PERSONAL PROTECTION 


NOT APPLICABLE WHEN BONDED ABRASIVE ARE HANDLED OR STORED. THE BONDED
ABRASIVES ARE INERT PRODUCTS, WHICH DO NOT CREATE ANY RISK WHEN HANDLED OR
STORED. WHEN USED ON GRINDING MACHINES, THEY REQUIRE SPECIFIC MEASURE TO
PROTECT THE OPERATORS. DURING GRINDING OPERATION 90% OR MORE OF THE
PARTICULATE OF THE DUST COME FROM THE MATERIAL BEING GROUND AND FOR WET
GRINDING, FROM AEROSOL GENERATED BY THE GRINDING FLUID. SPECIFIC ATTENTION
MUST THEREFORE BE GIVEN TO THE NATURE OF THE PART AND OF THE FLUID AND THE
APPROPRIATE EQUIPMENT TO EXTRACT THESE GENERATED MATERIALS MUST BE
INSTALLED.

FOR SAFE USE OF BONDED ABRASIVES REFER TO THE FEPA SAFETY CODE AND LEAFLETS
AND NATIONAL REGULATIONS.

8.1 THE FOLLOWING PERSONAL PROTECTIVE EQUIPMENT SHOULD BE USED DEPENDING ON
THE OPERATION AND THE MATERIAL BEING GROUND

EYE PROTECTION: MACHINE GUARDING AND SAFETY GOGGLES OR FACE SHIELD.

DUST PROTECTION: USE OF DUST MASK

HAND PROTECTION: USE OF BARRIER CREAM OR PROTECTIVE GLOVES

EARS PROTECTION: USE OF EARS MUFFS OR EQUIVALENT

SKIN PROTECTION: USE OF SUITABLE PROTECTIVE CLOTHING

8.2 HYGIENE MEASURES: NO SPECIFIC REQUIREMENTS.


9. PHYSICAL AND CHEMICAL PROPERTIES 


9.1 PHYSICAL STATE: SOLID

9.2. COLOUR: VARIABLE

9.3. ODOUR: NOT APPLICABLE (MAY GIVE OFF NON SPECIFIC ODOUR IN USE)

9.4 PH: NOT APPLICABLE

9.5 CHANGE OF PHYSICAL STATE: NOT APPLICABLE

9.6 BULK DENSITY: NOT APPLICABLE

9.7 VAPOUR PRESSURE: NOT APPLICABLE

9.8 FLASH POINT: NOT APPLICABLE

9.9 EXPLOSION PROPERTIES: NOT APPLICABLE

9.10 VISCOSITY: NOT APPLICABLE

9.11 SOLUBILITY IN WATER: NOT DEFINED


10. STABILITY AND REACTIVITY 


BONDED ABRASIVES ARE STABLE AND NON REACTIVE WHEN HANDLED OR STORED

10.1 CONDITIONS TO AVOID: EXCESSIVE HEAT OR HUMIDITY

10.2 MATERIALS TO AVOID:
STRONG ACIDS, STRONG BASES & STRONG OXIDIZING AGENTS MAY MODIFY THE
MECHANICAL CHARACTERISTICS OF THE PRODUCTS AND CREATE SAFETY HAZARDS WHEN
USED ON MACHINES

10.3 HAZARDOUS DECOMPOSITION OF PRODUCTS:
IF BONDED ABRASIVES ARE USED IN ACCORDANCE WITH INSTRUCTIONS, NO HAZARDOUS
DECOMPOSITION OF PRODUCTS ARE CREATED.

10.4 OTHER INDICATIONS: NONE


11. TOXICOLOGICAL INFORMATION 


NOT APPLICABLE WHEN HANDLED OR STORED

ACCORDING TO THE EXPERIENCE GATHERED FOR MANY YEARS, THE BONDED ABRASIVES
WHEN PROPERLY USED HAVE NO ADVERSE EFFECT ON HEALTH. REFER TO THE
PRELIMINARY NOTE ABOUT DUST AND AEROSOL


12. ECOLOGICAL INFORMATION 


12.1 MOBILITY:
WHEN THE BONDED ABRASIVES ARE USED, THE GRINDING DEBRIS IS EASILY RETAINED
WITHIN FIXED MACHINES OR WITH APPROPRIATE SCREENS FOR PORTABLE GRINDING
OPERATIONS.

12.2 PERSISTENCE AND DEGRADABILITY: NOT BIO-DEGRADABLE

12.3 BIOACCUMULATIVE POTENTIAL: NOT APPLICABLE

12.4 ECOTOXICITY: NOT APPLICABLE


13. DISPOSAL CONSIDERATIONS 


AFTER USE BONDED ABRASIVES MAY BE CONTAMINATED WITH HAZARDOUS MATERIALS
(PARTICLES OF MATERIAL GROUND OR COOLING AGENTS) AND SHOULD BE DISPOSED OF
IN ACCORDANCE WITH NATIONAL AND LOCAL REGULATIONS.


14. TRANSPORT 


THE BONDED ABRASIVES ARE NOT DANGEROUS PRODUCTS AND NO SPECIFIC REGULATIONS
FOR ANY TYPE OF TRANSPORTATION ARE REQUIRED. PROTECT FROM RAIN AND
EXCESSIVE TEMPERATURE AND HUMIDITY. NO SPECIAL PRECAUTIONS NECESSARY OTHER
THAN TO INSURE THAT NO DAMAGE TO THE PRODUCT OCCURS.


15. REGULATORY INFORMATIONS 


EC REGULATIONS:
NONE, ANY SPECIFIC MARKING REQUIRED UNDER EC DIRECTIVE N. 88/379; NATIONAL
OR LOCAL REGULATIONS: REFER TO RELEVANT TEXTS.


16. OTHER INFORMATION 


WARNING:
THE ABOVE INDICATIONS ARE BASED ON THE EXISTING PRACTICE AND DO NOT
CONSTITUTE GUARANTEE. THE LAWS AND REGULATIONS MUST BE STRICTLY FOLLOWED BY
THE USERS WHO REMAIN RESPONSIBLE FOR THE USE OF THE BONDED ABRASIVES.

PANNEER SELVAM. G,
SR. MANGER,
QUALITY ASSURANCE.

25/11/2013