Common Name: LITHIUM ION CELLS
Manufacturer: SHENZHEN BAK BATTERY CHINA
MSDS Revision Date: 12/27/2012
MSDS Format: No Format Specified
   
Grainger Item Number(s): 14L695, 20AU28, 20AU29, 20AU30, 20AU31, 38V822
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
SECTION 1 CHEMICAL PRODUCT AND COMPANY IDENTIFICATION 
SECTION 2 COMPOSITION/INFORMATION ON INGREDIENTS(1) 
SECTION 3 HAZARDS IDENTIFICATION 
SECTION 4 FIRST-AID MEASURES 
SECTION 5 FIRE-FIGHTING MEASURES 
SECTION 6 ACCIDENTAL RELEASE MEASURES 
SECTION 7 HANDLING AND STORAGE 
SECTION 8 EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 STABILITY AND REACTIVITY 
SECTION 11 TOXICOLOGICAL INFORMATION 
SECTION 12 ECOLOGICAL INFORMATION 
SECTION 13 DISPOSAL 
SECTION 14 TRANSPORT INFORMATION 
SECTION 15 REGULATORY INFORMATION 
SECTION 16 OTHER INFORMATION 



B
BAK

SHENZHEN BAK BATTERY CO., LTD.

MATERIAL SAFETY DATA SHEET

FOR LITHIUM ION CELLS


SECTION 1 CHEMICAL PRODUCT AND COMPANY IDENTIFICATION 


TRADE NAME: LITHIUM ION CELLS

MODEL:
ALL 18650 MODELS MANUFACTURED BY SHENZHEN BAK WITH CAPACITY LESS THAN OR
EQUAL TO 3 AHR.

NOMINAL VOLTAGE: 3.7V

MANUFACTURER: SHENZHEN BAK BATTERY CO., LTD.

ADDRESS:
BAK INDUSTRY PARK
KUI CHONG STREET
LONG GANG DISTRICT, SHENZHEN CITY, GUANGDONG PROVINCE
CHINA

TELEPHONE: +86-755-89770161


SECTION 2 COMPOSITION/INFORMATION ON INGREDIENTS(1) 


CHEMICAL NAME                      MOLECULAR  CAS NO.      CLASSIFICATION
                                   FORMULA

LITHIUM TRANSITION METAL OXIDE(2)  LixMO2     PROPRIETARY

CARBON (GRAPHITE)                  C          7440-44-0

ALUMINUM                           Al         7429-90-5

COPPER                             Cu         7440-50-8

STEEL                              Fe         7439-89-6

ELECTROLYTE                                   PROPRIETARY  FLAMMABLE LIQUID

NOTES:

1) NOT EVERY PRODUCT CONTAINS ALL OF THESE MATERIALS

2) M MEANS A COMBINATION OF Co, Ni OR Mn. THIS COMPONENT MAY CONSIST OF A
MIXTURE OF COMPOUNDS, EACH OF WHICH MAY CONTAIN THESE ELEMENTS.


SECTION 3 HAZARDS IDENTIFICATION 


LITHIUM ION CELLS ARE NOT HAZARDOUS WHEN USED ACCORDING TO THE INSTRUCTIONS
OF THE MANUFACTURER UNDER NORMAL CONDITIONS. IN CASE OF ABUSE, THERE IS A
RISK OF RUPTURE, FIRE, HEAT, OR LEAKAGE OF INTERNAL COMPONENTS, WHICH COULD
RELEASE HAZARDOUS MATERIALS.


SECTION 4 FIRST-AID MEASURES 


LITHIUM ION CELLS ARE NOT HAZARDOUS UNDER NORMAL CIRCUMSTANCES. IN CASE OF
FIRE OR RUPTURE, THE LEAKAGE OF INTERNAL HAZARDOUS SUBSTANCE AND FORMATION
OF HAZARDOUS SUBSTANCE MAY OCCUR, AND THE FOLLOWING MEASURES SHOULD BE
TAKEN IN CASE OF CONTACT WITH THESE:

EYES:
CHECK FOR AND REMOVE ANY CONTACT LENSES. IMMEDIATELY FLUSH WITH PLENTY OF
CLEAN WATER FOR AT LEST 15 MINUTES, SEEK MEDICAL ASSISTANCE.

SKIN:
IMMEDIATELY FLUSH WITH PLENTY OF CLEAN WATER FOR 15 MINUTES; SEEK MEDICAL
ASSISTANCE IF REACTION IS SEVERE.

INHALATION:
REMOVE TO FRESH AIR IMMEDIATELY, SEEK MEDICAL ASSISTANCE, AND VENTILATE THE
CONTAMINATED AREA.

INGESTION:
RINSE MOUTH WITH CLEAN WATER IMMEDIATELY. MAKE THE VICTIM VOMIT AND SEEK
MEDICAL ASSISTANCE.


SECTION 5 FIRE-FIGHTING MEASURES 


EXTINGUISH WITH PLENTY OF WATER, DRY POWDER EXTINGUISHERS, SANDS OR EARTH.
COMBUSTION" PRODUCTS AND DECOMPOSITION PRODUCTS INCLUDE:
CARBON MONOXIDE, CARBON DIOXIDE, HYDROGEN FLUORIDE, PHOSPHORUS FLUORIDE.


SECTION 6 ACCIDENTAL RELEASE MEASURES 


WHEN LEAKAGE OF CELLS HAPPENS, LIQUID COULD BE ABSORBED WITH SANDS, EARTH
OR OTHER INERT SUBSTANCE, AND THE CONTAMINATED AREA SHOULD BE VENTILATED.


SECTION 7 HANDLING AND STORAGE 


HANDLING PRECAUTIONS:
DO NOT SHORT POSITIVE AND NEGATIVE TERMINALS BY CONTACT WITH CONDUCTORS. DO
NOT OVERHEAT OR INCINERATE. DO NOT OPEN, PUNCTURE, CRUSH OR DEFORM CELLS

STORAGE:
STORE AND USE AWAY FROM HEAT, SPARKS, OPEN FLAME, OR ANY OTHER IGNITION
SOURCE. STORE IN A COOL, DRY ENVIRONMENT (LESS THAN 35 DEG. C, LESS THAN
85% RH).


SECTION 8 EXPOSURE CONTROLS/PERSONAL PROTECTION 


THERE IS NO PROTECTION REQUIRED UNDER NORMAL CONDITIONS. IN CASE OF LEAKAGE
VENTILATION IS REQUIRED. RESPIRATOR, EYE PROTECTION, PROTECTIVE GLOVES AND
PROTECTIVE CLOTHES ARE REQUIRED WHEN DEALING WITH FIRE AND LEAKAGE.


SECTION 9 PHYSICAL AND CHEMICAL PROPERTIES 


CELLS ARE NOT SINGLE CHEMICAL MATERIAL; THERE ARE NO SPECIFIC PHYSICAL AND
CHEMICAL PROPERTIES SUCH AS MELTING POINT AND BOILING POINT.


SECTION 10 STABILITY AND REACTIVITY 


CELLS ARE STABLE UNDER NORMAL CONDITIONS. THE FOLLOWING SUBSTANCE MAY
APPEAR IN CASE OF FIRE OR LEAKAGE:
ORGANIC CARBONATE, HYDROGEN FLUORIDE, CARBON MONOXIDE, CARBON DIOXIDE,
PHOSPHORUS FLUORIDE.


SECTION 11 TOXICOLOGICAL INFORMATION 


CELLS ARE NOT HAZARDOUS WHEN USED PROPERLY. IN CASE OF FIRE OR LEAKAGE
COMBUSTION AND DECOMPOSITION PRODUCTS MAY CAUSE IRRITATION AND TOXICITY TO
SKIN, EYE AND RESPIRATORY SYSTEMS.

TOXICITY DATA OF SOME SUBSTANCE IS LISTED:

HYDROGEN FLUORIDE:
EXTREMELY TOXIC, MAY BE FATAL IF INHALED OR INGESTED. READILY ABSORBED
THROUGH THE SKIN CONTACT MAY BE FATAL. POSSIBLE MUTAGEN.

LCLO: 50 PPM/30M (HUMAN BEINGS)
LC50: 1276 PPM/1H (RATS).

CARBON AND GRAPHITE:
SLIGHTLY HAZARDS IN CASE OF SKIN CONTACT (IRRITANT), INGESTION, INHALATION,
WHICH WILL CAUSE CHRONIC DAMAGE TO UPPER RESPIRATORY TRACT AND
CARDIOVASCULAR SYSTEM.

COPPER: DUST MAY. CAUSE RESPIRATORY IRRITATION.
LD50: 3.5 MG KG(-1) (MOUSE).


SECTION 12 ECOLOGICAL INFORMATION 


THERE IS NO INFLUENCE ON ECOLOGY OR ENVIRONMENT WHEN USED AND DISPOSED OF
PROPERLY.


SECTION 13 DISPOSAL 


DISCARDED CELLS SHOULD NOT BE TREATED AS ORDINARY TRASH. RECYCLING IS
RECOMMENDED AND IS REQUIRED BY LAW IN MANY JURISDICTIONS. DO NOT
INCINERATE. LEAKING OR DAMAGED CELLS SHOULD BE TREATED AS CHEMICAL WASTE;
PACKAGING IS NORMALLY NOT CONTAMINATED BY CEILS.


SECTION 14 TRANSPORT INFORMATION 


THE FOLLOWING REGULATIONS APPLY TO THE TRANSPORT OF LITHIUM ION CELLS
WORLDWIDE:

1) UN RECOMMENDATIONS ON THE TRANSPORT OF DANGEROUS GOODS ACCORDING TO
WHICH LITHIUM ION CELLS ARE ASSIGNED UN ID#3480, CLASS 9, PACKING GROUP II

2) INTERNATIONAL AIR TRANSPORT ASSOCIATION (IATA) DANGEROUS GOODS
REGULATIONS (DGR)

3) INTERNATIONAL MARITIME ORGANIZATION (IMO) INTERNATIONAL MARITIME
DANGEROUS GOODS (IMDG) CODE

4) IATA DGR 54TH EDITION FOR TRANSPORTATION

5) TRANSPORT FASHION: BY AIR, BY SEA

LITHIUM ION BATTERIES CONTAINING NO MORE THAN 1.5 G/CELL AND 8 G/BATTERY
PACK EQUIVALENT LITHIUM CAN BE SHIPPED AS 'NON-DANGEROUS GOODS' PROVIDING
THE CELLS HAVE PASSED THE REQUIRED TESTS ACCORDING TO UN38.3 (UN MANUAL OF
TESTS AND CRITERIA, PART III, SUBSECTION 38.3). IN THIS CASE" PACKING
INSTRUCTION 965-967 OF IATA-DGR AND SPECIAL PROVISIONS 188 OF IMO-IMDG CODE
ALSO APPLY.


SECTION 15 REGULATORY INFORMATION 


FOR SHIPPING REGULATIONS SEE SECTION 14.


SECTION 16 OTHER INFORMATION 


THIS DOCUMENT IS PROVIDED FOR TECHNICAL INFORMATION ONLY. THE INFORMATION
IS PROVIDED IN GOOD FAITH AND IS BELIEVED TO BE ACCURATE AS OF THE DATE OF
PREPARATION. BAK MAKES NO WARRANTY, EITHER EXPRESS OR IMPLIED, WITH RESPECT
TO THIS INFORMATION AND DISCLAIMS ALL LEGAL RESPONSIBILITY FROM RELIANCE ON
IT.

PREPARED/DATE: 2012-12-27

AUDITED/DATE:

APPROVED/DATE:

FILE NO./REV.: MSDS-163/