Common Name: MANGANESE DIOXIDE LITHIUM BATTERY
Manufacturer: PANASONIC JAPAN
MSDS Revision Date: 1/1/2013
   
Grainger Item Number(s): 20AT91
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
1 NAME OF PRODUCT AND MANUFACTURER 
2 HAZARDS IDENTIFICATION 
3 COMPOSITIONS 
4 FIRST AID MEASURES 
5 FIRE FIGHTING MEASURES 
6 MEASURES FOR ELECTROLYTE LEAKAGE FROM THE BATTERY 
7 HANDLING AND STORAGE 
8 EXPOSURE CONTROL 
9 PHYSICAL AND CHEMICAL PROPERTIES 
10 STABILITY AND REACTIVITY 
11 TOXICOLOGICAL INFORMATION 
12 ECOLOGICAL INFORMATION 
13 DISPOSAL CONSIDERATIONS 
14 TRANSPORT INFORMATION 
15 REGULATORY INFORMATION 
16 OTHER INFORMATION 



PANASONIC

ENERGY COMPANY
PANASONIC CORPORATION
1-1, MATSUSHITA-CHO
MORIGUCHI CITY
OSAKA 570-8511
JAPAN

TEL: +81-6-6991-1141

HTTP://PANASONIC.CO.JP/EC/EN

PRODUCT SAFETY DATA SHEET


1 NAME OF PRODUCT AND MANUFACTURER 


NAME OF PRODUCT: MANGANESE DIOXIDE LITHIUM BATTERY

NAME OF COMPANY: PANASONIC CORPORATION ENERGY COMPANY

ADDRESS:
1-1 MATSUSHITA-CHO
MORIGUCHI CITY
OSAKA, 570-8511
JAPAN

DIVISION: ENERGY DEVICE BUSINESS UNIT

DEPARTMENT: PRODUCT ENGINEERING GROUP

TELEPHONE NUMBER: +81-6-6994-4537

FOR EMERGENCY: +81-6-6991-1141

DOCUMENT NUMBER: CCRE-PSDS-1

EFFECTIVE DATE: JANUARY 1. 2013


2 HAZARDS IDENTIFICATION 


GHS CLASSIFICATION: NOT APPLICABLE

HAZARD:
ELECTROLYTE AND LITHIUM METAL ARE INFLAMMABLE.

RISK OF EXPLOSION BY FIRE IF BATTERIES ARE DISPOSED IN FIRE OR HEATED ABOVE
100 DEGREES C.

STACKING OR JUMBLING BATTERIES MAY CAUSE EXTERNAL SHORT CIRCUITS, HEAT
GENERATION, FIRE OR EXPLOSION.

TOXICITY:
VAPOR GENERATED FROM BURNING BATTERIES, MAY MAKE EYES, SKIN AND THROAT
IRRITATE.


3 COMPOSITIONS 


COMPONENT              MATERIAL                 CAS NO.       CONTENT

POSITIVE ELECTRODE     MANGANESE DIOXIDE        1313-13-9      12-50 WT%

NEGATIVE ELECTRODE     LITHIUM METAL            7439-93-2     0.5-6 WT%

ELECTROLYTE            1,2-DIMETHOXYETHANE       110-71-4     1.5-3.5 WT%

                       LITHIUM PERCHLORATE      7791-03-9     0.2-0.7 WT%

                       ORGANIC ELECTROLYTE                    2.5-7 WT%

LITHIUM CONTENT PER CELL:

MODEL NUMBER                LITHIUM CONTENT(G)

CR1025                      0.008

CR1216                      0.008

CR1220                      0.01

CR1612                      0.01

CR1616                      0.02

CR1620                      0.02

CR1632                      0.04

CR2012                      0.02

CR2016                      0.03

CR2025                      0.05

CR2032                      0.06

CR2320                      0.04

CR2330                      0.08

CR2354                      0.17

CR2412                      0.03

CR2450                      0.18

CR2450A                     0.17

CR2477                      0.29

CR3032                      0.15


4 FIRST AID MEASURES 


THE PRODUCT CONTAINS ORGANIC ELECTROLYTE. IN CASE OF ELECTROLYTE LEAKAGE
FROM THE BATTERY, ACTIONS DESCRIBED BELOW ARE REQUIRED.

EYE CONTACT:
FLUSH THE EYES WITH PLENTY OF CLEAN WATER FOR AT LEAST 15 MINUTES
IMMEDIATELY, WITHOUT RUBBING. TAKE A MEDICAL TREATMENT. IF APPROPRIATE
PROCEDURES ARE NOT TAKEN, THIS MAY CAUSE AN EYE IRRITATION.

SKIN CONTACT:
WASH THE CONTACT AREAS OFF IMMEDIATELY WITH PLENTY OF WATER AND SOAP.
IF APPROPRIATE PROCEDURES ARE NOT TAKEN, THIS MAY CAUSE SORES ON THE SKIN.

INHALATION: REMOVE TO FRESH AIR IMMEDIATELY. TAKE A MEDICAL TREATMENT.


5 FIRE FIGHTING MEASURES 


EXTINGUISHING METHOD:
SINCE VAPOR, GENERATED FROM BURNING BATTERIES MAY MAKE EYES, NOSE AND
THROAT IRRITATES, BE SURE TO EXTINGUISH THE FIRE ON THE WINDWARD SIDE.
WEAR THE RESPIRATORY PROTECTION EQUIPMENT IN SOME CASES.

FIRE EXTINGUISHING AGENT:
ALCOHOL-RESISTANT FOAM AND DRY SAND ARE EFFECTIVE.


6 MEASURES FOR ELECTROLYTE LEAKAGE FROM THE BATTERY 


TAKE UP WITH ABSORBENT CLOTH.
MOVE THE BATTERY AWAY FROM THE FIRE.


7 HANDLING AND STORAGE 


WHEN PACKING THE BATTERIES, DO NOT ALLOW BATTERY TERMINALS TO CONTACT EACH
OTHER, OR CONTACT WITH OTHER METALS. BE SURE TO PACK BATTERIES BY PROVIDING
PARTITIONS IN THE PACKAGING BOX, OR IN A SEPARATE PLASTIC BAG SO THAT THE
SINGLE BATTERIES ARE NOT MIXED TOGETHER.

USE STRONG MATERIAL FOR PACKAGING BOXES SO THAT THEY WILL NOT BE DAMAGED
BY VIBRATION, IMPACT, DROPPING AND STACKING DURING THEIR TRANSPORTATION.

DO NOT RECHARGE BATTERIES. DO NOT DEFORM BATTERIES.

DO NOT MIX DIFFERENT TYPE OF BATTERIES.

DO NOT SOLDER DIRECTLY ONTO BATTERIES.

DO NOT LET WATER PENETRATE INTO PACKAGING BOXES DURING THEIR STORAGE AND
TRANSPORTATION.

DO NOT STORE THE BATTERY IN PLACES OF THE HIGH TEMPERATURE OR UNDER DIRECT
SUNLIGHT OR IN FRONT OF A STOVE. PLEASE ALSO AVOID THE PLACES OF HIGH
HUMIDITY. BE SURE NOT TO EXPOSE THE BATTERY TO CONDENSATION, WATER DROP OR
NOT TO STORE IT UNDER FROZEN CONDITION.

FIRE FIGHTING APPARATUS SHOULD BE INSTALLED.


8 EXPOSURE CONTROL 


(IN CASE OF ELECTROLYTE LEAKAGE FROM THE BATTERY)

ACCEPTABLE CONCENTRATION: NOT SPECIFIED IN ACGIH.

FACILITIES:
PROVIDE APPROPRIATE VENTILATION SYSTEM SUCH AS LOCAL VENTILATOR IN THE
STORAGE PLACE.

PROTECTIVE CLOTHING:
GAS MASK FOR ORGANIC GASES, SAFETY GOGGLE, AND SAFETY GLOVE.


9 PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE: COIN SHAPE

VOLTAGE: 3 VOLTS


10 STABILITY AND REACTIVITY 


SINCE BATTERIES UTILIZE A CHEMICAL REACTION THEY ARE ACTUALLY CONSIDERED A
CHEMICAL PRODUCT. AS SUCH, BATTERY PERFORMANCE WILL DETERIORATE OVER TIME
EVEN IF STORED FOR A LONG PERIOD OF TIME WITHOUT BEING USED. IN ADDITION,
THE VARIOUS USAGE CONDITIONS SUCH AS DISCHARGE, AMBIENT TEMPERATURE, ETC.
ARE NOT MAINTAINED WITHIN THE SPECIFIED RANGES THE LIFE EXPECTANCY OF THE
BATTERY MAY BE SHORTENED OR THE DEVICE IN WHICH THE BATTERY IS USED MAY BE
DAMAGED BY ELECTROLYTE LEAKAGE.


11 TOXICOLOGICAL INFORMATION 


(IN CASE OF ELECTROLYTE LEAKAGE FROM THE BATTERY)

ACUTE TOXICITY:
ORAL(RAT) LD50: 2,000 MG/KG (ESTIMATED)

IRRITATION: IRRITATING TO EYE AND SKIN.

MUTAGENICITY: NOT SPECIFIED.

CHRONIC TOXICITY: NOT SPECIFIED.


12 ECOLOGICAL INFORMATION 


IN CASE OF THE WORN-OUT BATTERY WAS DISPOSED IN LAND, THE BATTERY CASE MAY
BE CORRODED, AND LEAK ELECTROLYTE. BUT, WE HAVE NO ECOLOGICAL INFORMATION.


13 DISPOSAL CONSIDERATIONS 


WHEN THE BATTERY IS WORN OUT, DISPOSE OF IT UNDER THE ORDINANCE OF EACH
LOCAL GOVERNMENT OR THE LAW ISSUED BY RELATING GOVERNMENT.


14 TRANSPORT INFORMATION 


DURING THE TRANSPORTATION OF A LARGE AMOUNT OF BATTERIES BY SHIP, TRAILER
OR RAILWAY, DO NOT LEAVE THEM IN THE PLACES OF HIGH TEMPERATURES AND DO NOT
ALLOW THEM TO BE EXPOSED TO CONDENSATION.

DURING THE TRANSPORTATION DO NOT ALLOW PACKAGES TO BE FALLEN DOWN OR
DAMAGED.

UN NUMBER:
EVEN THOUGH THE CELLS ARE CLASSIFIED AS LITHIUM METAL
BATTERIES(UN3090/UN3091), THEY ARE EXEMPTED FROM DANGEROUS GOODS BECAUSE
THEY MEET THE FOLLOWING:
1. FOR CELLS, THE LITHIUM CONTENT IS NOT MORE THAN 0.3G;

2. EACH CELL IS OF THE TYPE PROVEN TO MEET THE REQUIREMENTS OF EACH TEST
IN THE UN MANUAL OF TESTS AND CRITERIA, PART III, SUB-SECTION 38.3.

3. EACH CELL IS MANUFACTURED IN ISO9001 CERTIFIED FACTORY.

PROPER SHIPPING NAME: LITHIUM METAL BATTERIES

UN CLASS: NOT APPLICABLE

INFORMATION OF REFERENCE:

               REFERENCE           SPECIAL PROVISION        NOTE
               (REFERENCE NUMBER)

AIR TRANSPORT  IATA (2)            PACKING INSTRUCTION 968  CELLS
                                   SECTION II

                                   PACKING INSTRUCTION 969  CELLS PACKED
                                   SECTION II               WITH EQUIPMENT

                                   PACKING INSTRUCTION 970  CELLS CONTAINED
                                   SECTION II               IN EQUIPMENT

MARINE         IMDG (3)(4)         188
TRANSPORT


15 REGULATORY INFORMATION 


IATA DANGEROUS GOODS REGULATIONS

ICAO TECHNICAL INSTRUCTIONS FOR THE SAFE TRANSPORT OF DANGEROUS GOODS BY
AIR


16 OTHER INFORMATION 


THIS PSDS IS DESCRIBED ON THE BASIS OF PRESENT MATERIALS, INFORMATION AND
DATA. SO, PLEASE NOTICE THAT IT WILL BE REVISED BY NEW INFORMATION. ALSO
THIS SHEET IS SUPPLIED TO ENTREPRENEURS AS REFERENCE INFORMATION IN ORDER
TO HANDLE BATTERIES SAFELY. PLEASE NOTICE THAT ENTREPRENEUR HAVE TO DEAL
WITH BATTERIES AS THEY THINK FIT.

IN CALIFORNIA ONLY, PACKAGES THAT CONTAIN CR LITHIUM COIN CELLS AND THE
OWNERS/OPERATING INSTRUCTIONS OF PRODUCTS THAT CONTAIN CR LITHIUM COIN
CELLS MUST INCLUDE THE FOLLOWING STATEMENT:
"PERCHLORATE MATERIAL - SPECIAL HANDLING MAY APPLY, SEE
WWW.DTSC.CA.GOV/HAZARDOUSWASTE/PERCHLORATE".

THE EFFECTIVE DATE FOR THIS PERCHLORATE LABEL IS JULY 1, 2006 FOR
NON-CONSUMER PRODUCTS AND JANUARY 1, 2007 FOR CONSUMER PRODUCTS.

REFERENCES:
(1) UN RECOMMENDATIONS ON THE TRANSPORTATION OF DANGEROUS GOODS MODEL
REGULATIONS (ST/SG/AC.10/1/REV.17)

(2) IATA DANGEROUS GOODS REGULATIONS 54TH EDITION 2013

(3) IMO INTERNATIONAL MARITIME DANGEROUS GOODS CODE 2010 EDITION

(4) IMO INTERNATIONAL MARITIME DANGEROUS GOODS CODE 2012 EDITION