Common Name: LITHIUM ION POLYMER RECHARGEABLE BATTERY
Manufacturer: YAODE TECHNOLOGY CHINA
SDS Revision Date: 1/1/2013
SDS Format: ANSI-OSHA
   
Grainger Item Number(s): 20VC70, 20VC85
Manufacturer Model Number(s):



SDS Table of Contents
Click the desired link below to jump directly to that section in the SDS.
SECTION 1 - PRODUCT AND MANUFACTURER INFORMATION 
SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 
SECTION 3 - HAZARDS IDENTIFICATION / EMERGENCY OVER VIEW 
SECTION 4 - FIRST AID MEASURES 
SECTION 5 - FIRST FIGHTING MEASURES 
SECTION 6 - ACCIDENTAL RELEASE MEASURES 
SECTION 7 - HANDLING AND STORAGE 
SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 
SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 
SECTION 10 - STABILITY AND REACTIVITY 
SECTION 11 - TOXICOLOGICAL 
SECTION 12 - ECOLOGICAL 
SECTION 13 - DISPOSAL CONSIDERATIONS 
SECTION 14 - TRANSPORTATION 
SECTION 15 - REGULATORY 
SECTION 16 - OTHER INFORMATION 



REFERENCE NO.:

MATERIAL SAFETY DATA SHEET


SECTION 1 - PRODUCT AND MANUFACTURER INFORMATION 


PRODUCT COMPANY: YAODE TECHNOLOGY CO., LIMITED

ESTABLISHED ON 2008, YAODE TECHNOLOGY CO.,LIMITED IS A FOCUS IN
RECHARGEABLE LITHIUM BATTERY PRODUCTION, ASSEMBLY, SALES IN THE INTEGRATION
OF HIGH-TECH ENTERPRISES, ONE IN SHENZHEN, DONGGUAN, JIANGSU, ANHUI HAS A
MODERN PRODUCTION BASE.

PRODUCT NAME: LITHIUM ION POLYMER RECHARGEABLE BATTERY.

MODEL: H

PRODUCT TYPE: BATTERY

OMINAL VOLTAGE/VOLTAGE: 3.7V

MANUFACTURE DATE: 2013

DESIGNATED FOR RECHARGE: YES

HAZARD RATINGS*:

             NPCA/HMIS  NFPA 704
HEALTH       0          0
FLAMMABILITY 0          0
REACTIVITY   0          0

RATING KEY:
0=MINIMAL
1=SLIGHT
2=MODERATE
3=SERIOUS
4=SEVERE

NFPA: NATIONAL FIRE PROTECTION ASSOCIATION

NPCA/HMIS:
NATIONAL PAINT & COATINGS ASSOCIATION/ HAZARDOUS MATERIALS IDENTIFICATION
SYSTEM


SECTION 2 - COMPOSITION / INFORMATION ON INGREDIENTS 


NONE OF THE INGREDIENTS IN THIS PRODUCT IS CONSIDERED TO BE HAZARDOUS.

MATERIAL OR INGREDIENT                             WT %

LITHIUM COBALT DIOXIDE (LiCoO2)                    40.31

ELECTROLYTE                                        15.29

COPPER (Cu)                                        11.78

CARBON (C)                                         19.27

ALUMINUM (Al)                                       4.75

ALUMINUM LAMINATED FILM                            <6.0

SEPARATOR                                          <3.0

TAB                                                <1.0

FOR SINGLE CELL:

FLASH POINT                                        OVER 150 DEG. C

FLAVOR                                             NONE

TOXICITY                                           NONE

CORROSIVENESS                                      NONE


SECTION 3 - HAZARDS IDENTIFICATION / EMERGENCY OVER VIEW 


NONFLAMMABLE SOLID

INHALATION: PRODUCT IS NOT RESPIRABLE.

INGESTION: PRODUCT CANNOT BE INGESTED.

SKIN CONTACT: NO ADVERSE EFFECTS EXPECTED

EYE CONTACT:
NO ADVERSE EFFECTS EXPECTED. PRODUCT WILL NOT DIRECTLY CONTACT THE EYES.

CARCINOGENIC:
IARC: NO
NTP: NO
OSHA: NO

PS:
IARC = INTERNATIONAL AGENCY FOR RESEARCH ON CANCER
NTP = NATIONAL TOXICOLOGY PROGRAM
OSHA = OCCUPATIONAL SAFETY AND HEALTH ADMINISTRATION

SPECIFIC HAZARDS: CORROSIVE GAS MAY BE EMITTED DURING FIRE.

SPECIAL PROTECTIVE EQUIPMENT FOR FIREFIGHTERS:

RESPIRATORY PROTECTION:
RESPIRATORY EQUIPMENT OF A GAS CYLINDER STYLE OR PROTECTION-AGAINST-DUST
MASK

HAND PROTECTION: PROTECTIVE GLOVES

EYE PROTECTION:
GOGGLE OR PROTECTIVE GLASSES DESIGNED TO PROTECT AGAINST LIQUID SPLASHES

SKIN AND BODY PROTECTION: PROTECTIVE CLOTHES.

PRODUCTION OF MSDS PROVING UN MANUAL OF TESTS AND CRITERIA, PART 3,
SUB-SECTION 38.9 IS MET.


SECTION 4 - FIRST AID MEASURES 


INHALATION:
MAKE THE VICTIM BLOW HIS/HER NOSE, GARGLE. SEEK MEDICAL ATTENTION IF
NECESSARY.

INGESTION: NO FIRST AID NEEDED.

SKIN CONTACT:
REMOVE CONTAMINATED CLOTHES AND SHOES IMMEDIATELY. IMMEDIATELY
WASH EXTRANEOUS MATTER OR CONTACT REGION WITH SOAP AND PLENTY OF WATER.

EYE CONTACT:
DO NOT RUB EYES. IMMEDIATELY FLUSH EYES WITH WATER CONTINUOUSLY FOR AT
LEAST 15 MINUTES. SEEK MEDICAL ATTENTION.


SECTION 5 - FIRST FIGHTING MEASURES 


NONFLAMMABLE SOLID: THIS PRODUCT WILL NOT BURN.

EXTINGUISHING MEDIA:
PLENTY OF WATER, CARBON DIOXIDE GAS, NITROGEN GAS, CHEMICAL POWDER FIRE
EXTINGUISHING MEDIUM AND FIRE FOAM.

SPECIAL FIRE - FIGHTING PROCEDURES OR EQUIPMENT:
WHEN THE BATTERY BURNS WITH OTHER COMBUSTIBLES SIMULTANEOUSLY, TAKE FIRE
EXTINGUISHING METHOD WHICH CORRESPONDS TO THE COMBUSTIBLES. EXTINGUISH A
FIRE FROM THE WINDWARD AS MUCH AS POSSIBLE.

HAZARDOUS COMBUSTION PRODUCTS: NONE

UNUSUAL FIRE / EXPLOSION HAZARDS: NONE


SECTION 6 - ACCIDENTAL RELEASE MEASURES 


PICK UP AND PLACE IN APPROPRIATE CONTAINER


SECTION 7 - HANDLING AND STORAGE 


HANDLING:
ACCIDENTAL SHORT CIRCUIT FOR A FEW SECONDS WILL NOT SERIOUSLY AFFECT THE
BATTERY. HOWEVER, THIS BATTERY IS CAPABLE OF DELIVERING VERY HIGH SHORT
CIRCUIT CURRENTS. PROLONGED SHORT CIRCUITS WILL CAUSE HIGH TEMPERATURE THAT
CAN CAUSE SKIN BURNS. SOURCES OF SHORT CIRCUITS INCLUDE JUMBLED BATTERIES
IN BULK CONTAINERS, METAL JEWELRY, AND METAL COVERED TABLES OR METAL BELTS
USED FOR ASSEMBLY OF BATTERIES INTO DEVICES. IF SOLDERING OR WELDING TO THE
BATTERY IS REQUIRED, USE OF TAB LEAD ON THE BATTERIES IS RECOMMENDED. DO
NOT OPEN THE BATTERY. THE NEGATIVE ELECTRODE MATERIAL MAY BE INFLAMMABLE.
SHOULD AN INDIVIDUAL CELL FROM A BATTERY BECOME DISASSEMBLED, SPONTANEOUS
COMBUSTION OF THE NEGATIVE ELECTRODE IS POSSIBLE. THERE CAN BE A DELAY
BETWEEN EXPOSURE TO AIR AND SPONTANEOUS COMBUSTION.

STORAGE:
STORE IN A COOL, WELL VENTILATED AREA. ELEVATED TEMPERATURE CAN RESULT IN
REDUCED BATTERY CYCLE LIFE.


SECTION 8 - EXPOSURE CONTROLS/PERSONAL PROTECTION 


RESPIRATORY PROTECTION: RESPIRATOR WITH AIR CYLINDER, DUST MASK

HAND PROTECTION: PROTECTIVE GLOVES

EYE PROTECTION:
GOGGLE OR PROTECTIVE GLASSES DESIGNED TO PROTECT AGAINST LIQUID SPLASHES

SKIN AND BODY PROTECTION:
WORKING CLOTHES WITH LONG SLEEVE AND LONG TROUSERS


SECTION 9 - PHYSICAL AND CHEMICAL PROPERTIES 


APPEARANCE/STATE: SOLID

ODOR: NONE

STATE: SOLID

PH: N/A

VAPOR PRESSURE: N/A

BOILING POINT: N/A

SPECIFIC GRAVITY: N/A

DENSITY: N/A


SECTION 10 - STABILITY AND REACTIVITY 


STABILITY:
NONE IS DURING NORMAL OPERATION. AVOID EXPOSURE TO HEAT, OPEN AND
CORROSIVES.

REACTIVITY: NONE


SECTION 11 - TOXICOLOGICAL 


THIS PRODUCT DOES NOT ELICIT TOXICOLOGICAL PROPERTIES DURING HANDLING AND
USE.


SECTION 12 - ECOLOGICAL 


THIS PRODUCT IS NOT EXPECTED TO CAUSE TOXICITY TO THE ENVIRONMENT.
COMPONENTS OF THIS MATERIAL ARE NOT BIOMAGNIFIED OR BIO-CONCENTRATED IN THE
ENVIRONMENT.


SECTION 13 - DISPOSAL CONSIDERATIONS 


THIS PRODUCT MAY BE DISPOSED IN A MUNICIPAL LANDFILL.


SECTION 14 - TRANSPORTATION 


ACCORDING TO THE CLASSIFICATION OF LITHIUM CELLS AND BATTERIES OF UN
NOS.3480. LITHIUM CELLS AND BATTERIES MEET WITH ALL THE REQUIREMENT OF THE
UN MANUAL OF TEST CRITERIA, PART III, SUBSECTION 38.3. THOSE PRODUCTS FROM
PSE BATTERY HAD PASSED THE TEST. FOR A LITHIUM ION CELL, THE WATT-HOUR
RATING IS NOT MORE THAN 20WH, FOR THE LITHIUM ION BATTERY, THE WATT-HOUR IS
NOT MORE THAN 100WH. PACKING IS COMPLY WITH PART SECTION II OF PI 965 OF
IATA DGR 55TH EDITION 2014. SO, IT IS NOT RECOGNIZED AS "DANGEROUS GOOD"
AND MATCH THE REQUIREMENTS OF TRANSPORTATION OF LITHIUM CELLS AND
BATTERIES.


SECTION 15 - REGULATORY 


THIS REGULATORY INFORMATION INCLUDED HERE SHOULD NOT NECESSARILY BE
CONSIDERED ALL INCLUSIVE. NONE OF THE INGREDIENTS IN THIS PRODUCTS ARE
SUBJECTED TO THE REPORTING REQUIREMENTS OF THE CERCLA, THE CLEAN AIR ACT
AND THE CLEAN WATER ACT (US). THIS PRODUCT IS NOT FORMULATED WITH, NOR DO
THE MANUFACTURING OR FORMULATION PROCESS UTILIZE ANY CLASS I OR II OZONE
DEPLETING SUBSTANCE.


SECTION 16 - OTHER INFORMATION 


THE RECOMMENDATION AND INFORMATION CONTAINED IN THIS MSDS HAVE BEEN
COMPLIED FROM SOURCES BELIEVED TO REPRESENT THE MOST CURRENT INFORMATION
AVAILABLE WHEN THE MSDS WAS PREPARED. HOWEVER, THE MANUFACTURER /
DISTRIBUTOR OF THIS PRODUCT PROVIDES ANY WARRANTY, GUARANTY REPRESENTATION
AS TO THE CORRECTNESS OR SUFFICIENCY OF THIS INFORMATION. IF THIS PRODUCT
IS TO BE USED IN LARGE AMOUNT AND /OR AN UNUSUAL MANNER, THE USER IS
OBLIGED TO DETERMINE WHAT SAFETY MEASURES ARE APPROPRIATE, INCLUDING THE
APPLICABLE AND RELEVANT WORKPLACE AND ENVIRONMENTAL REGULATIONS PERTAINING
TO HANDLING, USE AND DISPOSAL.

ABBREVIATIONS USED IN THIS MSDS:

CERCLA:
COMPREHENSIVE ENVIRONMENTAL RESPONSE COMPENSATION AND LIABILITY ACT

CFR: CODE OF FEDERAL REGULATIONS

HEAD OFFICE:

ADD:
BUILDING 2, XINMEI INDUSTRIAL PARK
GUANGMING STREET
BAOAN DISTRICT SHENZHEN

TEL: 0086-0755-85260659

FAX: 0086-0755-85269013