Common Name: ACTIVATED CHEMILUMINESCENT PRODUCT (TEC COMPONENT) ALL COLORS
Manufacturer: CYALUME TECHNOLOGIES
MSDS Revision Date: 2/1/2012
MSDS Format: ANSI-OSHA
   
Grainger Item Number(s): 1LEC9, 1LED1, 1LED2, 1LED3, 1LED4, 1LED5, 31NJ24, 3NRA3, 3NRA4, 3NRA5, 3NRA6, 3NRA7, 3NRA8, 3NRA9, 3NRC1, 3NRN3, 3NRN4, 3RTU6, 5HM88, 5HM89, 5HM90, 5HM91, 5HM92, 5HM93, 5YB27, 6END0, 8ADZ4, 8AHN0, 8AHN1, 8MLF8, 8MLF9, 8MLG1, 8MLG2, 8MLG3, 8MMG9, 8TEC5, 8VMD2, 8XZM7, 8YY28, 9CHU1, 9DRA3, 9FWU0, 9HPA2, 9KZE8, 9KZT3, 9MGR2, 9PR29, 9RUP6
Manufacturer Model Number(s):



MSDS Table of Contents
Click the desired link below to jump directly to that section in the MSDS.
PRODUCT IDENTIFICATION 
COMPOSITION 
HEALTH HAZARD INFORMATION 
FIRST AID 
FIRE AND EXPLOSION HAZARD INFORMATION 
REACTIVITY DATA 
PHYSICAL PROPERTIES 
SPILL OR LEAK PROCEDURES 
WASTE DISPOSAL 
SPECIAL PRECAUTIONS 
TSCA INFORMATION 



CYALUME(R*) TECHNOLOGIES

CYALUME TECHNOLOGIES, INC.
96 WINDSOR STREET
WEST SPRINGFIELD, MA 01089

TEL: (413) 739-8252

MATERIAL SAFETY DATA

MSDS NO.: 6010

DATE: 2/1/12

SUPERSEDES: 8/30/08


PRODUCT IDENTIFICATION 


PRODUCT NAME:
"ACTIVATED" CHEMILUMINESCENT PRODUCT (TEC COMPONENT) ALL COLORS

SYNONYMS: ALL PRODUCTS

CHEMICAL FAMILY:
PLASTIC ARTICLE CONTAINING CHEMILUMINESCER AND ACTIVATOR COMPONENTS.

MOLECULAR FORMULA: MIXTURE

MOLECULAR WEIGHT.: MIXTURE


COMPOSITION 


COMPONENT                           CAS. #            WEIGHT %

POLYETHYLENE                        9002-88-4         35-56%

FOIL                                                  12-13%

CHEMILUMINESCER                                       24-30%

TEC ACTIVATOR                                         19-24%

OSHA REGULATED COMPONENTS:

COMPONENT          C.A.S. #    WEIGHT%    TWA/CEILING    REFERENCE

HYDROGEN PEROXIDE  7722-84-1   0.5-0.7%   1.4 MG/M3      OSHA/ACGIH

NFPA HAZARD RATING:
HEALTH     0 MATERIALS THAT ON EXPOSURE UNDER FIRE CONDITIONS WOULD OFFER
             NO HAZARD BEYOND THAT OF ORDINARY COMBUSTIBLE MATERIAL.
FIRE       1 MATERIAL THAT MUST BE PREHEATED BEFORE IGNITION CAN OCCUR.
REACTIVITY 0 MATERIALS THAT IN THEMSELVES ARE NORMALLY STABLE, EVEN UNDER
             FIRE EXPOSURE CONDITIONS, AND WHICH ARE NOT REACTIVE WITH
             WATER.


HEALTH HAZARD INFORMATION 


EFFECTS OF OVEREXPOSURE:
OVEREXPOSURE TO CHEMICAL INGREDIENTS IS NOT LIKELY TO CAUSE SIGNIFICANT
ACUTE TOXIC EFFECTS. THE ACUTE ORAL (RAT) AND ACUTE DERMAL (RABBIT) LD50
VALUES ARE GREATER THAN 5 G/KG FOR THE LUMINESCER, ACTIVATOR, FRESH
MIXTURE, AND SPENT MIXTURE. UPON ACCIDENTAL EYE EXPOSURE, MATERIAL SHOULD
BE IMMEDIATELY RINSED FROM THE EYES. NO SIGNIFICANT SKIN IRRITATION WAS
OBSERVED DURING ANIMAL TESTING.


FIRST AID 


IN CASE OF EYE CONTACT, IMMEDIATELY IRRIGATE WITH PLENTY OF WATER FOR 15
MINUTES. OBTAIN MEDICAL ATTENTION IF IRRITATION PERSISTS.

EXPOSURE CONTROL METHODS:
ENGINEERING CONTROLS ARE NOT USUALLY NECESSARY IF GOOD HYGIENE PRACTICES
ARE FOLLOWED. BEFORE EATING, DRINKING, OR SMOKING, WASH FACE AND HANDS
THOROUGHLY WITH SOAP AND WATER, AVOID UNNECESSARY SKIN CONTACT. IMPERVIOUS
GLOVES ARE RECOMMENDED TO PREVENT PROLONGED SKIN CONTACT. FOR OPERATIONS
WHERE EYE OR FACE CONTACT CAN OCCUR, EYE PROTECTION IS RECOMMENDED. WHERE
EXPOSURES ARE BELOW THE PERMISSIBLE EXPOSURE LIMIT (PEL), NO RESPIRATORY
PROTECTION IS REQUIRED. WHERE EXPOSURES EXCEED THE PEL, USE RESPIRATOR
APPROVED BY NIOSH FOR THE MATERIAL AND LEVEL OF EXPOSURE. SEE "GUIDE TO
INDUSTRIAL RESPIRATORY PROTECTION" (NIOSH).


FIRE AND EXPLOSION HAZARD INFORMATION 


FLASH POINT: >200 DEG. F (93.3 DEG. C)
METHOD: CLOSED CUP

FIRE FIGHTING:
USE WATER SPRAY, CARBON DIOXIDE OR DRY CHEMICAL TO EXTINGUISH FIRES. USE
WATER TO KEEP CONTAINERS COOL. WEAR SELF-CONTAINED POSITIVE PRESSURE
BREATHING APPARATUS.


REACTIVITY DATA 


STABILITY: STABLE

CONDITIONS TO AVOID: NONE KNOWN

POLYMERIZATION: WILL NOT OCCUR

CONDITION TO AVOID: NONE KNOWN

INCOMPATIBLE MATERIALS: NONE KNOWN

HAZARDOUS DECOMPOSITION PRODUCTS:
THERMAL DECOMPOSITION OR COMBUSTION MAY PRODUCE CARBON MONOXIDE AND/OR
CARBON DIOXIDE


PHYSICAL PROPERTIES 


APPEARANCE:
ARTICLE CONSISTING OF PLASTIC TUBE OR SHAPE CONTAINING BROKEN GLASS AMPOULE
AFTER ACTIVATION WITH OXALATE COMPONENT.

BOILING POINT: N.A.

MELTING POINT: 260 DEG. C

VAPOR PRESSURE: N.A.

SPECIFIC GRAVITY: <WATER

VAPOR DENSITY: N.A.

% VOLATILE (BY VOL.): N.A.

PH: N.A.

SATURATION IN AIR (BY VOL.): N.A.

EVAPORATION RATE: N.A.

SOLUBILITY IN WATER: NEGLIGIBLE


SPILL OR LEAK PROCEDURES 


STEPS TO BE TAKEN IN CASE MATERIAL IS RELEASED OR SPILLED:
COVER SPILLS WITH INERT ABSORBENT MATERIAL; SWEEP UP AND PLACE IN WASTE
DISPOSAL CONTAINER.


WASTE DISPOSAL 


DISPOSAL MUST BE MADE IN ACCORDANCE WITH APPLICABLE GOVERNMENTAL
REGULATIONS.


SPECIAL PRECAUTIONS 


HANDLING AND STORAGE/OTHER: NONE

D.O.T. SHIPPING INFORMATION:

PROPER SHIPPING NAME: NOT APPLICABLE

HAZARD CLASS: NOT APPLICABLE

UN/NA: NOT APPLICABLE

D.O.T. HAZARDOUS SUBSTANCES:
(REPORTABLE QUANTITY OF PRODUCT) NOT APPLICABLE

D.O.T. LABEL REQUIRED: NOT APPLICABLE


TSCA INFORMATION 


THIS PRODUCT IS MANUFACTURED IN COMPLIANCE WITH ALL PROVISIONS OF THE TOXIC
SUBSTANCES CONTROL ACT, 15 U.S.C.

ENVIRONMENTAL INFORMATION:
WASTES THAT ARE CLASSIFIED AS HAZARDOUS WASTE ARE POTENTIALLY SUBJECT TO
THE RCRA LAND DISPOSAL RESTRICTIONS. THE LAND DISPOSAL RESTRICTION
REGULATIONS ARE CONTAINED IN 40 CFR 268. ONLY WASTE WHICH MEET THE
REGULATORY DEFINITION OF A HAZARDOUS WASTE ARE SUBJECT TO THE LAND DISPOSAL
RESTRICTIONS.

ACTIVATED LIGHT STICKS DO NOT MEET THE DEFINITION OF A CHARACTERISTIC
HAZARDOUS WASTE AND THEREFORE, UNDER THE REGULATIONS, CAN BE DISPOSED OF
AS A SOLID WASTE IN SOLID WASTE LANDFILLS AND INCINERATORS UNLESS
PROHIBITED BY SITE-SPECIFIC SOLID WASTE FACILITY RESTRICTION.

THIS INFORMATION IS GIVEN WITHOUT ANY WARRANTY OR REPRESENTATION. WE DO NOT
ASSUME ANY LEGAL RESPONSIBILITY FOR SAME, NOR DO WE GIVE PERMISSION,
INDUCEMENT, OR RECOMMENDATION TO PRACTICE ANY PATENTED INVENTION WITHOUT A
LICENSE. IT IS OFFERED SOLELY FOR YOUR CONSIDERATION, INVESTIGATION AND
VERIFICATION. BEFORE USING ANY PRODUCT, READ ITS LABEL.

EMERGENCY PHONE: 800-228-5635 EXT. 162

MSDS: 6010-01

1-FEB-12

THIS IS A CONFIDENTIAL PROPRIETARY DOCUMENT. UNAUTHORIZED COPYING OR
REMOVAL FROM PREMISES IS STRICTLY FORBIDDEN. (C) 2009